summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 6a68452)
raw | patch | inline | side by side (parent: 6a68452)
author | Elliott Hughes <enh@google.com> | |
Wed, 10 Dec 2014 17:31:04 +0000 (09:31 -0800) | ||
committer | Elliott Hughes <enh@google.com> | |
Wed, 10 Dec 2014 19:48:19 +0000 (11:48 -0800) |
Although the LP32 mips sigset_t is large enough to represent all signals,
their jmp_buf is too small. This test succeeded on arm and x86 because the
RT signals were never in the 'expected' sigset_t, so the equality comparison
with the 'actual' sigset_t worked fine --- everyone was blind to the RT
signal. On mips the tests fail because the 'expected' sigset_t does contain
the RT signal but the 'actual' doesn't because the jmp_buf only saves and
restores the first 32 signals.
There are 32 free bits (currently used as padding) in the LP32 mips jmp_buf,
and they might choose to use those to provide better support than the other
two platforms, but I'll leave that to them. It will be easy to just remove
the #if defined(__LP64__) from this change in that case.
For mips64 it's not to late to increase the size of the jmp_buf and fix
the setjmp family, but since there are decisions to be made here for LP32,
I'll leave it all to Imagination folks...
Bug: 16918359
Change-Id: I6b723712fce0e9210dafa165d8599d950b2d3500
their jmp_buf is too small. This test succeeded on arm and x86 because the
RT signals were never in the 'expected' sigset_t, so the equality comparison
with the 'actual' sigset_t worked fine --- everyone was blind to the RT
signal. On mips the tests fail because the 'expected' sigset_t does contain
the RT signal but the 'actual' doesn't because the jmp_buf only saves and
restores the first 32 signals.
There are 32 free bits (currently used as padding) in the LP32 mips jmp_buf,
and they might choose to use those to provide better support than the other
two platforms, but I'll leave that to them. It will be easy to just remove
the #if defined(__LP64__) from this change in that case.
For mips64 it's not to late to increase the size of the jmp_buf and fix
the setjmp family, but since there are decisions to be made here for LP32,
I'll leave it all to Imagination folks...
Bug: 16918359
Change-Id: I6b723712fce0e9210dafa165d8599d950b2d3500
tests/setjmp_test.cpp | patch | blob | history |
diff --git a/tests/setjmp_test.cpp b/tests/setjmp_test.cpp
index 2ea01b32d8800115e2efa4705ac8c216709c60a2..8afd49479ed4b787dc6269afe9671bc834993e56 100644 (file)
--- a/tests/setjmp_test.cpp
+++ b/tests/setjmp_test.cpp
}
}
-static sigset_t SigSetOf(int signal, int rt_signal = 0) {
- sigset_t ss;
- sigemptyset(&ss);
- sigaddset(&ss, signal);
- if (rt_signal != 0) {
- sigaddset(&ss, rt_signal);
+// Two distinct signal sets, pipu
+struct SigSets {
+ SigSets() : one(MakeSigSet(0)), two(MakeSigSet(1)) {
}
- return ss;
-}
+
+ static sigset_t MakeSigSet(int offset) {
+ sigset_t ss;
+ sigemptyset(&ss);
+ sigaddset(&ss, SIGUSR1 + offset);
+#if defined(__LP64__)
+ // For arm and x86, sigset_t was too small for the RT signals.
+ // For mips, sigset_t was large enough but jmp_buf wasn't.
+ sigaddset(&ss, SIGRTMIN + offset);
+#endif
+ return ss;
+ }
+
+ sigset_t one;
+ sigset_t two;
+ sigset_t original;
+};
void AssertSigmaskEquals(const sigset_t& expected) {
sigset_t actual;
TEST(setjmp, _setjmp_signal_mask) {
// _setjmp/_longjmp do not save/restore the signal mask.
- sigset_t ss1(SigSetOf(SIGUSR1, SIGRTMIN + 8));
- sigset_t ss2(SigSetOf(SIGUSR2, SIGRTMIN + 9));
- sigset_t original_set;
- sigprocmask(SIG_SETMASK, &ss1, &original_set);
+ SigSets ss;
+ sigprocmask(SIG_SETMASK, &ss.one, &ss.original);
jmp_buf jb;
if (_setjmp(jb) == 0) {
- sigprocmask(SIG_SETMASK, &ss2, NULL);
+ sigprocmask(SIG_SETMASK, &ss.two, NULL);
_longjmp(jb, 1);
FAIL(); // Unreachable.
} else {
- AssertSigmaskEquals(ss2);
+ AssertSigmaskEquals(ss.two);
}
- sigprocmask(SIG_SETMASK, &original_set, NULL);
+ sigprocmask(SIG_SETMASK, &ss.original, NULL);
}
TEST(setjmp, setjmp_signal_mask) {
// setjmp/longjmp do save/restore the signal mask on bionic, but not on glibc.
// This is a BSD versus System V historical accident. POSIX leaves the
// behavior unspecified, so any code that cares needs to use sigsetjmp.
- sigset_t ss1(SigSetOf(SIGUSR1, SIGRTMIN + 8));
- sigset_t ss2(SigSetOf(SIGUSR2, SIGRTMIN + 9));
- sigset_t original_set;
- sigprocmask(SIG_SETMASK, &ss1, &original_set);
+ SigSets ss;
+ sigprocmask(SIG_SETMASK, &ss.one, &ss.original);
jmp_buf jb;
if (setjmp(jb) == 0) {
- sigprocmask(SIG_SETMASK, &ss2, NULL);
+ sigprocmask(SIG_SETMASK, &ss.two, NULL);
longjmp(jb, 1);
FAIL(); // Unreachable.
} else {
#if defined(__BIONIC__)
// bionic behaves like BSD and does save/restore the signal mask.
- AssertSigmaskEquals(ss1);
+ AssertSigmaskEquals(ss.one);
#else
// glibc behaves like System V and doesn't save/restore the signal mask.
- AssertSigmaskEquals(ss2);
+ AssertSigmaskEquals(ss.two);
#endif
}
- sigprocmask(SIG_SETMASK, &original_set, NULL);
+ sigprocmask(SIG_SETMASK, &ss.original, NULL);
}
TEST(setjmp, sigsetjmp_0_signal_mask) {
// sigsetjmp(0)/siglongjmp do not save/restore the signal mask.
- sigset_t ss1(SigSetOf(SIGUSR1, SIGRTMIN + 8));
- sigset_t ss2(SigSetOf(SIGUSR2, SIGRTMIN + 9));
- sigset_t original_set;
- sigprocmask(SIG_SETMASK, &ss1, &original_set);
+ SigSets ss;
+ sigprocmask(SIG_SETMASK, &ss.one, &ss.original);
sigjmp_buf sjb;
if (sigsetjmp(sjb, 0) == 0) {
- sigprocmask(SIG_SETMASK, &ss2, NULL);
+ sigprocmask(SIG_SETMASK, &ss.two, NULL);
siglongjmp(sjb, 1);
FAIL(); // Unreachable.
} else {
- AssertSigmaskEquals(ss2);
+ AssertSigmaskEquals(ss.two);
}
- sigprocmask(SIG_SETMASK, &original_set, NULL);
+ sigprocmask(SIG_SETMASK, &ss.original, NULL);
}
TEST(setjmp, sigsetjmp_1_signal_mask) {
// sigsetjmp(1)/siglongjmp does save/restore the signal mask.
- sigset_t ss1(SigSetOf(SIGUSR1, SIGRTMIN + 8));
- sigset_t ss2(SigSetOf(SIGUSR2, SIGRTMIN + 9));
- sigset_t original_set;
- sigprocmask(SIG_SETMASK, &ss1, &original_set);
+ SigSets ss;
+ sigprocmask(SIG_SETMASK, &ss.one, &ss.original);
sigjmp_buf sjb;
if (sigsetjmp(sjb, 1) == 0) {
- sigprocmask(SIG_SETMASK, &ss2, NULL);
+ sigprocmask(SIG_SETMASK, &ss.two, NULL);
siglongjmp(sjb, 1);
FAIL(); // Unreachable.
} else {
- AssertSigmaskEquals(ss1);
+ AssertSigmaskEquals(ss.one);
}
- sigprocmask(SIG_SETMASK, &original_set, NULL);
+ sigprocmask(SIG_SETMASK, &ss.original, NULL);
}