summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 44ef37c)
raw | patch | inline | side by side (parent: 44ef37c)
author | Narayan Kamath <narayan@google.com> | |
Wed, 19 Feb 2014 15:42:58 +0000 (15:42 +0000) | ||
committer | Narayan Kamath <narayan@google.com> | |
Wed, 19 Feb 2014 18:50:30 +0000 (18:50 +0000) |
Turns out stlport isn't broken. <cmath> (included
transitively via gtest in our case) is not required
to make C99 math macros (like signbit) available, nor is
it required to preserve them if they're already defined.
It is only required to make the equivalent functions in
namespace std available.
I couldn't find any documentation of required behaviour for
programs that include both <math.h> and <cmath>.
I've verified experimentally that llvm's libc++ and gnu
stl behave the same as stlport.
bug: 12935307
Change-Id: I9dc5cc0fd9f4f259abc8eefb280177cdd092a94b
transitively via gtest in our case) is not required
to make C99 math macros (like signbit) available, nor is
it required to preserve them if they're already defined.
It is only required to make the equivalent functions in
namespace std available.
I couldn't find any documentation of required behaviour for
programs that include both <math.h> and <cmath>.
I've verified experimentally that llvm's libc++ and gnu
stl behave the same as stlport.
bug: 12935307
Change-Id: I9dc5cc0fd9f4f259abc8eefb280177cdd092a94b
tests/math_test.cpp | patch | blob | history |
diff --git a/tests/math_test.cpp b/tests/math_test.cpp
index c8974d3b02b5633f7a3d0872c2fb665fe6d14f12..fc561bc8c211318c7a7f2fe5dbc3a41765ff781b 100644 (file)
--- a/tests/math_test.cpp
+++ b/tests/math_test.cpp
#define _DECLARE_C99_LDBL_MATH 1
+// This include (and the associated definition of __test_capture_signbit)
+// must be placed before any files that include <cmath> (gtest.h in this case).
+//
+// <math.h> is required to define generic macros signbit, isfinite and
+// several other such functions.
+//
+// <cmath> is required to undef declarations of these macros in the global
+// namespace and make equivalent functions available in namespace std. Our
+// stlport implementation does this only for signbit, isfinite, isinf and
+// isnan.
+//
+// NOTE: We don't write our test using std::signbit because we want to be
+// sure that we're testing the bionic version of signbit. The C++ libraries
+// are free to reimplement signbit or delegate to compiler builtins if they
+// please.
+#include <math.h>
+
+namespace {
+template<typename T> inline int test_capture_signbit(const T in) {
+ return signbit(in);
+}
+template<typename T> inline int test_capture_isfinite(const T in) {
+ return isfinite(in);
+}
+template<typename T> inline int test_capture_isnan(const T in) {
+ return isnan(in);
+}
+template<typename T> inline int test_capture_isinf(const T in) {
+ return isinf(in);
+}
+}
+
#include <gtest/gtest.h>
#include <fenv.h>
#include <limits.h>
-#include <math.h>
#include <stdint.h>
float float_subnormal() {
ASSERT_EQ(FP_ZERO, fpclassify(0.0));
}
-/* TODO: stlport breaks the isfinite macro
TEST(math, isfinite) {
- ASSERT_TRUE(isfinite(123.0f));
- ASSERT_TRUE(isfinite(123.0));
- ASSERT_FALSE(isfinite(HUGE_VALF));
- ASSERT_FALSE(isfinite(HUGE_VAL));
+ ASSERT_TRUE(test_capture_isfinite(123.0f));
+ ASSERT_TRUE(test_capture_isfinite(123.0));
+ ASSERT_FALSE(test_capture_isfinite(HUGE_VALF));
+ ASSERT_FALSE(test_capture_isfinite(HUGE_VAL));
}
-*/
TEST(math, isinf) {
- ASSERT_FALSE(isinf(123.0f));
- ASSERT_FALSE(isinf(123.0));
- ASSERT_TRUE(isinf(HUGE_VALF));
- ASSERT_TRUE(isinf(HUGE_VAL));
+ ASSERT_FALSE(test_capture_isinf(123.0f));
+ ASSERT_FALSE(test_capture_isinf(123.0));
+ ASSERT_TRUE(test_capture_isinf(HUGE_VALF));
+ ASSERT_TRUE(test_capture_isinf(HUGE_VAL));
}
TEST(math, isnan) {
- ASSERT_FALSE(isnan(123.0f));
- ASSERT_FALSE(isnan(123.0));
- ASSERT_TRUE(isnan(nanf("")));
- ASSERT_TRUE(isnan(nan("")));
+ ASSERT_FALSE(test_capture_isnan(123.0f));
+ ASSERT_FALSE(test_capture_isnan(123.0));
+ ASSERT_TRUE(test_capture_isnan(nanf("")));
+ ASSERT_TRUE(test_capture_isnan(nan("")));
}
TEST(math, isnormal) {
}
// TODO: isgreater, isgreaterequals, isless, islessequal, islessgreater, isunordered
-
-/* TODO: stlport breaks the signbit macro
TEST(math, signbit) {
- ASSERT_EQ(0, signbit(0.0f));
- ASSERT_EQ(0, signbit(0.0));
+ ASSERT_EQ(0, test_capture_signbit(0.0f));
+ ASSERT_EQ(0, test_capture_signbit(0.0));
- ASSERT_EQ(0, signbit(1.0f));
- ASSERT_EQ(0, signbit(1.0));
+ ASSERT_EQ(0, test_capture_signbit(1.0f));
+ ASSERT_EQ(0, test_capture_signbit(1.0));
- ASSERT_NE(0, signbit(-1.0f));
- ASSERT_NE(0, signbit(-1.0));
+ ASSERT_NE(0, test_capture_signbit(-1.0f));
+ ASSERT_NE(0, test_capture_signbit(-1.0));
}
-*/
TEST(math, __fpclassifyd) {
#if defined(__BIONIC__)