am cbb4606a: Merge "change unsigned int to uint32_t for api arc4random/arc4random_uni...
authorYabin Cui <yabinc@google.com>
Wed, 29 Oct 2014 12:32:36 +0000 (12:32 +0000)
committerAndroid Git Automerger <android-git-automerger@android.com>
Wed, 29 Oct 2014 12:32:36 +0000 (12:32 +0000)
* commit 'cbb4606ad00f084f984c92a8674400a112ea200e':
  change unsigned int to uint32_t for api arc4random/arc4random_uniform

libc/dns/gethnamaddr.c
libc/dns/include/resolv_cache.h
libc/dns/include/resolv_netid.h
libc/dns/include/resolv_private.h
libc/dns/net/getaddrinfo.c
libc/dns/resolv/res_cache.c
libc/dns/resolv/res_send.c
libc/kernel/uapi/linux/ion.h

index cc33c612cb78729c326c6203532155d2c80fa128..0bd838e86249223e2b033a2e0d7eae324ddc14db 100644 (file)
@@ -565,7 +565,7 @@ android_read_hostent(FILE* proxy)
        char buf[4];
        if (fread(buf, 1, sizeof(buf), proxy) != sizeof(buf)) return NULL;
 
-       /* This is reading serialized data from system/netd/DnsProxyListener.cpp
+       /* This is reading serialized data from system/netd/server/DnsProxyListener.cpp
         * and changes here need to be matched there */
        int result_code = strtol(buf, NULL, 10);
        if (result_code != DnsProxyQueryResult) {
@@ -763,7 +763,7 @@ gethostbyname_internal(const char *name, int af, res_state res, unsigned netid,
 
        netid = __netdClientDispatch.netIdForResolv(netid);
 
-       /* This is writing to system/netd/DnsProxyListener.cpp and changes
+       /* This is writing to system/netd/server/DnsProxyListener.cpp and changes
         * here need to be matched there */
        if (fprintf(proxy, "gethostbyname %u %s %d",
                        netid,
index 16f3e43a1207f91560c3044f9fd4275148bad187..e049d951ff9eb06e283c6e642befae4a1c73619b 100644 (file)
 #include <sys/cdefs.h>
 
 struct __res_state;
-struct resolv_cache;  /* forward */
-
-/* Gets the cache for a network. Returned cache might be NULL. */
-__LIBC_HIDDEN__
-extern struct resolv_cache* __get_res_cache(unsigned netid);
 
 /* sets the name server addresses to the provided res_state structure. The
  * name servers are retrieved from the cache which is associated
@@ -53,7 +48,7 @@ typedef enum {
 
 __LIBC_HIDDEN__
 extern ResolvCacheStatus
-_resolv_cache_lookup( struct resolv_cache*  cache,
+_resolv_cache_lookup( unsigned              netid,
                       const void*           query,
                       int                   querylen,
                       void*                 answer,
@@ -65,7 +60,7 @@ _resolv_cache_lookup( struct resolv_cache*  cache,
  */
 __LIBC_HIDDEN__
 extern void
-_resolv_cache_add( struct resolv_cache*  cache,
+_resolv_cache_add( unsigned              netid,
                    const void*           query,
                    int                   querylen,
                    const void*           answer,
@@ -74,7 +69,7 @@ _resolv_cache_add( struct resolv_cache*  cache,
 /* Notify the cache a request failed */
 __LIBC_HIDDEN__
 extern void
-_resolv_cache_query_failed( struct resolv_cache* cache,
+_resolv_cache_query_failed( unsigned     netid,
                    const void* query,
                    int         querylen);
 
index bada18a441bf17d68e1fd691c7699c4d6252edd1..e5521b809b82765e4207c496438c26019b114ee9 100644 (file)
@@ -36,7 +36,7 @@
 #include <netinet/in.h>
 
 /*
- * Passing NETID_UNSET as the netId causes system/netd/DnsProxyListener.cpp to
+ * Passing NETID_UNSET as the netId causes system/netd/server/DnsProxyListener.cpp to
  * fill in the appropriate default netId for the query.
  */
 #define NETID_UNSET 0u
@@ -72,6 +72,9 @@ struct hostent *android_gethostbyaddrfornet_proxy(const void *, socklen_t, int ,
 int android_getnameinfofornet(const struct sockaddr *, socklen_t, char *, size_t, char *, size_t,
                 int, unsigned, unsigned);
 
+/* delete the cache associated with a certain network */
+extern void _resolv_delete_cache_for_net(unsigned netid);
+
 __END_DECLS
 
 #endif /* _RESOLV_NETID_H */
index 5a1f25c0fdb1078d523c55bcb4dee24f9e30c0e8..4a832d0e3dd7b59b2470727e51dd27e5918b4c24 100644 (file)
@@ -498,6 +498,16 @@ __LIBC_HIDDEN__ void res_setnetid(res_state, unsigned);
 __LIBC_HIDDEN__ void res_setmark(res_state, unsigned);
 u_int  res_randomid(void);
 
+#ifdef __i386__
+# define __socketcall extern __attribute__((__cdecl__))
+#else
+# define __socketcall extern
+#endif
+
+__socketcall int __connect(int, const struct sockaddr*, socklen_t);
+
+#undef __socketcall
+
 __END_DECLS
 
 #pragma GCC visibility pop
index a4923187ec6ed4562c0d25bf3c96dfe23ba0319e..54439996539b51015397631f045468ce9cccf6eb 100644 (file)
@@ -369,7 +369,7 @@ _test_connect(int pf, struct sockaddr *addr, size_t addrlen, unsigned mark) {
                return 0;
        int ret;
        do {
-               ret = connect(s, addr, addrlen);
+               ret = __connect(s, addr, addrlen);
        } while (ret < 0 && errno == EINTR);
        int success = (ret == 0);
        do {
@@ -1803,7 +1803,7 @@ _find_src_addr(const struct sockaddr *addr, struct sockaddr *src_addr, unsigned
        if (mark != MARK_UNSET && setsockopt(sock, SOL_SOCKET, SO_MARK, &mark, sizeof(mark)) < 0)
                return 0;
        do {
-               ret = connect(sock, addr, len);
+               ret = __connect(sock, addr, len);
        } while (ret == -1 && errno == EINTR);
 
        if (ret == -1) {
index dd7769330f2f423f17f45a92a41999c6b1067599..15d04c2fa67a2c48a28372a9738bf04118008785 100644 (file)
@@ -1218,7 +1218,6 @@ typedef struct resolv_cache {
     int              max_entries;
     int              num_entries;
     Entry            mru_list;
-    pthread_mutex_t  lock;
     int              last_id;
     Entry*           entries;
     PendingReqInfo   pending_requests;
@@ -1236,6 +1235,15 @@ struct resolv_cache_info {
 
 #define  HTABLE_VALID(x)  ((x) != NULL && (x) != HTABLE_DELETED)
 
+static pthread_once_t        _res_cache_once = PTHREAD_ONCE_INIT;
+static void _res_cache_init(void);
+
+// lock protecting everything in the _resolve_cache_info structs (next ptr, etc)
+static pthread_mutex_t _res_cache_list_lock;
+
+/* gets cache associated with a network, or NULL if none exists */
+static struct resolv_cache* _find_named_cache_locked(unsigned netid);
+
 static void
 _cache_flush_pending_requests_locked( struct resolv_cache* cache )
 {
@@ -1256,18 +1264,18 @@ _cache_flush_pending_requests_locked( struct resolv_cache* cache )
     }
 }
 
-/* return 0 if no pending request is found matching the key
- * if a matching request is found the calling thread will wait
- * and return 1 when released */
+/* Return 0 if no pending request is found matching the key.
+ * If a matching request is found the calling thread will wait until
+ * the matching request completes, then update *cache and return 1. */
 static int
-_cache_check_pending_request_locked( struct resolv_cache* cache, Entry* key )
+_cache_check_pending_request_locked( struct resolv_cache** cache, Entry* key, unsigned netid )
 {
     struct pending_req_info *ri, *prev;
     int exist = 0;
 
-    if (cache && key) {
-        ri = cache->pending_requests.next;
-        prev = &cache->pending_requests;
+    if (*cache && key) {
+        ri = (*cache)->pending_requests.next;
+        prev = &(*cache)->pending_requests;
         while (ri) {
             if (ri->hash == key->hash) {
                 exist = 1;
@@ -1288,7 +1296,9 @@ _cache_check_pending_request_locked( struct resolv_cache* cache, Entry* key )
             struct timespec ts = {0,0};
             XLOG("Waiting for previous request");
             ts.tv_sec = _time_now() + PENDING_REQUEST_TIMEOUT;
-            pthread_cond_timedwait(&ri->cond, &cache->lock, &ts);
+            pthread_cond_timedwait(&ri->cond, &_res_cache_list_lock, &ts);
+            /* Must update *cache as it could have been deleted. */
+            *cache = _find_named_cache_locked(netid);
         }
     }
 
@@ -1325,17 +1335,25 @@ _cache_notify_waiting_tid_locked( struct resolv_cache* cache, Entry* key )
 
 /* notify the cache that the query failed */
 void
-_resolv_cache_query_failed( struct resolv_cache* cache,
+_resolv_cache_query_failed( unsigned    netid,
                    const void* query,
                    int         querylen)
 {
     Entry    key[1];
+    Cache*   cache;
+
+    if (!entry_init_key(key, query, querylen))
+        return;
+
+    pthread_mutex_lock(&_res_cache_list_lock);
+
+    cache = _find_named_cache_locked(netid);
 
-    if (cache && entry_init_key(key, query, querylen)) {
-        pthread_mutex_lock(&cache->lock);
+    if (cache) {
         _cache_notify_waiting_tid_locked(cache, key);
-        pthread_mutex_unlock(&cache->lock);
     }
+
+    pthread_mutex_unlock(&_res_cache_list_lock);
 }
 
 static void
@@ -1391,7 +1409,6 @@ _resolv_cache_create( void )
         cache->max_entries = _res_cache_get_max_entries();
         cache->entries = calloc(sizeof(*cache->entries), cache->max_entries);
         if (cache->entries) {
-            pthread_mutex_init( &cache->lock, NULL );
             cache->mru_list.mru_prev = cache->mru_list.mru_next = &cache->mru_list;
             XLOG("%s: cache created\n", __FUNCTION__);
         } else {
@@ -1586,7 +1603,7 @@ static void _cache_remove_expired(Cache* cache) {
 }
 
 ResolvCacheStatus
-_resolv_cache_lookup( struct resolv_cache*  cache,
+_resolv_cache_lookup( unsigned              netid,
                       const void*           query,
                       int                   querylen,
                       void*                 answer,
@@ -1597,6 +1614,7 @@ _resolv_cache_lookup( struct resolv_cache*  cache,
     Entry**    lookup;
     Entry*     e;
     time_t     now;
+    Cache*     cache;
 
     ResolvCacheStatus  result = RESOLV_CACHE_NOTFOUND;
 
@@ -1609,7 +1627,14 @@ _resolv_cache_lookup( struct resolv_cache*  cache,
         return RESOLV_CACHE_UNSUPPORTED;
     }
     /* lookup cache */
-    pthread_mutex_lock( &cache->lock );
+    pthread_once(&_res_cache_once, _res_cache_init);
+    pthread_mutex_lock(&_res_cache_list_lock);
+
+    cache = _find_named_cache_locked(netid);
+    if (cache == NULL) {
+        result = RESOLV_CACHE_UNSUPPORTED;
+        goto Exit;
+    }
 
     /* see the description of _lookup_p to understand this.
      * the function always return a non-NULL pointer.
@@ -1621,7 +1646,7 @@ _resolv_cache_lookup( struct resolv_cache*  cache,
         XLOG( "NOT IN CACHE");
         // calling thread will wait if an outstanding request is found
         // that matching this query
-        if (!_cache_check_pending_request_locked(cache, key)) {
+        if (!_cache_check_pending_request_locked(&cache, key, netid) || cache == NULL) {
             goto Exit;
         } else {
             lookup = _cache_lookup_p(cache, key);
@@ -1662,13 +1687,13 @@ _resolv_cache_lookup( struct resolv_cache*  cache,
     result = RESOLV_CACHE_FOUND;
 
 Exit:
-    pthread_mutex_unlock( &cache->lock );
+    pthread_mutex_unlock(&_res_cache_list_lock);
     return result;
 }
 
 
 void
-_resolv_cache_add( struct resolv_cache*  cache,
+_resolv_cache_add( unsigned              netid,
                    const void*           query,
                    int                   querylen,
                    const void*           answer,
@@ -1678,6 +1703,7 @@ _resolv_cache_add( struct resolv_cache*  cache,
     Entry*   e;
     Entry**  lookup;
     u_long   ttl;
+    Cache*   cache = NULL;
 
     /* don't assume that the query has already been cached
      */
@@ -1686,7 +1712,12 @@ _resolv_cache_add( struct resolv_cache*  cache,
         return;
     }
 
-    pthread_mutex_lock( &cache->lock );
+    pthread_mutex_lock(&_res_cache_list_lock);
+
+    cache = _find_named_cache_locked(netid);
+    if (cache == NULL) {
+        goto Exit;
+    }
 
     XLOG( "%s: query:", __FUNCTION__ );
     XLOG_QUERY(query,querylen);
@@ -1732,8 +1763,10 @@ _resolv_cache_add( struct resolv_cache*  cache,
     _cache_dump_mru(cache);
 #endif
 Exit:
-    _cache_notify_waiting_tid_locked(cache, key);
-    pthread_mutex_unlock( &cache->lock );
+    if (cache != NULL) {
+      _cache_notify_waiting_tid_locked(cache, key);
+    }
+    pthread_mutex_unlock(&_res_cache_list_lock);
 }
 
 /****************************************************************************/
@@ -1744,20 +1777,13 @@ Exit:
 /****************************************************************************/
 /****************************************************************************/
 
-static pthread_once_t        _res_cache_once = PTHREAD_ONCE_INIT;
-
 // Head of the list of caches.  Protected by _res_cache_list_lock.
 static struct resolv_cache_info _res_cache_list;
 
-// lock protecting everything in the _resolve_cache_info structs (next ptr, etc)
-static pthread_mutex_t _res_cache_list_lock;
-
 /* insert resolv_cache_info into the list of resolv_cache_infos */
 static void _insert_cache_info_locked(struct resolv_cache_info* cache_info);
 /* creates a resolv_cache_info */
 static struct resolv_cache_info* _create_cache_info( void );
-/* gets cache associated with a network, or NULL if none exists */
-static struct resolv_cache* _find_named_cache_locked(unsigned netid);
 /* gets a resolv_cache_info associated with a network, or NULL if not found */
 static struct resolv_cache_info* _find_cache_info_locked(unsigned netid);
 /* look up the named cache, and creates one if needed */
@@ -1785,22 +1811,6 @@ _res_cache_init(void)
     pthread_mutex_init(&_res_cache_list_lock, NULL);
 }
 
-struct resolv_cache*
-__get_res_cache(unsigned netid)
-{
-    struct resolv_cache *cache;
-
-    pthread_once(&_res_cache_once, _res_cache_init);
-    pthread_mutex_lock(&_res_cache_list_lock);
-
-    /* Does NOT create a cache if it does not exist. */
-    cache = _find_named_cache_locked(netid);
-
-    pthread_mutex_unlock(&_res_cache_list_lock);
-    XLOG("%s: netid=%u, cache=%p\n", __FUNCTION__, netid, cache);
-    return cache;
-}
-
 static struct resolv_cache*
 _get_res_cache_for_net_locked(unsigned netid)
 {
@@ -1837,12 +1847,36 @@ _flush_cache_for_net_locked(unsigned netid)
 {
     struct resolv_cache* cache = _find_named_cache_locked(netid);
     if (cache) {
-        pthread_mutex_lock(&cache->lock);
         _cache_flush_locked(cache);
-        pthread_mutex_unlock(&cache->lock);
     }
 }
 
+void _resolv_delete_cache_for_net(unsigned netid)
+{
+    pthread_once(&_res_cache_once, _res_cache_init);
+    pthread_mutex_lock(&_res_cache_list_lock);
+
+    struct resolv_cache_info* prev_cache_info = &_res_cache_list;
+
+    while (prev_cache_info->next) {
+        struct resolv_cache_info* cache_info = prev_cache_info->next;
+
+        if (cache_info->netid == netid) {
+            prev_cache_info->next = cache_info->next;
+            _cache_flush_locked(cache_info->cache);
+            free(cache_info->cache->entries);
+            free(cache_info->cache);
+            _free_nameservers_locked(cache_info);
+            free(cache_info);
+            break;
+        }
+
+        prev_cache_info = prev_cache_info->next;
+    }
+
+    pthread_mutex_unlock(&_res_cache_list_lock);
+}
+
 static struct resolv_cache_info*
 _create_cache_info(void)
 {
index de093856ab1b5b66a065e6e09041fa8ce91efb76..6439e31ce8bd4e4f1e290c3d8607cb7694a52b31 100644 (file)
@@ -367,7 +367,6 @@ res_nsend(res_state statp,
        int gotsomewhere, terrno, try, v_circuit, resplen, ns, n;
        char abuf[NI_MAXHOST];
 #if USE_RESOLV_CACHE
-        struct resolv_cache*  cache;
         ResolvCacheStatus     cache_status = RESOLV_CACHE_UNSUPPORTED;
 #endif
 
@@ -389,21 +388,17 @@ res_nsend(res_state statp,
        terrno = ETIMEDOUT;
 
 #if USE_RESOLV_CACHE
-       // get the cache associated with the network
-       cache = __get_res_cache(statp->netid);
-       if (cache != NULL) {
-               int  anslen = 0;
-               cache_status = _resolv_cache_lookup(
-                               cache, buf, buflen,
-                               ans, anssiz, &anslen);
-
-               if (cache_status == RESOLV_CACHE_FOUND) {
-                       return anslen;
-               } else {
-                       // had a cache miss for a known network, so populate the thread private
-                       // data so the normal resolve path can do its thing
-                       _resolv_populate_res_for_net(statp);
-               }
+       int  anslen = 0;
+       cache_status = _resolv_cache_lookup(
+                       statp->netid, buf, buflen,
+                       ans, anssiz, &anslen);
+
+       if (cache_status == RESOLV_CACHE_FOUND) {
+               return anslen;
+       } else if (cache_status != RESOLV_CACHE_UNSUPPORTED) {
+               // had a cache miss for a known network, so populate the thread private
+               // data so the normal resolve path can do its thing
+               _resolv_populate_res_for_net(statp);
        }
 
        if (statp->nscount == 0) {
@@ -602,7 +597,7 @@ res_nsend(res_state statp,
 
 #if USE_RESOLV_CACHE
                 if (cache_status == RESOLV_CACHE_NOTFOUND) {
-                    _resolv_cache_add(cache, buf, buflen,
+                    _resolv_cache_add(statp->netid, buf, buflen,
                                       ans, resplen);
                 }
 #endif
@@ -658,13 +653,13 @@ res_nsend(res_state statp,
                errno = terrno;
 
 #if USE_RESOLV_CACHE
-        _resolv_cache_query_failed(cache, buf, buflen);
+        _resolv_cache_query_failed(statp->netid, buf, buflen);
 #endif
 
        return (-1);
  fail:
 #if USE_RESOLV_CACHE
-       _resolv_cache_query_failed(cache, buf, buflen);
+       _resolv_cache_query_failed(statp->netid, buf, buflen);
 #endif
        res_nclose(statp);
        return (-1);
@@ -951,7 +946,7 @@ connect_with_timeout(int sock, const struct sockaddr *nsap, socklen_t salen, int
        origflags = fcntl(sock, F_GETFL, 0);
        fcntl(sock, F_SETFL, origflags | O_NONBLOCK);
 
-       res = connect(sock, nsap, salen);
+       res = __connect(sock, nsap, salen);
        if (res < 0 && errno != EINPROGRESS) {
                 res = -1;
                 goto done;
@@ -1108,7 +1103,7 @@ send_dg(res_state statp,
                        res_nclose(statp);
                        return (0);
                }
-               if (connect(EXT(statp).nssocks[ns], nsap, (socklen_t)nsaplen) < 0) {
+               if (__connect(EXT(statp).nssocks[ns], nsap, (socklen_t)nsaplen) < 0) {
                        Aerror(statp, stderr, "connect(dg)", errno, nsap,
                            nsaplen);
                        res_nclose(statp);
index f18939d1165b6e35beaac26ad00c8d8a88f4bce2..5af39d04f342961f7da2f71b9d0c60068057e5f1 100644 (file)
  ***
  ****************************************************************************
  ****************************************************************************/
-#ifndef _LINUX_ION_H
-#define _LINUX_ION_H
+#ifndef _UAPI_LINUX_ION_H
+#define _UAPI_LINUX_ION_H
+#include <linux/ioctl.h>
 #include <linux/types.h>
-struct ion_handle;
 /* WARNING: DO NOT EDIT, AUTO-GENERATED CODE - SEE TOP FOR INSTRUCTIONS */
+typedef int ion_user_handle_t;
 enum ion_heap_type {
  ION_HEAP_TYPE_SYSTEM,
  ION_HEAP_TYPE_SYSTEM_CONTIG,
- ION_HEAP_TYPE_CARVEOUT,
 /* WARNING: DO NOT EDIT, AUTO-GENERATED CODE - SEE TOP FOR INSTRUCTIONS */
+ ION_HEAP_TYPE_CARVEOUT,
+ ION_HEAP_TYPE_CHUNK,
+ ION_HEAP_TYPE_DMA,
  ION_HEAP_TYPE_CUSTOM,
+/* WARNING: DO NOT EDIT, AUTO-GENERATED CODE - SEE TOP FOR INSTRUCTIONS */
  ION_NUM_HEAPS = 16,
 };
 #define ION_HEAP_SYSTEM_MASK (1 << ION_HEAP_TYPE_SYSTEM)
-/* WARNING: DO NOT EDIT, AUTO-GENERATED CODE - SEE TOP FOR INSTRUCTIONS */
 #define ION_HEAP_SYSTEM_CONTIG_MASK (1 << ION_HEAP_TYPE_SYSTEM_CONTIG)
+/* WARNING: DO NOT EDIT, AUTO-GENERATED CODE - SEE TOP FOR INSTRUCTIONS */
 #define ION_HEAP_CARVEOUT_MASK (1 << ION_HEAP_TYPE_CARVEOUT)
+#define ION_HEAP_TYPE_DMA_MASK (1 << ION_HEAP_TYPE_DMA)
+#define ION_NUM_HEAP_IDS sizeof(unsigned int) * 8
 #define ION_FLAG_CACHED 1
-#define ION_FLAG_CACHED_NEEDS_SYNC 2
 /* WARNING: DO NOT EDIT, AUTO-GENERATED CODE - SEE TOP FOR INSTRUCTIONS */
+#define ION_FLAG_CACHED_NEEDS_SYNC 2
 struct ion_allocation_data {
  size_t len;
  size_t align;
- unsigned int heap_mask;
 /* WARNING: DO NOT EDIT, AUTO-GENERATED CODE - SEE TOP FOR INSTRUCTIONS */
+ unsigned int heap_id_mask;
  unsigned int flags;
struct ion_handle *handle;
ion_user_handle_t handle;
 };
-struct ion_fd_data {
 /* WARNING: DO NOT EDIT, AUTO-GENERATED CODE - SEE TOP FOR INSTRUCTIONS */
- struct ion_handle *handle;
+struct ion_fd_data {
+ ion_user_handle_t handle;
  int fd;
 };
-struct ion_handle_data {
 /* WARNING: DO NOT EDIT, AUTO-GENERATED CODE - SEE TOP FOR INSTRUCTIONS */
- struct ion_handle *handle;
+struct ion_handle_data {
+ ion_user_handle_t handle;
 };
 struct ion_custom_data {
- unsigned int cmd;
 /* WARNING: DO NOT EDIT, AUTO-GENERATED CODE - SEE TOP FOR INSTRUCTIONS */
+ unsigned int cmd;
  unsigned long arg;
 };
 #define ION_IOC_MAGIC 'I'
-#define ION_IOC_ALLOC _IOWR(ION_IOC_MAGIC, 0,   struct ion_allocation_data)
 /* WARNING: DO NOT EDIT, AUTO-GENERATED CODE - SEE TOP FOR INSTRUCTIONS */
+#define ION_IOC_ALLOC _IOWR(ION_IOC_MAGIC, 0,   struct ion_allocation_data)
 #define ION_IOC_FREE _IOWR(ION_IOC_MAGIC, 1, struct ion_handle_data)
 #define ION_IOC_MAP _IOWR(ION_IOC_MAGIC, 2, struct ion_fd_data)
 #define ION_IOC_SHARE _IOWR(ION_IOC_MAGIC, 4, struct ion_fd_data)
-#define ION_IOC_IMPORT _IOWR(ION_IOC_MAGIC, 5, struct ion_fd_data)
 /* WARNING: DO NOT EDIT, AUTO-GENERATED CODE - SEE TOP FOR INSTRUCTIONS */
+#define ION_IOC_IMPORT _IOWR(ION_IOC_MAGIC, 5, struct ion_fd_data)
 #define ION_IOC_SYNC _IOWR(ION_IOC_MAGIC, 7, struct ion_fd_data)
 #define ION_IOC_CUSTOM _IOWR(ION_IOC_MAGIC, 6, struct ion_custom_data)
 #endif
+/* WARNING: DO NOT EDIT, AUTO-GENERATED CODE - SEE TOP FOR INSTRUCTIONS */