]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/platform-bionic.git/commitdiff
merge from open-source master
authorThe Android Open Source Project <initial-contribution@android.com>
Thu, 8 Apr 2010 18:11:53 +0000 (11:11 -0700)
committerThe Android Open Source Project <initial-contribution@android.com>
Thu, 8 Apr 2010 18:11:53 +0000 (11:11 -0700)
Change-Id: If77618a329fc7b497c44c2585e644bc50e7e1406

1  2 
libc/bionic/malloc_debug_common.c

index a86255a0abb524dee554d2a0cb9c3f48f28d2562,0000000000000000000000000000000000000000..ec56826689536f5f284f0be6da7ef0728ad2925e
mode 100644,000000..100644
--- /dev/null
@@@ -1,488 -1,0 +1,488 @@@
-         goto done;
 +/*
 + * Copyright (C) 2009 The Android Open Source Project
 + * All rights reserved.
 + *
 + * Redistribution and use in source and binary forms, with or without
 + * modification, are permitted provided that the following conditions
 + * are met:
 + *  * Redistributions of source code must retain the above copyright
 + *    notice, this list of conditions and the following disclaimer.
 + *  * Redistributions in binary form must reproduce the above copyright
 + *    notice, this list of conditions and the following disclaimer in
 + *    the documentation and/or other materials provided with the
 + *    distribution.
 + *
 + * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
 + * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
 + * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS
 + * FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE
 + * COPYRIGHT OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT,
 + * INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING,
 + * BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS
 + * OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED
 + * AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY,
 + * OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT
 + * OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF
 + * SUCH DAMAGE.
 + */
 +
 +/*
 + * Contains definition of structures, global variables, and implementation of
 + * routines that are used by malloc leak detection code and other components in
 + * the system. The trick is that some components expect these data and
 + * routines to be defined / implemented in libc.so library, regardless
 + * whether or not MALLOC_LEAK_CHECK macro is defined. To make things even
 + * more tricky, malloc leak detection code, implemented in
 + * libc_malloc_debug.so also requires access to these variables and routines
 + * (to fill allocation entry hash table, for example). So, all relevant
 + * variables and routines are defined / implemented here and exported
 + * to all, leak detection code and other components via dynamic (libc.so),
 + * or static (libc.a) linking.
 + */
 +
 +#include <stdlib.h>
 +#include <pthread.h>
 +#include <unistd.h>
 +#include "dlmalloc.h"
 +#include "malloc_debug_common.h"
 +
 +/*
 + * In a VM process, this is set to 1 after fork()ing out of zygote.
 + */
 +int gMallocLeakZygoteChild = 0;
 +
 +pthread_mutex_t gAllocationsMutex = PTHREAD_MUTEX_INITIALIZER;
 +HashTable gHashTable;
 +
 +// =============================================================================
 +// output functions
 +// =============================================================================
 +
 +static int hash_entry_compare(const void* arg1, const void* arg2)
 +{
 +    HashEntry* e1 = *(HashEntry**)arg1;
 +    HashEntry* e2 = *(HashEntry**)arg2;
 +
 +    size_t nbAlloc1 = e1->allocations;
 +    size_t nbAlloc2 = e2->allocations;
 +    size_t size1 = e1->size & ~SIZE_FLAG_MASK;
 +    size_t size2 = e2->size & ~SIZE_FLAG_MASK;
 +    size_t alloc1 = nbAlloc1 * size1;
 +    size_t alloc2 = nbAlloc2 * size2;
 +
 +    // sort in descending order by:
 +    // 1) total size
 +    // 2) number of allocations
 +    //
 +    // This is used for sorting, not determination of equality, so we don't
 +    // need to compare the bit flags.
 +    int result;
 +    if (alloc1 > alloc2) {
 +        result = -1;
 +    } else if (alloc1 < alloc2) {
 +        result = 1;
 +    } else {
 +        if (nbAlloc1 > nbAlloc2) {
 +            result = -1;
 +        } else if (nbAlloc1 < nbAlloc2) {
 +            result = 1;
 +        } else {
 +            result = 0;
 +        }
 +    }
 +    return result;
 +}
 +
 +/*
 + * Retrieve native heap information.
 + *
 + * "*info" is set to a buffer we allocate
 + * "*overallSize" is set to the size of the "info" buffer
 + * "*infoSize" is set to the size of a single entry
 + * "*totalMemory" is set to the sum of all allocations we're tracking; does
 + *   not include heap overhead
 + * "*backtraceSize" is set to the maximum number of entries in the back trace
 + */
 +void get_malloc_leak_info(uint8_t** info, size_t* overallSize,
 +        size_t* infoSize, size_t* totalMemory, size_t* backtraceSize)
 +{
 +    // don't do anything if we have invalid arguments
 +    if (info == NULL || overallSize == NULL || infoSize == NULL ||
 +            totalMemory == NULL || backtraceSize == NULL) {
 +        return;
 +    }
 +
 +    pthread_mutex_lock(&gAllocationsMutex);
 +
 +    if (gHashTable.count == 0) {
 +        *info = NULL;
 +        *overallSize = 0;
 +        *infoSize = 0;
 +        *totalMemory = 0;
 +        *backtraceSize = 0;
 +        goto done;
 +    }
 +
 +    void** list = (void**)dlmalloc(sizeof(void*) * gHashTable.count);
 +
 +    // get the entries into an array to be sorted
 +    int index = 0;
 +    int i;
 +    for (i = 0 ; i < HASHTABLE_SIZE ; i++) {
 +        HashEntry* entry = gHashTable.slots[i];
 +        while (entry != NULL) {
 +            list[index] = entry;
 +            *totalMemory = *totalMemory +
 +                ((entry->size & ~SIZE_FLAG_MASK) * entry->allocations);
 +            index++;
 +            entry = entry->next;
 +        }
 +    }
 +
 +    // XXX: the protocol doesn't allow variable size for the stack trace (yet)
 +    *infoSize = (sizeof(size_t) * 2) + (sizeof(intptr_t) * BACKTRACE_SIZE);
 +    *overallSize = *infoSize * gHashTable.count;
 +    *backtraceSize = BACKTRACE_SIZE;
 +
 +    // now get A byte array big enough for this
 +    *info = (uint8_t*)dlmalloc(*overallSize);
 +
 +    if (*info == NULL) {
 +        *overallSize = 0;
-             /* TODO: only clear out the part we're not overwriting? */
-             memset(head, 0, *infoSize);
++        goto out_nomem_info;
 +    }
 +
 +    qsort((void*)list, gHashTable.count, sizeof(void*), hash_entry_compare);
 +
 +    uint8_t* head = *info;
 +    const int count = gHashTable.count;
 +    for (i = 0 ; i < count ; i++) {
 +        HashEntry* entry = list[i];
 +        size_t entrySize = (sizeof(size_t) * 2) + (sizeof(intptr_t) * entry->numEntries);
 +        if (entrySize < *infoSize) {
 +            /* we're writing less than a full entry, clear out the rest */
++            memset(head + entrySize, 0, *infoSize - entrySize);
 +        } else {
 +            /* make sure the amount we're copying doesn't exceed the limit */
 +            entrySize = *infoSize;
 +        }
 +        memcpy(head, &(entry->size), entrySize);
 +        head += *infoSize;
 +    }
 +
++out_nomem_info:
 +    dlfree(list);
 +
 +done:
 +    pthread_mutex_unlock(&gAllocationsMutex);
 +}
 +
 +void free_malloc_leak_info(uint8_t* info)
 +{
 +    dlfree(info);
 +}
 +
 +struct mallinfo mallinfo()
 +{
 +    return dlmallinfo();
 +}
 +
 +void* valloc(size_t bytes) {
 +    /* assume page size of 4096 bytes */
 +    return memalign( getpagesize(), bytes );
 +}
 +
 +/* Support for malloc debugging.
 + * Note that if USE_DL_PREFIX is not defined, it's assumed that memory
 + * allocation routines are implemented somewhere else, so all our custom
 + * malloc routines should not be compiled at all.
 + */
 +#ifdef USE_DL_PREFIX
 +
 +/* Table for dispatching malloc calls, initialized with default dispatchers. */
 +const MallocDebug __libc_malloc_default_dispatch __attribute__((aligned(32))) =
 +{
 +    dlmalloc, dlfree, dlcalloc, dlrealloc, dlmemalign
 +};
 +
 +/* Selector of dispatch table to use for dispatching malloc calls. */
 +const MallocDebug* __libc_malloc_dispatch = &__libc_malloc_default_dispatch;
 +
 +void* malloc(size_t bytes) {
 +    return __libc_malloc_dispatch->malloc(bytes);
 +}
 +void free(void* mem) {
 +    __libc_malloc_dispatch->free(mem);
 +}
 +void* calloc(size_t n_elements, size_t elem_size) {
 +    return __libc_malloc_dispatch->calloc(n_elements, elem_size);
 +}
 +void* realloc(void* oldMem, size_t bytes) {
 +    return __libc_malloc_dispatch->realloc(oldMem, bytes);
 +}
 +void* memalign(size_t alignment, size_t bytes) {
 +    return __libc_malloc_dispatch->memalign(alignment, bytes);
 +}
 +
 +/* We implement malloc debugging only in libc.so, so code bellow
 + * must be excluded if we compile this file for static libc.a
 + */
 +#ifndef LIBC_STATIC
 +#include <sys/system_properties.h>
 +#include <dlfcn.h>
 +#include "logd.h"
 +
 +// =============================================================================
 +// log functions
 +// =============================================================================
 +
 +#define debug_log(format, ...)  \
 +   __libc_android_log_print(ANDROID_LOG_DEBUG, "libc", (format), ##__VA_ARGS__ )
 +#define error_log(format, ...)  \
 +   __libc_android_log_print(ANDROID_LOG_ERROR, "libc", (format), ##__VA_ARGS__ )
 +#define info_log(format, ...)  \
 +   __libc_android_log_print(ANDROID_LOG_INFO, "libc", (format), ##__VA_ARGS__ )
 +
 +/* Table for dispatching malloc calls, depending on environment. */
 +static MallocDebug gMallocUse __attribute__((aligned(32))) = {
 +    dlmalloc, dlfree, dlcalloc, dlrealloc, dlmemalign
 +};
 +
 +extern char*  __progname;
 +
 +/* Handle to shared library where actual memory allocation is implemented.
 + * This library is loaded and memory allocation calls are redirected there
 + * when libc.debug.malloc environment variable contains value other than
 + * zero:
 + * 1  - For memory leak detections.
 + * 5  - For filling allocated / freed memory with patterns defined by
 + *      CHK_SENTINEL_VALUE, and CHK_FILL_FREE macros.
 + * 10 - For adding pre-, and post- allocation stubs in order to detect
 + *      buffer overruns.
 + * Note that emulator's memory allocation instrumentation is not controlled by
 + * libc.debug.malloc value, but rather by emulator, started with -memcheck
 + * option. Note also, that if emulator has started with -memcheck option,
 + * emulator's instrumented memory allocation will take over value saved in
 + * libc.debug.malloc. In other words, if emulator has started with -memcheck
 + * option, libc.debug.malloc value is ignored.
 + * Actual functionality for debug levels 1-10 is implemented in
 + * libc_malloc_debug_leak.so, while functionality for emultor's instrumented
 + * allocations is implemented in libc_malloc_debug_qemu.so and can be run inside
 +  * the emulator only.
 + */
 +static void* libc_malloc_impl_handle = NULL;
 +
 +/* Make sure we have MALLOC_ALIGNMENT that matches the one that is
 + * used in dlmalloc. Emulator's memchecker needs this value to properly
 + * align its guarding zones.
 + */
 +#ifndef MALLOC_ALIGNMENT
 +#define MALLOC_ALIGNMENT ((size_t)8U)
 +#endif  /* MALLOC_ALIGNMENT */
 +
 +/* Initializes memory allocation framework once per process. */
 +static void malloc_init_impl(void)
 +{
 +    const char* so_name = NULL;
 +    MallocDebugInit malloc_debug_initialize = NULL;
 +    unsigned int qemu_running = 0;
 +    unsigned int debug_level = 0;
 +    unsigned int memcheck_enabled = 0;
 +    char env[PROP_VALUE_MAX];
 +    char memcheck_tracing[PROP_VALUE_MAX];
 +
 +    /* Get custom malloc debug level. Note that emulator started with
 +     * memory checking option will have priority over debug level set in
 +     * libc.debug.malloc system property. */
 +    if (__system_property_get("ro.kernel.qemu", env) && atoi(env)) {
 +        qemu_running = 1;
 +        if (__system_property_get("ro.kernel.memcheck", memcheck_tracing)) {
 +            if (memcheck_tracing[0] != '0') {
 +                // Emulator has started with memory tracing enabled. Enforce it.
 +                debug_level = 20;
 +                memcheck_enabled = 1;
 +            }
 +        }
 +    }
 +
 +    /* If debug level has not been set by memcheck option in the emulator,
 +     * lets grab it from libc.debug.malloc system property. */
 +    if (!debug_level && __system_property_get("libc.debug.malloc", env)) {
 +        debug_level = atoi(env);
 +    }
 +
 +    /* Debug level 0 means that we should use dlxxx allocation
 +     * routines (default). */
 +    if (!debug_level) {
 +        return;
 +    }
 +
 +    // Lets see which .so must be loaded for the requested debug level
 +    switch (debug_level) {
 +        case 1:
 +        case 5:
 +        case 10:
 +            so_name = "/system/lib/libc_malloc_debug_leak.so";
 +            break;
 +        case 20:
 +            // Quick check: debug level 20 can only be handled in emulator.
 +            if (!qemu_running) {
 +                error_log("%s: Debug level %d can only be set in emulator\n",
 +                          __progname, debug_level);
 +                return;
 +            }
 +            // Make sure that memory checking has been enabled in emulator.
 +            if (!memcheck_enabled) {
 +                error_log("%s: Memory checking is not enabled in the emulator\n",
 +                          __progname);
 +                return;
 +            }
 +            so_name = "/system/lib/libc_malloc_debug_qemu.so";
 +            break;
 +        default:
 +            error_log("%s: Debug level %d is unknown\n",
 +                      __progname, debug_level);
 +            return;
 +    }
 +
 +    // Load .so that implements the required malloc debugging functionality.
 +    libc_malloc_impl_handle = dlopen(so_name, RTLD_LAZY);
 +    if (libc_malloc_impl_handle == NULL) {
 +        error_log("%s: Missing module %s required for malloc debug level %d\n",
 +                 __progname, so_name, debug_level);
 +        return;
 +    }
 +
 +    // Initialize malloc debugging in the loaded module.
 +    malloc_debug_initialize =
 +            dlsym(libc_malloc_impl_handle, "malloc_debug_initialize");
 +    if (malloc_debug_initialize == NULL) {
 +        error_log("%s: Initialization routine is not found in %s\n",
 +                  __progname, so_name);
 +        dlclose(libc_malloc_impl_handle);
 +        return;
 +    }
 +    if (malloc_debug_initialize()) {
 +        dlclose(libc_malloc_impl_handle);
 +        return;
 +    }
 +
 +    if (debug_level == 20) {
 +        // For memory checker we need to do extra initialization.
 +        int (*memcheck_initialize)(int, const char*) =
 +                dlsym(libc_malloc_impl_handle, "memcheck_initialize");
 +        if (memcheck_initialize == NULL) {
 +            error_log("%s: memcheck_initialize routine is not found in %s\n",
 +                      __progname, so_name);
 +            dlclose(libc_malloc_impl_handle);
 +            return;
 +        }
 +        if (memcheck_initialize(MALLOC_ALIGNMENT, memcheck_tracing)) {
 +            dlclose(libc_malloc_impl_handle);
 +            return;
 +        }
 +    }
 +
 +    // Initialize malloc dispatch table with appropriate routines.
 +    switch (debug_level) {
 +        case 1:
 +            __libc_android_log_print(ANDROID_LOG_INFO, "libc",
 +                    "%s using MALLOC_DEBUG = %d (leak checker)\n",
 +                    __progname, debug_level);
 +            gMallocUse.malloc =
 +                dlsym(libc_malloc_impl_handle, "leak_malloc");
 +            gMallocUse.free =
 +                dlsym(libc_malloc_impl_handle, "leak_free");
 +            gMallocUse.calloc =
 +                dlsym(libc_malloc_impl_handle, "leak_calloc");
 +            gMallocUse.realloc =
 +                dlsym(libc_malloc_impl_handle, "leak_realloc");
 +            gMallocUse.memalign =
 +                dlsym(libc_malloc_impl_handle, "leak_memalign");
 +            break;
 +        case 5:
 +            __libc_android_log_print(ANDROID_LOG_INFO, "libc",
 +                    "%s using MALLOC_DEBUG = %d (fill)\n",
 +                    __progname, debug_level);
 +            gMallocUse.malloc =
 +                dlsym(libc_malloc_impl_handle, "fill_malloc");
 +            gMallocUse.free =
 +                dlsym(libc_malloc_impl_handle, "fill_free");
 +            gMallocUse.calloc = dlcalloc;
 +            gMallocUse.realloc =
 +                dlsym(libc_malloc_impl_handle, "fill_realloc");
 +            gMallocUse.memalign =
 +                dlsym(libc_malloc_impl_handle, "fill_memalign");
 +            break;
 +        case 10:
 +            __libc_android_log_print(ANDROID_LOG_INFO, "libc",
 +                    "%s using MALLOC_DEBUG = %d (sentinels, fill)\n",
 +                    __progname, debug_level);
 +            gMallocUse.malloc =
 +                dlsym(libc_malloc_impl_handle, "chk_malloc");
 +            gMallocUse.free =
 +                dlsym(libc_malloc_impl_handle, "chk_free");
 +            gMallocUse.calloc =
 +                dlsym(libc_malloc_impl_handle, "chk_calloc");
 +            gMallocUse.realloc =
 +                dlsym(libc_malloc_impl_handle, "chk_realloc");
 +            gMallocUse.memalign =
 +                dlsym(libc_malloc_impl_handle, "chk_memalign");
 +            break;
 +        case 20:
 +            __libc_android_log_print(ANDROID_LOG_INFO, "libc",
 +                "%s[%u] using MALLOC_DEBUG = %d (instrumented for emulator)\n",
 +                __progname, getpid(), debug_level);
 +            gMallocUse.malloc =
 +                dlsym(libc_malloc_impl_handle, "qemu_instrumented_malloc");
 +            gMallocUse.free =
 +                dlsym(libc_malloc_impl_handle, "qemu_instrumented_free");
 +            gMallocUse.calloc =
 +                dlsym(libc_malloc_impl_handle, "qemu_instrumented_calloc");
 +            gMallocUse.realloc =
 +                dlsym(libc_malloc_impl_handle, "qemu_instrumented_realloc");
 +            gMallocUse.memalign =
 +                dlsym(libc_malloc_impl_handle, "qemu_instrumented_memalign");
 +            break;
 +        default:
 +            break;
 +    }
 +
 +    // Make sure dispatch table is initialized
 +    if ((gMallocUse.malloc == NULL) ||
 +        (gMallocUse.free == NULL) ||
 +        (gMallocUse.calloc == NULL) ||
 +        (gMallocUse.realloc == NULL) ||
 +        (gMallocUse.memalign == NULL)) {
 +        error_log("%s: Cannot initialize malloc dispatch table for debug level"
 +                  " %d: %p, %p, %p, %p, %p\n",
 +                  __progname, debug_level,
 +                  gMallocUse.malloc, gMallocUse.free,
 +                  gMallocUse.calloc, gMallocUse.realloc,
 +                  gMallocUse.memalign);
 +        dlclose(libc_malloc_impl_handle);
 +        libc_malloc_impl_handle = NULL;
 +    } else {
 +        __libc_malloc_dispatch = &gMallocUse;
 +    }
 +}
 +
 +static pthread_once_t  malloc_init_once_ctl = PTHREAD_ONCE_INIT;
 +
 +#endif  // !LIBC_STATIC
 +#endif  // USE_DL_PREFIX
 +
 +/* Initializes memory allocation framework.
 + * This routine is called from __libc_init routines implemented
 + * in libc_init_static.c and libc_init_dynamic.c files.
 + */
 +void malloc_debug_init(void)
 +{
 +    /* We need to initialize malloc iff we implement here custom
 +     * malloc routines (i.e. USE_DL_PREFIX is defined) for libc.so */
 +#if defined(USE_DL_PREFIX) && !defined(LIBC_STATIC)
 +    if (pthread_once(&malloc_init_once_ctl, malloc_init_impl)) {
 +        error_log("Unable to initialize malloc_debug component.");
 +    }
 +#endif  // USE_DL_PREFIX && !LIBC_STATIC
 +}