summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 86d06dc)
raw | patch | inline | side by side (parent: 86d06dc)
author | Elliott Hughes <enh@google.com> | |
Tue, 9 Dec 2014 00:23:10 +0000 (16:23 -0800) | ||
committer | Elliott Hughes <enh@google.com> | |
Tue, 9 Dec 2014 00:23:10 +0000 (16:23 -0800) |
The use of 32-bit units for 64-bit stores and loads was driving me crazy.
Bug: 16918359
Change-Id: Ifb73aad8f8985a2adfcf5913b783ad9424f23e06
Bug: 16918359
Change-Id: Ifb73aad8f8985a2adfcf5913b783ad9424f23e06
libc/arch-arm64/bionic/setjmp.S | patch | blob | history |
index d1747e43586543921af62eec433e3b413c9274f8..5c956ff1a67f3c1418076173be911baff6fc9c01 100644 (file)
// Core x19 - x30, sp (see section 5.1.1)
// VFP d8 - d15 (see section 5.1.2)
//
-// NOTE: All the registers saved here will have 64bit vales (except FPSR).
+// NOTE: All the registers saved here will have 64 bit vales.
// AAPCS mandates that the higher part of q registers do not need to
// be saved by the callee.
-// The structure of jmp_buf for AArch64:
-//
-// NOTE: _JBLEN is the size of jmp_buf in longs(64bit on AArch64)! The table
-// below computes the offsets in words(32bit).
-//
-// word name description
-// -------------------------------------------------------------------------
-// 0 sigflag 0 => signal mask not valid
-// 1 unused unused (for alignment)
-// 2-3 sigmask signal mask (not used with _setjmp / _longjmp)
-// 4 core_base base of core registers (x19-x30, sp)
-// 30 float_base base of float registers (d8-d15)
-// 46- reserved reserved entries (room to grow)
-// 64
-//
-// NOTE: The instructions that load/store core/vfp registers expect 8-byte
-// alignment. Contrary to the previous setjmp header for ARM we do not
-// need to save status/control registers for VFP (it is not a
-// requirement for setjmp).
-
#define _JB_SIGFLAG 0
-#define _JB_SIGMASK (_JB_SIGFLAG + 2)
-#define _JB_CORE_BASE (_JB_SIGMASK + 2)
-#define _JB_FLOAT_BASE (_JB_CORE_BASE + (31-19+1)*2)
+#define _JB_SIGMASK (_JB_SIGFLAG + 1)
+#define _JB_X30_SP (_JB_SIGMASK + 1)
+#define _JB_X28_X29 (_JB_X30_SP + 2)
+#define _JB_X26_X27 (_JB_X28_X29 + 2)
+#define _JB_X24_X25 (_JB_X26_X27 + 2)
+#define _JB_X22_X23 (_JB_X24_X25 + 2)
+#define _JB_X20_X21 (_JB_X22_X23 + 2)
+#define _JB_X19 (_JB_X20_X21 + 2)
+#define _JB_D14_D15 (_JB_X19 + 1)
+#define _JB_D12_D13 (_JB_D14_D15 + 2)
+#define _JB_D10_D11 (_JB_D12_D13 + 1)
+#define _JB_D8_D9 (_JB_D10_D11 + 1)
ENTRY(setjmp)
mov w1, #1
// int sigsetjmp(sigjmp_buf env, int save_signal_mask);
ENTRY(sigsetjmp)
// Record whether or not we're saving the signal mask.
- str w1, [x0, #(_JB_SIGFLAG * 4)]
+ str w1, [x0, #(_JB_SIGFLAG * 8)]
// Do we need to save the signal mask?
cbz w1, 1f
stp x0, x30, [sp, #-16]!
// The 'how' argument is ignored if new_mask is NULL.
mov x1, #0 // NULL.
- add x2, x0, #(_JB_SIGMASK * 4) // old_mask.
+ add x2, x0, #(_JB_SIGMASK * 8) // old_mask.
bl sigprocmask
ldp x0, x30, [sp], #16
1:
// Save core registers.
mov x10, sp
- stp x30, x10, [x0, #(_JB_CORE_BASE * 4 + 16 * 0)]
- stp x28, x29, [x0, #(_JB_CORE_BASE * 4 + 16 * 1)]
- stp x26, x27, [x0, #(_JB_CORE_BASE * 4 + 16 * 2)]
- stp x24, x25, [x0, #(_JB_CORE_BASE * 4 + 16 * 3)]
- stp x22, x23, [x0, #(_JB_CORE_BASE * 4 + 16 * 4)]
- stp x20, x21, [x0, #(_JB_CORE_BASE * 4 + 16 * 5)]
- str x19, [x0, #(_JB_CORE_BASE * 4 + 16 * 6)]
+ stp x30, x10, [x0, #(_JB_X30_SP * 8)]
+ stp x28, x29, [x0, #(_JB_X28_X29 * 8)]
+ stp x26, x27, [x0, #(_JB_X26_X27 * 8)]
+ stp x24, x25, [x0, #(_JB_X24_X25 * 8)]
+ stp x22, x23, [x0, #(_JB_X22_X23 * 8)]
+ stp x20, x21, [x0, #(_JB_X20_X21 * 8)]
+ str x19, [x0, #(_JB_X19 * 8)]
// Save floating point registers.
- stp d14, d15, [x0, #(_JB_FLOAT_BASE * 4 + 16 * 0)]
- stp d12, d13, [x0, #(_JB_FLOAT_BASE * 4 + 16 * 1)]
- stp d10, d11, [x0, #(_JB_FLOAT_BASE * 4 + 16 * 2)]
- stp d8, d9, [x0, #(_JB_FLOAT_BASE * 4 + 16 * 3)]
+ stp d14, d15, [x0, #(_JB_D14_D15 * 8)]
+ stp d12, d13, [x0, #(_JB_D12_D13 * 8)]
+ stp d10, d11, [x0, #(_JB_D10_D11 * 8)]
+ stp d8, d9, [x0, #(_JB_D8_D9 * 8)]
mov w0, #0
ret
// void siglongjmp(sigjmp_buf env, int value);
ENTRY(siglongjmp)
// Do we need to restore the signal mask?
- ldr w9, [x0, #(_JB_SIGFLAG * 4)]
+ ldr w9, [x0, #(_JB_SIGFLAG * 8)]
cbz w9, 1f
// Restore signal mask.
mov x19, x1 // Save 'value'.
mov x2, x0
mov x0, #2 // SIG_SETMASK
- add x1, x2, #(_JB_SIGMASK * 4) // new_mask.
+ add x1, x2, #(_JB_SIGMASK * 8) // new_mask.
mov x2, #0 // NULL.
bl sigprocmask
mov x1, x19 // Restore 'value'.
1:
// Restore core registers.
- ldp x30, x10, [x0, #(_JB_CORE_BASE * 4 + 16 * 0)]
+ ldp x30, x10, [x0, #(_JB_X30_SP * 8)]
mov sp, x10
- ldp x28, x29, [x0, #(_JB_CORE_BASE * 4 + 16 * 1)]
- ldp x26, x27, [x0, #(_JB_CORE_BASE * 4 + 16 * 2)]
- ldp x24, x25, [x0, #(_JB_CORE_BASE * 4 + 16 * 3)]
- ldp x22, x23, [x0, #(_JB_CORE_BASE * 4 + 16 * 4)]
- ldp x20, x21, [x0, #(_JB_CORE_BASE * 4 + 16 * 5)]
- ldr x19, [x0, #(_JB_CORE_BASE * 4 + 16 * 6)]
+ ldp x28, x29, [x0, #(_JB_X28_X29 * 8)]
+ ldp x26, x27, [x0, #(_JB_X26_X27 * 8)]
+ ldp x24, x25, [x0, #(_JB_X24_X25 * 8)]
+ ldp x22, x23, [x0, #(_JB_X22_X23 * 8)]
+ ldp x20, x21, [x0, #(_JB_X20_X21 * 8)]
+ ldr x19, [x0, #(_JB_X19 * 8)]
// Restore floating point registers.
- ldp d14, d15, [x0, #(_JB_FLOAT_BASE * 4 + 16 * 0)]
- ldp d12, d13, [x0, #(_JB_FLOAT_BASE * 4 + 16 * 1)]
- ldp d10, d11, [x0, #(_JB_FLOAT_BASE * 4 + 16 * 2)]
- ldp d8, d9, [x0, #(_JB_FLOAT_BASE * 4 + 16 * 3)]
+ ldp d14, d15, [x0, #(_JB_D14_D15 * 8)]
+ ldp d12, d13, [x0, #(_JB_D12_D13 * 8)]
+ ldp d10, d11, [x0, #(_JB_D10_D11 * 8)]
+ ldp d8, d9, [x0, #(_JB_D8_D9 * 8)]
// Validate sp (sp mod 16 = 0) and lr (lr mod 4 = 0).
tst x30, #3