]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/platform-bionic.git/commitdiff
Use mmap to create the pthread_internal_t.
authorYabin Cui <yabinc@google.com>
Tue, 25 Nov 2014 22:18:12 +0000 (14:18 -0800)
committerYabin Cui <yabinc@google.com>
Tue, 25 Nov 2014 23:25:06 +0000 (15:25 -0800)
Bug: 16847284
Change-Id: Ic8c85f95afac1d8422ecb69674c688d1fecb6a44

libc/bionic/pthread_create.cpp
libc/bionic/pthread_exit.cpp
libc/bionic/pthread_internal.h
libc/bionic/pthread_internals.cpp

index fc8afa2ff9401e9184c1dc863eefc1ef97772eef..8bb1be9d9e0289dac26c9ce483e7fda92812b0b8 100644 (file)
@@ -158,9 +158,8 @@ int pthread_create(pthread_t* thread_out, pthread_attr_t const* attr,
   // Inform the rest of the C library that at least one thread was created.
   __isthreaded = 1;
 
-  pthread_internal_t* thread = reinterpret_cast<pthread_internal_t*>(calloc(sizeof(*thread), 1));
+  pthread_internal_t* thread = __create_thread_struct();
   if (thread == NULL) {
-    __libc_format_log(ANDROID_LOG_WARN, "libc", "pthread_create failed: couldn't allocate thread");
     return EAGAIN;
   }
 
@@ -179,7 +178,7 @@ int pthread_create(pthread_t* thread_out, pthread_attr_t const* attr,
     // The caller didn't provide a stack, so allocate one.
     thread->attr.stack_base = __create_thread_stack(thread);
     if (thread->attr.stack_base == NULL) {
-      free(thread);
+      __free_thread_struct(thread);
       return EAGAIN;
     }
   } else {
@@ -230,7 +229,7 @@ int pthread_create(pthread_t* thread_out, pthread_attr_t const* attr,
     if (!thread->user_allocated_stack()) {
       munmap(thread->attr.stack_base, thread->attr.stack_size);
     }
-    free(thread);
+    __free_thread_struct(thread);
     __libc_format_log(ANDROID_LOG_WARN, "libc", "pthread_create failed: clone failed: %s", strerror(errno));
     return clone_errno;
   }
index 6cd5311ede5fc1ef47428eddf02f4d40ae88fd4e..479088032566e0c2e2abd12f9dda03f650204ef3 100644 (file)
@@ -37,6 +37,7 @@
 extern "C" __noreturn void _exit_with_stack_teardown(void*, size_t);
 extern "C" __noreturn void __exit(int);
 extern "C" int __set_tid_address(int*);
+extern "C" void __set_tls(void*);
 
 /* CAVEAT: our implementation of pthread_cleanup_push/pop doesn't support C++ exceptions
  *         and thread cancelation
@@ -75,6 +76,9 @@ void pthread_exit(void* return_value) {
   // space (see pthread_key_delete).
   pthread_key_clean_all();
 
+  // Clear tls to prevent further use of __get_tls(), see b/16847284.
+  __set_tls(NULL);
+
   if (thread->alternate_signal_stack != NULL) {
     // Tell the kernel to stop using the alternate signal stack.
     stack_t ss;
@@ -112,12 +116,6 @@ void pthread_exit(void* return_value) {
   }
   pthread_mutex_unlock(&g_thread_list_lock);
 
-  // Perform a second key cleanup. When using jemalloc, a call to free from
-  // _pthread_internal_remove_locked causes the memory associated with a key
-  // to be reallocated.
-  // TODO: When b/16847284 is fixed this call can be removed.
-  pthread_key_clean_all();
-
   if (user_allocated_stack) {
     // Cleaning up this thread's stack is the creator's responsibility, not ours.
     __exit(0);
index 392e781e4b7e913fd3fed7f1b86a7bbc9fbb01e4..4308a98144d0cae803949df70fbb198be28d3a68 100644 (file)
@@ -94,6 +94,9 @@ struct pthread_internal_t {
   char dlerror_buffer[__BIONIC_DLERROR_BUFFER_SIZE];
 };
 
+__LIBC_HIDDEN__ pthread_internal_t* __create_thread_struct();
+__LIBC_HIDDEN__ void __free_thread_struct(pthread_internal_t*);
+
 __LIBC_HIDDEN__ int __init_thread(pthread_internal_t* thread, bool add_to_thread_list);
 __LIBC_HIDDEN__ void __init_tls(pthread_internal_t* thread);
 __LIBC_HIDDEN__ void __init_alternate_signal_stack(pthread_internal_t*);
index 2270d96f3010ed73be5c10f60c76fc16a7a6866f..33cddd74e771683f587a9398275b234e60ee0449 100644 (file)
 
 #include "pthread_internal.h"
 
+#include <errno.h>
 #include <stdlib.h>
+#include <string.h>
+#include <sys/mman.h>
 
 #include "private/bionic_futex.h"
 #include "private/bionic_tls.h"
+#include "private/libc_logging.h"
 #include "private/ScopedPthreadMutexLocker.h"
 
 pthread_internal_t* g_thread_list = NULL;
 pthread_mutex_t g_thread_list_lock = PTHREAD_MUTEX_INITIALIZER;
 
+pthread_internal_t* __create_thread_struct() {
+  void* result = mmap(NULL, sizeof(pthread_internal_t), PROT_READ | PROT_WRITE,
+                      MAP_PRIVATE | MAP_ANONYMOUS | MAP_NORESERVE, -1, 0);
+  if (result == MAP_FAILED) {
+    __libc_format_log(ANDROID_LOG_WARN, "libc",
+                      "__create_thread_struct() failed: %s", strerror(errno));
+    return NULL;
+  }
+  return reinterpret_cast<pthread_internal_t*>(result);
+}
+
+void __free_thread_struct(pthread_internal_t* thread) {
+  int result = munmap(thread, sizeof(pthread_internal_t));
+  if (result != 0) {
+    __libc_format_log(ANDROID_LOG_WARN, "libc",
+                      "__free_thread_struct() failed: %s", strerror(errno));
+  }
+}
+
 void _pthread_internal_remove_locked(pthread_internal_t* thread) {
   if (thread->next != NULL) {
     thread->next->prev = thread->prev;
@@ -50,7 +73,7 @@ void _pthread_internal_remove_locked(pthread_internal_t* thread) {
   // The main thread is not heap-allocated. See __libc_init_tls for the declaration,
   // and __libc_init_common for the point where it's added to the thread list.
   if ((thread->attr.flags & PTHREAD_ATTR_FLAG_MAIN_THREAD) == 0) {
-    free(thread);
+    __free_thread_struct(thread);
   }
 }