Allow stdatomic.h to be included from mingw prebuilt.
[android-sdk/platform-bionic.git] / libc / include / stdatomic.h
2014-11-13 Hans BoehmAllow stdatomic.h to be included from mingw prebuilt.
2014-10-16 Dmitriy IvanovMerge "Fix misleading comment."
2014-10-16 Dan Albertam 90aa7e37: Merge "Only use <atomic> for C++11 and...
2014-10-16 Dan AlbertMerge "Only use <atomic> for C++11 and newer."
2014-10-16 Dan AlbertOnly use <atomic> for C++11 and newer.
2014-10-10 Christopher Ferrisam c891e240: Add back symbols to fix Greed for Glory...
2014-10-09 Christopher Ferrisresolved conflicts for merge of c9734d24 to lmp-dev...
2014-10-07 Elliott Hughesam 1543fdf6: Work around a bug in Immersion\'s libImmEm...
2014-10-07 Christopher Ferrisam 2cf15571: am 40bc7cd4: (-s ours) DO NOT MERGE Re...
2014-10-07 Christopher Ferrisam 40bc7cd4: (-s ours) DO NOT MERGE Re-add .save direc...
2014-10-06 Christopher Ferrisresolved conflicts for merge of d11eac34 to lmp-dev...
2014-10-06 Dan AlbertMerge "Add compile time test infrastructure for bionic."
2014-10-04 Elliott Hughesresolved conflicts for merge of a5087148 to lmp-dev...
2014-10-03 Elliott Hughesam ea9800e9: Explain why clock(3) isn\'t broken.
2014-10-02 Dmitriy IvanovMerge "Add RTLD_NODELETE flag support"
2014-10-01 Hans Boehmam 2d111d9e: Merge "Make memory_order_acquire visible...
2014-10-01 Hans BoehmMerge "Make memory_order_acquire visible in global...
2014-10-01 Hans BoehmMake memory_order_acquire visible in global namespace
2014-09-09 Lorenzo ColittiMerge "When comparing DNS server configs, also compare...
2014-09-03 Dmitriy IvanovMerge "Make string tests check all alignment combinations"
2014-09-03 Hans Boehmam 9ac60bf8: Make stdatomic.h work with gcc4.6 host...
2014-09-03 Andreas Gamperesolved conflicts for merge of 2b10e2f1 to lmp-dev...
2014-09-02 Hans Boehmresolved conflicts for merge of c8cf3513 to lmp-dev...
2014-09-02 Elliott HughesMerge "Upgrade bionic to tzdata2014g." into lmp-dev
2014-09-02 Hans BoehmMake stdatomic.h work with gcc4.6 host compiler
2014-09-02 Hans BoehmUndefine _Atomic before redefining
2014-09-02 Hans BoehmFix, generalize stdatomic.h; improve test.
2014-09-01 Dmitriy Ivanovresolved conflicts for merge of c191a8ad to lmp-dev...
2014-09-01 Dmitriy IvanovMerge "Look into ld_preloads before current library...
2014-09-01 Dmitriy IvanovMerge "Erase elements in LinkedList::remove_if"
2014-08-31 Elliott Hughesresolved conflicts for merge of b2eb09a9 to lmp-dev...
2014-08-30 Hans Boehmam e505cc66: Merge "Make stdatomic.h work with gcc4...
2014-08-30 Hans BoehmMerge "Make stdatomic.h work with gcc4.6 host compiler"
2014-08-30 Hans BoehmMake stdatomic.h work with gcc4.6 host compiler
2014-08-29 Elliott Hughesam bbe06e0d: Merge "Use __GNUC_PREREQ rather than __GNU...
2014-08-29 Elliott HughesUse __GNUC_PREREQ rather than __GNUC_PREREQ__ to match...
2014-08-29 Elliott HughesMerge "Use __GNUC_PREREQ rather than __GNUC_PREREQ__...
2014-08-29 Elliott HughesUse __GNUC_PREREQ rather than __GNUC_PREREQ__ to match...
2014-08-28 Elliott Hughesam 67f1f3b1: Have pthread_attr_getstack for the main...
2014-08-28 Elliott Hughesresolved conflicts for merge of a0eeb0b6 to lmp-dev...
2014-08-27 Chih-Hung HsiehMerge "Fix strlen function type for mips."
2014-08-27 Christopher Ferrisam 598d25bf: Merge "Replace snprintf calls in linker...
2014-08-27 Chih-Hung HsiehMerge "Replace ambiguous cmp instruction with cmpl."
2014-08-27 Chih-Hung HsiehMerge "Add missing type casts before comparison."
2014-08-27 Elliott Hughesam 6cc4e3b6: Merge "call uselocale() before freelocale...
2014-08-27 Christopher Ferrisam 3f7635f4: Use the default unwind code.
2014-08-27 Hans Boehmam 6bfcefe0: Merge "Undefine _Atomic before redefining"
2014-08-26 Hans BoehmMerge "Undefine _Atomic before redefining"
2014-08-26 Elliott HughesMerge "Switch to OpenBSD res_random."
2014-08-26 Hans BoehmUndefine _Atomic before redefining
2014-08-22 Hans Boehmam a4a8c4fe: Merge "Fix, generalize stdatomic.h; improv...
2014-08-22 Hans BoehmMerge "Fix, generalize stdatomic.h; improve test."
2014-08-22 Hans BoehmFix, generalize stdatomic.h; improve test.
2014-08-16 Christopher FerrisMerge "Fix leak_realloc, copy entire allocation." into...
2014-08-15 Dmitriy IvanovMerge "Keep symbols for linker" into lmp-dev
2014-08-15 Hans BoehmHave stdatomic.h punt to C++ atomic when possible
2014-08-15 Hans Boehmam 7d05f741: Merge "Have stdatomic.h punt to C++ atomic...
2014-08-15 Hans BoehmMerge "Have stdatomic.h punt to C++ atomic when possible"
2014-08-15 Hans BoehmHave stdatomic.h punt to C++ atomic when possible
2014-07-20 Christopher Ferrisam b0815aea: Make sure not to construct illegal propert...
2014-07-20 Elliott Hughesam fbd00819: Merge "Clean up some misinformation around...
2014-07-20 Christopher Ferrisam a6945179: Merge "Add gen syscalls step to instructio...
2014-07-20 Elliott Hughesam 291da8d3: Remove SIOCKILLADDR from <sys/socket.h>.
2014-07-20 Elliott Hughesam b5bef263: (-s ours) Remove PR_SET_TIMERSLACK_PID...
2014-07-20 Christopher Ferrisam e8bc5813: Use the mmap/munmap for allocation routines.
2014-07-19 Hans BoehmDefine atomic_charN_t only if charN_t is supported.
2014-07-18 Elliott Hughesam b4669685: Fix private/bionic_name_mem.h build breakage.
2014-07-18 Elliott Hughesresolved conflicts for merge of d648f557 to lmp-dev...
2014-07-17 Elliott Hughesam 9a7fdb2d: ptrace(3) should be varargs.
2014-07-17 Elliott Hughesam 3002131d: Use VDSO for clock_gettime(2) and gettimeo...
2014-07-17 Hans Boehmam 43363ab7: Merge "Define atomic_charN_t only if charN...
2014-07-16 Hans BoehmMerge "Define atomic_charN_t only if charN_t is supported."
2014-07-17 Hans BoehmDefine atomic_charN_t only if charN_t is supported.
2014-06-17 Elliott HughesMerge "Add a flag control that PRIVATE libm can be...
2014-05-30 Elliott HughesMerge remote-tracking branch 'goog/master' into merge...
2014-05-28 Christopher FerrisMerge "Add optimized AArch64 versions of bcopy and...
2014-05-28 Narayan KamathMerge "Revert "Lose the hand-written futex assembler.""
2014-05-27 Elliott HughesMerge "Clear the return address register in __bionic_cl...
2014-05-26 Elliott HughesMerge "Restore __srget and __swbuf for LP32."
2014-05-25 Elliott Hughesam 6571b81b: am 21296dfe: am bc904896: Merge "Add C11...
2014-05-25 Elliott Hughesam 21296dfe: am bc904896: Merge "Add C11 <stdatomic...
2014-05-25 Elliott Hughesam bc904896: Merge "Add C11 <stdatomic.h>."
2014-05-25 Elliott HughesMerge "Add C11 <stdatomic.h>."
2014-05-24 Elliott HughesAdd C11 <stdatomic.h>.