]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/platform-bionic.git/history - linker/debugger.cpp
Support gethostbyname_r_ERANGE.
[android-sdk/platform-bionic.git] / linker / debugger.cpp
2014-10-10 Christopher Ferrisam c891e240: Add back symbols to fix Greed for Glory...
2014-10-09 Christopher Ferrisresolved conflicts for merge of c9734d24 to lmp-dev...
2014-10-07 Elliott Hughesam 1543fdf6: Work around a bug in Immersion\'s libImmEm...
2014-10-07 Christopher Ferrisam 2cf15571: am 40bc7cd4: (-s ours) DO NOT MERGE Re...
2014-10-07 Christopher Ferrisam 40bc7cd4: (-s ours) DO NOT MERGE Re-add .save direc...
2014-10-06 Christopher Ferrisresolved conflicts for merge of d11eac34 to lmp-dev...
2014-10-04 Elliott Hughesresolved conflicts for merge of a5087148 to lmp-dev...
2014-10-03 Elliott Hughesam ea9800e9: Explain why clock(3) isn\'t broken.
2014-09-25 Elliott Hughesam aaad5485: Merge "Re-expose more stdio implementation...
2014-09-24 Christopher Ferrisam 6c69afdb: Fix sys_stat.mkfifo when not run as root.
2014-09-24 Dan AlbertMerge "Coverage configs for bionic."
2014-09-24 Dan AlbertMerge "Add a dummy atexit(3) to the linker."
2014-09-24 Dan Albertam 086bb382: Fix incorrect parameter types for locale...
2014-09-23 Elliott Hughesam 93951cfa: Merge "Fix a couple more cases of missing...
2014-09-23 Elliott HughesMerge "Fix a couple more cases of missing CLOEXEC."
2014-09-23 Elliott HughesFix a couple more cases of missing CLOEXEC.
2014-09-14 Christopher Ferrisam 027d2717: Pull input.h from v3.16.1 kernel headers.
2014-09-12 Elliott Hughesam 7e00b44e: Expose __swsetup for LP32 binary compatibi...
2014-09-12 Elliott Hughesam 27efc488: Add pthread_gettid_np and re-expose __get_...
2014-09-11 Elliott Hughesam 9e833bf0: Fix mips __fadvise64.S build failure.
2014-09-11 Elliott Hughesam 176c3278: Merge "Add posix_fadvise(3)." into lmp-dev
2014-09-11 Lorenzo Colittiam 33a73bfa: When comparing DNS server configs, also...
2014-09-09 Lorenzo ColittiMerge "When comparing DNS server configs, also compare...
2014-09-08 Elliott Hughesresolved conflicts for merge of 7efad83d to lmp-dev...
2014-09-08 Elliott Hughesresolved conflicts for merge of c8f6b82f to lmp-dev...
2014-09-08 Elliott Hughesam 51c8355d: Add arc4random_addrandom binary compatibility.
2014-09-06 Christopher Ferrisam 47ed03f7: Merge "Add dlmalloc_usable_size for 32...
2014-09-05 Elliott Hughesam 5beddb7d: Fix pthread_attr_getstack__main_thread.
2014-09-03 Elliott Hughesam 1e010d60: Add back a dummy arc4random_stir for compa...
2014-09-03 Dmitriy IvanovMerge "Make string tests check all alignment combinations"
2014-09-03 Elliott Hughesam cb093d1f: Merge "Upgrade bionic to tzdata2014g....
2014-09-03 Hans Boehmam 9ac60bf8: Make stdatomic.h work with gcc4.6 host...
2014-09-03 Andreas Gamperesolved conflicts for merge of 2b10e2f1 to lmp-dev...
2014-09-02 Hans Boehmresolved conflicts for merge of c8cf3513 to lmp-dev...
2014-09-01 Dmitriy Ivanovresolved conflicts for merge of c191a8ad to lmp-dev...
2014-09-01 Dmitriy IvanovMerge "Erase elements in LinkedList::remove_if"
2014-08-31 Elliott Hughesresolved conflicts for merge of b2eb09a9 to lmp-dev...
2014-08-29 Dmitriy Ivanovam 83b637fa: Merge "Replace NULL with nullptr"
2014-08-29 Dmitriy IvanovMerge "Replace NULL with nullptr"
2014-08-29 Dmitriy IvanovReplace NULL with nullptr
2014-08-29 Chih-Hung HsiehMerge "Ignore all __weak_alias in OpenBSD libC."
2014-08-27 Elliott HughesMerge "Fix pthread_getattr_np for the main thread....
2014-08-27 Elliott HughesMerge "Have pthread_attr_getstack for the main thread...
2014-08-27 Christopher FerrisMerge "Replace snprintf calls in linker."
2014-08-27 Chih-Hung Hsieham fbe9d3df: Merge "Fix strlen function type for mips."
2014-08-27 Christopher FerrisReplace snprintf calls in linker.
2014-08-27 Yigit BoyarMerge branch 'lmp-dev-plus-aosp' of https://googleplex...
2014-08-27 Christopher Ferrisam 598d25bf: Merge "Replace snprintf calls in linker...
2014-08-27 Christopher FerrisMerge "Replace snprintf calls in linker." into lmp-dev
2014-08-27 Christopher FerrisReplace snprintf calls in linker.
2014-08-26 Elliott HughesMerge "Switch to OpenBSD res_random."
2014-07-29 Elliott HughesMerge "[MIPSR6] Use C-coded string ops on mips32r6...
2014-07-24 Elliott HughesMerge "Implement twalk(3), add unit tests."
2014-07-24 Colin Crossam 49fbec6d: HACK: remove %m support from printf.
2014-07-23 Nick Kralevichdebuggerd: if PR_GET_DUMPABLE=0, don't ask for dumping
2014-07-23 Nick Kralevicham f9650757: Merge "debuggerd: if PR_GET_DUMPABLE=0...
2014-07-23 Nick KralevichMerge "debuggerd: if PR_GET_DUMPABLE=0, don't ask for...
2014-07-23 Nick Kralevichdebuggerd: if PR_GET_DUMPABLE=0, don't ask for dumping
2014-07-23 Elliott HughesMerge "[MIPSR6] setjmp supports mips32r6 and FP64A...
2014-06-17 Elliott HughesMerge "Add a flag control that PRIVATE libm can be...
2014-05-22 Calin JuravleMerge "Mutex-free implementation of pthread_rwlock"
2014-05-20 Christopher FerrisMerge "denver: optimize memmove"
2014-05-19 Christopher FerrisMerge "Accuracy tests for libm"
2014-05-17 The Android Automergermerge in master-release history after reset to de546168...
2014-05-17 Elliott Hughesam ad064403: am 6e37ebfe: am 6c83305c: Merge "Rethrow...
2014-05-17 Elliott Hughesam 6e37ebfe: am 6c83305c: Merge "Rethrow SIGTRAP too."
2014-05-17 Elliott Hughesam 6c83305c: Merge "Rethrow SIGTRAP too."
2014-05-17 Elliott HughesMerge "Rethrow SIGTRAP too."
2014-05-17 Elliott HughesRethrow SIGTRAP too.
2014-05-17 Elliott Hughesam 0a26974e: am dc9ac844: am 2071b983: Merge "debugger...
2014-05-17 Elliott Hughesam dc9ac844: am 2071b983: Merge "debugger.cpp should...
2014-05-17 Elliott Hughesam 2071b983: Merge "debugger.cpp should know the names...
2014-05-17 Elliott HughesMerge "Fix the newly-introduced warning and turn on...
2014-05-17 Elliott HughesMerge "debugger.cpp should know the names of the signal...
2014-05-16 Elliott Hughesdebugger.cpp should know the names of the signals it...
2014-05-15 The Android Automergermerge in master-release history after reset to 5491a4fd...
2014-05-14 Dmitriy IvanovMerge "Fix for linker allocator"
2014-05-14 Elliott Hughesam b2da973f: am 6eb0fe2b: am 15c13bd6: Merge "Switch...
2014-05-14 Elliott Hughesam 6eb0fe2b: am 15c13bd6: Merge "Switch to g_ for globals."
2014-05-14 Elliott Hughesam 15c13bd6: Merge "Switch to g_ for globals."
2014-05-14 Elliott HughesMerge "Switch to g_ for globals."
2014-05-14 Elliott HughesSwitch to g_ for globals.
2014-04-29 Bill YiMerge klp-dev-plus-aosp into stage-aosp-master
2014-04-26 The Android Automergermerge in master-release history after reset to 12e848eb...
2014-04-26 Elliott Hughesam 8fe46b47: am f2dc7d17: Merge "Pass si_code through...
2014-04-26 Elliott Hughesam f2dc7d17: Merge "Pass si_code through to debuggerd."
2014-04-26 Elliott HughesMerge "Pass si_code through to debuggerd."
2014-04-26 Elliott HughesPass si_code through to debuggerd.
2014-04-24 Greg HackmannMerge "Revert "Reserve space in pthread structures...
2014-04-24 Calin JuravleMerge "Remove an unsed include dir"
2014-04-24 Calin JuravleMerge "Removed non-existing include dir"
2014-04-24 Calin JuravleMerge "Reserve space in pthread structures for future...
2014-04-22 The Android Automergermerge in master-release history after reset to master
2014-04-22 Torne (Richard Coles)Merge "Allow sharing the RELRO section via a file."
2014-04-22 Torne (Richard Coles)Merge "Support loading libraries to a reserved address."
2014-04-22 Torne (Richard Coles)Merge "Add android_dlopen_ext() interface to linker."
2014-04-21 Elliott Hughesam a3d82df0: am 8abf44c4: Merge "Make libc signal handl...
2014-04-21 Elliott Hughesam 8abf44c4: Merge "Make libc signal handler output...
2014-04-19 Elliott HughesMerge "Make libc signal handler output more like debugg...
2014-04-19 Elliott HughesMake libc signal handler output more like debuggerd.
next