]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/platform-bionic.git/history - linker/linked_list.h
Merge "Remove bogus transitive includes."
[android-sdk/platform-bionic.git] / linker / linked_list.h
2014-12-09 Yabin CuiMerge "support _POSIX_REALTIME_SIGNALS"
2014-12-02 Yabin CuiMerge "Use mmap to create the pthread_internal_t."
2014-12-02 Dmitriy IvanovMerge "Count references for groups instead of instances"
2014-12-02 Dmitriy IvanovCount references for groups instead of instances
2014-11-01 Dmitriy IvanovMerge "Revert "Use local copy of the library name on...
2014-10-31 Dmitriy Ivanovam f33ad400: Merge "Fix symbol lookup order during...
2014-10-31 Dmitriy IvanovMerge "Fix symbol lookup order during relocation"
2014-10-31 Dmitriy IvanovFix symbol lookup order during relocation
2014-10-28 Dmitriy Ivanovam 566f2bc6: Merge "Fix relocation to look for symbols...
2014-10-24 Elliott HughesMerge "Add mkfifoat(3)."
2014-10-23 Dmitriy IvanovMerge "Fix relocation to look for symbols in local...
2014-10-23 Dmitriy IvanovFix relocation to look for symbols in local group
2014-10-10 Christopher Ferrisam c891e240: Add back symbols to fix Greed for Glory...
2014-10-09 Christopher Ferrisresolved conflicts for merge of c9734d24 to lmp-dev...
2014-10-07 Elliott Hughesam 1543fdf6: Work around a bug in Immersion\'s libImmEm...
2014-10-07 Christopher Ferrisam 2cf15571: am 40bc7cd4: (-s ours) DO NOT MERGE Re...
2014-10-07 Christopher Ferrisam 40bc7cd4: (-s ours) DO NOT MERGE Re-add .save direc...
2014-10-06 Christopher Ferrisresolved conflicts for merge of d11eac34 to lmp-dev...
2014-10-04 Elliott Hughesresolved conflicts for merge of a5087148 to lmp-dev...
2014-10-03 Elliott Hughesam ea9800e9: Explain why clock(3) isn\'t broken.
2014-09-25 Elliott Hughesam aaad5485: Merge "Re-expose more stdio implementation...
2014-09-24 Christopher Ferrisam 6c69afdb: Fix sys_stat.mkfifo when not run as root.
2014-09-24 Dan Albertam 086bb382: Fix incorrect parameter types for locale...
2014-09-14 Christopher Ferrisam 027d2717: Pull input.h from v3.16.1 kernel headers.
2014-09-12 Elliott Hughesam 7e00b44e: Expose __swsetup for LP32 binary compatibi...
2014-09-12 Elliott Hughesam 27efc488: Add pthread_gettid_np and re-expose __get_...
2014-09-11 Elliott Hughesam 9e833bf0: Fix mips __fadvise64.S build failure.
2014-09-11 Elliott Hughesam 176c3278: Merge "Add posix_fadvise(3)." into lmp-dev
2014-09-11 Lorenzo Colittiam 33a73bfa: When comparing DNS server configs, also...
2014-09-09 Lorenzo ColittiMerge "When comparing DNS server configs, also compare...
2014-09-09 Dmitriy Ivanovam 3c3624f3: Merge "Load libraries in breadth-first...
2014-09-09 Dmitriy IvanovMerge "Load libraries in breadth-first order"
2014-09-08 Elliott Hughesresolved conflicts for merge of 7efad83d to lmp-dev...
2014-09-08 Dmitriy IvanovLoad libraries in breadth-first order
2014-09-08 Elliott Hughesresolved conflicts for merge of c8f6b82f to lmp-dev...
2014-09-08 Elliott Hughesam 51c8355d: Add arc4random_addrandom binary compatibility.
2014-09-06 Christopher Ferrisam 47ed03f7: Merge "Add dlmalloc_usable_size for 32...
2014-09-05 Elliott Hughesam 5beddb7d: Fix pthread_attr_getstack__main_thread.
2014-09-03 Elliott Hughesam 1e010d60: Add back a dummy arc4random_stir for compa...
2014-09-03 Dmitriy IvanovMerge "Make string tests check all alignment combinations"
2014-09-03 Elliott Hughesam cb093d1f: Merge "Upgrade bionic to tzdata2014g....
2014-09-03 Hans Boehmam 9ac60bf8: Make stdatomic.h work with gcc4.6 host...
2014-09-03 Andreas Gamperesolved conflicts for merge of 2b10e2f1 to lmp-dev...
2014-09-02 Dan AlbertMerge "Prevent a few test pthread keys from leaking."
2014-09-02 Hans Boehmresolved conflicts for merge of c8cf3513 to lmp-dev...
2014-09-02 Elliott HughesMerge "Upgrade bionic to tzdata2014g."
2014-09-02 Dmitriy IvanovMerge "Introduce size-based r/w allocators"
2014-09-02 Dmitriy Ivanovam 4cafa3ce: Merge "Implement LinkedList::visit()"
2014-09-02 Dmitriy IvanovMerge "Implement LinkedList::visit()"
2014-09-02 Dmitriy IvanovImplement LinkedList::visit()
2014-09-01 Dmitriy Ivanovresolved conflicts for merge of c191a8ad to lmp-dev...
2014-09-01 Dmitriy Ivanovam 11387985: Merge "Erase elements in LinkedList::remov...
2014-09-01 Dmitriy IvanovMerge "Erase elements in LinkedList::remove_if"
2014-08-31 Elliott Hughesresolved conflicts for merge of b2eb09a9 to lmp-dev...
2014-08-30 Dmitriy IvanovErase elements in LinkedList::remove_if
2014-08-28 Elliott Hughesam 67f1f3b1: Have pthread_attr_getstack for the main...
2014-08-28 Elliott Hughesresolved conflicts for merge of a0eeb0b6 to lmp-dev...
2014-08-27 Chih-Hung HsiehMerge "Fix strlen function type for mips."
2014-08-27 Christopher Ferrisam 598d25bf: Merge "Replace snprintf calls in linker...
2014-08-27 Chih-Hung HsiehMerge "Replace ambiguous cmp instruction with cmpl."
2014-08-27 Chih-Hung HsiehMerge "Add missing type casts before comparison."
2014-08-27 Elliott Hughesam 6cc4e3b6: Merge "call uselocale() before freelocale...
2014-08-27 Christopher Ferrisam 3f7635f4: Use the default unwind code.
2014-08-26 Dmitriy Ivanovam d2bd3c47: Merge "Enable __cxa_atexit && __cxa_finali...
2014-08-26 Elliott HughesMerge "Switch to OpenBSD res_random."
2014-08-26 Elliott HughesMerge "libc should use O_CLOEXEC when opening files...
2014-08-26 Dmitriy IvanovMerge "Enable __cxa_atexit && __cxa_finalize for linker"
2014-08-26 Dmitriy IvanovEnable __cxa_atexit && __cxa_finalize for linker
2014-08-13 Dmitriy Ivanovam db0785cb: Merge "Optimize symbol lookup"
2014-08-13 Dmitriy IvanovOptimize symbol lookup
2014-08-13 Dmitriy IvanovMerge "Optimize symbol lookup"
2014-08-13 Dmitriy IvanovOptimize symbol lookup
2014-08-12 Dan AlbertMerge "Hide __libc_init_vdso()."
2014-08-12 Hans BoehmMerge "Add memory ordering constraint, convert to C11...
2014-08-12 Dmitriy IvanovMerge "Added test for ifunc support in dynamic linker."
2014-08-12 Dan AlbertMerge "Hide ScopedTrace."
2014-08-06 Christopher FerrisMerge "Do a second key cleanup in pthread_exit." into...
2014-08-06 Elliott HughesMerge "Workaround b/16818336 which fails build under...
2014-08-06 Dmitriy Ivanovam db7a17d4: Revert "Revert "Fix dlsym(3) to do breadth...
2014-08-05 Dan Albertam de69069f: Merge "Fixes build."
2014-08-05 Dan Albertam a7ef8188: Merge "Revert "Replaces vfork() implementa...
2014-08-04 Dmitriy IvanovRevert "Revert "Fix dlsym(3) to do breadth first search.""
2014-08-04 Dmitriy Ivanovam 1b1966d9: Revert "Fix dlsym(3) to do breadth first...
2014-08-04 Dmitriy IvanovRevert "Fix dlsym(3) to do breadth first search."
2014-07-29 Dmitriy Ivanovam 2b591b37: Merge "Fix dlsym(3) to do breadth first...
2014-07-29 Dmitriy IvanovFix dlsym(3) to do breadth first search.
2014-07-29 Elliott HughesMerge "[MIPSR6] Use C-coded string ops on mips32r6...
2014-07-29 Dmitriy IvanovMerge "Fix dlsym(3) to do breadth first search."
2014-07-29 Elliott HughesMerge "Revert "Added a bionic systrace class and tracin...
2014-07-29 Dan AlbertMerge "en_US.UTF-8 is also supported." into lmp-dev
2014-07-29 Dmitriy IvanovFix dlsym(3) to do breadth first search.
2014-07-28 Christopher FerrisMerge "Use libunwindbacktrace for debug malloc code."
2014-07-28 Dan AlbertMerge "Fix mbsrtowcs(3)'s handling of len parameter...
2014-07-25 Dan AlbertMerge "There is no _MIN for unsigned types." into lmp-dev
2014-07-25 Dan AlbertMerge "__libc_fatal should print a newline to stderr...
2014-06-17 Elliott HughesMerge "Add a flag control that PRIVATE libm can be...
2014-06-16 Elliott Hughesam fe6e646c: Update NOTICE files.
2014-06-07 Elliott Hughesam 3b9da0f9: Fix the printf family for non-ASCII.
2014-06-06 Elliott Hughesam 5f409720: Merge "Use __libc_fatal() for failed mallo...
2014-06-06 Elliott Hughesresolved conflicts for merge of bd7a892c to master
next