am 6cdab387: Merge "Restore <nsswitch.h> which is BSD API, not private."
[android-sdk/platform-bionic.git] / linker /
2014-06-30 Elliott HughesMerge "Restore <nsswitch.h> which is BSD API, not private."
2014-06-30 Elliott Hughesam 260846f3: Merge "Reinstate the x86 dynamic linker...
2014-06-30 Dmitriy Ivanovam e5c759ff: Merge "Disallow dlopen("egl/blah.so")...
2014-06-30 Christopher FerrisMerge "Add extra strchr testing."
2014-06-28 Colin Crossam ddc44974: Merge "Revert "HACK: linker: check for...
2014-06-26 Colin CrossMerge "Revert "HACK: linker: check for handle==0xffffff...
2014-06-26 Dmitriy IvanovMerge "Disallow dlopen("egl/blah.so") on LP64"
2014-06-29 Dmitriy IvanovDisallow dlopen("egl/blah.so") on LP64
2014-06-26 Elliott HughesMerge "Reinstate the x86 dynamic linker warning for...
2014-06-30 Elliott HughesReinstate the x86 dynamic linker warning for text reloc...
2014-06-20 Dan AlbertMerge "Remove SHA1 from LP64 in favor of libcrypto."
2014-06-20 Christopher FerrisMerge "[MIPS64] Regenerate mips kernel headers with...
2014-06-20 Christopher FerrisMerge "[MIPS64] Adjust kernel/tools for mips32,mips64...
2014-06-19 Nick Kralevicham 8a7cffc8: Merge "Reenable support for non-PIE execut...
2014-06-18 Dan AlbertMerge "Revert "Hide _tolower_tab_ and _toupper_tab_...
2014-06-18 Dan AlbertMerge "Hide _tolower_tab_ and _toupper_tab_ on LP64."
2014-06-18 Dmitriy Ivanovam 64dfbd24: Merge "Fix weak function lookups"
2014-06-17 Elliott HughesMerge "Update localtime.c."
2014-06-17 Christopher FerrisMerge "add 64-bit bionic implementation for denver...
2014-06-17 Nick KralevichMerge "Reenable support for non-PIE executables"
2014-06-19 Nick KralevichReenable support for non-PIE executables
2014-06-17 Dan AlbertMerge "Hide __atexit and remove __atexit_invalid."
2014-06-17 Dmitriy IvanovMerge "Fix weak function lookups"
2014-06-17 Dmitriy IvanovFix weak function lookups
2014-06-17 Elliott HughesMerge "Add a flag control that PRIVATE libm can be...
2014-06-16 Colin CrossRevert "HACK: linker: check for handle==0xffffffff...
2014-06-13 Elliott Hughesam ae3c6af3: Merge "[MIPS64] linker64 requires startup...
2014-06-12 Dan AlbertMerge "Remove ioprio_get(2) and ioprio_set(2) from...
2014-06-12 Elliott HughesMerge "[MIPS64] linker64 requires startup code"
2014-06-13 Chris Dearman[MIPS64] linker64 requires startup code
2014-06-04 Dan AlbertMerge "Adds functionality specified by uchar.h"
2014-06-04 Dan AlbertMerge "Removes bcopy and bzero from bionic."
2014-06-03 Elliott Hughesam bd6b8497: Merge "Remove an unused parameter from...
2014-06-03 Elliott HughesMerge "Remove an unused parameter from the dlopen imple...
2014-06-03 Elliott Hughesam be15d16b: Merge "Turn on -Wunused and fix the mistak...
2014-06-03 Elliott HughesRemove an unused parameter from the dlopen implementation.
2014-06-03 Elliott HughesMerge "Turn on -Wunused and fix the mistakes it uncovers."
2014-06-03 Elliott HughesTurn on -Wunused and fix the mistakes it uncovers.
2014-05-28 Narayan KamathMerge "Revert "Lose the hand-written futex assembler.""
2014-05-23 Calin JuravleMerge "Migrate pthread_rwlock implementation away from...
2014-05-23 Elliott HughesMerge "Hide various stdio implementation details."
2014-05-23 Elliott HughesMerge "Lose the hand-written futex assembler."
2014-05-23 Dmitriy Ivanovam d97458eb: am ce00354f: Merge "Do not add arcs to...
2014-05-23 Dmitriy Ivanovam ce00354f: Merge "Do not add arcs to the soinfo graph...
2014-05-23 Dmitriy IvanovMerge "Do not add arcs to the soinfo graph on dlopen"
2014-05-23 Bjorn AnderssonDo not add arcs to the soinfo graph on dlopen
2014-05-22 Elliott Hughesam 8a326a17: am 4f6ed4a1: Merge "Remove unnecessary...
2014-05-22 Elliott Hughesam 4f6ed4a1: Merge "Remove unnecessary #includes of...
2014-05-22 Elliott HughesMerge "Remove unnecessary #includes of <sys/atomics...
2014-05-22 Elliott HughesRemove unnecessary #includes of <sys/atomics.h>.
2014-05-22 Calin JuravleMerge "Add dprintf test"
2014-05-22 Calin JuravleMerge "Switch to POSIX dprintf/vdprintf."
2014-05-22 Dmitriy Ivanovam 5bfa06de: am 3eb9f1f6: Merge "Removed dlsym handle...
2014-05-22 Dmitriy Ivanovam 3eb9f1f6: Merge "Removed dlsym handle != NULL check...
2014-05-22 Dmitriy IvanovMerge "Removed dlsym handle != NULL check for lp64"
2014-05-22 Calin JuravleMerge "Add padding to mips ucontext_t."
2014-05-22 Calin JuravleMerge "Clean up ucontext.h TODOs."
2014-05-22 Calin JuravleMerge "Mutex-free implementation of pthread_rwlock"
2014-05-22 Dmitriy IvanovRemoved dlsym handle != NULL check for lp64
2014-05-21 Christopher FerrisMerge "Support for jemalloc to replace dlmalloc."
2014-05-21 Neil FullerMerge "Change update-tzdata.py to update ICU data as...
2014-05-20 Colin Crossam 8a6217df: am 3d2bc5d6: Merge "HACK: linker: check...
2014-05-20 Colin Crossam 3d2bc5d6: Merge "HACK: linker: check for handle...
2014-05-20 Colin CrossMerge "HACK: linker: check for handle==0xffffffff on...
2014-05-20 Colin CrossHACK: linker: check for handle==0xffffffff on LP64
2014-05-20 Christopher FerrisMerge "denver: optimize memmove"
2014-05-20 Dmitriy Ivanovam 87ce52ac: am f092feb8: Merge "Add R_X86_64_64 to...
2014-05-20 Dmitriy Ivanovam 5277e772: am 0a8f296e: Merge "Add RTLD_NOLOAD suppor...
2014-05-20 Dmitriy Ivanovam f092feb8: Merge "Add R_X86_64_64 to the list of...
2014-05-20 Dmitriy Ivanovam 0a8f296e: Merge "Add RTLD_NOLOAD support and some...
2014-05-20 Dmitriy IvanovMerge "Add R_X86_64_64 to the list of possible weak...
2014-05-20 Dmitriy IvanovMerge "Add RTLD_NOLOAD support and some related changes."
2014-05-20 Dmitriy IvanovAdd RTLD_NOLOAD support and some related changes.
2014-05-20 Elliott HughesMerge "Add a script for finding symbols in bionic that...
2014-05-20 Dmitriy Ivanovam 486628a3: am 0b9a72ce: Merge "Fix lookup-by-base...
2014-05-20 Dmitriy Ivanovam 0b9a72ce: Merge "Fix lookup-by-base-name for lp64"
2014-05-20 Dmitriy IvanovMerge "Fix lookup-by-base-name for lp64"
2014-05-20 Pavel ChupinAdd R_X86_64_64 to the list of possible weak relocs
2014-05-20 Dmitriy IvanovFix lookup-by-base-name for lp64
2014-05-19 Christopher FerrisMerge "Accuracy tests for libm"
2014-05-17 Elliott Hughesam 6e37ebfe: am 6c83305c: Merge "Rethrow SIGTRAP too."
2014-05-17 Elliott Hughesam 6c83305c: Merge "Rethrow SIGTRAP too."
2014-05-17 Elliott HughesMerge "Rethrow SIGTRAP too."
2014-05-17 Elliott HughesRethrow SIGTRAP too.
2014-05-17 Elliott Hughesam dc9ac844: am 2071b983: Merge "debugger.cpp should...
2014-05-17 Elliott Hughesam 2071b983: Merge "debugger.cpp should know the names...
2014-05-17 Elliott HughesMerge "Fix the newly-introduced warning and turn on...
2014-05-17 Elliott HughesMerge "debugger.cpp should know the names of the signal...
2014-05-16 Elliott Hughesdebugger.cpp should know the names of the signals it...
2014-05-16 Elliott HughesMerge "With libstdc++ in libc, __futex_wait and __futex...
2014-05-16 Elliott HughesMerge "Move libstdc++ into libc."
2014-05-16 Christopher FerrisMerge "Fix comment typo."
2014-05-16 Dmitriy IvanovMerge "Register _cleanup function with atexit"
2014-05-15 Elliott HughesMerge "Scrub uapi headers slightly harder."
2014-05-15 Dmitriy Ivanovam b17cc880: am 86bc436e: Merge "Improve detection...
2014-05-15 Dmitriy Ivanovam 86bc436e: Merge "Improve detection of already loaded...
2014-05-15 Dmitriy IvanovMerge "Improve detection of already loaded libraries"
2014-05-14 Elliott HughesMerge "Add tests for fprintf behavior when the underlyi...
2014-05-14 Dmitriy IvanovImprove detection of already loaded libraries
2014-05-14 Dmitriy Ivanovam 283ec625: am 6897b7b8: Merge "Fix for linker allocator"
next