]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/platform-bionic.git/history - tests/stdlib_test.cpp
Fix nan output in the printf family.
[android-sdk/platform-bionic.git] / tests / stdlib_test.cpp
2014-11-12 Yabin CuiMerge "implement missing seekdir and telldir"
2014-11-07 Elliott Hughesam 08a70184: Merge "Add POSIX lcong48."
2014-11-06 Elliott HughesMerge "Add POSIX lcong48."
2014-11-06 Elliott HughesAdd POSIX lcong48.
2014-11-06 Elliott HughesMerge "Fix our <complex.h> support."
2014-11-06 Yabin Cuiam 99cf8d08: Merge "make all bionic death tests not...
2014-11-06 Yabin CuiMerge "make all bionic death tests not dumpable"
2014-11-06 Yabin Cuimake all bionic death tests not dumpable
2014-10-30 Elliott HughesMerge "limits.h: add define for HOST_NAME_MAX"
2014-10-29 Elliott Hughesam d50495a5: Merge "Extra strtod/strtof tests."
2014-10-29 Elliott HughesMerge "Extra strtod/strtof tests."
2014-10-29 Elliott HughesExtra strtod/strtof tests.
2014-10-10 Christopher Ferrisam c891e240: Add back symbols to fix Greed for Glory...
2014-10-09 Christopher Ferrisresolved conflicts for merge of c9734d24 to lmp-dev...
2014-10-07 Elliott Hughesam 1543fdf6: Work around a bug in Immersion\'s libImmEm...
2014-10-07 Christopher Ferrisam 2cf15571: am 40bc7cd4: (-s ours) DO NOT MERGE Re...
2014-10-07 Christopher Ferrisam 40bc7cd4: (-s ours) DO NOT MERGE Re-add .save direc...
2014-10-06 Christopher Ferrisresolved conflicts for merge of d11eac34 to lmp-dev...
2014-10-04 Elliott Hughesresolved conflicts for merge of a5087148 to lmp-dev...
2014-10-03 Elliott Hughesam ea9800e9: Explain why clock(3) isn\'t broken.
2014-10-02 Dmitriy IvanovMerge "Add RTLD_NODELETE flag support"
2014-10-01 Christopher FerrisMerge "Add stpcpy assembler version."
2014-10-01 Dan AlbertMerge "Add coverage flag for libm."
2014-10-01 Elliott Hughesam 252c1ac9: Merge "Update our FreeBSD realpath(3)...
2014-09-30 Elliott HughesMerge "Update our FreeBSD realpath(3) to upstream head."
2014-09-30 Elliott HughesUpdate our FreeBSD realpath(3) to upstream head.
2014-09-25 Elliott Hughesam aaad5485: Merge "Re-expose more stdio implementation...
2014-09-24 Christopher Ferrisam 6c69afdb: Fix sys_stat.mkfifo when not run as root.
2014-09-24 Dan AlbertMerge "Coverage configs for bionic."
2014-09-24 Dan AlbertMerge "Add a dummy atexit(3) to the linker."
2014-09-24 Dan Albertam 086bb382: Fix incorrect parameter types for locale...
2014-09-24 Dan AlbertMerge "Fix incorrect parameter types for locale funcs."
2014-09-24 Christopher FerrisMerge "Remove the unnecessary generic-neon code."
2014-09-24 Elliott Hughesam c57e5c82: Merge "CLOEXEC support in fdopen, freopen...
2014-09-24 Elliott HughesMerge "CLOEXEC support in fdopen, freopen, and mkostemp...
2014-09-24 Elliott HughesCLOEXEC support in fdopen, freopen, and mkostemp/mkostemps.
2014-09-23 Elliott Hughesam 87b6906f: Merge "Pull in upstream fixes to reject...
2014-09-23 Elliott HughesMerge "Pull in upstream fixes to reject invalid bases."
2014-09-23 Elliott HughesPull in upstream fixes to reject invalid bases.
2014-08-26 Elliott HughesMerge "Switch to OpenBSD res_random."
2014-07-29 Elliott HughesMerge "[MIPSR6] Use C-coded string ops on mips32r6...
2014-07-29 Elliott HughesMerge "Revert "Added a bionic systrace class and tracin...
2014-07-29 Elliott Hughesam a7dc7600: Merge "Fix linkage of grantpt(3)."
2014-07-29 Elliott HughesFix linkage of grantpt(3).
2014-07-28 Elliott HughesMerge "Fix linkage of grantpt(3)."
2014-07-26 Elliott HughesFix linkage of grantpt(3).
2014-07-16 Hans BoehmMerge "Define atomic_charN_t only if charN_t is supported."
2014-07-14 Elliott Hughesam caaf71eb: Sync upstream-openbsd.
2014-07-14 Dmitriy Ivanovresolved conflicts for merge of 38778e3b to lmp-dev...
2014-07-14 Elliott HughesImplement rand/srand in terms of random/srandom.
2014-07-14 Elliott Hughesam 673bff01: Merge "Implement rand/srand in terms of...
2014-07-14 Elliott HughesMerge "Implement rand/srand in terms of random/srandom."
2014-07-14 Elliott HughesImplement rand/srand in terms of random/srandom.
2014-06-26 Colin CrossMerge "Revert "HACK: linker: check for handle==0xffffff...
2014-06-17 Christopher FerrisMerge "add 64-bit bionic implementation for denver...
2014-06-17 Elliott HughesMerge "Add a flag control that PRIVATE libm can be...
2014-06-16 Elliott Hughesam fe6e646c: Update NOTICE files.
2014-06-12 Elliott Hughesam d13ff0f0: am 346fa721: Merge "Get the full set of...
2014-06-12 Elliott Hughesam 346fa721: Merge "Get the full set of PRNG functions...
2014-06-12 Christopher FerrisMerge "Fix %u format that should have been %zu."
2014-06-12 Christopher FerrisMerge "Put all allocation functions into dispatch table."
2014-06-12 Elliott HughesMerge "Use default hidden visibility to build libc_dns."
2014-06-12 Elliott HughesMerge "Get the full set of PRNG functions in <stdlib.h>"
2014-06-12 Elliott HughesGet the full set of PRNG functions in <stdlib.h>
2014-05-14 The Android Automergermerge in master-release history after reset to 7fbc7481...
2014-05-14 Calin JuravleMerge "Change wctype_t from int to long."
2014-05-14 Calin JuravleMerge "Change wctype_t from enum to int"
2014-05-14 Dmitriy IvanovMerge "Remove page level mprotects"
2014-05-13 Elliott Hughesam 7aba9ef3: am 492e8f72: am 4482091b: Merge "Consisten...
2014-05-13 Elliott Hughesam 492e8f72: am 4482091b: Merge "Consistently use ...
2014-05-13 Elliott Hughesam 4482091b: Merge "Consistently use #if defined(__BION...
2014-05-13 Elliott HughesMerge "Upgrade to tzdata2014c."
2014-05-13 Elliott HughesMerge "Consistently use #if defined(__BIONIC__) in...
2014-05-13 Elliott HughesConsistently use #if defined(__BIONIC__) in tests.
2014-05-06 Torne (Richard Coles)Merge "Handle empty relro segment or incorrectly sized...
2014-05-01 The Android Automergermerge in master-release history after reset to fc4d9263...
2014-04-30 Dan Albertam 9f2d5003: am a51f7153: am 45667317: Merge "Adds...
2014-04-30 Calin JuravleMerge "Fix cpu_set_t"
2014-04-30 Dan Albertam a51f7153: am 45667317: Merge "Adds quick_exit(3...
2014-04-30 Dan Albertam 45667317: Merge "Adds quick_exit(3) and at_quick_exi...
2014-04-30 Dan AlbertMerge "Adds quick_exit(3) and at_quick_exit(3) from...
2014-04-30 Dan AlbertAdds quick_exit(3) and at_quick_exit(3) from freebsd
2014-04-29 Bill YiMerge klp-dev-plus-aosp into stage-aosp-master
2014-04-09 The Android Automergermerge in master-release history after reset to master
2014-04-09 Calin JuravleMerge "Use glibc structure for __cmsg_nxthdr."
2014-04-09 Elliott HughesMerge "Flesh out <locale.h>."
2014-04-09 Elliott Hughesam 901b2839: am 7f38a3c9: Merge "Implement _Exit(3)."
2014-04-09 Elliott Hughesam 7f38a3c9: Merge "Implement _Exit(3)."
2014-04-09 Elliott HughesMerge "Implement _Exit(3)."
2014-04-09 Elliott HughesImplement _Exit(3).
2014-03-21 Chad Brubakerresolved conflicts for merge of 081db840 to klp-dev...
2014-03-21 Chad Brubakeram 1d3d0360: am 081db840: Allow overlap in resolv uid...
2014-03-21 Chad Brubakeram 081db840: Allow overlap in resolv uid => DNS iface...
2014-03-18 The Android Automergermerge in master-release history after reset to master
2014-03-18 Christopher Ferrisam 6bde44a6: am 849e162d: Merge "Use the float/double...
2014-03-17 Christopher Ferrisam 849e162d: Merge "Use the float/double assert macros."
2014-03-17 Christopher Ferrisam 849e162d: Merge "Use the float/double assert macros."
2014-03-17 Christopher FerrisMerge "Use the float/double assert macros."
2014-03-17 Christopher FerrisUse the float/double assert macros.
2014-03-13 Elliott Hughesam 0e79338d: Merge "Ensure we always have symbols for...
next