]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/platform-bionic.git/history - tests/string_test.cpp
Merge "Remove bogus transitive includes."
[android-sdk/platform-bionic.git] / tests / string_test.cpp
2014-11-12 Yabin CuiMerge "implement missing seekdir and telldir"
2014-11-12 Elliott HughesMerge "gethostname.c: change to report ENAMETOOLONG...
2014-11-12 Elliott HughesMerge "bionic tests: migrate gethostname test to unistd...
2014-11-10 Christopher FerrisMerge "Add align/overread tests for strlcpy/strlcat."
2014-11-10 Christopher FerrisAdd align/overread tests for strlcpy/strlcat.
2014-10-10 Christopher Ferrisam c891e240: Add back symbols to fix Greed for Glory...
2014-10-09 Christopher Ferrisresolved conflicts for merge of c9734d24 to lmp-dev...
2014-10-07 Elliott Hughesam 1543fdf6: Work around a bug in Immersion\'s libImmEm...
2014-10-07 Christopher Ferrisam 2cf15571: am 40bc7cd4: (-s ours) DO NOT MERGE Re...
2014-10-07 Christopher Ferrisam 40bc7cd4: (-s ours) DO NOT MERGE Re-add .save direc...
2014-10-06 Christopher Ferrisresolved conflicts for merge of d11eac34 to lmp-dev...
2014-10-04 Elliott Hughesresolved conflicts for merge of a5087148 to lmp-dev...
2014-10-03 Elliott Hughesam ea9800e9: Explain why clock(3) isn\'t broken.
2014-09-25 Elliott Hughesam aaad5485: Merge "Re-expose more stdio implementation...
2014-09-24 Christopher Ferrisam 6c69afdb: Fix sys_stat.mkfifo when not run as root.
2014-09-24 Dan Albertam 086bb382: Fix incorrect parameter types for locale...
2014-09-14 Christopher Ferrisam 027d2717: Pull input.h from v3.16.1 kernel headers.
2014-09-12 Elliott Hughesam 7e00b44e: Expose __swsetup for LP32 binary compatibi...
2014-09-12 Elliott Hughesam 27efc488: Add pthread_gettid_np and re-expose __get_...
2014-09-11 Elliott Hughesam 9e833bf0: Fix mips __fadvise64.S build failure.
2014-09-11 Elliott Hughesam 176c3278: Merge "Add posix_fadvise(3)." into lmp-dev
2014-09-11 Lorenzo Colittiam 33a73bfa: When comparing DNS server configs, also...
2014-09-09 Lorenzo ColittiMerge "When comparing DNS server configs, also compare...
2014-09-08 Elliott Hughesresolved conflicts for merge of 7efad83d to lmp-dev...
2014-09-08 Elliott Hughesresolved conflicts for merge of c8f6b82f to lmp-dev...
2014-09-08 Elliott Hughesam 51c8355d: Add arc4random_addrandom binary compatibility.
2014-09-06 Christopher Ferrisam 47ed03f7: Merge "Add dlmalloc_usable_size for 32...
2014-09-05 Chih-Hung HsiehMerge "Enable clang compilation with libc but not linker."
2014-09-05 Elliott Hughesam 5beddb7d: Fix pthread_attr_getstack__main_thread.
2014-09-05 Dmitriy Ivanovam 001815ed: Merge "Reset enviroment for math_tests"
2014-09-05 Dmitriy IvanovMerge "Reset enviroment for math_tests"
2014-09-05 Dmitriy IvanovReset enviroment for math_tests
2014-09-04 Dmitriy IvanovMerge "Revert "Register __libc_fini as early as possible.""
2014-09-04 Dmitriy IvanovMerge "Load libraries in breadth-first order"
2014-09-03 Elliott Hughesam 1e010d60: Add back a dummy arc4random_stir for compa...
2014-09-03 Dmitriy IvanovMerge "Register __libc_fini as early as possible."
2014-09-03 Dmitriy Ivanovam 8da304b9: Merge "Make string tests check all alignme...
2014-09-03 Dmitriy IvanovMerge "Make string tests check all alignment combinations"
2014-09-03 Elliott Hughesam cb093d1f: Merge "Upgrade bionic to tzdata2014g....
2014-09-03 Hans Boehmam 9ac60bf8: Make stdatomic.h work with gcc4.6 host...
2014-09-03 Andreas Gamperesolved conflicts for merge of 2b10e2f1 to lmp-dev...
2014-09-02 Hans Boehmresolved conflicts for merge of c8cf3513 to lmp-dev...
2014-09-01 Dmitriy Ivanovresolved conflicts for merge of c191a8ad to lmp-dev...
2014-09-01 Dmitriy IvanovMerge "Erase elements in LinkedList::remove_if"
2014-08-31 Elliott Hughesresolved conflicts for merge of b2eb09a9 to lmp-dev...
2014-08-29 Dmitriy IvanovMerge "Replace NULL with nullptr"
2014-08-29 Elliott Hughesam 29f06943: Merge "Add GNU-compatible strerror_r."
2014-08-29 Chih-Hung HsiehMerge "Ignore all __weak_alias in OpenBSD libC."
2014-08-29 Elliott HughesMerge "Add GNU-compatible strerror_r."
2014-08-28 Elliott HughesAdd GNU-compatible strerror_r.
2014-08-28 Elliott Hughesam 67f1f3b1: Have pthread_attr_getstack for the main...
2014-08-28 Elliott Hughesresolved conflicts for merge of a0eeb0b6 to lmp-dev...
2014-08-27 Christopher Ferrisam 598d25bf: Merge "Replace snprintf calls in linker...
2014-08-27 Elliott Hughesam 6cc4e3b6: Merge "call uselocale() before freelocale...
2014-08-27 Christopher Ferrisam 3f7635f4: Use the default unwind code.
2014-08-26 Elliott HughesMerge "Switch to OpenBSD res_random."
2014-08-22 Elliott Hughesam 84d0683a: Fix unistd.getpid_caching_and_clone.
2014-08-21 Elliott Hughesam 2d80400a: Fix some 32-bit-isms in <stdio.h>.
2014-08-19 Hans BoehmMerge "Work around atomic_load(const T*) issues."
2014-08-19 Elliott Hughesam b9d674c8: Merge "Implement the GNU basename(3) in...
2014-08-19 Elliott HughesMerge "Implement the GNU basename(3) in addition to...
2014-08-19 Elliott HughesImplement the GNU basename(3) in addition to the POSIX...
2014-08-14 Dmitriy IvanovMake string tests check all alignment combinations
2014-08-06 Elliott HughesMerge "Explain how wcswcs ended up in ndk_cruft.cpp."
2014-07-30 Christopher Ferrisam 0f7ed163: Merge "Fix memchr with a zero length."
2014-07-30 Christopher FerrisFix memchr with a zero length.
2014-07-30 Christopher FerrisMerge "Fix memchr with a zero length."
2014-07-30 Christopher FerrisFix memchr with a zero length.
2014-07-02 Dan AlbertMerge "Revert "Revert "Hide _tolower_tab_ and _toupper_...
2014-07-01 Dan AlbertMerge "Revert "Revert "Prevent symbols from libgcc...
2014-06-30 Christopher FerrisMerge "Add optimized stpcpy."
2014-06-30 Nick KralevichMerge "add CLOEXEC to various DNS related code"
2014-06-30 Christopher Ferrisam 6464c7e4: am eac2bbf0: Merge "Add extra strchr testing."
2014-06-30 Christopher Ferrisam eac2bbf0: Merge "Add extra strchr testing."
2014-06-30 Christopher FerrisMerge "Add extra strchr testing."
2014-06-30 Christopher FerrisAdd extra strchr testing.
2014-06-26 Colin CrossMerge "Revert "HACK: linker: check for handle==0xffffff...
2014-06-17 Christopher FerrisMerge "add 64-bit bionic implementation for denver...
2014-06-17 Elliott HughesMerge "Add a flag control that PRIVATE libm can be...
2014-06-17 Elliott HughesMerge "Add <linux/tty.h> to libc/include/sys/ioctl.h"
2014-06-16 Elliott Hughesam fe6e646c: Update NOTICE files.
2014-06-14 Dan Albertam 38ebfc09: am 72dc1c22: Merge "Revert "Backing this...
2014-06-14 Dan Albertam 54c61d57: am b84783ec: Merge "Backing this one out...
2014-06-14 Dan Albertam 72dc1c22: Merge "Revert "Backing this one out since...
2014-06-14 Dan Albertam 263fe685: am 65b1c90a: Merge "Hides valloc(3)/pvallo...
2014-06-14 Dan Albertam b84783ec: Merge "Backing this one out since the...
2014-06-14 Dan Albertam 65b1c90a: Merge "Hides valloc(3)/pvalloc(3) on LP64."
2014-06-13 Elliott Hughesam cc24144e: am 5d25d548: Merge "Remove __memcmp16...
2014-06-13 Elliott Hughesam 5d25d548: Merge "Remove __memcmp16 from bionic."
2014-06-12 Christopher FerrisMerge "Fix %u format that should have been %zu."
2014-06-12 Dan AlbertMerge "Revert "Backing this one out since the counterpa...
2014-06-14 Dan AlbertRevert "Backing this one out since the counterpart...
2014-06-14 Dan AlbertBacking this one out since the counterpart needs to...
2014-06-13 Dan AlbertHides valloc(3)/pvalloc(3) on LP64.
2014-06-12 Dan AlbertMerge "Backing this one out since the counterpart needs...
2014-06-12 Elliott HughesMerge "Remove __memcmp16 from bionic."
2014-06-12 Elliott HughesRemove __memcmp16 from bionic.
2014-06-12 Dan AlbertMerge "Hides valloc(3)/pvalloc(3) on LP64."
2014-06-12 Dan AlbertMerge "Remove ioprio_get(2) and ioprio_set(2) from...
2014-06-12 Elliott HughesMerge "Add a hack to <stdlib.h> until we can fix libvpx."
next