]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/platform-bionic.git/history - tests/time_test.cpp
Sync <net/if_types.h> with upstream.
[android-sdk/platform-bionic.git] / tests / time_test.cpp
2014-12-09 Yabin CuiMerge "support _POSIX_REALTIME_SIGNALS"
2014-12-02 Dmitriy IvanovMerge "Count references for groups instead of instances"
2014-12-02 Dmitriy IvanovMerge "Resolve "unused DT entry" warnings for DT_VERNEE...
2014-12-02 Christopher FerrisMerge "Specify .cpu cortex-a15"
2014-12-01 Yabin CuiMerge "support _POSIX_CPUTIME"
2014-11-27 Yabin Cuisupport _POSIX_CPUTIME
2014-11-19 Yabin CuiMerge "fix shared gid support in getpwnam/getgrnam"
2014-11-17 Elliott HughesMerge "libc: Fix mktime returns an uncorrect time in...
2014-11-15 Satoru Takeuchilibc: Fix mktime returns an uncorrect time in empty...
2014-10-24 Christopher Ferrisam efd2ec8f: Merge "Fix race condition in timer disarm...
2014-10-22 Elliott HughesMerge "Update bionic to tzdata2014i."
2014-10-22 Christopher FerrisMerge "Fix race condition in timer disarm/delete."
2014-10-22 Christopher FerrisFix race condition in timer disarm/delete.
2014-10-15 Dan AlbertMerge "We don't actually need all of libc++ here."
2014-10-14 Elliott Hughesam 97df16ba: Merge "Add clock_settime and clock_nanosleep."
2014-10-14 Elliott HughesMerge "Add clock_settime and clock_nanosleep."
2014-10-14 Haruki HasegawaAdd clock_settime and clock_nanosleep.
2014-10-10 Christopher Ferrisam c891e240: Add back symbols to fix Greed for Glory...
2014-10-09 Christopher Ferrisresolved conflicts for merge of c9734d24 to lmp-dev...
2014-10-07 Elliott Hughesam 1543fdf6: Work around a bug in Immersion\'s libImmEm...
2014-10-07 Christopher Ferrisam 2cf15571: am 40bc7cd4: (-s ours) DO NOT MERGE Re...
2014-10-07 Christopher Ferrisam 40bc7cd4: (-s ours) DO NOT MERGE Re-add .save direc...
2014-10-06 Christopher Ferrisresolved conflicts for merge of d11eac34 to lmp-dev...
2014-10-06 Dan AlbertMerge "Add compile time test infrastructure for bionic."
2014-10-06 Dmitriy IvanovMerge "Add file_offset parameter to android_extinfo"
2014-10-04 Elliott Hughesresolved conflicts for merge of a5087148 to lmp-dev...
2014-10-04 Elliott Hughesam 4ef0e59f: Merge "Reimplement clock(3) using clock_ge...
2014-10-04 Elliott HughesMerge "Reimplement clock(3) using clock_gettime(3)"
2014-10-04 Alex Van BruntReimplement clock(3) using clock_gettime(3)
2014-10-03 Elliott Hughesam ea9800e9: Explain why clock(3) isn\'t broken.
2014-09-25 Elliott Hughesam aaad5485: Merge "Re-expose more stdio implementation...
2014-09-24 Christopher Ferrisam 6c69afdb: Fix sys_stat.mkfifo when not run as root.
2014-09-24 Dan AlbertMerge "Coverage configs for bionic."
2014-09-24 Dan AlbertMerge "Add a dummy atexit(3) to the linker."
2014-09-24 Dan Albertam 086bb382: Fix incorrect parameter types for locale...
2014-09-22 Elliott HughesMerge "Unit test for abort(3)."
2014-09-20 Elliott Hughesam 413de5b0: Merge "Add semaphore tests, fix sem_destroy."
2014-09-20 Elliott HughesMerge "Add semaphore tests, fix sem_destroy."
2014-09-20 Elliott HughesAdd semaphore tests, fix sem_destroy.
2014-09-14 Christopher Ferrisam 027d2717: Pull input.h from v3.16.1 kernel headers.
2014-09-12 Elliott Hughesam 7e00b44e: Expose __swsetup for LP32 binary compatibi...
2014-09-12 Elliott Hughesam 27efc488: Add pthread_gettid_np and re-expose __get_...
2014-09-11 Elliott Hughesam 9e833bf0: Fix mips __fadvise64.S build failure.
2014-09-11 Elliott Hughesam 176c3278: Merge "Add posix_fadvise(3)." into lmp-dev
2014-09-11 Lorenzo Colittiam 33a73bfa: When comparing DNS server configs, also...
2014-09-09 Lorenzo ColittiMerge "When comparing DNS server configs, also compare...
2014-09-08 Elliott Hughesresolved conflicts for merge of 7efad83d to lmp-dev...
2014-09-08 Elliott Hughesresolved conflicts for merge of c8f6b82f to lmp-dev...
2014-09-08 Elliott Hughesam 51c8355d: Add arc4random_addrandom binary compatibility.
2014-09-06 Christopher Ferrisam 47ed03f7: Merge "Add dlmalloc_usable_size for 32...
2014-09-05 Elliott Hughesam 5beddb7d: Fix pthread_attr_getstack__main_thread.
2014-09-03 Elliott Hughesam 1e010d60: Add back a dummy arc4random_stir for compa...
2014-09-03 Dmitriy IvanovMerge "Make string tests check all alignment combinations"
2014-09-03 Elliott Hughesam cb093d1f: Merge "Upgrade bionic to tzdata2014g....
2014-09-03 Hans Boehmam 9ac60bf8: Make stdatomic.h work with gcc4.6 host...
2014-09-03 Andreas Gamperesolved conflicts for merge of 2b10e2f1 to lmp-dev...
2014-09-02 Hans Boehmresolved conflicts for merge of c8cf3513 to lmp-dev...
2014-09-01 Dmitriy Ivanovresolved conflicts for merge of c191a8ad to lmp-dev...
2014-08-31 Elliott Hughesresolved conflicts for merge of b2eb09a9 to lmp-dev...
2014-08-28 Elliott Hughesam 67f1f3b1: Have pthread_attr_getstack for the main...
2014-08-28 Elliott Hughesresolved conflicts for merge of a0eeb0b6 to lmp-dev...
2014-08-27 Christopher Ferrisam 598d25bf: Merge "Replace snprintf calls in linker...
2014-08-27 Elliott Hughesam 6cc4e3b6: Merge "call uselocale() before freelocale...
2014-08-27 Christopher Ferrisam 3f7635f4: Use the default unwind code.
2014-08-26 Elliott HughesMerge "Switch to OpenBSD res_random."
2014-08-22 Elliott Hughesam 84d0683a: Fix unistd.getpid_caching_and_clone.
2014-08-21 Elliott Hughesam 2d80400a: Fix some 32-bit-isms in <stdio.h>.
2014-08-19 Dan Albertam 1506fc17: Expose android_set_abort_message().
2014-08-19 Elliott Hughesam 6f4220c4: Merge "Move the meat of <features.h> into...
2014-08-19 Elliott HughesMerge "Move the meat of <features.h> into <sys/cdefs...
2014-08-19 Elliott HughesMove the meat of <features.h> into <sys/cdefs.h>.
2014-07-29 Elliott HughesMerge "[MIPSR6] Use C-coded string ops on mips32r6...
2014-07-25 Elliott HughesStart hiding "private/bionic_time.h".
2014-07-25 Elliott Hughesam 50a9630c: Merge "Start hiding "private/bionic_time...
2014-07-24 Elliott HughesMerge "Start hiding "private/bionic_time.h"."
2014-07-25 Elliott HughesStart hiding "private/bionic_time.h".
2014-07-16 Hans BoehmMerge "Define atomic_charN_t only if charN_t is supported."
2014-07-16 Elliott HughesUse VDSO for clock_gettime(2) and gettimeofday(2).
2014-07-16 Elliott Hughesam f13aa6fc: Merge "Use VDSO for clock_gettime(2) and...
2014-07-16 Elliott HughesMerge "Use VDSO for clock_gettime(2) and gettimeofday...
2014-07-16 Elliott HughesUse VDSO for clock_gettime(2) and gettimeofday(2).
2014-06-17 Elliott HughesMerge "Add a flag control that PRIVATE libm can be...
2014-05-20 Dan Albertam 9e69a2e8: am 898f8053: am 05b37cfc: Merge "Revert...
2014-05-20 Dan Albertam a484e2d4: am 1f71e131: am 036bf65a: Merge "Removes...
2014-05-20 Dan Albertam 898f8053: am 05b37cfc: Merge "Revert "Removes bionic...
2014-05-19 Dan Albertam 05b37cfc: Merge "Revert "Removes bionic\'s dependenc...
2014-05-19 Dan AlbertMerge "Revert "Removes bionic's dependence on stlport""
2014-05-19 Dan AlbertRevert "Removes bionic's dependence on stlport"
2014-05-19 Dan Albertam 1f71e131: am 036bf65a: Merge "Removes bionic\'s...
2014-05-19 Dan Albertam 036bf65a: Merge "Removes bionic\'s dependence on...
2014-05-19 Dan AlbertMerge "Removes bionic's dependence on stlport"
2014-05-19 Dan AlbertRemoves bionic's dependence on stlport
2014-04-29 Bill YiMerge klp-dev-plus-aosp into stage-aosp-master
2014-04-27 The Android Automergermerge in master-release history after reset to 95dfea20...
2014-04-27 Elliott Hughesam 50769026: am 3ac3f3fd: Merge "Don\'t use so much...
2014-04-27 Elliott Hughesam 3ac3f3fd: Merge "Don\'t use so much stack in tzcode."
2014-04-26 Elliott HughesMerge "Don't use so much stack in tzcode."
2014-04-26 Elliott HughesDon't use so much stack in tzcode.
2014-04-09 Calin JuravleMerge "Use glibc structure for __cmsg_nxthdr."
2014-04-08 The Android Automergermerge in master-release history after reset to master
next