libc: Add AF_RPMSG and PF_RPMSG
[android-sdk/platform-bionic.git] / tests /
2014-10-07 Christopher Ferrisam 40bc7cd4: (-s ours) DO NOT MERGE Re-add .save direc...
2014-09-25 The Android Automergermerge in lmp-release history after reset to aaad548535c...
2014-09-25 Elliott HughesMerge "Re-expose more stdio implementation details...
2014-09-24 Christopher FerrisFix sys_stat.mkfifo when not run as root.
2014-09-14 The Android Automergermerge in lmp-release history after reset to 7e00b44e80d...
2014-09-13 The Android Automergermerge in lmp-release history after reset to 1d12f186edc...
2014-09-13 The Android Automergermerge in lmp-release history after reset to 7e00b44e80d...
2014-09-11 Elliott HughesMerge "Add posix_fadvise(3)." into lmp-dev
2014-09-11 Elliott HughesAdd posix_fadvise(3).
2014-09-09 The Android Automergermerge in lmp-release history after reset to 7efad83d430...
2014-09-08 Elliott HughesMerge "Don't expose non-standard basename_r and dirname...
2014-09-07 The Android Automergermerge in lmp-release history after reset to 47ed03f70c6...
2014-09-06 Christopher FerrisMerge "Add dlmalloc_usable_size for 32 bit arches....
2014-09-06 The Android Automergermerge in lmp-release history after reset to dc3814bcf91...
2014-09-06 The Android Automergermerge in lmp-release history after reset to 5beddb7d642...
2014-09-05 Elliott HughesDon't expose non-standard basename_r and dirname_r...
2014-09-05 Elliott HughesFix pthread_attr_getstack__main_thread.
2014-09-03 The Android Automergermerge in lmp-release history after reset to cb093d1f557...
2014-09-02 Elliott HughesMerge "Upgrade bionic to tzdata2014g." into lmp-dev
2014-09-02 Hans BoehmMake stdatomic.h work with gcc4.6 host compiler
2014-09-02 Hans BoehmFix, generalize stdatomic.h; improve test.
2014-08-31 The Android Automergermerge in lmp-release history after reset to b2eb09a9ed9...
2014-08-27 Elliott HughesHave pthread_attr_getstack for the main thread report...
2014-08-27 Elliott HughesMerge "Fix pthread_getattr_np for the main thread....
2014-08-27 Christopher FerrisMerge "Replace snprintf calls in linker." into lmp-dev
2014-08-27 Elliott HughesMerge "call uselocale() before freelocale() to make...
2014-08-27 Wally Yaucall uselocale() before freelocale() to make sure that...
2014-08-26 Elliott HughesFix pthread_getattr_np for the main thread.
2014-08-23 The Android Automergermerge in lmp-release history after reset to 84d0683a824...
2014-08-22 Elliott HughesFix unistd.getpid_caching_and_clone.
2014-08-20 The Android Automergermerge in lmp-release history after reset to 1506fc178e9...
2014-08-18 Dmitriy IvanovMerge "Revert "Add support for protected local symbol...
2014-08-18 Dmitriy IvanovRevert "Add support for protected local symbol lookup."
2014-08-07 The Android Automergermerge in lmp-release history after reset to 3e7b8e2a8bd...
2014-08-06 Christopher FerrisMerge "Do a second key cleanup in pthread_exit." into...
2014-08-07 Christopher FerrisDo a second key cleanup in pthread_exit.
2014-08-06 Elliott HughesMerge "Fix the tzdata update tools." into lmp-dev
2014-08-06 Dan AlbertMerge "Proper MB_CUR_MAX." into lmp-dev
2014-08-06 Dan AlbertProper MB_CUR_MAX.
2014-08-06 Dan AlbertMerge "Fix mbsrtowcs(3) src param for finished string...
2014-08-06 Dan AlbertFix mbsrtowcs(3) src param for finished string.
2014-08-06 Elliott HughesMerge "Workaround b/16818336 which fails build under...
2014-08-06 The Android Automergermerge in lmp-release history after reset to db7a17d4ff5...
2014-08-05 The Android Automergermerge in lmp-release history after reset to 1b1966d9448...
2014-08-04 Dmitriy IvanovRevert "Revert "Fix dlsym(3) to do breadth first search.""
2014-08-04 Dmitriy IvanovRevert "Fix dlsym(3) to do breadth first search."
2014-08-02 The Android Automergermerge in lmp-release history after reset to 61833de6139...
2014-07-30 Christopher FerrisFix memchr with a zero length.
2014-07-30 Elliott HughesOnly wipe TLS for user-supplied stacks.
2014-07-29 Elliott HughesMerge "Revert "Added a bionic systrace class and tracin...
2014-07-29 Dan AlbertMerge "en_US.UTF-8 is also supported." into lmp-dev
2014-07-29 Dan AlbertFix mbsrtowcs(3)'s handling of len parameter.
2014-07-29 Elliott HughesFix linkage of grantpt(3).
2014-07-29 The Android Automergermerge in lmp-release history after reset to 1a5db57d5a0...
2014-07-28 Elliott Hughessyscall(3)'s return type should be long.
2014-07-28 Elliott HughesUse vsnprintf(3) in syslog(3).
2014-07-26 The Android Automergermerge in lmp-release history after reset to c1a6a725602...
2014-07-25 Elliott HughesStart hiding "private/bionic_time.h".
2014-07-25 Dan AlbertMerge "There is no _MIN for unsigned types." into lmp-dev
2014-07-28 Dan AlbertMerge "Fix mbsrtowcs(3)'s handling of len parameter...
2014-07-25 Dan AlbertMerge "__libc_fatal should print a newline to stderr...
2014-07-29 Dmitriy IvanovFix dlsym(3) to do breadth first search.
2014-07-24 Raghu Gandham[MIPS] Fix atomic_is_lock_free test for mips32.
2014-07-24 Elliott HughesImplement twalk(3), add unit tests.
2014-07-24 The Android Automergermerge in lmp-release history after reset to c86950cb3f5...
2014-07-23 Nick Kralevichdebuggerd: if PR_GET_DUMPABLE=0, don't ask for dumping
2014-07-22 Elliott HughesRewrite syslog(3) to use Android logging.
2014-07-16 Elliott HughesUse VDSO for clock_gettime(2) and gettimeofday(2).
2014-07-14 Elliott HughesImplement rand/srand in terms of random/srandom.
2014-07-12 Christopher Ferrisam 55230dd0: am 96502e27: Merge "Make jemalloc the...
2014-07-12 Dmitriy Ivanovam ab164750: am 3c12ae56: Merge "Add test for construct...
2014-07-12 Christopher Ferrisam 96502e27: Merge "Make jemalloc the default choice."
2014-07-12 Ying Wangam 6cdd0cfd: Merge "TARGET_OUT_DATA_NATIVE_TESTS now...
2014-07-12 Dmitriy Ivanovam 3c12ae56: Merge "Add test for constructor function."
2014-07-11 Dmitriy Ivanovam ca673e73: am b9c5d606: am 006e0770: Merge "Change...
2014-07-11 Elliott Hughesam 7e43f0d4: resolved conflicts for merge of aedc14b1...
2014-07-10 Elliott HughesMerge "EM_ARM and EM_AARCH64 are now in the uapi header."
2014-07-10 Christopher FerrisMerge "Add optimized memchr implementation from newlib"
2014-07-10 Christopher FerrisMerge "Make jemalloc the default choice."
2014-07-11 Christopher FerrisMake jemalloc the default choice.
2014-07-09 Ying Wangam 02406f68: am 6cdd0cfd: Merge "TARGET_OUT_DATA_NATIVE...
2014-07-09 Ying Wangam 6cdd0cfd: Merge "TARGET_OUT_DATA_NATIVE_TESTS now...
2014-07-09 Dmitriy Ivanovam b9247ada: am 3c12ae56: Merge "Add test for construct...
2014-07-09 Ying WangMerge "TARGET_OUT_DATA_NATIVE_TESTS now points to ...
2014-07-09 Elliott HughesMerge "Remove __CTOR_LIST__ from mips/mips64."
2014-07-09 Elliott HughesMerge "Don't zero r1 on entry to the dynamic linker."
2014-07-09 Dmitriy Ivanovam 3c12ae56: Merge "Add test for constructor function."
2014-07-09 Ying WangTARGET_OUT_DATA_NATIVE_TESTS now points to $(TARGET_OUT...
2014-07-08 Dmitriy IvanovMerge "Add test for constructor function."
2014-07-09 Dmitriy IvanovAdd test for constructor function.
2014-07-02 Dmitriy Ivanovam 8551bfb0: am 950a435f: Merge "Load library using...
2014-07-02 Dmitriy Ivanovam f308174a: am 87b654ce: Merge "Disable local/protecte...
2014-07-02 Dmitriy Ivanovam 950a435f: Merge "Load library using file handle."
2014-07-02 Elliott HughesMerge "Fix all resolv warnings and turn on -Werror."
2014-07-02 Dmitriy IvanovMerge "Load library using file handle."
2014-07-02 Elliott HughesMerge "Switch to upstream OpenBSD mktemp.c."
2014-07-02 Dan AlbertMerge "Revert "Revert "Hide _tolower_tab_ and _toupper_...
2014-07-02 Dmitriy IvanovLoad library using file handle.
2014-07-02 Dmitriy Ivanovam 87b654ce: Merge "Disable local/protected symbol...
2014-07-02 Elliott Hughesam 7ec1ba3e: am 4d299a2c: Merge "Build all bionic test...
next