Remove bogus #include <endian.h> from <sys/stat.h>.
Bug: 17062519
Change-Id: I3dc21ee8b90580f112c73c72aff5d3bec4778026
Bug: 17062519
Change-Id: I3dc21ee8b90580f112c73c72aff5d3bec4778026
Merge "Fix struct stat member types for x86-64."
Fix struct stat member types for x86-64.
Bug: 17062519
Change-Id: I93b1e8b1d4b6918ab7c3a985e2f7da277077375e
Bug: 17062519
Change-Id: I93b1e8b1d4b6918ab7c3a985e2f7da277077375e
Merge "Disable ASAN for more of our libraries."
Disable ASAN for more of our libraries.
Since ASAN depends on these libraries, we need to exclude them from
being instrumented.
Change-Id: I62005b6d04ee7b2283c4bd54ace5304386c67358
Since ASAN depends on these libraries, we need to exclude them from
being instrumented.
Change-Id: I62005b6d04ee7b2283c4bd54ace5304386c67358
Merge "Sync with upstream for gethnamaddr.c."
Sync with upstream for gethnamaddr.c.
Bug: 18566967
Change-Id: I37e7410226b49eec67614e20b2c1d5e3e47817a5
Bug: 18566967
Change-Id: I37e7410226b49eec67614e20b2c1d5e3e47817a5
Merge "Add another test for weak-reference"
Add another test for weak-reference
This one covers undefined weak reference in .so
referenced via JUMP_SLOT relocation.
Bug: 17526061
Change-Id: Ib8764bd30c1f686c4818ebbc6683cf42dee908b2
This one covers undefined weak reference in .so
referenced via JUMP_SLOT relocation.
Bug: 17526061
Change-Id: Ib8764bd30c1f686c4818ebbc6683cf42dee908b2
Merge "Fix <net/route.h>."
Fix <net/route.h>.
Previously it couldn't be included alone. Also add a header and include guard,
and fix its siblings' include guards.
Bug: https://code.google.com/p/android/issues/detail?id=82638
Change-Id: I32139a4bda0a6b015508a2319bf4e1a1453345f2
Previously it couldn't be included alone. Also add a header and include guard,
and fix its siblings' include guards.
Bug: https://code.google.com/p/android/issues/detail?id=82638
Change-Id: I32139a4bda0a6b015508a2319bf4e1a1453345f2
Merge "Move the generic arm memcmp.S into the generic directory."
Move the generic arm memcmp.S into the generic directory.
Change-Id: I48e4d14a0dcddbb246edbac6d0329619574ab44d
Change-Id: I48e4d14a0dcddbb246edbac6d0329619574ab44d
Merge "Remove arm assembler not referenced from any makefile."
Remove arm assembler not referenced from any makefile.
I also suspect that libc/arch-arm/bionic/memcmp.S is supposed to like in the
generic directory these days, but this change just removes dead code.
Change-Id: I9072488df6e9b7261d79b6014914a0e937cb387b
I also suspect that libc/arch-arm/bionic/memcmp.S is supposed to like in the
generic directory these days, but this change just removes dead code.
Change-Id: I9072488df6e9b7261d79b6014914a0e937cb387b
Merge "Fix pthread key num calculation."
Merge "[MIPS] Add sgidefs.h for mips64"
[MIPS] Add sgidefs.h for mips64
Sgidefs.h is needed by strace.
Replaced now-duplicate arch-mips64/include directory
by symlink to arch-mips/include.
Change-Id: I7808602cfa452eca3ffbdb94903f4c5bdb33efa3
Sgidefs.h is needed by strace.
Replaced now-duplicate arch-mips64/include directory
by symlink to arch-mips/include.
Change-Id: I7808602cfa452eca3ffbdb94903f4c5bdb33efa3
Merge "make stack_protector_DeathTest work for gcc4.9"
make stack_protector_DeathTest work for gcc4.9
Bug: 18721888
Change-Id: I5f0b5c84319f56dbc4efb88e9d828138944667ae
Bug: 18721888
Change-Id: I5f0b5c84319f56dbc4efb88e9d828138944667ae
Merge "fix runtime issues for scripts"
Merge "Clean up DNS proxying."
Clean up DNS proxying.
Remove code duplication and fall back to trying directly if the proxy
isn't available. With this, tests still work if netd is dead (perhaps
because you've run "adb shell stop", or because you're running on the host).
Bug: 18547878
Change-Id: Ia4a9aa18b1fc79e09735107246989fa7fc6c8455
Remove code duplication and fall back to trying directly if the proxy
isn't available. With this, tests still work if netd is dead (perhaps
because you've run "adb shell stop", or because you're running on the host).
Bug: 18547878
Change-Id: Ia4a9aa18b1fc79e09735107246989fa7fc6c8455
Merge "Fix missing symbol for debug malloc."
Merge "Fix the setjmp tests for mips."
Fix the setjmp tests for mips.
Although the LP32 mips sigset_t is large enough to represent all signals,
their jmp_buf is too small. This test succeeded on arm and x86 because the
RT signals were never in the 'expected' sigset_t, so the equality comparison
with the 'actual' sigset_t worked fine --- everyone was blind to the RT
signal. On mips the tests fail because the 'expected' sigset_t does contain
the RT signal but the 'actual' doesn't because the jmp_buf only saves and
restores the first 32 signals.
There are 32 free bits (currently used as padding) in the LP32 mips jmp_buf,
and they might choose to use those to provide better support than the other
two platforms, but I'll leave that to them. It will be easy to just remove
the #if defined(__LP64__) from this change in that case.
For mips64 it's not to late to increase the size of the jmp_buf and fix
the setjmp family, but since there are decisions to be made here for LP32,
I'll leave it all to Imagination folks...
Bug: 16918359
Change-Id: I6b723712fce0e9210dafa165d8599d950b2d3500
Although the LP32 mips sigset_t is large enough to represent all signals,
their jmp_buf is too small. This test succeeded on arm and x86 because the
RT signals were never in the 'expected' sigset_t, so the equality comparison
with the 'actual' sigset_t worked fine --- everyone was blind to the RT
signal. On mips the tests fail because the 'expected' sigset_t does contain
the RT signal but the 'actual' doesn't because the jmp_buf only saves and
restores the first 32 signals.
There are 32 free bits (currently used as padding) in the LP32 mips jmp_buf,
and they might choose to use those to provide better support than the other
two platforms, but I'll leave that to them. It will be easy to just remove
the #if defined(__LP64__) from this change in that case.
For mips64 it's not to late to increase the size of the jmp_buf and fix
the setjmp family, but since there are decisions to be made here for LP32,
I'll leave it all to Imagination folks...
Bug: 16918359
Change-Id: I6b723712fce0e9210dafa165d8599d950b2d3500
Merge "Fix arm64 clone stack handling."
Merge "Use machine/timespec.h to separate timespec definition."
Fix missing symbol for debug malloc.
Bug: 18686270
Change-Id: I800a6f0940060218413df652d74aca91f6a339f8
Bug: 18686270
Change-Id: I800a6f0940060218413df652d74aca91f6a339f8
Fix arm64 clone stack handling.
Make sure we adjust the stack pointer so a signal can't overwrite data.
Bug: 15195265
Change-Id: I5ab9469a82cb214c32f40a713268a1ab74a4c6fa
Make sure we adjust the stack pointer so a signal can't overwrite data.
Bug: 15195265
Change-Id: I5ab9469a82cb214c32f40a713268a1ab74a4c6fa
Merge "Use the stmdb instead of str to save the fn/arg"
Use the stmdb instead of str to save the fn/arg
Directly save data into stack without properly adjustment
of stack point is dangous. For example, if a signal comes,
kernel will put sigframe into userspace's stack, which
will overwrite the saved data if sp is not adjusted properly.
Bug: 15195265
Change-Id: Iea0cadfd3b94d50cf40252ad52fe5950811b9192
Signed-off-by: Jiangli Yuan <a6808c@motorola.com>
Directly save data into stack without properly adjustment
of stack point is dangous. For example, if a signal comes,
kernel will put sigframe into userspace's stack, which
will overwrite the saved data if sp is not adjusted properly.
Bug: 15195265
Change-Id: Iea0cadfd3b94d50cf40252ad52fe5950811b9192
Signed-off-by: Jiangli Yuan <a6808c@motorola.com>
fix runtime issues for scripts
now, some script to update kernel-headers is not working.
because of wrong variable value and test codes.
so this issue is fixed.
Change-Id: Iffae9607858cc3c1c58fa24244be217b5a1ab06e
now, some script to update kernel-headers is not working.
because of wrong variable value and test codes.
so this issue is fixed.
Change-Id: Iffae9607858cc3c1c58fa24244be217b5a1ab06e
Use machine/timespec.h to separate timespec definition.
Bug: 18627763
Change-Id: Ib1c406320f0ecc3705d19183a48f986cdf57c279
Bug: 18627763
Change-Id: Ib1c406320f0ecc3705d19183a48f986cdf57c279
Merge "Fix ptsname(3) and ttyname(3) to use TLS."
Fix ptsname(3) and ttyname(3) to use TLS.
Be safe by default.
Change-Id: I6c4a3f1fd4eee3a651b3162ce95b7e873de57521
Be safe by default.
Change-Id: I6c4a3f1fd4eee3a651b3162ce95b7e873de57521
Merge "Move BSD stuff together in <sys/endian.h>."
Move BSD stuff together in <sys/endian.h>.
Change-Id: I8bb511840f3cd98d5008034e405d82e923bd3203
Change-Id: I8bb511840f3cd98d5008034e405d82e923bd3203
Merge "<net/route.h> should include IPv6 too."
<net/route.h> should include IPv6 too.
Change-Id: I866097d8468aa8f326117d072444ebbc2a690719
Change-Id: I866097d8468aa8f326117d072444ebbc2a690719
Merge "Sync <net/if_types.h> with upstream."
Sync <net/if_types.h> with upstream.
Change-Id: I2c2ca47f5a21b78754c03deb3e9467ab79d9d033
Change-Id: I2c2ca47f5a21b78754c03deb3e9467ab79d9d033
Merge "support _POSIX_REALTIME_SIGNALS"
Merge "Change _POSIX_CPUTIME macro to make it compitable with glibc."
Change _POSIX_CPUTIME macro to make it compitable with glibc.
Change-Id: I7a8dbb74bd622693c9fef60bd779687207517b7d
Change-Id: I7a8dbb74bd622693c9fef60bd779687207517b7d
Merge "Simplify our endian.h implementation."
Simplify our endian.h implementation.
We can rely on the compiler's builtins. Tested on arm, arm64, mips, x86,
and x86-64.
Change-Id: I0f774ed7e85b3c791a3178d8ef17c6500e6a9ace
We can rely on the compiler's builtins. Tested on arm, arm64, mips, x86,
and x86-64.
Change-Id: I0f774ed7e85b3c791a3178d8ef17c6500e6a9ace
Merge "Merge mips setjmp/longjmp family."
Merge mips setjmp/longjmp family.
Bug: 16918359
Change-Id: I9033a7d178d431ddb09f1cfa6e4bf95ae02346e9
Bug: 16918359
Change-Id: I9033a7d178d431ddb09f1cfa6e4bf95ae02346e9
Merge "Switch arch-mips64/include/machine to a symlink."
Switch arch-mips64/include/machine to a symlink.
Imagination already did the work to make the contents of these directories
identical. Let's take advantage of that fact.
Change-Id: Ib101ba39041fb500c9c618fa2020e72aa2ccd9c2
Imagination already did the work to make the contents of these directories
identical. Let's take advantage of that fact.
Change-Id: Ib101ba39041fb500c9c618fa2020e72aa2ccd9c2
Merge "Use 64-bit units in the aarch64 setjmp implementation."
Use 64-bit units in the aarch64 setjmp implementation.
The use of 32-bit units for 64-bit stores and loads was driving me crazy.
Bug: 16918359
Change-Id: Ifb73aad8f8985a2adfcf5913b783ad9424f23e06
The use of 32-bit units for 64-bit stores and loads was driving me crazy.
Bug: 16918359
Change-Id: Ifb73aad8f8985a2adfcf5913b783ad9424f23e06
Merge "Switch arm and arm64 over to the x86 style of jmpbuf."
Switch arm and arm64 over to the x86 style of jmpbuf.
Specifically, use the argument to sigsetjmp as a flag in the buffer
to indicate whether or not the signal mask is valid.
Bug: 16918359
Change-Id: I5bb1f1220f14c105c6bc57e0c28c1dc366d1438f
Specifically, use the argument to sigsetjmp as a flag in the buffer
to indicate whether or not the signal mask is valid.
Bug: 16918359
Change-Id: I5bb1f1220f14c105c6bc57e0c28c1dc366d1438f
Merge "Fix signal mask save/restore for x86-64."
Fix signal mask save/restore for x86-64.
Bug: 16918359
Change-Id: I30bf61e7d5f1c21daa3a1a21d361e98d77220bf3
Bug: 16918359
Change-Id: I30bf61e7d5f1c21daa3a1a21d361e98d77220bf3
Merge "Fix signal mask save/restore for arm64."
Fix signal mask save/restore for arm64.
Bug: 16918359
Change-Id: Ieb15f7f1658f5accee05665b72ba17831a80ea9d
Bug: 16918359
Change-Id: Ieb15f7f1658f5accee05665b72ba17831a80ea9d
Merge "Clean up the x86-64 and x86 setjmp families."
Clean up the x86-64 and x86 setjmp families.
Bug: 16918359
Change-Id: Ic8ca0af9ea99636bc71f19d46071f1cea6eef982
Bug: 16918359
Change-Id: Ic8ca0af9ea99636bc71f19d46071f1cea6eef982
Merge "Clean up arm setjmp family."
Merge "Clean up the arm64 setjmp."
Clean up the arm64 setjmp.
Note that this doesn't address the fact that we don't save/restore the
real-time signals. But it does let us pass the tests we currently fail.
Bug: 16918359
Change-Id: I063a6926164289a71026a412da7f5dd2ca9a74b3
Note that this doesn't address the fact that we don't save/restore the
real-time signals. But it does let us pass the tests we currently fail.
Bug: 16918359
Change-Id: I063a6926164289a71026a412da7f5dd2ca9a74b3
Merge "Add cache related sysconf queries"
Add cache related sysconf queries
Several cache related queries are added, such as
_SC_LEVEL1_DCACHE_LINESIZE, _SC_LEVEL1_DCACHE_SIZE and etc. For the
moment, we always return 0 for these queries.
Change-Id: I36f67af8128672d8c1eef49d6f2431cca5a94719
Several cache related queries are added, such as
_SC_LEVEL1_DCACHE_LINESIZE, _SC_LEVEL1_DCACHE_SIZE and etc. For the
moment, we always return 0 for these queries.
Change-Id: I36f67af8128672d8c1eef49d6f2431cca5a94719
Merge "Restore symbols from <arpa/nameser.h>."
Merge "implement posix_madvise"
Restore symbols from <arpa/nameser.h>.
Bug: 18627252
Bug: https://code.google.com/p/android/issues/detail?id=81690
Change-Id: I45b6c09cf2b5aabb80900e267d27cc0ec93d4dd8
Bug: 18627252
Bug: https://code.google.com/p/android/issues/detail?id=81690
Change-Id: I45b6c09cf2b5aabb80900e267d27cc0ec93d4dd8
Merge "Make the missing symbols script more useful."
Make the missing symbols script more useful.
If something's in POSIX, we don't need to show it in the glibc list.
If something's not implemented by glibc, we don't need to show it in the
POSIX list (because it's probably either a macro or obsolete).
Change-Id: Ied0f8d97d3fffb280c22e9cdf6782430d776c02f
If something's in POSIX, we don't need to show it in the glibc list.
If something's not implemented by glibc, we don't need to show it in the
POSIX list (because it's probably either a macro or obsolete).
Change-Id: Ied0f8d97d3fffb280c22e9cdf6782430d776c02f
Merge "Code using neon uses ARCH_ARM_HAVE_NEON."
Code using neon uses ARCH_ARM_HAVE_NEON.
Bug: 18556103
Change-Id: Ia8674dda223f81d616d15ee47b402ab4a3f98079
Bug: 18556103
Change-Id: Ia8674dda223f81d616d15ee47b402ab4a3f98079
Merge "Remove __ARM_HAVE_VFP."
Merge "Implement <pty.h>."
Implement <pty.h>.
Based on the package/apps/Terminal implementation. I'll switch them over
shortly. This also lets us build the toybox version of netcat.
Change-Id: Ia922a100141a67409264b43b937eeca07b21f344
Based on the package/apps/Terminal implementation. I'll switch them over
shortly. This also lets us build the toybox version of netcat.
Change-Id: Ia922a100141a67409264b43b937eeca07b21f344
Merge "change argument type in madvise"
change argument type in madvise
Make madvise prototype the same as linux man page.
Bug: 18539500
Change-Id: If3fd0e1d9539b9e10531ab9087bc4040e32b6e9b
Make madvise prototype the same as linux man page.
Bug: 18539500
Change-Id: If3fd0e1d9539b9e10531ab9087bc4040e32b6e9b
Merge "Fix warning: overriding commands for target"
Fix warning: overriding commands for target
Change-Id: I00fb4d6a8ff388722b75de9a0f4316619aaf9320
Change-Id: I00fb4d6a8ff388722b75de9a0f4316619aaf9320
Merge "Switch x86 and x86-64 to __builtin_bswap*."
Merge "Switch aarch64 to __builtin_bswap16."
Switch x86 and x86-64 to __builtin_bswap*.
Bug: 18597513
Change-Id: I0781208efb3b560d7c6fa48f41be7bc6fc83521e
Bug: 18597513
Change-Id: I0781208efb3b560d7c6fa48f41be7bc6fc83521e
Switch aarch64 to __builtin_bswap16.
It generates the same code.
Bug: 18597513
Change-Id: I164296da8c676668983dd93697c6dfa05f10ec56
It generates the same code.
Bug: 18597513
Change-Id: I164296da8c676668983dd93697c6dfa05f10ec56
Merge "Fix soinfo_unload"
Fix soinfo_unload
1. Take into consideration that the local_group_root_
is not set for all of not linked libraries.
2. We need to check visited list earlier to avoid double
soinfo_free.
Change-Id: Iabc0a06a97c63f7e6bd4641731f50bb1466fed4f
1. Take into consideration that the local_group_root_
is not set for all of not linked libraries.
2. We need to check visited list earlier to avoid double
soinfo_free.
Change-Id: Iabc0a06a97c63f7e6bd4641731f50bb1466fed4f
Merge "Remove __ARM_HAVE_HALFWORD_MULTIPLY."
Remove __ARM_HAVE_HALFWORD_MULTIPLY.
Bug: 18556103
Change-Id: I17e498539f77ddf7d1fb980ee93155d3c3ccd85e
Bug: 18556103
Change-Id: I17e498539f77ddf7d1fb980ee93155d3c3ccd85e
Merge "Remove __ARM_HAVE_LDREXD."
Remove __ARM_HAVE_LDREXD.
No one uses this.
Bug: 18556103
Change-Id: Icecc3a7b5cb0a36960f27d030d8f4f8ee471f86c
No one uses this.
Bug: 18556103
Change-Id: Icecc3a7b5cb0a36960f27d030d8f4f8ee471f86c
Merge "Kill <machine/exec.h>."
Merge "Extract bionic-prepare-run-on-host to inc file."
Extract bionic-prepare-run-on-host to inc file.
Make benchmark run-on-host depend on bionic-prepare-run-on-host.
Change-Id: I0bdbf561b2580d607a49b7c83cc273320ac55429
Make benchmark run-on-host depend on bionic-prepare-run-on-host.
Change-Id: I0bdbf561b2580d607a49b7c83cc273320ac55429
Merge "Avoid pathological behavior in OpenBSD's fread."