Switch arm and arm64 over to the x86 style of jmpbuf.
Specifically, use the argument to sigsetjmp as a flag in the buffer
to indicate whether or not the signal mask is valid.
Bug: 16918359
Change-Id: I5bb1f1220f14c105c6bc57e0c28c1dc366d1438f
Specifically, use the argument to sigsetjmp as a flag in the buffer
to indicate whether or not the signal mask is valid.
Bug: 16918359
Change-Id: I5bb1f1220f14c105c6bc57e0c28c1dc366d1438f
Merge "Fix signal mask save/restore for x86-64."
Fix signal mask save/restore for x86-64.
Bug: 16918359
Change-Id: I30bf61e7d5f1c21daa3a1a21d361e98d77220bf3
Bug: 16918359
Change-Id: I30bf61e7d5f1c21daa3a1a21d361e98d77220bf3
Merge "Fix signal mask save/restore for arm64."
Fix signal mask save/restore for arm64.
Bug: 16918359
Change-Id: Ieb15f7f1658f5accee05665b72ba17831a80ea9d
Bug: 16918359
Change-Id: Ieb15f7f1658f5accee05665b72ba17831a80ea9d
Merge "Clean up the x86-64 and x86 setjmp families."
Clean up the x86-64 and x86 setjmp families.
Bug: 16918359
Change-Id: Ic8ca0af9ea99636bc71f19d46071f1cea6eef982
Bug: 16918359
Change-Id: Ic8ca0af9ea99636bc71f19d46071f1cea6eef982
Merge "Clean up arm setjmp family."
Merge "Clean up the arm64 setjmp."
Clean up the arm64 setjmp.
Note that this doesn't address the fact that we don't save/restore the
real-time signals. But it does let us pass the tests we currently fail.
Bug: 16918359
Change-Id: I063a6926164289a71026a412da7f5dd2ca9a74b3
Note that this doesn't address the fact that we don't save/restore the
real-time signals. But it does let us pass the tests we currently fail.
Bug: 16918359
Change-Id: I063a6926164289a71026a412da7f5dd2ca9a74b3
Merge "Add cache related sysconf queries"
Add cache related sysconf queries
Several cache related queries are added, such as
_SC_LEVEL1_DCACHE_LINESIZE, _SC_LEVEL1_DCACHE_SIZE and etc. For the
moment, we always return 0 for these queries.
Change-Id: I36f67af8128672d8c1eef49d6f2431cca5a94719
Several cache related queries are added, such as
_SC_LEVEL1_DCACHE_LINESIZE, _SC_LEVEL1_DCACHE_SIZE and etc. For the
moment, we always return 0 for these queries.
Change-Id: I36f67af8128672d8c1eef49d6f2431cca5a94719
Merge "Restore symbols from <arpa/nameser.h>."
Merge "implement posix_madvise"
Restore symbols from <arpa/nameser.h>.
Bug: 18627252
Bug: https://code.google.com/p/android/issues/detail?id=81690
Change-Id: I45b6c09cf2b5aabb80900e267d27cc0ec93d4dd8
Bug: 18627252
Bug: https://code.google.com/p/android/issues/detail?id=81690
Change-Id: I45b6c09cf2b5aabb80900e267d27cc0ec93d4dd8
Merge "Make the missing symbols script more useful."
Make the missing symbols script more useful.
If something's in POSIX, we don't need to show it in the glibc list.
If something's not implemented by glibc, we don't need to show it in the
POSIX list (because it's probably either a macro or obsolete).
Change-Id: Ied0f8d97d3fffb280c22e9cdf6782430d776c02f
If something's in POSIX, we don't need to show it in the glibc list.
If something's not implemented by glibc, we don't need to show it in the
POSIX list (because it's probably either a macro or obsolete).
Change-Id: Ied0f8d97d3fffb280c22e9cdf6782430d776c02f
Merge "Code using neon uses ARCH_ARM_HAVE_NEON."
Code using neon uses ARCH_ARM_HAVE_NEON.
Bug: 18556103
Change-Id: Ia8674dda223f81d616d15ee47b402ab4a3f98079
Bug: 18556103
Change-Id: Ia8674dda223f81d616d15ee47b402ab4a3f98079
Merge "Remove __ARM_HAVE_VFP."
Merge "Implement <pty.h>."
Implement <pty.h>.
Based on the package/apps/Terminal implementation. I'll switch them over
shortly. This also lets us build the toybox version of netcat.
Change-Id: Ia922a100141a67409264b43b937eeca07b21f344
Based on the package/apps/Terminal implementation. I'll switch them over
shortly. This also lets us build the toybox version of netcat.
Change-Id: Ia922a100141a67409264b43b937eeca07b21f344
Merge "change argument type in madvise"
change argument type in madvise
Make madvise prototype the same as linux man page.
Bug: 18539500
Change-Id: If3fd0e1d9539b9e10531ab9087bc4040e32b6e9b
Make madvise prototype the same as linux man page.
Bug: 18539500
Change-Id: If3fd0e1d9539b9e10531ab9087bc4040e32b6e9b
Merge "Fix warning: overriding commands for target"
Fix warning: overriding commands for target
Change-Id: I00fb4d6a8ff388722b75de9a0f4316619aaf9320
Change-Id: I00fb4d6a8ff388722b75de9a0f4316619aaf9320
Merge "Switch x86 and x86-64 to __builtin_bswap*."
Merge "Switch aarch64 to __builtin_bswap16."
Switch x86 and x86-64 to __builtin_bswap*.
Bug: 18597513
Change-Id: I0781208efb3b560d7c6fa48f41be7bc6fc83521e
Bug: 18597513
Change-Id: I0781208efb3b560d7c6fa48f41be7bc6fc83521e
Switch aarch64 to __builtin_bswap16.
It generates the same code.
Bug: 18597513
Change-Id: I164296da8c676668983dd93697c6dfa05f10ec56
It generates the same code.
Bug: 18597513
Change-Id: I164296da8c676668983dd93697c6dfa05f10ec56
Merge "Fix soinfo_unload"
Fix soinfo_unload
1. Take into consideration that the local_group_root_
is not set for all of not linked libraries.
2. We need to check visited list earlier to avoid double
soinfo_free.
Change-Id: Iabc0a06a97c63f7e6bd4641731f50bb1466fed4f
1. Take into consideration that the local_group_root_
is not set for all of not linked libraries.
2. We need to check visited list earlier to avoid double
soinfo_free.
Change-Id: Iabc0a06a97c63f7e6bd4641731f50bb1466fed4f
Merge "Remove __ARM_HAVE_HALFWORD_MULTIPLY."
Remove __ARM_HAVE_HALFWORD_MULTIPLY.
Bug: 18556103
Change-Id: I17e498539f77ddf7d1fb980ee93155d3c3ccd85e
Bug: 18556103
Change-Id: I17e498539f77ddf7d1fb980ee93155d3c3ccd85e
Merge "Remove __ARM_HAVE_LDREXD."
Remove __ARM_HAVE_LDREXD.
No one uses this.
Bug: 18556103
Change-Id: Icecc3a7b5cb0a36960f27d030d8f4f8ee471f86c
No one uses this.
Bug: 18556103
Change-Id: Icecc3a7b5cb0a36960f27d030d8f4f8ee471f86c
Merge "Kill <machine/exec.h>."
Merge "Extract bionic-prepare-run-on-host to inc file."
Extract bionic-prepare-run-on-host to inc file.
Make benchmark run-on-host depend on bionic-prepare-run-on-host.
Change-Id: I0bdbf561b2580d607a49b7c83cc273320ac55429
Make benchmark run-on-host depend on bionic-prepare-run-on-host.
Change-Id: I0bdbf561b2580d607a49b7c83cc273320ac55429
Merge "Avoid pathological behavior in OpenBSD's fread."
Avoid pathological behavior in OpenBSD's fread.
Bug: https://code.google.com/p/android/issues/detail?id=81155
Bug: 18556607
Change-Id: Idc60976b79610e2202cc42dc393dcb4ca6c42e05
Bug: https://code.google.com/p/android/issues/detail?id=81155
Bug: 18556607
Change-Id: Idc60976b79610e2202cc42dc393dcb4ca6c42e05
Merge "Fix mips build"
Merge "Create /system/lib(64)? symlinks for host tests."
Fix mips build
Change-Id: Iddbf06784d19556a55d833e20a68e6ccf5a7c5be
Change-Id: Iddbf06784d19556a55d833e20a68e6ccf5a7c5be
Create /system/lib(64)? symlinks for host tests.
Replace LD_LIBRARY_PATH with default path for
the tests run on host.
Bug: 18589961
Change-Id: Id4a84b73d25c2ca9c557fcfa19b8169daeaa016b
Replace LD_LIBRARY_PATH with default path for
the tests run on host.
Bug: 18589961
Change-Id: Id4a84b73d25c2ca9c557fcfa19b8169daeaa016b
Merge "Use mmap to create the pthread_internal_t."
Merge "Count references for groups instead of instances"
Count references for groups instead of instances
Count references on the group level to avoid
partially unloading function that might be
referenced by other libraries in the local_group
Bonus: with this change we can correctly unload recursively
linked libraries. is_recursive check is removed.
Also dynamic executables (not .so) with 0 DT_NEEDED libraries
are now correctly linked.
Change-Id: Idfa83baef402840599b93a875f2881d9f020dbcd
Count references on the group level to avoid
partially unloading function that might be
referenced by other libraries in the local_group
Bonus: with this change we can correctly unload recursively
linked libraries. is_recursive check is removed.
Also dynamic executables (not .so) with 0 DT_NEEDED libraries
are now correctly linked.
Change-Id: Idfa83baef402840599b93a875f2881d9f020dbcd
Use mmap to create the pthread_internal_t.
Bug: 16847284
Change-Id: I488fa236f57aa3acb29b4ffbbab2fab51b0653be
Bug: 16847284
Change-Id: I488fa236f57aa3acb29b4ffbbab2fab51b0653be
Merge "restore sigprocmask in setjmp/longjmp test."
restore sigprocmask in setjmp/longjmp test.
Bug: 18571921
Change-Id: Ib8ca7a36abd3ccc729c20c0e32d45b1b33069f65
Bug: 18571921
Change-Id: Ib8ca7a36abd3ccc729c20c0e32d45b1b33069f65
Merge "Resolve "unused DT entry" warnings for DT_VERNEED and DT_VERNEEDNUM."
Resolve "unused DT entry" warnings for DT_VERNEED and DT_VERNEEDNUM.
Change-Id: Id18310811a6d183878a1d4d26cc2498f4fd00c55
Signed-off-by: Alexander Ivchenko <alexander.ivchenko@intel.com>
Change-Id: Id18310811a6d183878a1d4d26cc2498f4fd00c55
Signed-off-by: Alexander Ivchenko <alexander.ivchenko@intel.com>
Merge "Specify .cpu cortex-a15"
Merge "Build our benchmarks against glibc too."
Build our benchmarks against glibc too.
Bug: 18556607
Change-Id: I455ac8b93c0835836180e549486bc52d393ee6a6
Bug: 18556607
Change-Id: I455ac8b93c0835836180e549486bc52d393ee6a6
Merge "Benchmark fread/fwrite both buffered and unbuffered."
Merge "Fix running the bionic benchmarks on the host."
Benchmark fread/fwrite both buffered and unbuffered.
Bug: 18556607
Change-Id: I53905aedcea75fe550d9c423fb701c2c9bf8e831
Bug: 18556607
Change-Id: I53905aedcea75fe550d9c423fb701c2c9bf8e831
Fix running the bionic benchmarks on the host.
Bug: 18556607
Change-Id: I4e75bfcde788b43e1926be1b0146acf09b496390
Bug: 18556607
Change-Id: I4e75bfcde788b43e1926be1b0146acf09b496390
Merge "support _POSIX_CPUTIME"
Merge "libc: Fix headers to allow direct inclusion."
libc: Fix headers to allow direct inclusion.
These headers are missing a few #includes to allow their direct
inclusion from C
http://b.android.com/79841
Change-Id: Ifc712c17f4da70b26adb67d4d49ed659f53c3621
These headers are missing a few #includes to allow their direct
inclusion from C
http://b.android.com/79841
Change-Id: Ifc712c17f4da70b26adb67d4d49ed659f53c3621
Specify .cpu cortex-a15
When building with clang without this change, as errors out saying pldw
is an unsupported instruction (because it isn't part of the ARMv7 core
instruction set).
Let as know using pldw is fine.
Change-Id: Ie1f9c4b873e93ab2b3b374d2d46e476a4e581710
Signed-off-by: Bernhard Rosenkränzer <Bernhard.Rosenkranzer@linaro.org>
When building with clang without this change, as errors out saying pldw
is an unsupported instruction (because it isn't part of the ARMv7 core
instruction set).
Let as know using pldw is fine.
Change-Id: Ie1f9c4b873e93ab2b3b374d2d46e476a4e581710
Signed-off-by: Bernhard Rosenkränzer <Bernhard.Rosenkranzer@linaro.org>
Merge "Add error-check when mapping socket to fd"
Add error-check when mapping socket to fd
The call to fdopen can fail in several ways.
The fprintf on the next line will then dereference a
NULL-pointer FILE*.
Added a NULL-check, closed the socket, returned system error
and added a comment about it.
Change-Id: I7a6b26aa3c79452b1fdd76af12dfa75da88cbad7
The call to fdopen can fail in several ways.
The fprintf on the next line will then dereference a
NULL-pointer FILE*.
Added a NULL-check, closed the socket, returned system error
and added a comment about it.
Change-Id: I7a6b26aa3c79452b1fdd76af12dfa75da88cbad7
Merge "Move a private x86-64 header file out of the limelight."
Move a private x86-64 header file out of the limelight.
Currently this is on everyone's include path and is getting exported
via the NDK.
Change-Id: Ia417839fb65c7e0afddcd9fae3438665dae8e752
Currently this is on everyone's include path and is getting exported
via the NDK.
Change-Id: Ia417839fb65c7e0afddcd9fae3438665dae8e752
Merge "[MIPS] Rewrite of setjmp/longjmp for mips64 and mipsr6"
Merge "bionic tests: add setjmp/_setjmp/sigsetjmp tests."
bionic tests: add setjmp/_setjmp/sigsetjmp tests.
Bug: 17288973
Change-Id: I2808eee58cbddae1b16fbe19a715b72d6dbaaec3
Signed-off-by: Yongqin Liu <yongqin.liu@linaro.org>
Bug: 17288973
Change-Id: I2808eee58cbddae1b16fbe19a715b72d6dbaaec3
Signed-off-by: Yongqin Liu <yongqin.liu@linaro.org>
Merge "Revert "Use mmap to create the pthread_internal_t.""
Revert "Use mmap to create the pthread_internal_t."
Unfortunately, this change provokes random crashes for ART, and
I have seen libc crashes on the device that might be related to it.
Reverting it fixes the ART crashes. there is unfortunately no
stack trace for the crashes, but just a "Segmentation fault" message.
This reverts commit cc5f6543e3f91385b9a912438965b7e8265df54a.
Change-Id: I68dca8e1e9b9edcce7eb84596e8db619e40e8052
Unfortunately, this change provokes random crashes for ART, and
I have seen libc crashes on the device that might be related to it.
Reverting it fixes the ART crashes. there is unfortunately no
stack trace for the crashes, but just a "Segmentation fault" message.
This reverts commit cc5f6543e3f91385b9a912438965b7e8265df54a.
Change-Id: I68dca8e1e9b9edcce7eb84596e8db619e40e8052
[MIPS] Rewrite of setjmp/longjmp for mips64 and mipsr6
Change-Id: Idcd13413520dd503bc9cf782553675313e500a83
Change-Id: Idcd13413520dd503bc9cf782553675313e500a83
Merge "Use mmap to create the pthread_internal_t."
Use mmap to create the pthread_internal_t.
Bug: 16847284
Change-Id: Ic8c85f95afac1d8422ecb69674c688d1fecb6a44
Bug: 16847284
Change-Id: Ic8c85f95afac1d8422ecb69674c688d1fecb6a44
Merge "flesh out sysconf(3) and the _POSIX_* constants"
Merge "Sync with upstream OpenBSD fts.c."
Merge "Move some pthread functions to signal.h."
Sync with upstream OpenBSD fts.c.
Change-Id: Ia7e26b603f6461095b5a8d7e8a6cdf4f8279fa84
Change-Id: Ia7e26b603f6461095b5a8d7e8a6cdf4f8279fa84
flesh out sysconf(3) and the _POSIX_* constants
Bug: 17571891
Change-Id: I81036615486bde65969ae5662587fcc88348474e
Bug: 17571891
Change-Id: I81036615486bde65969ae5662587fcc88348474e
Merge "Bring our <machine/endian.h> files back in sync."
Bring our <machine/endian.h> files back in sync.
They'd drifted slightly which led to a compilation error in toybox,
which was assuming pid_t was defined. arm and arm64 were picking it
up via <endian.h> but x86 wasn't.
Change-Id: I58401e6c0066959dfc3b305b020876aaf7074bbf
They'd drifted slightly which led to a compilation error in toybox,
which was assuming pid_t was defined. arm and arm64 were picking it
up via <endian.h> but x86 wasn't.
Change-Id: I58401e6c0066959dfc3b305b020876aaf7074bbf
Merge "Mips: remove arch-specific atexit.h"
Mips: remove arch-specific atexit.h
Change-Id: I687ff4ead6c5e81db44782bf851cb84f87bfe085
Change-Id: I687ff4ead6c5e81db44782bf851cb84f87bfe085
Merge "Mips: Remove unused files"
Mips: Remove unused files
Change-Id: If98b832ee32f6dcd9f5d7ae21c601c210adfad6b
Change-Id: If98b832ee32f6dcd9f5d7ae21c601c210adfad6b
Merge "Mips: Reuse atexit.h from libc/arch-common"
Mips: Reuse atexit.h from libc/arch-common
Change-Id: Ica1670e6d3d1b6b0c64df93720efa65586e67727
Change-Id: Ica1670e6d3d1b6b0c64df93720efa65586e67727
Merge "Revert "<sched.h> should offer both __sched_priority and sched_priority.""
Move some pthread functions to signal.h.
POSIX specifies that pthread_kill(3) and pthread_sigmask(3) are
supposed to live in signal.h rather than pthread.h.
Since signal.h now needs pthread_t and pthread_attr_t, I've moved
those defintions into include/machine/pthread_types.h to keep the
namespace clean. I also sorted some includes. The combination of these
two things seems to have exploded into a cascade of missing includes,
so this patch also cleans up all those.
Change-Id: Icfa92a39432fe83f542a797e5a113289d7e4ad0c
POSIX specifies that pthread_kill(3) and pthread_sigmask(3) are
supposed to live in signal.h rather than pthread.h.
Since signal.h now needs pthread_t and pthread_attr_t, I've moved
those defintions into include/machine/pthread_types.h to keep the
namespace clean. I also sorted some includes. The combination of these
two things seems to have exploded into a cascade of missing includes,
so this patch also cleans up all those.
Change-Id: Icfa92a39432fe83f542a797e5a113289d7e4ad0c
Revert "<sched.h> should offer both __sched_priority and sched_priority."
This was only ever added to keep strace compiling, but strace has
since (actually, prior) fixed their source to use the less ugly name,
so we don't need this anymore (good riddance, #define!).
This reverts commit bbb34f9536db8234b0b43bd5333256fa4accc50e.
This was only ever added to keep strace compiling, but strace has
since (actually, prior) fixed their source to use the less ugly name,
so we don't need this anymore (good riddance, #define!).
This reverts commit bbb34f9536db8234b0b43bd5333256fa4accc50e.
Merge "Rename test_forked -> test_isolated"
Rename test_forked -> test_isolated
Change-Id: Ie72627e986c159832cbd3635d8ff5b1af3d5b1eb
Change-Id: Ie72627e986c159832cbd3635d8ff5b1af3d5b1eb
Merge "Add test_forked() option"