/* asoundlib.h ** ** Copyright 2011, The Android Open Source Project ** ** Redistribution and use in source and binary forms, with or without ** modification, are permitted provided that the following conditions are met: ** * Redistributions of source code must retain the above copyright ** notice, this list of conditions and the following disclaimer. ** * Redistributions in binary form must reproduce the above copyright ** notice, this list of conditions and the following disclaimer in the ** documentation and/or other materials provided with the distribution. ** * Neither the name of The Android Open Source Project nor the names of ** its contributors may be used to endorse or promote products derived ** from this software without specific prior written permission. ** ** THIS SOFTWARE IS PROVIDED BY The Android Open Source Project ``AS IS'' AND ** ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE ** IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ** ARE DISCLAIMED. IN NO EVENT SHALL The Android Open Source Project BE LIABLE ** FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL ** DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR ** SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER ** CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT ** LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY ** OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH ** DAMAGE. */ #ifndef ASOUNDLIB_H #define ASOUNDLIB_H #include #if defined(__cplusplus) extern "C" { #endif /* * PCM API */ struct pcm; #define PCM_OUT 0x00000000 #define PCM_IN 0x10000000 #define PCM_MMAP 0x00000001 #define PCM_NOIRQ 0x00000002 /* PCM runtime states */ #define PCM_STATE_OPEN 0 #define PCM_STATE_SETUP 1 #define PCM_STATE_PREPARED 2 #define PCM_STATE_RUNNING 3 #define PCM_STATE_XRUN 4 #define PCM_STATE_DRAINING 5 #define PCM_STATE_PAUSED 6 #define PCM_STATE_SUSPENDED 7 #define PCM_STATE_DISCONNECTED 8 /* Bit formats */ enum pcm_format { PCM_FORMAT_S16_LE = 0, PCM_FORMAT_S32_LE, PCM_FORMAT_MAX, }; /* Configuration for a stream */ struct pcm_config { unsigned int channels; unsigned int rate; unsigned int period_size; unsigned int period_count; enum pcm_format format; /* Values to use for the ALSA start, stop and silence thresholds. Setting * any one of these values to 0 will cause the default tinyalsa values to be * used instead. Tinyalsa defaults are as follows. * * start_threshold : period_count * period_size * stop_threshold : period_count * period_size * silence_threshold : 0 */ unsigned int start_threshold; unsigned int stop_threshold; unsigned int silence_threshold; int avail_min; }; /* Mixer control types */ enum mixer_ctl_type { MIXER_CTL_TYPE_BOOL, MIXER_CTL_TYPE_INT, MIXER_CTL_TYPE_ENUM, MIXER_CTL_TYPE_BYTE, MIXER_CTL_TYPE_IEC958, MIXER_CTL_TYPE_INT64, MIXER_CTL_TYPE_UNKNOWN, MIXER_CTL_TYPE_MAX, }; /* Open and close a stream */ struct pcm *pcm_open(unsigned int card, unsigned int device, unsigned int flags, struct pcm_config *config); int pcm_close(struct pcm *pcm); int pcm_is_ready(struct pcm *pcm); /* Set and get config */ int pcm_get_config(struct pcm *pcm, struct pcm_config *config); int pcm_set_config(struct pcm *pcm, struct pcm_config *config); /* Returns a human readable reason for the last error */ const char *pcm_get_error(struct pcm *pcm); /* Returns the buffer size (int frames) that should be used for pcm_write. * This will be 1/2 of the actual fifo size. */ unsigned int pcm_get_buffer_size(struct pcm *pcm); unsigned int pcm_frames_to_bytes(struct pcm *pcm, unsigned int frames); unsigned int pcm_bytes_to_frames(struct pcm *pcm, unsigned int frames); /* Returns the pcm latency in ms */ unsigned int pcm_get_latency(struct pcm *pcm); /* Returns available frames in pcm buffer and corresponding time stamp. * For an input stream, frames available are frames ready for the * application to read. * For an output stream, frames available are the number of empty frames available * for the application to write. */ int pcm_get_htimestamp(struct pcm *pcm, unsigned int *avail, struct timespec *tstamp); /* Write data to the fifo. * Will start playback on the first write or on a write that * occurs after a fifo underrun. */ int pcm_write(struct pcm *pcm, void *data, unsigned int count); int pcm_read(struct pcm *pcm, void *data, unsigned int count); /* * mmap() support. */ int pcm_mmap_write(struct pcm *pcm, void *data, unsigned int count); int pcm_mmap_begin(struct pcm *pcm, void **areas, unsigned int *offset, unsigned int *frames); int pcm_mmap_commit(struct pcm *pcm, unsigned int offset, unsigned int frames); /* Start and stop a PCM channel that doesn't transfer data */ int pcm_start(struct pcm *pcm); int pcm_stop(struct pcm *pcm); /* Change avail_min after the stream has been opened with no need to stop the stream. * Only accepted if opened with PCM_MMAP and PCM_NOIRQ flags */ int pcm_set_avail_min(struct pcm *pcm, int avail_min); /* * MIXER API */ struct mixer; struct mixer_ctl; /* Open and close a mixer */ struct mixer *mixer_open(unsigned int card); void mixer_close(struct mixer *mixer); /* Obtain mixer controls */ unsigned int mixer_get_num_ctls(struct mixer *mixer); struct mixer_ctl *mixer_get_ctl(struct mixer *mixer, unsigned int id); struct mixer_ctl *mixer_get_ctl_by_name(struct mixer *mixer, const char *name); /* Get info about mixer controls */ int mixer_ctl_get_name(struct mixer_ctl *ctl, char *name, unsigned int size); enum mixer_ctl_type mixer_ctl_get_type(struct mixer_ctl *ctl); const char *mixer_ctl_get_type_string(struct mixer_ctl *ctl); unsigned int mixer_ctl_get_num_values(struct mixer_ctl *ctl); unsigned int mixer_ctl_get_num_enums(struct mixer_ctl *ctl); int mixer_ctl_get_enum_string(struct mixer_ctl *ctl, unsigned int enum_id, char *string, unsigned int size); /* Set and get mixer controls */ int mixer_ctl_get_percent(struct mixer_ctl *ctl, unsigned int id); int mixer_ctl_set_percent(struct mixer_ctl *ctl, unsigned int id, int percent); int mixer_ctl_get_value(struct mixer_ctl *ctl, unsigned int id); int mixer_ctl_set_value(struct mixer_ctl *ctl, unsigned int id, int value); int mixer_ctl_set_enum_by_string(struct mixer_ctl *ctl, const char *string); /* Determe range of integer mixer controls */ int mixer_ctl_get_range_min(struct mixer_ctl *ctl); int mixer_ctl_get_range_max(struct mixer_ctl *ctl); #if defined(__cplusplus) } /* extern "C" */ #endif #endif