index 655fe76895ce6248ae2f5d513101fb7db274c066..4b6e4ecaf8fbbf64273794fbac91fe0e407a7095 100644 (file)
#define ASOUNDLIB_H
#include <sys/time.h>
+#include <stddef.h>
#if defined(__cplusplus)
extern "C" {
#define PCM_IN 0x10000000
#define PCM_MMAP 0x00000001
#define PCM_NOIRQ 0x00000002
+#define PCM_NORESTART 0x00000004 /* PCM_NORESTART - when set, calls to
+ * pcm_write for a playback stream will not
+ * attempt to restart the stream in the case
+ * of an underflow, but will return -EPIPE
+ * instead. After the first -EPIPE error, the
+ * stream is considered to be stopped, and a
+ * second call to pcm_write will attempt to
+ * restart the stream.
+ */
+#define PCM_MONOTONIC 0x00000008 /* see pcm_get_htimestamp */
/* PCM runtime states */
#define PCM_STATE_OPEN 0
/* Bit formats */
enum pcm_format {
- PCM_FORMAT_S16_LE = 0,
- PCM_FORMAT_S32_LE,
+ PCM_FORMAT_INVALID = -1,
+ PCM_FORMAT_S16_LE = 0, /* 16-bit signed */
+ PCM_FORMAT_S32_LE, /* 32-bit signed */
+ PCM_FORMAT_S8, /* 8-bit signed */
+ PCM_FORMAT_S24_LE, /* 24-bits in 4-bytes */
+ PCM_FORMAT_S24_3LE, /* 24-bits in 3-bytes */
PCM_FORMAT_MAX,
};
+/* Bitmask has 256 bits (32 bytes) in asound.h */
+struct pcm_mask {
+ unsigned int bits[32 / sizeof(unsigned int)];
+};
+
/* Configuration for a stream */
struct pcm_config {
unsigned int channels;
int avail_min;
};
+/* PCM parameters */
+enum pcm_param
+{
+ /* mask parameters */
+ PCM_PARAM_ACCESS,
+ PCM_PARAM_FORMAT,
+ PCM_PARAM_SUBFORMAT,
+ /* interval parameters */
+ PCM_PARAM_SAMPLE_BITS,
+ PCM_PARAM_FRAME_BITS,
+ PCM_PARAM_CHANNELS,
+ PCM_PARAM_RATE,
+ PCM_PARAM_PERIOD_TIME,
+ PCM_PARAM_PERIOD_SIZE,
+ PCM_PARAM_PERIOD_BYTES,
+ PCM_PARAM_PERIODS,
+ PCM_PARAM_BUFFER_TIME,
+ PCM_PARAM_BUFFER_SIZE,
+ PCM_PARAM_BUFFER_BYTES,
+ PCM_PARAM_TICK_TIME,
+};
+
/* Mixer control types */
enum mixer_ctl_type {
MIXER_CTL_TYPE_BOOL,
MIXER_CTL_TYPE_MAX,
};
+#ifdef OMAP_ENHANCEMENT
+#define MAX_CARD_COUNT 32
+
+int mixer_get_card_name(int card, char *str, size_t strlen);
+#endif
+
/* Open and close a stream */
struct pcm *pcm_open(unsigned int card, unsigned int device,
unsigned int flags, struct pcm_config *config);
int pcm_close(struct pcm *pcm);
int pcm_is_ready(struct pcm *pcm);
+/* Obtain the parameters for a PCM */
+struct pcm_params *pcm_params_get(unsigned int card, unsigned int device,
+ unsigned int flags);
+void pcm_params_free(struct pcm_params *pcm_params);
+
+struct pcm_mask *pcm_params_get_mask(struct pcm_params *pcm_params,
+ enum pcm_param param);
+unsigned int pcm_params_get_min(struct pcm_params *pcm_params,
+ enum pcm_param param);
+void pcm_params_set_min(struct pcm_params *pcm_params,
+ enum pcm_param param, unsigned int val);
+unsigned int pcm_params_get_max(struct pcm_params *pcm_params,
+ enum pcm_param param);
+void pcm_params_set_max(struct pcm_params *pcm_params,
+ enum pcm_param param, unsigned int val);
+
+/* Converts the pcm parameters to a human readable string.
+ * The string parameter is a caller allocated buffer of size bytes,
+ * which is then filled up to size - 1 and null terminated,
+ * if size is greater than zero.
+ * The return value is the number of bytes copied to string
+ * (not including null termination) if less than size; otherwise,
+ * the number of bytes required for the buffer.
+ */
+int pcm_params_to_string(struct pcm_params *params, char *string, unsigned int size);
+
+/* Returns 1 if the pcm_format is present (format bit set) in
+ * the pcm_params structure; 0 otherwise, or upon unrecognized format.
+ */
+int pcm_params_format_test(struct pcm_params *params, enum pcm_format format);
+
/* Set and get config */
int pcm_get_config(struct pcm *pcm, struct pcm_config *config);
int pcm_set_config(struct pcm *pcm, struct pcm_config *config);
/* Returns a human readable reason for the last error */
const char *pcm_get_error(struct pcm *pcm);
+/* Returns the sample size in bits for a PCM format.
+ * As with ALSA formats, this is the storage size for the format, whereas the
+ * format represents the number of significant bits. For example,
+ * PCM_FORMAT_S24_LE uses 32 bits of storage.
+ */
+unsigned int pcm_format_to_bits(enum pcm_format format);
+
/* Returns the buffer size (int frames) that should be used for pcm_write. */
unsigned int pcm_get_buffer_size(struct pcm *pcm);
unsigned int pcm_frames_to_bytes(struct pcm *pcm, unsigned int frames);
unsigned int pcm_get_latency(struct pcm *pcm);
/* Returns available frames in pcm buffer and corresponding time stamp.
+ * The clock is CLOCK_MONOTONIC if flag PCM_MONOTONIC was specified in pcm_open,
+ * otherwise the clock is CLOCK_REALTIME.
* For an input stream, frames available are frames ready for the
* application to read.
* For an output stream, frames available are the number of empty frames available
* mmap() support.
*/
int pcm_mmap_write(struct pcm *pcm, const void *data, unsigned int count);
+int pcm_mmap_read(struct pcm *pcm, void *data, unsigned int count);
int pcm_mmap_begin(struct pcm *pcm, void **areas, unsigned int *offset,
unsigned int *frames);
int pcm_mmap_commit(struct pcm *pcm, unsigned int offset, unsigned int frames);
+/* Prepare the PCM substream to be triggerable */
+int pcm_prepare(struct pcm *pcm);
/* Start and stop a PCM channel that doesn't transfer data */
int pcm_start(struct pcm *pcm);
int pcm_stop(struct pcm *pcm);
+/* Interrupt driven API */
+int pcm_wait(struct pcm *pcm, int timeout);
+
/* Change avail_min after the stream has been opened with no need to stop the stream.
* Only accepted if opened with PCM_MMAP and PCM_NOIRQ flags
*/
struct mixer *mixer_open(unsigned int card);
void mixer_close(struct mixer *mixer);
+/* Get info about a mixer */
+const char *mixer_get_name(struct mixer *mixer);
+
/* Obtain mixer controls */
unsigned int mixer_get_num_ctls(struct mixer *mixer);
struct mixer_ctl *mixer_get_ctl(struct mixer *mixer, unsigned int id);
struct mixer_ctl *mixer_get_ctl_by_name(struct mixer *mixer, const char *name);
/* Get info about mixer controls */
-int mixer_ctl_get_name(struct mixer_ctl *ctl, char *name, unsigned int size);
+const char *mixer_ctl_get_name(struct mixer_ctl *ctl);
enum mixer_ctl_type mixer_ctl_get_type(struct mixer_ctl *ctl);
const char *mixer_ctl_get_type_string(struct mixer_ctl *ctl);
unsigned int mixer_ctl_get_num_values(struct mixer_ctl *ctl);
unsigned int mixer_ctl_get_num_enums(struct mixer_ctl *ctl);
-int mixer_ctl_get_enum_string(struct mixer_ctl *ctl, unsigned int enum_id,
- char *string, unsigned int size);
+const char *mixer_ctl_get_enum_string(struct mixer_ctl *ctl,
+ unsigned int enum_id);
+
+/* Some sound cards update their controls due to external events,
+ * such as HDMI EDID byte data changing when an HDMI cable is
+ * connected. This API allows the count of elements to be updated.
+ */
+void mixer_ctl_update(struct mixer_ctl *ctl);
/* Set and get mixer controls */
int mixer_ctl_get_percent(struct mixer_ctl *ctl, unsigned int id);
int mixer_ctl_set_percent(struct mixer_ctl *ctl, unsigned int id, int percent);
int mixer_ctl_get_value(struct mixer_ctl *ctl, unsigned int id);
+int mixer_ctl_get_array(struct mixer_ctl *ctl, void *array, size_t count);
int mixer_ctl_set_value(struct mixer_ctl *ctl, unsigned int id, int value);
+int mixer_ctl_set_array(struct mixer_ctl *ctl, const void *array, size_t count);
int mixer_ctl_set_enum_by_string(struct mixer_ctl *ctl, const char *string);
/* Determe range of integer mixer controls */