2 years agobeagle-x15: Update kernel prebuilts master android-q-preview-1 android-q-preview-2.5 android-q-preview-4 android-q-preview-5 android-q-preview-6
beagle-x15: Update kernel prebuilts
Adds the evm board fit/dtbo dependencies.
NOTE: This is *not* a clang-built kernel.
4.14.91 / 7877512:
Includes kernel/common merges, and the following changes:
fb462e2e0ae4 ANDROID: build: Package additional overlay files
Change-Id: I47addb959b645ba437b571a318e4b4138ae5f8e3
Signed-off-by: Alistair Strachan <astrachan@google.com>
Adds the evm board fit/dtbo dependencies.
NOTE: This is *not* a clang-built kernel.
4.14.91 / 7877512:
Includes kernel/common merges, and the following changes:
fb462e2e0ae4 ANDROID: build: Package additional overlay files
Change-Id: I47addb959b645ba437b571a318e4b4138ae5f8e3
Signed-off-by: Alistair Strachan <astrachan@google.com>
beagle-x15: Update kernel prebuilts, add GPU driver
This change adds a binary ko for the GPU driver. The GPU driver's source
code can be downloaded from:
https://android.googlesource.com/kernel/omap/+/b8ff2b8640800a538ed08b504ac35a8b45126c1f/modules/eurasia_km
This is *not* a clang-built kernel.
4.14.86 / 34fa22c:
Includes kernel/common merges, and the following changes:
34fa22c821ca gx_km: fix pvrsrvkm.ko double list_del error
b8ff2b864080 Enable build of pvrsrvkm.ko with build.sh wrapper.
df9067fe631c Add PowerVR SGX kernel mode driver
56a814a04a97 Package only the needed dtb file
6734ff66804e Realign defconfig with kernel/configs.
d5af25068e81 ANDROID: Regenerate defconfig with savedefconfig
b42c03148f8a ANDROID: Move from clang 4679922 to r346389b.
ce092cb80a62 android-base.config: Revert: Deprecate xt_qtaguid module
9a725075965e android-4.14: kernel/configs: sync android base and recommended config
298cc580859d ti_config_fragments: v8_baseport: Enable Crypto Test Module
2137823854b6 dmaengine: ti: k3-udma: Fix descriptor alignment for memcpy
b0de09cd5a18 ti_config_fragments: arm64_prune: disable virt extension
da74ef48119b ti_config_fragments: v8_baseport: disable profiling
41a007199757 irqchip: ti-sci-inta: Fix build warning with allmodconfig
64c13a8428f4 PCI: keystone: Fix wrong paranthesis usage in dma_set_mask
055fbe6d42be misc: pci_endpoint_test: Fix wrong paranthesis usage in dma_set_mask
1dead88f9382 usb: gadget: uvc: Move userspace API definition to public header
c7c5838b2382 ARM: dts: am335x-evm: fix number of cpsw
e99de67c5d2c drm/bridge: tc358767: add GPIO & interrupt registers
18cc4b734997 drm/bridge: tc358767: use DP connector if no panel set
b0be6fbebec1 drm/bridge: tc358767: fix output H/V syncs
16885cf6202d drm/bridge: tc358767: reject modes which require too much BW
bde85702860f drm/bridge: tc358767: fix initial DP0/1_SRCCTRL value
35f638300f0e drm/bridge: tc358767: fix single lane configuration
0de05f3ff142 drm/bridge: tc358767: add defines for DP1_SRCCTRL & PHY_2LANE
b712929b8b10 drm/bridge: tc358767: add bus flags
ad9e5f10c5b6 ti_config_fragments: v8_android.cfg: Add SYSTEM and CMA ION heaps
ce3096ae8569 remoteproc/k3-r5: cleanup k3_r5_cluster_rproc_exit() for split-mode
858a6c477edd remoteproc/k3-r5: cleanup failure paths in k3_r5_cluster_rproc_init()
24282280e1a6 remoteproc: use a local copy for the name field
cc4cc551b9d5 remoteproc/k3-r5: fix missing put_device() in cluster OF init code
66d22fca4607 mmc: sdhci-of-arasan: am654: add a set_power callback
956447115477 mmc: sdhci-of-arasan: Add sdhci_arasan_set_power
940d059a6038 Revert "usb: dwc3: prevent setting PRTCAP to OTG from debugfs"
c339e8666891 ti_config_fragments: v8_android.cfg : disable devtmpfs
46bb67753612 crypto: omap-sham: split up data to multiple sg elements with huge data
84671666f5e4 firmware: ti_sci: allow frequency change for disabled clocks by default
2419f21396b9 remoteproc/k3-r5: fix the R5 boot state machine for multiple combinations
6069b8049e7f remoteproc: add prepare and unprepare ops
9515cb8ffa90 remoteproc/k3-r5: fix use after free with reserved memory regions
510eedd32636 drm/tidss: Fix copy-paste error in fb uv-plane address calculations
69d762bd056b drm/tidss: The CRTC state needs to be written to HW also in enable()
d71a13bcf292 drm/omap: omap_wb_m2m: add cropping parameter support
a748b43bffc0 drm/omap: omap_wb_m2m: g/s_selection ioctl always fails
098eee719bd9 drm/omap: omap_wb: remove unneeded vb2_dma_addr_plus_data_offset()
5903cac4e76a arm64: dts: ti: k3-am654-base-board: split the R5F memory regions
6a28d115b972 remoteproc/k3-r5: add support for fixed reserved memory regions
236b12d25333 dt-bindings: remoteproc: k3-r5f: Update bindings for multiple memory regions
a4b052a35239 of: reserved_mem: Accessor for acquiring reserved_mem
5d88eea39ec6 net: ethernet: ti: am65-cpsw-nuss: use round robin mode for cppi tx queues
Bug: none
Test: local
Change-Id: I89d8dc221f656c23f2e28842c1f6841ef989207c
Signed-off-by: Alistair Strachan <astrachan@google.com>
This change adds a binary ko for the GPU driver. The GPU driver's source
code can be downloaded from:
https://android.googlesource.com/kernel/omap/+/b8ff2b8640800a538ed08b504ac35a8b45126c1f/modules/eurasia_km
This is *not* a clang-built kernel.
4.14.86 / 34fa22c:
Includes kernel/common merges, and the following changes:
34fa22c821ca gx_km: fix pvrsrvkm.ko double list_del error
b8ff2b864080 Enable build of pvrsrvkm.ko with build.sh wrapper.
df9067fe631c Add PowerVR SGX kernel mode driver
56a814a04a97 Package only the needed dtb file
6734ff66804e Realign defconfig with kernel/configs.
d5af25068e81 ANDROID: Regenerate defconfig with savedefconfig
b42c03148f8a ANDROID: Move from clang 4679922 to r346389b.
ce092cb80a62 android-base.config: Revert: Deprecate xt_qtaguid module
9a725075965e android-4.14: kernel/configs: sync android base and recommended config
298cc580859d ti_config_fragments: v8_baseport: Enable Crypto Test Module
2137823854b6 dmaengine: ti: k3-udma: Fix descriptor alignment for memcpy
b0de09cd5a18 ti_config_fragments: arm64_prune: disable virt extension
da74ef48119b ti_config_fragments: v8_baseport: disable profiling
41a007199757 irqchip: ti-sci-inta: Fix build warning with allmodconfig
64c13a8428f4 PCI: keystone: Fix wrong paranthesis usage in dma_set_mask
055fbe6d42be misc: pci_endpoint_test: Fix wrong paranthesis usage in dma_set_mask
1dead88f9382 usb: gadget: uvc: Move userspace API definition to public header
c7c5838b2382 ARM: dts: am335x-evm: fix number of cpsw
e99de67c5d2c drm/bridge: tc358767: add GPIO & interrupt registers
18cc4b734997 drm/bridge: tc358767: use DP connector if no panel set
b0be6fbebec1 drm/bridge: tc358767: fix output H/V syncs
16885cf6202d drm/bridge: tc358767: reject modes which require too much BW
bde85702860f drm/bridge: tc358767: fix initial DP0/1_SRCCTRL value
35f638300f0e drm/bridge: tc358767: fix single lane configuration
0de05f3ff142 drm/bridge: tc358767: add defines for DP1_SRCCTRL & PHY_2LANE
b712929b8b10 drm/bridge: tc358767: add bus flags
ad9e5f10c5b6 ti_config_fragments: v8_android.cfg: Add SYSTEM and CMA ION heaps
ce3096ae8569 remoteproc/k3-r5: cleanup k3_r5_cluster_rproc_exit() for split-mode
858a6c477edd remoteproc/k3-r5: cleanup failure paths in k3_r5_cluster_rproc_init()
24282280e1a6 remoteproc: use a local copy for the name field
cc4cc551b9d5 remoteproc/k3-r5: fix missing put_device() in cluster OF init code
66d22fca4607 mmc: sdhci-of-arasan: am654: add a set_power callback
956447115477 mmc: sdhci-of-arasan: Add sdhci_arasan_set_power
940d059a6038 Revert "usb: dwc3: prevent setting PRTCAP to OTG from debugfs"
c339e8666891 ti_config_fragments: v8_android.cfg : disable devtmpfs
46bb67753612 crypto: omap-sham: split up data to multiple sg elements with huge data
84671666f5e4 firmware: ti_sci: allow frequency change for disabled clocks by default
2419f21396b9 remoteproc/k3-r5: fix the R5 boot state machine for multiple combinations
6069b8049e7f remoteproc: add prepare and unprepare ops
9515cb8ffa90 remoteproc/k3-r5: fix use after free with reserved memory regions
510eedd32636 drm/tidss: Fix copy-paste error in fb uv-plane address calculations
69d762bd056b drm/tidss: The CRTC state needs to be written to HW also in enable()
d71a13bcf292 drm/omap: omap_wb_m2m: add cropping parameter support
a748b43bffc0 drm/omap: omap_wb_m2m: g/s_selection ioctl always fails
098eee719bd9 drm/omap: omap_wb: remove unneeded vb2_dma_addr_plus_data_offset()
5903cac4e76a arm64: dts: ti: k3-am654-base-board: split the R5F memory regions
6a28d115b972 remoteproc/k3-r5: add support for fixed reserved memory regions
236b12d25333 dt-bindings: remoteproc: k3-r5f: Update bindings for multiple memory regions
a4b052a35239 of: reserved_mem: Accessor for acquiring reserved_mem
5d88eea39ec6 net: ethernet: ti: am65-cpsw-nuss: use round robin mode for cppi tx queues
Bug: none
Test: local
Change-Id: I89d8dc221f656c23f2e28842c1f6841ef989207c
Signed-off-by: Alistair Strachan <astrachan@google.com>
Move the 4.14 kernel/dtb blob into a subdirectory
Preparation for staging the 4.19 kernel. This does not update the
kernel, which will happen in a follow-up change.
Bug: 110964307
Change-Id: I093f9411ea5212da397e418b17513dd7fded8291
Signed-off-by: Alistair Strachan <astrachan@google.com>
Preparation for staging the 4.19 kernel. This does not update the
kernel, which will happen in a follow-up change.
Bug: 110964307
Change-Id: I093f9411ea5212da397e418b17513dd7fded8291
Signed-off-by: Alistair Strachan <astrachan@google.com>
beagle-x15: Update kernel and dtb prebuilts
This is *not* a clang-built kernel.
4.14.77 / 5225796:
Includes kernel/common merges, and the following changes:
8ea64388199a drm/tidss: dispc7: Remove unneeded semicolon at the end of switch-block
dcf2afb691b6 drm/tidss: dispc7: Remove double spaces from scaling code
5d52abdba59e drm/tidss: dispc7: Simplify assignment of VP POL FREQ bits in vp_enable()
28ab93b21d29 drm/tidss: Add TI custom "background" color property and functionality
6d64c4fc75e5 drm/tidss: Add TI custom transparency key properties and functionality
e355eb115eeb drm/tidss: dispc7: Add conversion modes to argb8888_to_argb12121212()
9cf961207c3c drm/tidss: Add skeleton code for custom crtc properties
878637fcb3cd drm/tidss: Add missing dispc_ops->vp_setup() call to crtc_atomic_flush()
b7c15402d198 drm/tidss: dispc7: Statically assign OLDI and DPI bus types to vp
182f3a7ee497 arm64: dts: Add k3-am654-evm-tc358876.dtso
d833d54f1bc6 arm64: dts: am654-base-board: add mcu_i2c0 pinmux
9817dac8d0d9 ti_config_fragments: audio_display: add TC358767
88d937fb6409 drm/omap: fix missing scaler pixel fmt limitations
957de960ca9f drm/omap: DMM: Fix interrupt request/free sequence during probe/remove
8cd561ec8c64 drm/tidss: Add missing static to dispc[67]_plane_feat() functions
7075ad4f4079 drm/tidss: dispc7: Drop entry print in dispc7_init() to dbg level
e1cb34cae559 drm/tidss: dispc7: Cleanup OVR handling
dbfa47b02dfc ti_config_fragments: v8_baseport: enable K3 thermal
858fe3fdacb3 soc/dmaengine: ti: Move cppi5.h header under dma as ti-cppi5.h
0fb6a509765e dmaengine: ti: k3-udma: Set the supported metadata modes
5467a929ad78 dmaengine: Update the descriptor metadata support as per mainline
2e27be9f8391 dmaengine: ti: k3-udma: Do not set device_attach_metadata callback
830b22a4cdce dmaengine: ti: k3-udma: Remove unnecessary dev_width <-> elsize conversions
c468578d33a4 soc: ti: cppi5: Alignment fixes
3828542e1bb3 dmaengine: ti: k3-udma: Use the cppi5 helpers for TR descriptor setup
69c3ff1da0a5 soc: ti: cppi5: Update the TR descriptor init helper
e8a66e065dd1 soc: ti: cppi5: Rename cppi5_desc_is_epib_present to cppi5_hdesc_epib_present
055c49afaef9 soc: ti: cppi5: Collect generic Packet/TR descriptor helpers in one place
2b4db50b8718 dmaengine: ti: k3-udma: Use cppi5_tr_calc_size() from cppi5.h
5194c913786c soc: ti: cppi5: Fix TR packet size calculation
5ee9dcf6f9cc soc: ti: cppi5: Move TR inline functions after the definition
9f66d8bb2a9b dmaengine: ti: k3-udma: Use the cppi5_desc_hdr_t instead cppi50_tr_req_desc
ec7876fd7362 dmaengine: ti: k3-udma: Fix (again) the TR descriptor size calculation
491736a0175c dmaengine: ti: k3-udma: Rename slave_thread_id to remote_thread_id
09f0b2d59f8e soc: ti: Add header file for k3-navss-desc-pool (tree-wide)
a51ec0e7d6e8 soc: ti: cppi5: Change prefixes from knav_udmap_ to cppi5_ (tree-wide)
eea78358778c crypto: sa2ul: Omit error print for DMA channel in case of deferred probe
31e92437e554 arm64: dts: k3-am6: Remove the ghost psil node
1fa32757d083 soc: ti: k3: navss: Remove the psil driver
9a6729525b98 ti_config_fragments: v8_baseport: Drop CONFIG_TI_K3_NAVSS_PSILCFG
4487f706c6f9 dmaengine: ti: Kconfig: Drop TI_K3_NAVSS_PSILCFG for k3-udma
4b2442cb96cc dmaengine: ti: k3-udma: glue: Switch to use the local PSI-L thread API
ccbc4bfe3520 dmaengine: ti: k3-udma: Handle the PSI-L pairing/unpairing locally
02ae8bd22f4c arm64: dts: k3-am6: Add tisci-dev-id to NAVSS nodes
9e3a6cdd46ce dt-bindings: dma: ti: k3-udma: Update for PSI-L thread management
630232505826 dmaengine: ti: k3-udma: Mark the TR descriptor as 64 byte aligned
437c45be2275 dmaengine: ti: k3-udma: Use dma_pool for DMA_MEM_TO_MEM channels
df2f7c4c3ae2 dmaengine: ti: k3-udma: Use dma_pool for packet mode channel descriptors
d156c61f7b36 dmaengine: ti: k3-udma: Simplify push to ring parameters
9f51a3ec4991 dmaengine: ti: k3-udma: Pre-calculate the descriptor size for packet mode
679d8562be09 dmaengine: ti: k3-udma: Do not count the terminated transfer's length
7d008b247d2c dmaengine: ti: k3-udma: Do a complete reset of the channel to recover
a5bb829b9496 dmaengine: ti: k3-udma: Replace magic numbers with defines
96c71bf64caf dmaengine: ti: k3-udma: Correct the packet descriptor alignment
53fc776ee23d dmaengine: ti: k3-udma: Do not allow slave transfers bigger than 4M-1
c00fab16a483 dmaengine: ti: k3-udma: Remove unused struct definitions and defines
13b45e25c4b0 net: ti: icssg_prueth: fix command done check and cancel command
0553d5319117 net: ti: icssg_prueth: clear SMEM portion for the slice
3660df54bc8c net: ti: icssg_prueth: Add ethtool support
a74551970fad net: ti: icssg_prueth: Follow proper shutdown sequence
5f93d6522d12 net: ti: icssg_prueth: Support Promiscuous mode properly
dd9065e081fc net: ti: icssg: Add classifier helpers
b863f126e70b net: ti: icssg_prueth: Increase port buffer in MSMC
173ca0c47432 arm64: dts: ti: Add mii-g-rt to prueth nodes
f31378bb7063 dt-bindings: net: ti,icssg-prueth: Add mii-g-rt property
dd584d9f4b2e ti_config_fragments/android.cfg: am57x: Enable USB2 PHY driver as built-in
7fa5cc8466b5 drm/omap: fbdev: avoid double initializer entry
6c5450db37a9 drm/omap: fbdev: use 'screen_buffer' field
3e980d6f2184 drm/omap: acx565akm: use __be32 when reading status
949776b07b96 ti_config_fragments: v8_android.cfg: Add CMA area for display dumb buffers
1e23cd2a4bc2 arm64: dts: ti: k3-am6: Disable HS400 speed mode
20e72a7c2044 arm64: dts: ti: am65x-android-fstab: Mount early partitions from eMMC
ac1b75f98396 phy: ti: phy-ti-am654: Fix "Failed to find the parent" warnings
b8a148464953 phy: ti: phy-ti-am654: Fix boot lockup
613d2bd55bd2 drm/omap: dss6: Add missing ops helper for overlay support
2485c3ec6106 Revert "rpmsg: core: add support to power domains for devices"
8172579d3e02 HACK: drm/omap: increase DSS5 max tv pclk to 192MHz
04cb0abf1f31 drm/omap: add omap_plane_print_state helper
040ff879d3fb drm/omap: Add wide display support using multiple overlays
5fd6987ac3c8 drm/omap: Add ovl checking funcs to dispc_ops
57a234d3d222 drm/omap: Add ability to check if requested plane modes can be supported
c8980ed4dfb5 drm: fix use of freed memory in drm_mode_setcrtc
bae6303b987e arm: dts: am57xx-idk-common: Hook smps12 regulator as cpu vdd-supply
a095d4a03a20 crypto: sa2ul: Clean up dma and unregister crypto algos upon remove
f172c72de523 crypto: sa2ul: remove context cache from the code
ec5f414b0cb6 phy: ti: phy-ti-am654: Fix compilation warning
057d75c4352f ti_config_fragments/connectivity.cfg: announce new USB devices
c825ccdc8eeb net: ethernet: ti: am65-cpsw-nuss: rework initialization
e099fefebdba net: ethernet: ti: am65-cpts: rework initialization
a17688e543a6 drivers: net: davinci_mdio: use devm to unregister mdio_bus
a7a1ec53cfa2 net: ethernet: ti: am65-cpsw-nuss: enable modular build
9e4ca8726392 net: ethernet: ti: am65-cpsw-nuss: fix dma err handling in probe
273802b3e240 arm64: dts: k3-am654-idk: Add rotary encoder DT node
0121765bc09c tools: PCI: Add 'h' in optstring of getopt()
1d82111bd7fa phy: phy-am654-mmc: Calibrate IO Lines on init
29726bb3bbca arm64: dts: am654-base-board: Enable PHY mode
0cd1928d0247 arm64: dts: k3-am6: Increase OSPI RCLK to 166MHz
aaf3c42f4811 arm64: dts: k3-am6 : Switch OSPI data region to MCU_FSS0_DAT_REG3
85326f06ea88 spi-nor: cadence-quadspi: Add support for PHY configuration
9f0b99fffc9a spi-nor: cadence-quadspi: Enable support for DQS line
a5a464884a8c dt-bindings: cadence-quadspi: Add DT bindings to OSPI PHY
c8f2fe3b61ab dt-bindings: spi: Add DT property for DQS line
054f2d0a6581 spi-nor: cadence-quadspi: Don't set mode bits
32f13769b0aa spi-nor: Fix definition of Octal Read capability bit
bbd5095b8d59 arm64: dts: ti: k3-am6: Add Support for DDR52 mode
c5d0339171c2 arm64: dts: ti: k3-am6: Disable support for UHS modes in MMC/SD
7d569c59b662 phy: ti: Convert PHY_AM654_MMC to a tristate Kconfig
f6e73255a61a dmaengine: ti: k3-udma: Abort the driver probe if no channels available
b17f488f5143 arm64: dts: k3-am6: Update the NAVSS/UDMAP/PDMA nodes to match with TRM
d825dac21747 dmaengine: ti: k3-udma: Support for channel performance levels
a4be23d494c3 dmaengine: ti: k3-udma: Remove no longer valid compatible support
b14bcc7da6d3 arm64: dts: k3-am6: Change the compatible for the UDMAP nodes
f73a6c1c1b69 dmaengine: ti: k3-udma: Add compatibles for UDMAP in am654
0bc763df2e88 dmaengine: ti: k3-udma: Query the allocated ranges from sysfw
93ac2d2f8693 arm64: dts: k3-am6: Add parameters for sysfw RM ranges for udmas
2818cf8cdf19 dt-bindings: dma: ti: k3-udma: Update the documentation
bd0d343e08a3 ASoC: davinci-mcasp: Use future proof way to check for UDMAP
38aea93113b8 firmware: ti_sci: rename back rx_flow_cfg
a0758977f50c firmware: ti_sci: drop old udma rm api
6035dda5df17 dmaengine: ti: k3-udma: switch to new udma rm api
6af1a7c7a4f2 dmaengine: ti: k3-udma: switch glue layer to new udma rm api
fdf2ed2f0297 firmware: ti_sci: add new udma resource management api
611d704a5e93 firmware: ti_sci: drop old ra rm api
621299f9ea1b soc: ti: k3: ringacc: switch to new ra rm api
e5e74dbc8641 firmware: ti_sci: add new ringacc resource management api
c6f6b792128c soc: ti: k3: ringacc: update doc
e70c18b06762 soc: ti: k3: ringacc: drop unused field event_id from sruct k3_nav_ring
cb517a4a03ab net: ethernet: ti: am65-cpsw-nuss: fix kmemleak false-positive reports for rx sk buffers
53b209e4ed3a ARM: DRA7: hwmod_data: Fix second MMU's data on DSPs
5433c6f705ea arm64: dts: k3-am6: rename mcu cpsw node
3a340474dea6 can: m_can: fix uninitialized variable usage
e83dbe1fa527 arm64: dts: k3-am6: Enable PCIe GEN3 mode
42e7863b6d90 HACK: usb: dwc3: of-simple: Add support for AM654 USB
8ae438450295 usb: dwc3: of-simple: Don't fail if no clock entries
280b9f7b7825 Revert "dt-bindings: usb: Add binding for ti, am654-dwc3 device"
2b8af8dec57a Revert "usb: dwc3: Add glue layer for TI's AM654 SoC"
675781f56ed9 ti_config_fragments/connectivity.cfg: Enable USB2 PHY driver
5eb28c7ccaf5 arm64: boot: dts: ti: k3-am6: Update USB PHYs to use TI USB2 PHY driver
2e6c9862d870 phy: ti: usb2: Add support for AM654 USB2 PHY
967bbe4e03a3 dt-bindings: phy: ti: Add support for AM654x USB2 PHY
99c24c4e69ad phy: ti: Don't depend on OMAP_OCP2SCP
726a8f40ec46 ti_config_fragments/cconnectivity.cfg: Enable support for broadcom wireless
7ca75e304195 drm/tidss: Use normalized zpos for plane placement
42d48f1f19d9 drm/tidss: dispc7: Make pre-multiplied alpha the default blending mode
d9282e229f84 drm/tidss: dispc7: Add per-plane alpha property support
330c31f93851 drm/blend: Add a generic alpha property
9b0f8e37b00f drm/docs: Align layout of optional plane blending properties
18942ae66597 drm/atomic-helper: Make zpos property kerneldoc less misleading
7f19dd81f79e drm/tidss: crtc: Add CTM support and implement it for dispc7
e05de7862b9f drm/tidss: Implement CSC properties
96d6e9fd7e5a drm/tidss: dispc7: Implement scaling support with proper FIR coefficients
18b25eaa5291 drm/tidss: plane: Visible area should not be cut at subpixel boundary
7a5f74c155a5 drm/tidss: Add plane_check() to struct dispc_ops
164da8028ee0 drm/tidss: dispc7: Update mflag setup for AM654 and enable it
eb7963e17c3a PCI: keystone: Set DMA mask and coherent DMA mask
69b3274e94cb misc: pci_endpoint_test: Use streaming DMA APIs for buffer allocation
a37b80112669 PCI: endpoint: functions/pci-epf-test: Use data_transfer API for tranferring data
34482a29a988 PCI: designware-ep: Populate epf_init and data_transfer callbacks to use DMA
24e601406ac5 PCI: endpoint: Add callbacks for EPF initialization and data transfer
9166249ccdba PCI: endpoint: Add helpers to use dmaengine APIs for data transfers
b471ad1f6bf1 PCI: endpoint: Protect concurrent access to pci_epf_ops with mutex
9cce71630951 PCI: endpoint: Protect concurrent access to memory allocation with mutex
2b83bc5729dd PCI: endpoint: Replace spinlock with mutex
aeaaa14ca39e PCI: endpoint: Use notification chain mechanism to notify EPC events to EPF
db4be8a82830 ti_config_fragments: audio_display: disable a few unneeded options
1d9557fd05ed ti_config_fragments/v8_defconfig_map.txt: add audio_display.cfg to RT config
7ee5a1f33946 arm64: boot: dts: ti: k3-am6: Add mii_g_rt nodes in ICSSG
be520149c661 dt-bindings: remoteproc: ti-pruss: Update bindings to add MII_G_RT info
8d3a6677c9a4 HACK: Input: goodix: fix driver auto-loading for all variants
eff8e33a4922 media: ti-vpe: vip: Move v4l2_dev to shared struct
9344970d7e1f media: ti-vpe: vip: Use appropriate object name in trace log
26362c5fb0b1 media: ti-vpe: vip: Add name storage for major struct
a9b992d9de3b media: ti-vpe: vip: Set bus_info to show VIP resource used
5fa1434261b1 ti_config_fragments/v8_defconfig_map.txt: Add audio/display config for Android
c9278efb2d7a remoteproc/pru: deny rproc sysfs ops for PRU client driven boots
ee02f6bb1ca3 Revert "remoteproc: deny sysfs operations with MPM userspace loader"
1fa313fa64b8 remoteproc/keystone: set deny_sysfs_ops flag for MPM userspace loader
e37d18218c94 remoteproc/wkup_m3: set deny_sysfs_ops flag
385e53ab58f8 remoteproc: introduce deny_sysfs_ops flag
b959b5927f8b arm64: dts: k3-am654-idk: Add Support for MCAN
c345fd7c379a can: m_can: Add support for enabling transceiver through the STB line
d4dccb940a17 arm64: dts: ti: k3-am6: Add Support for MCAN
a8e2d6598344 dt-bindings: net: can: m_can: Add Documentation for stb-gpios
f6399a0a5939 Revert "HACK: char: hwrng: omap-rng: Set the TRNG Bit in Engine Enable Control"
ec2a5b9d7a0c crypto: sa2ul: Fix allmodconfig compiler warnings
ce834f0061ae crypto: sa2ul: Add MODULE_LICENSE
59536ed444b7 PM / core: fix deferred probe breaking suspend resume order
c9ad08e94ceb ti_config_fragments: v8_baseport: disable CONFIG_SLUB_DEBUG
b6c44d00a0ff ti_config_fragments: arm64_prune: disable CONFIG_NUMA
a168b0230616 ARM: dts: ti: dra71-evm-lcd-auo-g101evn01.0: Add backlight phandle for the lcd
7579e9b41584 ARM: dts: dra7x-evm-lcd-auo-g101evn01.0: Add backlight phandle for the lcd
a6275fee4d50 net: ethernet: ti: cpsw: fix runtime_pm while add/kill vlan
d7774a110f77 net: ethernet: ti: cpsw: clear all entries when delete vid
1ec60987504b net: ethernet: ti: cpts: mark expected switch fall-through
93855ce9caf6 net: ethernet: ti: cpsw: replace unnecessarily macroses on functions
555585ace729 net: ethernet: ti: cpsw: add missed RX_CTAG feature for second slave
f8d405f0998e net: ethernet: ti: cpts: break cycle once late ts is matched
3face3f00a0d net: ethernet: ti: cpsw: allow PTP 224.0.0.107 to be timestamped
66ccc90206fc net: ethernet: ti: cpsw: use BIT macro
d23054b66f23 net: ethernet: ti: davinci_cpdma: make function cpdma_desc_pool_create static
3ab6f3fe1e92 net: ti: cpsw: include gpio/consumer.h
ad2f3a7504d4 net: davinci: fix building davinci mdio code without CONFIG_OF
fc4a92561e0c ti: ethernet: davinci: Fix cast to int warnings
9c8685b6db98 net: ethernet: ti: cpsw: Fix cpsw_add_ch_strings() printk format
30bb1a8cbb2d net: ethernet: ti: cpts: Fix timestamp print
e1996a131460 ti: ethernet: cpdma: Use correct format for genpool_*
e12aca382d05 net: ethernet: ti: cpsw: disable mq feature for "AM33xx ES1.0" devices
98323813ca1f net: ethernet: ti: cpdma: correct error handling for chan create
0f1c26b03d46 net: ethernet: ti: Use ERR_CAST instead of ERR_PTR(PTR_ERR())
b860721152c7 usb: dwc3: gadget: Fix OTG events when gadget driver isn't loaded
d2dd9611c035 arm64: dts: k3-am6: Add crypto accelarator node
43439b7d9c46 crypto: sa2ul: Add 3DES ECB & CBC Mode support
a658205e3089 crypto: sa2ul: Add hmac(sha256) HMAC algorithm support
81fbf1268f5d crypto: sa2ul: Add hmac(sha1) HMAC algorithm support
1e7f745608b2 crypto: sa2ul: Add hmac(sha256)cbc(aes) AEAD Algo support
bed85f9e7d81 crypto: sha256_generic: Export the Transform function
b108ce82deb1 crypto: sa2ul: Add aead support for hmac(sha1)cbc(aes) algorithm
e0b95960bee9 crypto: sa2ul: Add AES ECB Mode support
8637086f5515 crypto: sa2ul: Add crypto driver
5a2e9d569d79 dt-bindings: crypto: k3: Add sa2ul bindings documentation
7aad3e1c1723 firmware: ti_sci: Add doc for rm helper apis
4b65b0d5c98d arm64: dts: ti: k3-am654-base-board: Add android early mount partitions
2d7aaaa7e7f2 ti_config_fragments: v8_android.cfg: Set page size to 4k
48d0bb34570a ti_config_fragments: v8_android.cfg: Enable Android fragment file
958fadd98fb1 dt-bindings: irqchip: Introduce TISCI Interrupt Aggregator bindings
ac558d8362b9 irqchip: ti-sci-inta: Update docs and misc fixes
39aab23fba67 irqchip: ti-sci-inta: Allow GIC to be a interrupt parent
7de1a5621fd4 dt-bindings: irqchip: Introduce TISCI Interrupt router bindings
0b4c83de9538 irqchip: ti-sci-intr: Update doc and error handling
135ae363dc20 arm64: dts: k3-am6: Remove unused dma-channels property from udma nodes
589bd7ee6c0f dmaengine: ti: k3-udma: New function for resource tracking initialization
291d52d50879 dmaengine: ti: k3-udma: Ignore the dma-channels property from DT
6e9f3fc0e4dc dmaengine: ti: k3-udma: Move tisci lookup early in probe
5be2c6b80e69 dmaengine: ti: k3-udma: Tidy up the probe function by *dev = &pdev->dev
93fcdbc8223e dmaengine: ti: k3-udma: Fix missing tdcm caused kernel oops
d43ee6ec0cfb dmaengine: ti: k3-udma: Try to hard reset the channel on teardown timeout
ae58b04a94e6 dmaengine: ti: k3-udma: Dump the channel state data when teardown fails
a961cf5f3eff dmaengine: ti: k3-udma: Support for changed staticTR without termination
d467e6c7b5e3 dmaengine: ti: k3-udma: Fix early TX packet completion
842a3545edb0 dmaengine: ti: k3-udma: Introduce channel states
35d082b7a2cc dmaengine: ti: k3-udma: Reset counters as part of channel reset
86c27f2a86f6 dmaengine: ti: k3-udma: Set WAIT flag for type15 TR for memcpy
a645f26f2f91 dmaengine: ti: k3-udma: Disable TR events for salve_sg and memcpy
09a86e601f8e dmaengine: ti: k3-udma: Correct the interrupt name string
1e187ed354ce dmaengine: ti: k3-udma: Exclude rchan1 as it is reserved for sysfw use
e75b48e302da soc: ti: k3: ringacc: fix releasing of shared rings
40cbfbf7b1ec ti_config_fragments: connectivity.cfg: Enable McSPI
ac8605af6b42 arm64: dts: k3-am654: Enable main domain McSPI0
478082caa97c arm64: dts: k3-am6: Add McSPI DT nodes
4f5de6bb50f8 spi: Kconfig; Enable McSPI driver for K3 platforms
3da5415faa3e spi: spi-omap2-mcspi: Fix can_dma() callback
f1b4174359fb dt-bindings: spi: omap-spi: Add compatible for AM654 SoC
5d6cca4b1ed8 HACK: net: ethernet: ti: cpsw: fix broadcast/multicast rate limit enabling
0ed2fbaa8a39 HACK: net: ethernet: ti: am65-cpsw-nuss: add broadcast/multicast rate limit support
ae75d0c8fbb4 net: ethernet: ti: am65-cpsw-nuss: fix copy-paste err in am65_cpsw_get_channels
5a71404fd2e1 ASoC: davinci-mcasp: Add support for FIFO usage caused delay reporting
36ce35160f06 ASoC: dmaengine_pcm: Consider DMA cache caused delay in pointer callback
f211eec22623 ti_config_fragments/v8_defconfig_map.txt: Include android config fragment
3f0ec39ad8b4 ti_config_fragments/v8_defconfig_map.txt: add Android configuration
65774b3083ec mmc: sdhci-of-arasan: Fix error handling in sdhci_arasan_suspend()
cf099d1a52dd mmc: sdhci-of-arasan: Fix error handling in _probe() and _remove()
6a67278c800e ti_config_fragments: v8_baseport: enable CONFIG_PM
b72cd2731425 ti_config_fragments: audio_display: Enable UDMA platform driver for ASoC
0dc6889cdd8d arm64: dts: ti: Add overlay for AM65x GP application board
5e49e1294880 ASoC: davinci-mcasp: Add support for platforms using UDMA
875efdccc93e ASoC: ti: Add UDMA platform driver
d9c9a321d0bd ASoC: ti: New directory for Texas Instruments SoCs
c15714252d8c remoteproc/k3-r5: add loading support for on-chip SRAM regions
b494fd5616bf arm64: boot: dts: ti: k3-am6: Add aliases for rproc nodes
44dc2a65ba1d arm64: dts: ti: k3-am654-evm: Add DDR carveout memory nodes for R5Fs
d4e01b174ffe arm64: dts: ti: k3-am6: Add MCU R5 cluster node
6585b104ce1b ti_config_fragments: v8_rpmsg: Enable rpmsg-proto module
6de6e1116b36 ti_config_fragments: v8_rpmsg: Enable K3 R5F remoteproc support
ed3bef4239f6 HACK: remoteproc: silence devmem error for rprocs with no MMU
8cdfa3a5d4b8 remoteproc/k3-r5: add a remoteproc driver for MCU (dual-R5F) subsystem
03e3d08645a1 dt-bindings: remoteproc: Add bindings for MCU R5 clusters on TI K3 SoCs
ce36a300f82e remoteproc/k3-r5: add TI-SCI processor control helper functions
d64d3157dad9 firmware: ti_sci: Add support for processor control
5c2256e2f3e1 arm64: dts: ti: k3-am6: Add the MCU RAM node
f9030dbba842 HACK: net: ethernet: ti: am65-cpsw-nuss: disable tx csum offload by default
c376675fc844 mmc: sdhci-of-arasan: Add support for runtime PM
22897cefcde5 irqchip: ti-sci-inta: Fix ack_event in interrupt context
83d6e33090ed dmaengine: ti: k3-udma: Add irq_domain to udma_dev
537acaa0df4d mmc: sdhci-of-arasan: Set slot type in the corecfg registers
3a238e416d8b arm64: dts: k3-am6: Add corecfg register space for MMC
df5754144436 remoteproc: Fix kernel crashes for rprocs using HighMem CMA pools
1ef6727825f1 net: ethernet: ti: am65-cpsw-nuss: fix vlan ingress filtering
de1ac2849b70 media: ti-vpe: vpe: ensure buffers are cleaned up properly in abort cases
6cc0c1306c79 media: ti-vpe: vpe: fix a v4l2-compliance failure about frame sequence number
0505c950ab74 media: ti-vpe: vpe: fix a v4l2-compliance failure about invalid sizeimage
4041f1200e7f media: ti-vpe: vpe: Make sure YUYV is set as default format
70e5f2715dff media: ti-vpe: vpe: fix a v4l2-compliance warning about invalid pixel format
db9158faa94f media: ti-vpe: vpe: fix a v4l2-compliance failure causing a kernel panic
6256912cac0d ti_config_fragments/connectivity.cfg: Enable USB Audio
2f6872da466b Revert "sched/core: Require cpu_active() in select_task_rq(), for user tasks"
03a4af1ff28f soc: ti: k3-navss-psilcfg: Omit error message if tisci is not yet ready
66220ee1e5c5 dmaengine: ti: k3-udma: Fix error when channel request fails
7b1c23710e39 dmaengine: ti: k3-udma: Correct the virq error checking
eff226709f04 drm/omap: Fix zpos handling when Transparency Color Key mode is enabled
e6bb04966e7b iommu/omap: Fix cache flushes on L2 table entries
5cc7b09232dc ti_config_fragments/defconfig_map.txt: Update soc name for android defconfig
d833145011af irqchip: ti-sci-inta: Use vint as hwirq
296a6ae63820 irqchip: ti-sci-inta: Fix finding last event
6391ded98a9a android-4.14: kernel/configs: sync android base and recommended config
9248f2321dbc android: include android-base-x86.config to stay in sync with fetch script
b2ebc4140b72 ti_config_fragments/defconfig_map.txt: rename android*.cfg to have .config
3dd0f64f941f android: rename android*.cfg to android*.config
a2888ef62d03 HACK: Input: goodix: fix driver auto-loading
937a47fcc426 net: ti: icssg-prueth: fix cmd failed error message
14eb073fe581 net: ti: icssg-prueth: Fix lock-up on TX teardown
2235c214c112 drm/omap: fix plane's set/get_property
8bdc6bf71578 drm/tidss: Do not warn about slightly off pixel clock rate
34c4d3177d4e drm/tidss: dispc7: Use vp_prepare() and vp_unprepare() for OLDI
ed9469e6e70e drm/tidss: Add optional vp_prepare() and vp_unprepare() to dispc api
63a371b94b0c arm64: dts: ti: Fix wrong display enable gpio and touch reset gpio
831f7af28637 arm64: dts: k3-am6: Fix UART DMA entries
8626adc832fd serial: 8250_omap: Fix build errors when CONFIG_SERIAL_8250_DMA=n
ec2851d89294 mtd: spi-nor: cadence-quadspi: Fix dma coherent mask definition
026147ef9c5f phy: ti: Add depends on COMMON_CLK for PHY_AM654
4b954767a9df Revert "dt-bindings: irqchip: Introduce TI SCI irqchip bindings"
eb5c93899602 Revert "irqchip: tisci: Add the TI SCI irqchip driver"
3dc576b901cf ti_config_fragments: v8_baseport: Enable TI_SCI_INTA/R_IRQCHIP
a1eb6ed4cbc7 dmaengine: ti: k3-udma: Adapt glue layer to new tisci_irq API
b8e1ab78444c dmaengine: ti: k3-udma: Change to the new tisci_irq API
95f42166e376 arm64: dts: ti: Add Interrupt controller nodes
153d5d8cf5f3 irqchip: ti-sci-inta: Add support for Interrupt Aggregator driver
f04d303abde4 irqchip: ti-sci-intr: Add support for Interrupt Router driver
0550d1c0fdb0 firmware: ti_sci: Add helpers to mange resources
299bedb04914 firmware: ti_sci: Update IRQ management ops
9bbbfcdfd936 firmware: ti_sci: Add support for RM core ops
2b46b22087b0 Revert "ti_config_fragments: v8_baseport: Enable TI_SCI_IRQCHIP"
2f008ba6c433 PCI: keystone: Fix compilation error when CONFIG_PCI=n
a8bdb9814e47 net: ethernet: ti: am65-cpsw-nuss: fix tx checksum offload
e4ab1cc28090 arm64: dts: k3-am6: Exclude sysfw reserved rings in main NAVSS ringacc
0dc77f570bd4 dmaengine: ti: k3-udma: Exclude sysfw used channels and flow
c5c49f8f5892 remoteproc/pru: allow fw intc resource fallback for PRUs with no DT irqs
29ea314efed4 remoteproc/pru: fix ti,pru-interrupt-map range checks for K3 SoCs
a2101ec7d921 remoteproc/pruss_intc: fix interrupt configuration for SYSEVENT > 31
2ab837b13d60 dmaengine: ti: k3-udma: glue: Plug rflow leaks
0fb6d637848f arm64: dts: k3-am6: Add dma-coherent property to OSPI nodes
680c9a3fd327 mtd: spi-nor: cadence-quadspi: Set coherent dma mask as required
f7f2f0338c5c mtd: spi-nor: cadence-quadspi: Convert driver data to struct
620eee523531 arm64: dts: ti: Describe the SERDES clock inputs, outputs and mux in dt
ff518e356cdf phy: ti: phy-ti-am654: Add support to select PLL mux and left/right output mux
733ecdcb3176 dt-bindings: phy: ti: Add specification for the clocks
1ffe9cd1a9aa arm64: dts: k3-am6: Add DMA entries for UART nodes
12f7ded85cf6 serial: 8250_omap: Add DMA support for UARTs on AM654 SoC
cd26a69ba3e9 serial: 8250_omap: Get FIFO/DMA triggers from driver data
31c485ff8cd6 serial: 8250_omap; Support EFR2 register
1a7d3b834fcb serial: 8250_omap: Extend driver data to pass DMA configuration
a38b758c6add serial: 8250_omap: Introduce new callback to handle RX DMA
78e5f64d5e93 serial: 8250_omap: Terminate DMA before pushing data on RX timeout
1ca43ffc3e8a serial: 8250_omap: account for DMA cached data
49bd5d4099cf serial: 8250_omap: Work around errata spurious IRQs with DMA
5a62b97df9c3 arm64: dts: k3-am654-idk: add aliases for PRUSS eth
3363e17fad86 arm64: dts: ti: k3-am654-base-board: Enable UHS modes in sdhci1
8a6fd53ca38f mmc: sdhci-of-arasan: Don't register rockchip specific callback for am65x
327e5e96b774 ti_config_fragments/connectivity.cfg: Enable TSCADC
b198a4560dfb arm64: dts: k3-am654-base-board: Enable ADCs
5c37bcfdcee6 arm64: dts: k3-am6: Add ADC DT nodes
cd89154f8fab iio: adc: ti_am335x_adc: Use ADC dev pointer while allocating DMA buffer
beaf5a789885 mfd: ti_am335x_tscadc: Provide unique name for child mfd cells
ea64e415f7ea dt-bindings: ti-tsc-adc: Document compatible properties for tscadc IP
cd4cb1ec19d7 phy: phy-am654-mmc: Reset all accessed registers to default values on power_off
bcc9ab4758b2 dmaengine: ti: k3-udma: Fix channel teardown handling
420649eb6d6a dmaengine: ti: k3-udma: Rename udma_stop_hard to udma_reset_chan
c066288743a5 dmaengine: ti: k3-udma: Use teardown for memcpy channels when stopping
29bf30535bbb dmaengine: ti: k3-udma: Use different counters for packets and TRs
49b95774419c dmaengine: ti: k3-udma: Do pause/resume on the remote (peer) side only
8093bbc128f8 soc: ti: k3: add COMPILE_TEST to kbuild for DMA modules
6a7809c327e4 net: ethernet: ti: am65-cpsw-nuss: fix modular build
0009141bc95f net: ethernet: ti: am65-cpsw-nuss: fix ndev features declaration
092102c0ab75 net: ethernet: ti: am65-cpsw-nuss: add tx checksum offload support
d8f30f6d7a42 net: ethernet: ti: am65-cpsw-nuss: add rx checksum offload support
815a993f42ae arm64: dts: k3-am654-base-board: add aliases for PRUSS eth
b584e47acc3d HACK: char: hwrng: omap-rng: Set the TRNG Bit in Engine Enable Control
b3d2f1fb75e2 arm64: dts: ti: am6: Add the trng node
69ccb5bcdc51 char: hwrng: Kconfig: Or ARCH_K3 dependency for HW_RANDOM_OMAP
0b9772d46485 arm64: dts: ti: am6: Add VTM node
26040fec9bbf arm64: dts: ti: am654: Add thermal zones
f5b96dc1cc72 thermal: k3: Add support for bandgap sensors
22c1561fdf97 dt-bindings: thermal: k3: Add VTM bindings documentation
024da2ce28bc arm64: dts: ti: k3-am6: Add dma-coherent and dma-ranges to NAVSS nodes
3f0bec4eb60c dmaengine: ti: k3-udma: Optimizations for memcpy
f2d96344387c dmaengine: ti: k3-udma: Use dma_zalloc_coherent for cppi5 descriptors
9848bab3d2e4 dmaengine: ti: k3-udma: Do not use threaded irq
04159dce85d0 dmaengine: ti: k3-udma: Do not use hardwired fetch_size for channels
5d51ba64b2ec dmaengine: ti: k3-udma: Use list_for_each_entry_safe in purge_desc_work
a1cb52bce3ee dmaengine: ti: k3-udma: Fix race condition with terminated descriptors
1d54c8f8fac2 dmaengine: ti: k3-udma: Resume the paused rchan when stopping it
c7a2598d1c61 dmaengine: ti: k3-udma: Set rx_error_handling in rflow config
04012535ae57 dmaengine: ti: k3-udma: Fix race of packet completion in while irqs are off
f29f9f3ba679 dmaengine: dma_request_chan_by_mask() to handle deferred probing
4d4b8f0aa8b0 dmaengine: ti: k3-udma: Correct the TR descriptor size calculation
f840272000fc dmaengine: ti: k3-udma: Move out the memcpy code from the interrupt handler
6dde68a49f17 arm64: ti: Build all dtbos along with dtbs
fcfb62a2e57a arm64: dts: Add reset-gpios property to drive PERST# signal
2149cbbc43da PCI: keystone: Add support to deassert PERST# signal
a617c28a9457 dt-bindings: PCI: Add dt-binding for driving PERST# signal
e203d84a4cc4 PCI: keystone: Add support to set link speed based on "max-link-speed" dt property
fad067486a9f dt-bindings: PCI: Add dt-binding to specifiy maximum link speed in pci-keystone
51227ad1e482 mtd: spi-nor: cadence-quadspi: Handle probe deferral while requesting DMA channel
bfa720010a8b mmc: sdhci-of-arasan: Add Support for HS400
70004ad02341 arm64: dts: ti: k3-am654-base-board: Add driver strength for both SD card and eMMC phy nodes
2f686d5e00c8 phy: am654-mmc-phy: Add support for variable drive strength
f7e20b7866c6 dt-bindings: phy: am654-mmc-phy: Introduce property to configure driver strength
e459adbcb160 can: m_can: Move acessing of message ram to after clocks are enabled
b76924f6d7c7 can: m_can: Fix runtime resume call
4a051afdae0f arm64: dts: ti: k3-am6: Add the missing mailbox cluster 11
Bug: none
Test: local
Change-Id: I53b1614c16d093206e6dd2d9c72357f064aa4989
Signed-off-by: Alistair Strachan <astrachan@google.com>
This is *not* a clang-built kernel.
4.14.77 / 5225796:
Includes kernel/common merges, and the following changes:
8ea64388199a drm/tidss: dispc7: Remove unneeded semicolon at the end of switch-block
dcf2afb691b6 drm/tidss: dispc7: Remove double spaces from scaling code
5d52abdba59e drm/tidss: dispc7: Simplify assignment of VP POL FREQ bits in vp_enable()
28ab93b21d29 drm/tidss: Add TI custom "background" color property and functionality
6d64c4fc75e5 drm/tidss: Add TI custom transparency key properties and functionality
e355eb115eeb drm/tidss: dispc7: Add conversion modes to argb8888_to_argb12121212()
9cf961207c3c drm/tidss: Add skeleton code for custom crtc properties
878637fcb3cd drm/tidss: Add missing dispc_ops->vp_setup() call to crtc_atomic_flush()
b7c15402d198 drm/tidss: dispc7: Statically assign OLDI and DPI bus types to vp
182f3a7ee497 arm64: dts: Add k3-am654-evm-tc358876.dtso
d833d54f1bc6 arm64: dts: am654-base-board: add mcu_i2c0 pinmux
9817dac8d0d9 ti_config_fragments: audio_display: add TC358767
88d937fb6409 drm/omap: fix missing scaler pixel fmt limitations
957de960ca9f drm/omap: DMM: Fix interrupt request/free sequence during probe/remove
8cd561ec8c64 drm/tidss: Add missing static to dispc[67]_plane_feat() functions
7075ad4f4079 drm/tidss: dispc7: Drop entry print in dispc7_init() to dbg level
e1cb34cae559 drm/tidss: dispc7: Cleanup OVR handling
dbfa47b02dfc ti_config_fragments: v8_baseport: enable K3 thermal
858fe3fdacb3 soc/dmaengine: ti: Move cppi5.h header under dma as ti-cppi5.h
0fb6a509765e dmaengine: ti: k3-udma: Set the supported metadata modes
5467a929ad78 dmaengine: Update the descriptor metadata support as per mainline
2e27be9f8391 dmaengine: ti: k3-udma: Do not set device_attach_metadata callback
830b22a4cdce dmaengine: ti: k3-udma: Remove unnecessary dev_width <-> elsize conversions
c468578d33a4 soc: ti: cppi5: Alignment fixes
3828542e1bb3 dmaengine: ti: k3-udma: Use the cppi5 helpers for TR descriptor setup
69c3ff1da0a5 soc: ti: cppi5: Update the TR descriptor init helper
e8a66e065dd1 soc: ti: cppi5: Rename cppi5_desc_is_epib_present to cppi5_hdesc_epib_present
055c49afaef9 soc: ti: cppi5: Collect generic Packet/TR descriptor helpers in one place
2b4db50b8718 dmaengine: ti: k3-udma: Use cppi5_tr_calc_size() from cppi5.h
5194c913786c soc: ti: cppi5: Fix TR packet size calculation
5ee9dcf6f9cc soc: ti: cppi5: Move TR inline functions after the definition
9f66d8bb2a9b dmaengine: ti: k3-udma: Use the cppi5_desc_hdr_t instead cppi50_tr_req_desc
ec7876fd7362 dmaengine: ti: k3-udma: Fix (again) the TR descriptor size calculation
491736a0175c dmaengine: ti: k3-udma: Rename slave_thread_id to remote_thread_id
09f0b2d59f8e soc: ti: Add header file for k3-navss-desc-pool (tree-wide)
a51ec0e7d6e8 soc: ti: cppi5: Change prefixes from knav_udmap_ to cppi5_ (tree-wide)
eea78358778c crypto: sa2ul: Omit error print for DMA channel in case of deferred probe
31e92437e554 arm64: dts: k3-am6: Remove the ghost psil node
1fa32757d083 soc: ti: k3: navss: Remove the psil driver
9a6729525b98 ti_config_fragments: v8_baseport: Drop CONFIG_TI_K3_NAVSS_PSILCFG
4487f706c6f9 dmaengine: ti: Kconfig: Drop TI_K3_NAVSS_PSILCFG for k3-udma
4b2442cb96cc dmaengine: ti: k3-udma: glue: Switch to use the local PSI-L thread API
ccbc4bfe3520 dmaengine: ti: k3-udma: Handle the PSI-L pairing/unpairing locally
02ae8bd22f4c arm64: dts: k3-am6: Add tisci-dev-id to NAVSS nodes
9e3a6cdd46ce dt-bindings: dma: ti: k3-udma: Update for PSI-L thread management
630232505826 dmaengine: ti: k3-udma: Mark the TR descriptor as 64 byte aligned
437c45be2275 dmaengine: ti: k3-udma: Use dma_pool for DMA_MEM_TO_MEM channels
df2f7c4c3ae2 dmaengine: ti: k3-udma: Use dma_pool for packet mode channel descriptors
d156c61f7b36 dmaengine: ti: k3-udma: Simplify push to ring parameters
9f51a3ec4991 dmaengine: ti: k3-udma: Pre-calculate the descriptor size for packet mode
679d8562be09 dmaengine: ti: k3-udma: Do not count the terminated transfer's length
7d008b247d2c dmaengine: ti: k3-udma: Do a complete reset of the channel to recover
a5bb829b9496 dmaengine: ti: k3-udma: Replace magic numbers with defines
96c71bf64caf dmaengine: ti: k3-udma: Correct the packet descriptor alignment
53fc776ee23d dmaengine: ti: k3-udma: Do not allow slave transfers bigger than 4M-1
c00fab16a483 dmaengine: ti: k3-udma: Remove unused struct definitions and defines
13b45e25c4b0 net: ti: icssg_prueth: fix command done check and cancel command
0553d5319117 net: ti: icssg_prueth: clear SMEM portion for the slice
3660df54bc8c net: ti: icssg_prueth: Add ethtool support
a74551970fad net: ti: icssg_prueth: Follow proper shutdown sequence
5f93d6522d12 net: ti: icssg_prueth: Support Promiscuous mode properly
dd9065e081fc net: ti: icssg: Add classifier helpers
b863f126e70b net: ti: icssg_prueth: Increase port buffer in MSMC
173ca0c47432 arm64: dts: ti: Add mii-g-rt to prueth nodes
f31378bb7063 dt-bindings: net: ti,icssg-prueth: Add mii-g-rt property
dd584d9f4b2e ti_config_fragments/android.cfg: am57x: Enable USB2 PHY driver as built-in
7fa5cc8466b5 drm/omap: fbdev: avoid double initializer entry
6c5450db37a9 drm/omap: fbdev: use 'screen_buffer' field
3e980d6f2184 drm/omap: acx565akm: use __be32 when reading status
949776b07b96 ti_config_fragments: v8_android.cfg: Add CMA area for display dumb buffers
1e23cd2a4bc2 arm64: dts: ti: k3-am6: Disable HS400 speed mode
20e72a7c2044 arm64: dts: ti: am65x-android-fstab: Mount early partitions from eMMC
ac1b75f98396 phy: ti: phy-ti-am654: Fix "Failed to find the parent" warnings
b8a148464953 phy: ti: phy-ti-am654: Fix boot lockup
613d2bd55bd2 drm/omap: dss6: Add missing ops helper for overlay support
2485c3ec6106 Revert "rpmsg: core: add support to power domains for devices"
8172579d3e02 HACK: drm/omap: increase DSS5 max tv pclk to 192MHz
04cb0abf1f31 drm/omap: add omap_plane_print_state helper
040ff879d3fb drm/omap: Add wide display support using multiple overlays
5fd6987ac3c8 drm/omap: Add ovl checking funcs to dispc_ops
57a234d3d222 drm/omap: Add ability to check if requested plane modes can be supported
c8980ed4dfb5 drm: fix use of freed memory in drm_mode_setcrtc
bae6303b987e arm: dts: am57xx-idk-common: Hook smps12 regulator as cpu vdd-supply
a095d4a03a20 crypto: sa2ul: Clean up dma and unregister crypto algos upon remove
f172c72de523 crypto: sa2ul: remove context cache from the code
ec5f414b0cb6 phy: ti: phy-ti-am654: Fix compilation warning
057d75c4352f ti_config_fragments/connectivity.cfg: announce new USB devices
c825ccdc8eeb net: ethernet: ti: am65-cpsw-nuss: rework initialization
e099fefebdba net: ethernet: ti: am65-cpts: rework initialization
a17688e543a6 drivers: net: davinci_mdio: use devm to unregister mdio_bus
a7a1ec53cfa2 net: ethernet: ti: am65-cpsw-nuss: enable modular build
9e4ca8726392 net: ethernet: ti: am65-cpsw-nuss: fix dma err handling in probe
273802b3e240 arm64: dts: k3-am654-idk: Add rotary encoder DT node
0121765bc09c tools: PCI: Add 'h' in optstring of getopt()
1d82111bd7fa phy: phy-am654-mmc: Calibrate IO Lines on init
29726bb3bbca arm64: dts: am654-base-board: Enable PHY mode
0cd1928d0247 arm64: dts: k3-am6: Increase OSPI RCLK to 166MHz
aaf3c42f4811 arm64: dts: k3-am6 : Switch OSPI data region to MCU_FSS0_DAT_REG3
85326f06ea88 spi-nor: cadence-quadspi: Add support for PHY configuration
9f0b99fffc9a spi-nor: cadence-quadspi: Enable support for DQS line
a5a464884a8c dt-bindings: cadence-quadspi: Add DT bindings to OSPI PHY
c8f2fe3b61ab dt-bindings: spi: Add DT property for DQS line
054f2d0a6581 spi-nor: cadence-quadspi: Don't set mode bits
32f13769b0aa spi-nor: Fix definition of Octal Read capability bit
bbd5095b8d59 arm64: dts: ti: k3-am6: Add Support for DDR52 mode
c5d0339171c2 arm64: dts: ti: k3-am6: Disable support for UHS modes in MMC/SD
7d569c59b662 phy: ti: Convert PHY_AM654_MMC to a tristate Kconfig
f6e73255a61a dmaengine: ti: k3-udma: Abort the driver probe if no channels available
b17f488f5143 arm64: dts: k3-am6: Update the NAVSS/UDMAP/PDMA nodes to match with TRM
d825dac21747 dmaengine: ti: k3-udma: Support for channel performance levels
a4be23d494c3 dmaengine: ti: k3-udma: Remove no longer valid compatible support
b14bcc7da6d3 arm64: dts: k3-am6: Change the compatible for the UDMAP nodes
f73a6c1c1b69 dmaengine: ti: k3-udma: Add compatibles for UDMAP in am654
0bc763df2e88 dmaengine: ti: k3-udma: Query the allocated ranges from sysfw
93ac2d2f8693 arm64: dts: k3-am6: Add parameters for sysfw RM ranges for udmas
2818cf8cdf19 dt-bindings: dma: ti: k3-udma: Update the documentation
bd0d343e08a3 ASoC: davinci-mcasp: Use future proof way to check for UDMAP
38aea93113b8 firmware: ti_sci: rename back rx_flow_cfg
a0758977f50c firmware: ti_sci: drop old udma rm api
6035dda5df17 dmaengine: ti: k3-udma: switch to new udma rm api
6af1a7c7a4f2 dmaengine: ti: k3-udma: switch glue layer to new udma rm api
fdf2ed2f0297 firmware: ti_sci: add new udma resource management api
611d704a5e93 firmware: ti_sci: drop old ra rm api
621299f9ea1b soc: ti: k3: ringacc: switch to new ra rm api
e5e74dbc8641 firmware: ti_sci: add new ringacc resource management api
c6f6b792128c soc: ti: k3: ringacc: update doc
e70c18b06762 soc: ti: k3: ringacc: drop unused field event_id from sruct k3_nav_ring
cb517a4a03ab net: ethernet: ti: am65-cpsw-nuss: fix kmemleak false-positive reports for rx sk buffers
53b209e4ed3a ARM: DRA7: hwmod_data: Fix second MMU's data on DSPs
5433c6f705ea arm64: dts: k3-am6: rename mcu cpsw node
3a340474dea6 can: m_can: fix uninitialized variable usage
e83dbe1fa527 arm64: dts: k3-am6: Enable PCIe GEN3 mode
42e7863b6d90 HACK: usb: dwc3: of-simple: Add support for AM654 USB
8ae438450295 usb: dwc3: of-simple: Don't fail if no clock entries
280b9f7b7825 Revert "dt-bindings: usb: Add binding for ti, am654-dwc3 device"
2b8af8dec57a Revert "usb: dwc3: Add glue layer for TI's AM654 SoC"
675781f56ed9 ti_config_fragments/connectivity.cfg: Enable USB2 PHY driver
5eb28c7ccaf5 arm64: boot: dts: ti: k3-am6: Update USB PHYs to use TI USB2 PHY driver
2e6c9862d870 phy: ti: usb2: Add support for AM654 USB2 PHY
967bbe4e03a3 dt-bindings: phy: ti: Add support for AM654x USB2 PHY
99c24c4e69ad phy: ti: Don't depend on OMAP_OCP2SCP
726a8f40ec46 ti_config_fragments/cconnectivity.cfg: Enable support for broadcom wireless
7ca75e304195 drm/tidss: Use normalized zpos for plane placement
42d48f1f19d9 drm/tidss: dispc7: Make pre-multiplied alpha the default blending mode
d9282e229f84 drm/tidss: dispc7: Add per-plane alpha property support
330c31f93851 drm/blend: Add a generic alpha property
9b0f8e37b00f drm/docs: Align layout of optional plane blending properties
18942ae66597 drm/atomic-helper: Make zpos property kerneldoc less misleading
7f19dd81f79e drm/tidss: crtc: Add CTM support and implement it for dispc7
e05de7862b9f drm/tidss: Implement CSC properties
96d6e9fd7e5a drm/tidss: dispc7: Implement scaling support with proper FIR coefficients
18b25eaa5291 drm/tidss: plane: Visible area should not be cut at subpixel boundary
7a5f74c155a5 drm/tidss: Add plane_check() to struct dispc_ops
164da8028ee0 drm/tidss: dispc7: Update mflag setup for AM654 and enable it
eb7963e17c3a PCI: keystone: Set DMA mask and coherent DMA mask
69b3274e94cb misc: pci_endpoint_test: Use streaming DMA APIs for buffer allocation
a37b80112669 PCI: endpoint: functions/pci-epf-test: Use data_transfer API for tranferring data
34482a29a988 PCI: designware-ep: Populate epf_init and data_transfer callbacks to use DMA
24e601406ac5 PCI: endpoint: Add callbacks for EPF initialization and data transfer
9166249ccdba PCI: endpoint: Add helpers to use dmaengine APIs for data transfers
b471ad1f6bf1 PCI: endpoint: Protect concurrent access to pci_epf_ops with mutex
9cce71630951 PCI: endpoint: Protect concurrent access to memory allocation with mutex
2b83bc5729dd PCI: endpoint: Replace spinlock with mutex
aeaaa14ca39e PCI: endpoint: Use notification chain mechanism to notify EPC events to EPF
db4be8a82830 ti_config_fragments: audio_display: disable a few unneeded options
1d9557fd05ed ti_config_fragments/v8_defconfig_map.txt: add audio_display.cfg to RT config
7ee5a1f33946 arm64: boot: dts: ti: k3-am6: Add mii_g_rt nodes in ICSSG
be520149c661 dt-bindings: remoteproc: ti-pruss: Update bindings to add MII_G_RT info
8d3a6677c9a4 HACK: Input: goodix: fix driver auto-loading for all variants
eff8e33a4922 media: ti-vpe: vip: Move v4l2_dev to shared struct
9344970d7e1f media: ti-vpe: vip: Use appropriate object name in trace log
26362c5fb0b1 media: ti-vpe: vip: Add name storage for major struct
a9b992d9de3b media: ti-vpe: vip: Set bus_info to show VIP resource used
5fa1434261b1 ti_config_fragments/v8_defconfig_map.txt: Add audio/display config for Android
c9278efb2d7a remoteproc/pru: deny rproc sysfs ops for PRU client driven boots
ee02f6bb1ca3 Revert "remoteproc: deny sysfs operations with MPM userspace loader"
1fa313fa64b8 remoteproc/keystone: set deny_sysfs_ops flag for MPM userspace loader
e37d18218c94 remoteproc/wkup_m3: set deny_sysfs_ops flag
385e53ab58f8 remoteproc: introduce deny_sysfs_ops flag
b959b5927f8b arm64: dts: k3-am654-idk: Add Support for MCAN
c345fd7c379a can: m_can: Add support for enabling transceiver through the STB line
d4dccb940a17 arm64: dts: ti: k3-am6: Add Support for MCAN
a8e2d6598344 dt-bindings: net: can: m_can: Add Documentation for stb-gpios
f6399a0a5939 Revert "HACK: char: hwrng: omap-rng: Set the TRNG Bit in Engine Enable Control"
ec2a5b9d7a0c crypto: sa2ul: Fix allmodconfig compiler warnings
ce834f0061ae crypto: sa2ul: Add MODULE_LICENSE
59536ed444b7 PM / core: fix deferred probe breaking suspend resume order
c9ad08e94ceb ti_config_fragments: v8_baseport: disable CONFIG_SLUB_DEBUG
b6c44d00a0ff ti_config_fragments: arm64_prune: disable CONFIG_NUMA
a168b0230616 ARM: dts: ti: dra71-evm-lcd-auo-g101evn01.0: Add backlight phandle for the lcd
7579e9b41584 ARM: dts: dra7x-evm-lcd-auo-g101evn01.0: Add backlight phandle for the lcd
a6275fee4d50 net: ethernet: ti: cpsw: fix runtime_pm while add/kill vlan
d7774a110f77 net: ethernet: ti: cpsw: clear all entries when delete vid
1ec60987504b net: ethernet: ti: cpts: mark expected switch fall-through
93855ce9caf6 net: ethernet: ti: cpsw: replace unnecessarily macroses on functions
555585ace729 net: ethernet: ti: cpsw: add missed RX_CTAG feature for second slave
f8d405f0998e net: ethernet: ti: cpts: break cycle once late ts is matched
3face3f00a0d net: ethernet: ti: cpsw: allow PTP 224.0.0.107 to be timestamped
66ccc90206fc net: ethernet: ti: cpsw: use BIT macro
d23054b66f23 net: ethernet: ti: davinci_cpdma: make function cpdma_desc_pool_create static
3ab6f3fe1e92 net: ti: cpsw: include gpio/consumer.h
ad2f3a7504d4 net: davinci: fix building davinci mdio code without CONFIG_OF
fc4a92561e0c ti: ethernet: davinci: Fix cast to int warnings
9c8685b6db98 net: ethernet: ti: cpsw: Fix cpsw_add_ch_strings() printk format
30bb1a8cbb2d net: ethernet: ti: cpts: Fix timestamp print
e1996a131460 ti: ethernet: cpdma: Use correct format for genpool_*
e12aca382d05 net: ethernet: ti: cpsw: disable mq feature for "AM33xx ES1.0" devices
98323813ca1f net: ethernet: ti: cpdma: correct error handling for chan create
0f1c26b03d46 net: ethernet: ti: Use ERR_CAST instead of ERR_PTR(PTR_ERR())
b860721152c7 usb: dwc3: gadget: Fix OTG events when gadget driver isn't loaded
d2dd9611c035 arm64: dts: k3-am6: Add crypto accelarator node
43439b7d9c46 crypto: sa2ul: Add 3DES ECB & CBC Mode support
a658205e3089 crypto: sa2ul: Add hmac(sha256) HMAC algorithm support
81fbf1268f5d crypto: sa2ul: Add hmac(sha1) HMAC algorithm support
1e7f745608b2 crypto: sa2ul: Add hmac(sha256)cbc(aes) AEAD Algo support
bed85f9e7d81 crypto: sha256_generic: Export the Transform function
b108ce82deb1 crypto: sa2ul: Add aead support for hmac(sha1)cbc(aes) algorithm
e0b95960bee9 crypto: sa2ul: Add AES ECB Mode support
8637086f5515 crypto: sa2ul: Add crypto driver
5a2e9d569d79 dt-bindings: crypto: k3: Add sa2ul bindings documentation
7aad3e1c1723 firmware: ti_sci: Add doc for rm helper apis
4b65b0d5c98d arm64: dts: ti: k3-am654-base-board: Add android early mount partitions
2d7aaaa7e7f2 ti_config_fragments: v8_android.cfg: Set page size to 4k
48d0bb34570a ti_config_fragments: v8_android.cfg: Enable Android fragment file
958fadd98fb1 dt-bindings: irqchip: Introduce TISCI Interrupt Aggregator bindings
ac558d8362b9 irqchip: ti-sci-inta: Update docs and misc fixes
39aab23fba67 irqchip: ti-sci-inta: Allow GIC to be a interrupt parent
7de1a5621fd4 dt-bindings: irqchip: Introduce TISCI Interrupt router bindings
0b4c83de9538 irqchip: ti-sci-intr: Update doc and error handling
135ae363dc20 arm64: dts: k3-am6: Remove unused dma-channels property from udma nodes
589bd7ee6c0f dmaengine: ti: k3-udma: New function for resource tracking initialization
291d52d50879 dmaengine: ti: k3-udma: Ignore the dma-channels property from DT
6e9f3fc0e4dc dmaengine: ti: k3-udma: Move tisci lookup early in probe
5be2c6b80e69 dmaengine: ti: k3-udma: Tidy up the probe function by *dev = &pdev->dev
93fcdbc8223e dmaengine: ti: k3-udma: Fix missing tdcm caused kernel oops
d43ee6ec0cfb dmaengine: ti: k3-udma: Try to hard reset the channel on teardown timeout
ae58b04a94e6 dmaengine: ti: k3-udma: Dump the channel state data when teardown fails
a961cf5f3eff dmaengine: ti: k3-udma: Support for changed staticTR without termination
d467e6c7b5e3 dmaengine: ti: k3-udma: Fix early TX packet completion
842a3545edb0 dmaengine: ti: k3-udma: Introduce channel states
35d082b7a2cc dmaengine: ti: k3-udma: Reset counters as part of channel reset
86c27f2a86f6 dmaengine: ti: k3-udma: Set WAIT flag for type15 TR for memcpy
a645f26f2f91 dmaengine: ti: k3-udma: Disable TR events for salve_sg and memcpy
09a86e601f8e dmaengine: ti: k3-udma: Correct the interrupt name string
1e187ed354ce dmaengine: ti: k3-udma: Exclude rchan1 as it is reserved for sysfw use
e75b48e302da soc: ti: k3: ringacc: fix releasing of shared rings
40cbfbf7b1ec ti_config_fragments: connectivity.cfg: Enable McSPI
ac8605af6b42 arm64: dts: k3-am654: Enable main domain McSPI0
478082caa97c arm64: dts: k3-am6: Add McSPI DT nodes
4f5de6bb50f8 spi: Kconfig; Enable McSPI driver for K3 platforms
3da5415faa3e spi: spi-omap2-mcspi: Fix can_dma() callback
f1b4174359fb dt-bindings: spi: omap-spi: Add compatible for AM654 SoC
5d6cca4b1ed8 HACK: net: ethernet: ti: cpsw: fix broadcast/multicast rate limit enabling
0ed2fbaa8a39 HACK: net: ethernet: ti: am65-cpsw-nuss: add broadcast/multicast rate limit support
ae75d0c8fbb4 net: ethernet: ti: am65-cpsw-nuss: fix copy-paste err in am65_cpsw_get_channels
5a71404fd2e1 ASoC: davinci-mcasp: Add support for FIFO usage caused delay reporting
36ce35160f06 ASoC: dmaengine_pcm: Consider DMA cache caused delay in pointer callback
f211eec22623 ti_config_fragments/v8_defconfig_map.txt: Include android config fragment
3f0ec39ad8b4 ti_config_fragments/v8_defconfig_map.txt: add Android configuration
65774b3083ec mmc: sdhci-of-arasan: Fix error handling in sdhci_arasan_suspend()
cf099d1a52dd mmc: sdhci-of-arasan: Fix error handling in _probe() and _remove()
6a67278c800e ti_config_fragments: v8_baseport: enable CONFIG_PM
b72cd2731425 ti_config_fragments: audio_display: Enable UDMA platform driver for ASoC
0dc6889cdd8d arm64: dts: ti: Add overlay for AM65x GP application board
5e49e1294880 ASoC: davinci-mcasp: Add support for platforms using UDMA
875efdccc93e ASoC: ti: Add UDMA platform driver
d9c9a321d0bd ASoC: ti: New directory for Texas Instruments SoCs
c15714252d8c remoteproc/k3-r5: add loading support for on-chip SRAM regions
b494fd5616bf arm64: boot: dts: ti: k3-am6: Add aliases for rproc nodes
44dc2a65ba1d arm64: dts: ti: k3-am654-evm: Add DDR carveout memory nodes for R5Fs
d4e01b174ffe arm64: dts: ti: k3-am6: Add MCU R5 cluster node
6585b104ce1b ti_config_fragments: v8_rpmsg: Enable rpmsg-proto module
6de6e1116b36 ti_config_fragments: v8_rpmsg: Enable K3 R5F remoteproc support
ed3bef4239f6 HACK: remoteproc: silence devmem error for rprocs with no MMU
8cdfa3a5d4b8 remoteproc/k3-r5: add a remoteproc driver for MCU (dual-R5F) subsystem
03e3d08645a1 dt-bindings: remoteproc: Add bindings for MCU R5 clusters on TI K3 SoCs
ce36a300f82e remoteproc/k3-r5: add TI-SCI processor control helper functions
d64d3157dad9 firmware: ti_sci: Add support for processor control
5c2256e2f3e1 arm64: dts: ti: k3-am6: Add the MCU RAM node
f9030dbba842 HACK: net: ethernet: ti: am65-cpsw-nuss: disable tx csum offload by default
c376675fc844 mmc: sdhci-of-arasan: Add support for runtime PM
22897cefcde5 irqchip: ti-sci-inta: Fix ack_event in interrupt context
83d6e33090ed dmaengine: ti: k3-udma: Add irq_domain to udma_dev
537acaa0df4d mmc: sdhci-of-arasan: Set slot type in the corecfg registers
3a238e416d8b arm64: dts: k3-am6: Add corecfg register space for MMC
df5754144436 remoteproc: Fix kernel crashes for rprocs using HighMem CMA pools
1ef6727825f1 net: ethernet: ti: am65-cpsw-nuss: fix vlan ingress filtering
de1ac2849b70 media: ti-vpe: vpe: ensure buffers are cleaned up properly in abort cases
6cc0c1306c79 media: ti-vpe: vpe: fix a v4l2-compliance failure about frame sequence number
0505c950ab74 media: ti-vpe: vpe: fix a v4l2-compliance failure about invalid sizeimage
4041f1200e7f media: ti-vpe: vpe: Make sure YUYV is set as default format
70e5f2715dff media: ti-vpe: vpe: fix a v4l2-compliance warning about invalid pixel format
db9158faa94f media: ti-vpe: vpe: fix a v4l2-compliance failure causing a kernel panic
6256912cac0d ti_config_fragments/connectivity.cfg: Enable USB Audio
2f6872da466b Revert "sched/core: Require cpu_active() in select_task_rq(), for user tasks"
03a4af1ff28f soc: ti: k3-navss-psilcfg: Omit error message if tisci is not yet ready
66220ee1e5c5 dmaengine: ti: k3-udma: Fix error when channel request fails
7b1c23710e39 dmaengine: ti: k3-udma: Correct the virq error checking
eff226709f04 drm/omap: Fix zpos handling when Transparency Color Key mode is enabled
e6bb04966e7b iommu/omap: Fix cache flushes on L2 table entries
5cc7b09232dc ti_config_fragments/defconfig_map.txt: Update soc name for android defconfig
d833145011af irqchip: ti-sci-inta: Use vint as hwirq
296a6ae63820 irqchip: ti-sci-inta: Fix finding last event
6391ded98a9a android-4.14: kernel/configs: sync android base and recommended config
9248f2321dbc android: include android-base-x86.config to stay in sync with fetch script
b2ebc4140b72 ti_config_fragments/defconfig_map.txt: rename android*.cfg to have .config
3dd0f64f941f android: rename android*.cfg to android*.config
a2888ef62d03 HACK: Input: goodix: fix driver auto-loading
937a47fcc426 net: ti: icssg-prueth: fix cmd failed error message
14eb073fe581 net: ti: icssg-prueth: Fix lock-up on TX teardown
2235c214c112 drm/omap: fix plane's set/get_property
8bdc6bf71578 drm/tidss: Do not warn about slightly off pixel clock rate
34c4d3177d4e drm/tidss: dispc7: Use vp_prepare() and vp_unprepare() for OLDI
ed9469e6e70e drm/tidss: Add optional vp_prepare() and vp_unprepare() to dispc api
63a371b94b0c arm64: dts: ti: Fix wrong display enable gpio and touch reset gpio
831f7af28637 arm64: dts: k3-am6: Fix UART DMA entries
8626adc832fd serial: 8250_omap: Fix build errors when CONFIG_SERIAL_8250_DMA=n
ec2851d89294 mtd: spi-nor: cadence-quadspi: Fix dma coherent mask definition
026147ef9c5f phy: ti: Add depends on COMMON_CLK for PHY_AM654
4b954767a9df Revert "dt-bindings: irqchip: Introduce TI SCI irqchip bindings"
eb5c93899602 Revert "irqchip: tisci: Add the TI SCI irqchip driver"
3dc576b901cf ti_config_fragments: v8_baseport: Enable TI_SCI_INTA/R_IRQCHIP
a1eb6ed4cbc7 dmaengine: ti: k3-udma: Adapt glue layer to new tisci_irq API
b8e1ab78444c dmaengine: ti: k3-udma: Change to the new tisci_irq API
95f42166e376 arm64: dts: ti: Add Interrupt controller nodes
153d5d8cf5f3 irqchip: ti-sci-inta: Add support for Interrupt Aggregator driver
f04d303abde4 irqchip: ti-sci-intr: Add support for Interrupt Router driver
0550d1c0fdb0 firmware: ti_sci: Add helpers to mange resources
299bedb04914 firmware: ti_sci: Update IRQ management ops
9bbbfcdfd936 firmware: ti_sci: Add support for RM core ops
2b46b22087b0 Revert "ti_config_fragments: v8_baseport: Enable TI_SCI_IRQCHIP"
2f008ba6c433 PCI: keystone: Fix compilation error when CONFIG_PCI=n
a8bdb9814e47 net: ethernet: ti: am65-cpsw-nuss: fix tx checksum offload
e4ab1cc28090 arm64: dts: k3-am6: Exclude sysfw reserved rings in main NAVSS ringacc
0dc77f570bd4 dmaengine: ti: k3-udma: Exclude sysfw used channels and flow
c5c49f8f5892 remoteproc/pru: allow fw intc resource fallback for PRUs with no DT irqs
29ea314efed4 remoteproc/pru: fix ti,pru-interrupt-map range checks for K3 SoCs
a2101ec7d921 remoteproc/pruss_intc: fix interrupt configuration for SYSEVENT > 31
2ab837b13d60 dmaengine: ti: k3-udma: glue: Plug rflow leaks
0fb6d637848f arm64: dts: k3-am6: Add dma-coherent property to OSPI nodes
680c9a3fd327 mtd: spi-nor: cadence-quadspi: Set coherent dma mask as required
f7f2f0338c5c mtd: spi-nor: cadence-quadspi: Convert driver data to struct
620eee523531 arm64: dts: ti: Describe the SERDES clock inputs, outputs and mux in dt
ff518e356cdf phy: ti: phy-ti-am654: Add support to select PLL mux and left/right output mux
733ecdcb3176 dt-bindings: phy: ti: Add specification for the clocks
1ffe9cd1a9aa arm64: dts: k3-am6: Add DMA entries for UART nodes
12f7ded85cf6 serial: 8250_omap: Add DMA support for UARTs on AM654 SoC
cd26a69ba3e9 serial: 8250_omap: Get FIFO/DMA triggers from driver data
31c485ff8cd6 serial: 8250_omap; Support EFR2 register
1a7d3b834fcb serial: 8250_omap: Extend driver data to pass DMA configuration
a38b758c6add serial: 8250_omap: Introduce new callback to handle RX DMA
78e5f64d5e93 serial: 8250_omap: Terminate DMA before pushing data on RX timeout
1ca43ffc3e8a serial: 8250_omap: account for DMA cached data
49bd5d4099cf serial: 8250_omap: Work around errata spurious IRQs with DMA
5a62b97df9c3 arm64: dts: k3-am654-idk: add aliases for PRUSS eth
3363e17fad86 arm64: dts: ti: k3-am654-base-board: Enable UHS modes in sdhci1
8a6fd53ca38f mmc: sdhci-of-arasan: Don't register rockchip specific callback for am65x
327e5e96b774 ti_config_fragments/connectivity.cfg: Enable TSCADC
b198a4560dfb arm64: dts: k3-am654-base-board: Enable ADCs
5c37bcfdcee6 arm64: dts: k3-am6: Add ADC DT nodes
cd89154f8fab iio: adc: ti_am335x_adc: Use ADC dev pointer while allocating DMA buffer
beaf5a789885 mfd: ti_am335x_tscadc: Provide unique name for child mfd cells
ea64e415f7ea dt-bindings: ti-tsc-adc: Document compatible properties for tscadc IP
cd4cb1ec19d7 phy: phy-am654-mmc: Reset all accessed registers to default values on power_off
bcc9ab4758b2 dmaengine: ti: k3-udma: Fix channel teardown handling
420649eb6d6a dmaengine: ti: k3-udma: Rename udma_stop_hard to udma_reset_chan
c066288743a5 dmaengine: ti: k3-udma: Use teardown for memcpy channels when stopping
29bf30535bbb dmaengine: ti: k3-udma: Use different counters for packets and TRs
49b95774419c dmaengine: ti: k3-udma: Do pause/resume on the remote (peer) side only
8093bbc128f8 soc: ti: k3: add COMPILE_TEST to kbuild for DMA modules
6a7809c327e4 net: ethernet: ti: am65-cpsw-nuss: fix modular build
0009141bc95f net: ethernet: ti: am65-cpsw-nuss: fix ndev features declaration
092102c0ab75 net: ethernet: ti: am65-cpsw-nuss: add tx checksum offload support
d8f30f6d7a42 net: ethernet: ti: am65-cpsw-nuss: add rx checksum offload support
815a993f42ae arm64: dts: k3-am654-base-board: add aliases for PRUSS eth
b584e47acc3d HACK: char: hwrng: omap-rng: Set the TRNG Bit in Engine Enable Control
b3d2f1fb75e2 arm64: dts: ti: am6: Add the trng node
69ccb5bcdc51 char: hwrng: Kconfig: Or ARCH_K3 dependency for HW_RANDOM_OMAP
0b9772d46485 arm64: dts: ti: am6: Add VTM node
26040fec9bbf arm64: dts: ti: am654: Add thermal zones
f5b96dc1cc72 thermal: k3: Add support for bandgap sensors
22c1561fdf97 dt-bindings: thermal: k3: Add VTM bindings documentation
024da2ce28bc arm64: dts: ti: k3-am6: Add dma-coherent and dma-ranges to NAVSS nodes
3f0bec4eb60c dmaengine: ti: k3-udma: Optimizations for memcpy
f2d96344387c dmaengine: ti: k3-udma: Use dma_zalloc_coherent for cppi5 descriptors
9848bab3d2e4 dmaengine: ti: k3-udma: Do not use threaded irq
04159dce85d0 dmaengine: ti: k3-udma: Do not use hardwired fetch_size for channels
5d51ba64b2ec dmaengine: ti: k3-udma: Use list_for_each_entry_safe in purge_desc_work
a1cb52bce3ee dmaengine: ti: k3-udma: Fix race condition with terminated descriptors
1d54c8f8fac2 dmaengine: ti: k3-udma: Resume the paused rchan when stopping it
c7a2598d1c61 dmaengine: ti: k3-udma: Set rx_error_handling in rflow config
04012535ae57 dmaengine: ti: k3-udma: Fix race of packet completion in while irqs are off
f29f9f3ba679 dmaengine: dma_request_chan_by_mask() to handle deferred probing
4d4b8f0aa8b0 dmaengine: ti: k3-udma: Correct the TR descriptor size calculation
f840272000fc dmaengine: ti: k3-udma: Move out the memcpy code from the interrupt handler
6dde68a49f17 arm64: ti: Build all dtbos along with dtbs
fcfb62a2e57a arm64: dts: Add reset-gpios property to drive PERST# signal
2149cbbc43da PCI: keystone: Add support to deassert PERST# signal
a617c28a9457 dt-bindings: PCI: Add dt-binding for driving PERST# signal
e203d84a4cc4 PCI: keystone: Add support to set link speed based on "max-link-speed" dt property
fad067486a9f dt-bindings: PCI: Add dt-binding to specifiy maximum link speed in pci-keystone
51227ad1e482 mtd: spi-nor: cadence-quadspi: Handle probe deferral while requesting DMA channel
bfa720010a8b mmc: sdhci-of-arasan: Add Support for HS400
70004ad02341 arm64: dts: ti: k3-am654-base-board: Add driver strength for both SD card and eMMC phy nodes
2f686d5e00c8 phy: am654-mmc-phy: Add support for variable drive strength
f7e20b7866c6 dt-bindings: phy: am654-mmc-phy: Introduce property to configure driver strength
e459adbcb160 can: m_can: Move acessing of message ram to after clocks are enabled
b76924f6d7c7 can: m_can: Fix runtime resume call
4a051afdae0f arm64: dts: ti: k3-am6: Add the missing mailbox cluster 11
Bug: none
Test: local
Change-Id: I53b1614c16d093206e6dd2d9c72357f064aa4989
Signed-off-by: Alistair Strachan <astrachan@google.com>
beagle-x15: Initial kernel and dtb binaries
Initial 4.14.54 kernel built from the sources here:
https://android.googlesource.com/kernel/omap/+/android-beagle-x15-4.14
4b2b8e15735a5ebb821ea3e97da16e1f2ddb6302
This kernel is not particularly useful for testing as it is old and
lacks some changes needed by the GPU driver. It will be updated shortly.
Bug: 110964307
Change-Id: I674687f8f480af9a1551281644f58c86449ac9e9
Signed-off-by: Alistair Strachan <astrachan@google.com>
Initial 4.14.54 kernel built from the sources here:
https://android.googlesource.com/kernel/omap/+/android-beagle-x15-4.14
4b2b8e15735a5ebb821ea3e97da16e1f2ddb6302
This kernel is not particularly useful for testing as it is old and
lacks some changes needed by the GPU driver. It will be updated shortly.
Bug: 110964307
Change-Id: I674687f8f480af9a1551281644f58c86449ac9e9
Signed-off-by: Alistair Strachan <astrachan@google.com>
Initial empty repository