Merge commit 'e0067bdc75566629c9143818c8f3970c16c8825e' Bug: 110964307 Bug: 116741782 Signed-off-by: Alistair Strachan <astrachan@google.com> Change-Id: I2130490f8fa61743217cbf2081640773960ea843
Initial empty repository
kmstest: Separate reservation phase from command line parsing In the new order the planes are not reserved before the whole command line is parsed. This way we know the color format of the framebuffer that is going to be on the reserved plane and we can select a plane that supports the format. After this patch kmstest makes no distinction between primary and overlay planes if atomic mode setting is supported. If no plane is specified then a default plane, matching the screen size is created. Signed-off-by: Jyri Sarha <jsarha@ti.com> Signed-off-by: Tomi Valkeinen <tomi.valkeinen@ti.com>
kmstest: Implement simplistic propery support behind -P flag. Non atomic modesetting is not supported and there is no translation from various property types to unsigned 64-bit integer. Instead the property values are simply converted from string with stoull(str, 0, 0). Signed-off-by: Tomi Valkeinen <tomi.valkeinen@ti.com>
py: pyvid: Provide stream_off binding The videodevice module defines a stream_off function call, but this is not available in the python bindings interface. Provide the binding of VideoStreamer::stream_off. Signed-off-by: Kieran Bingham <kieran.bingham@ideasonboard.com> Signed-off-by: Tomi Valkeinen <tomi.valkeinen@ti.com>
py: Add Card crtcs and encoders properties back to the Python bindings Commit 706a44abb3aa ("Update to latest pybind11") removed the crtcs and encoders properties from the Card class. Add them back by wrapping the associated C++ methods manually due to a limitation of pybind11. Fixes: 706a44abb3aa ("Update to latest pybind11") Signed-off-by: Laurent Pinchart <laurent.pinchart@ideasonboard.com> Signed-off-by: Tomi Valkeinen <tomi.valkeinen@ti.com>
Fix Python bindings for Connector::get_possible_crtcs() method The method returns an std::vector of DRMObject, which isn't supported by the latest pybind11 as explained in commit 706a44abb3aa. Fix it by wrapping the method manually. Fixes: 706a44abb3aa ("Update to latest pybind11") Signed-off-by: Laurent Pinchart <laurent.pinchart@ideasonboard.com> Signed-off-by: Tomi Valkeinen <tomi.valkeinen@ti.com>
Update to latest pybind11 Update to latest pybind11 HEAD. We can't use the latest tag (v2.2.0) as it has a regression. There were two problems when updating: 1) Difficulty in managing DrmObject derived classes Most of the DrmObjects are owned by Card, and can't be allocated or freed, but a few of them are allocated and freed by the user. For the former, we need to use unique_ptr with py::nodelete, but that prevents the latter from working. The solution was to not tell the python that the latter classes derive from DrmObject. This seems to be missing feature in pybind11, but I think we can live with it. 2) DrmObjects in STL containers vector<T> where T is a DrmObject derived class doesn't work. We need to have a manual wrapper to return vector<unique_ptr<T, py::nodelete>> instead. This also seems to be a pybind11 missing feature. Signed-off-by: Tomi Valkeinen <tomi.valkeinen@ti.com>