]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android/external-libkmsxx.git/blob - libkms++/blob.cpp
testpat: draw pattern separately
[android/external-libkmsxx.git] / libkms++ / blob.cpp
1 #include <xf86drm.h>
2 #include <xf86drmMode.h>
4 #include "kms++.h"
6 using namespace std;
8 namespace kms
9 {
11 Blob::Blob(Card& card, uint32_t blob_id)
12         : DrmObject(card, blob_id, DRM_MODE_OBJECT_BLOB), m_created(false)
13 {
14         // XXX should we verify that the blob_id is a blob object?
15 }
17 Blob::Blob(Card& card, void* data, size_t len)
18         : DrmObject(card, DRM_MODE_OBJECT_BLOB), m_created(true)
19 {
20         uint32_t id;
22         int r = drmModeCreatePropertyBlob(card.fd(), data, len, &id);
23         if (r)
24                 throw invalid_argument("FAILED TO CREATE PROP\n");
26         set_id(id);
27 }
29 Blob::~Blob()
30 {
31         if (m_created)
32                 drmModeDestroyPropertyBlob(card().fd(), id());
33 }
35 vector<uint8_t> Blob::data()
36 {
37         drmModePropertyBlobPtr blob = drmModeGetPropertyBlob(card().fd(), id());
39         if (!blob)
40                 throw invalid_argument("Blob data not available");
42         uint8_t* data = (uint8_t*)blob->data;
44         auto v = vector<uint8_t>(data, data + blob->length);
46         drmModeFreePropertyBlob(blob);
48         return v;
49 }
51 }