]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android/external-libkmsxx.git/blob - utils/kmstest.cpp
ccddccbc7f27d6db9a89c48199179c3e20af1296
[android/external-libkmsxx.git] / utils / kmstest.cpp
1 #include <cstdio>
2 #include <cstring>
3 #include <algorithm>
4 #include <regex>
5 #include <set>
6 #include <chrono>
8 #include <sys/select.h>
10 #include <kms++/kms++.h>
11 #include <kms++/modedb.h>
13 #include <kms++util/kms++util.h>
15 using namespace std;
16 using namespace kms;
18 struct PlaneInfo
19 {
20         Plane* plane;
22         unsigned x;
23         unsigned y;
24         unsigned w;
25         unsigned h;
27         vector<DumbFramebuffer*> fbs;
28 };
30 struct OutputInfo
31 {
32         Connector* connector;
34         Crtc* crtc;
35         Plane* primary_plane;
36         Videomode mode;
37         bool user_set_crtc;
38         vector<DumbFramebuffer*> fbs;
40         vector<PlaneInfo> planes;
41 };
43 static bool s_use_dmt;
44 static bool s_use_cea;
45 static unsigned s_num_buffers = 1;
46 static bool s_flip_mode;
47 static bool s_flip_sync;
49 static set<Crtc*> s_used_crtcs;
50 static set<Plane*> s_used_planes;
52 __attribute__ ((unused))
53 static void print_regex_match(smatch sm)
54 {
55         for (unsigned i = 0; i < sm.size(); ++i) {
56                 string str = sm[i].str();
57                 printf("%u: %s\n", i, str.c_str());
58         }
59 }
61 static void get_default_connector(Card& card, OutputInfo& output)
62 {
63         output.connector = card.get_first_connected_connector();
64         output.mode = output.connector->get_default_mode();
65 }
67 static void parse_connector(Card& card, const string& str, OutputInfo& output)
68 {
69         Connector* conn = resolve_connector(card, str);
71         if (!conn)
72                 EXIT("No connector '%s'", str.c_str());
74         if (!conn->connected())
75                 EXIT("Connector '%s' not connected", conn->fullname().c_str());
77         output.connector = conn;
78         output.mode = output.connector->get_default_mode();
79 }
81 static void get_default_crtc(Card& card, OutputInfo& output)
82 {
83         Crtc* crtc = output.connector->get_current_crtc();
85         if (crtc && s_used_crtcs.find(crtc) == s_used_crtcs.end()) {
86                 s_used_crtcs.insert(crtc);
87                 output.crtc = crtc;
88                 return;
89         }
91         for (const auto& possible : output.connector->get_possible_crtcs()) {
92                 if (s_used_crtcs.find(possible) == s_used_crtcs.end()) {
93                         s_used_crtcs.insert(possible);
94                         output.crtc = possible;
95                         return;
96                 }
97         }
99         EXIT("Could not find available crtc");
102 static void parse_crtc(Card& card, const string& crtc_str, OutputInfo& output)
104         // @12:1920x1200@60
105         const regex mode_re("(?:(@?)(\\d+):)?(?:(\\d+)x(\\d+)(i)?)(?:@([\\d\\.]+))?");
107         smatch sm;
108         if (!regex_match(crtc_str, sm, mode_re))
109                 EXIT("Failed to parse crtc option '%s'", crtc_str.c_str());
111         if (sm[2].matched) {
112                 bool use_id = sm[1].length() == 1;
113                 unsigned num = stoul(sm[2].str());
115                 if (use_id) {
116                         Crtc* c = card.get_crtc(num);
117                         if (!c)
118                                 EXIT("Bad crtc id '%u'", num);
120                         output.crtc = c;
121                 } else {
122                         auto crtcs = card.get_crtcs();
124                         if (num >= crtcs.size())
125                                 EXIT("Bad crtc number '%u'", num);
127                         output.crtc = crtcs[num];
128                 }
129         } else {
130                 output.crtc = output.connector->get_current_crtc();
131         }
133         unsigned w = stoul(sm[3]);
134         unsigned h = stoul(sm[4]);
135         bool ilace = sm[5].matched ? true : false;
136         float refresh = sm[6].matched ? stof(sm[6]) : 0;
138         bool found_mode = false;
140         try {
141                 output.mode = output.connector->get_mode(w, h, refresh, ilace);
142                 found_mode = true;
143         } catch (exception& e) { }
145         if (!found_mode && s_use_dmt) {
146                 try {
147                         output.mode = find_dmt(w, h, refresh, ilace);
148                         found_mode = true;
149                         printf("Found mode from DMT\n");
150                 } catch (exception& e) { }
151         }
153         if (!found_mode && s_use_cea) {
154                 try {
155                         output.mode = find_cea(w, h, refresh, ilace);
156                         found_mode = true;
157                         printf("Found mode from CEA\n");
158                 } catch (exception& e) { }
159         }
161         if (!found_mode)
162                 throw invalid_argument("Mode not found");
165 static void parse_plane(Card& card, const string& plane_str, const OutputInfo& output, PlaneInfo& pinfo)
167         // 3:400,400-400x400
168         const regex plane_re("(?:(@?)(\\d+):)?(?:(\\d+),(\\d+)-)?(\\d+)x(\\d+)");
170         smatch sm;
171         if (!regex_match(plane_str, sm, plane_re))
172                 EXIT("Failed to parse plane option '%s'", plane_str.c_str());
174         if (sm[2].matched) {
175                 bool use_id = sm[1].length() == 1;
176                 unsigned num = stoul(sm[2].str());
178                 if (use_id) {
179                         Plane* p = card.get_plane(num);
180                         if (!p)
181                                 EXIT("Bad plane id '%u'", num);
183                         pinfo.plane = p;
184                 } else {
185                         auto planes = card.get_planes();
187                         if (num >= planes.size())
188                                 EXIT("Bad plane number '%u'", num);
190                         pinfo.plane = planes[num];
191                 }
192         } else {
193                 for (Plane* p : output.crtc->get_possible_planes()) {
194                         if (s_used_planes.find(p) != s_used_planes.end())
195                                 continue;
197                         if (p->plane_type() != PlaneType::Overlay)
198                                 continue;
200                         pinfo.plane = p;
201                 }
203                 if (!pinfo.plane)
204                         EXIT("Failed to find available plane");
205         }
207         s_used_planes.insert(pinfo.plane);
209         pinfo.w = stoul(sm[5]);
210         pinfo.h = stoul(sm[6]);
212         if (sm[3].matched)
213                 pinfo.x = stoul(sm[3]);
214         else
215                 pinfo.x = output.mode.hdisplay / 2 - pinfo.w / 2;
217         if (sm[4].matched)
218                 pinfo.y = stoul(sm[4]);
219         else
220                 pinfo.y = output.mode.vdisplay / 2 - pinfo.h / 2;
223 static vector<DumbFramebuffer*> get_default_fb(Card& card, unsigned width, unsigned height)
225         vector<DumbFramebuffer*> v;
227         for (unsigned i = 0; i < s_num_buffers; ++i)
228                 v.push_back(new DumbFramebuffer(card, width, height, PixelFormat::XRGB8888));
230         return v;
233 static vector<DumbFramebuffer*> parse_fb(Card& card, const string& fb_str, unsigned def_w, unsigned def_h)
235         unsigned w = def_w;
236         unsigned h = def_h;
237         PixelFormat format = PixelFormat::XRGB8888;
239         if (!fb_str.empty()) {
240                 // XXX the regexp is not quite correct
241                 // 400x400-NV12
242                 const regex fb_re("(?:(\\d+)x(\\d+))?(?:-)?(\\w\\w\\w\\w)?");
244                 smatch sm;
245                 if (!regex_match(fb_str, sm, fb_re))
246                         EXIT("Failed to parse fb option '%s'", fb_str.c_str());
248                 if (sm[1].matched)
249                         w = stoul(sm[1]);
250                 if (sm[2].matched)
251                         h = stoul(sm[2]);
252                 if (sm[3].matched)
253                         format = FourCCToPixelFormat(sm[3]);
254         }
256         vector<DumbFramebuffer*> v;
258         for (unsigned i = 0; i < s_num_buffers; ++i)
259                 v.push_back(new DumbFramebuffer(card, w, h, format));
261         return v;
264 static const char* usage_str =
265                 "Usage: testpat [OPTION]...\n\n"
266                 "Show a test pattern on a display or plane\n\n"
267                 "Options:\n"
268                 "      --device=DEVICE       DEVICE is the path to DRM card to open\n"
269                 "  -c, --connector=CONN      CONN is <connector>\n"
270                 "  -r, --crtc=CRTC           CRTC is [<crtc>:]<w>x<h>[@<Hz>]\n"
271                 "  -p, --plane=PLANE         PLANE is [<plane>:][<x>,<y>-]<w>x<h>\n"
272                 "  -f, --fb=FB               FB is [<w>x<h>][-][<4cc>]\n"
273                 "      --dmt                 Search for the given mode from DMT tables\n"
274                 "      --cea                 Search for the given mode from CEA tables\n"
275                 "      --flip                Do page flipping for each output\n"
276                 "      --sync                Synchronize page flipping\n"
277                 "\n"
278                 "<connector>, <crtc> and <plane> can be given by index (<idx>) or id (<id>).\n"
279                 "<connector> can also be given by name.\n"
280                 "\n"
281                 "Options can be given multiple times to set up multiple displays or planes.\n"
282                 "Options may apply to previous options, e.g. a plane will be set on a crtc set in\n"
283                 "an earlier option.\n"
284                 "If you omit parameters, testpat tries to guess what you mean\n"
285                 "\n"
286                 "Examples:\n"
287                 "\n"
288                 "Set eDP-1 mode to 1920x1080@60, show XR24 framebuffer on the crtc, and a 400x400 XB24 plane:\n"
289                 "    testpat -c eDP-1 -r 1920x1080@60 -f XR24 -p 400x400 -f XB24\n\n"
290                 "XR24 framebuffer on first connected connector in the default mode:\n"
291                 "    testpat -f XR24\n\n"
292                 "XR24 framebuffer on a 400x400 plane on the first connected connector in the default mode:\n"
293                 "    testpat -p 400x400 -f XR24\n\n"
294                 "Test pattern on the second connector with default mode:\n"
295                 "    testpat -c 1\n"
296                 ;
298 static void usage()
300         puts(usage_str);
303 enum class ObjectType
305         Connector,
306         Crtc,
307         Plane,
308         Framebuffer,
309 };
311 struct Arg
313         ObjectType type;
314         string arg;
315 };
317 static string s_device_path = "/dev/dri/card0";
319 static vector<Arg> parse_cmdline(int argc, char **argv)
321         vector<Arg> args;
323         OptionSet optionset = {
324                 Option("|device=",
325                 [&](string s)
326                 {
327                         s_device_path = s;
328                 }),
329                 Option("c|connector=",
330                 [&](string s)
331                 {
332                         args.push_back(Arg { ObjectType::Connector, s });
333                 }),
334                 Option("r|crtc=", [&](string s)
335                 {
336                         args.push_back(Arg { ObjectType::Crtc, s });
337                 }),
338                 Option("p|plane=", [&](string s)
339                 {
340                         args.push_back(Arg { ObjectType::Plane, s });
341                 }),
342                 Option("f|fb=", [&](string s)
343                 {
344                         args.push_back(Arg { ObjectType::Framebuffer, s });
345                 }),
346                 Option("|dmt", []()
347                 {
348                         s_use_dmt = true;
349                 }),
350                 Option("|cea", []()
351                 {
352                         s_use_cea = true;
353                 }),
354                 Option("|flip", []()
355                 {
356                         s_flip_mode = true;
357                         s_num_buffers = 2;
358                 }),
359                 Option("|sync", []()
360                 {
361                         s_flip_sync = true;
362                 }),
363                 Option("h|help", [&]()
364                 {
365                         usage();
366                         exit(-1);
367                 }),
368         };
370         optionset.parse(argc, argv);
372         if (optionset.params().size() > 0) {
373                 usage();
374                 exit(-1);
375         }
377         return args;
380 static vector<OutputInfo> setups_to_outputs(Card& card, const vector<Arg>& output_args)
382         vector<OutputInfo> outputs;
384         if (output_args.size() == 0) {
385                 // no output args, show a pattern on all screens
386                 for (auto& pipe : card.get_connected_pipelines()) {
387                         OutputInfo output = { };
388                         output.connector = pipe.connector;
389                         output.crtc = pipe.crtc;
390                         output.mode = output.connector->get_default_mode();
392                         output.fbs = get_default_fb(card, output.mode.hdisplay, output.mode.vdisplay);
394                         outputs.push_back(output);
395                 }
397                 return outputs;
398         }
400         OutputInfo* current_output = 0;
401         PlaneInfo* current_plane = 0;
403         for (auto& arg : output_args) {
404                 switch (arg.type) {
405                 case ObjectType::Connector:
406                 {
407                         outputs.push_back(OutputInfo { });
408                         current_output = &outputs.back();
410                         parse_connector(card, arg.arg, *current_output);
411                         current_plane = 0;
413                         break;
414                 }
416                 case ObjectType::Crtc:
417                 {
418                         if (!current_output) {
419                                 outputs.push_back(OutputInfo { });
420                                 current_output = &outputs.back();
421                         }
423                         if (!current_output->connector)
424                                 get_default_connector(card, *current_output);
426                         parse_crtc(card, arg.arg, *current_output);
428                         current_output->user_set_crtc = true;
430                         current_plane = 0;
432                         break;
433                 }
435                 case ObjectType::Plane:
436                 {
437                         if (!current_output) {
438                                 outputs.push_back(OutputInfo { });
439                                 current_output = &outputs.back();
440                         }
442                         if (!current_output->connector)
443                                 get_default_connector(card, *current_output);
445                         if (!current_output->crtc)
446                                 get_default_crtc(card, *current_output);
448                         current_output->planes.push_back(PlaneInfo { });
449                         current_plane = &current_output->planes.back();
451                         parse_plane(card, arg.arg, *current_output, *current_plane);
453                         break;
454                 }
456                 case ObjectType::Framebuffer:
457                 {
458                         if (!current_output) {
459                                 outputs.push_back(OutputInfo { });
460                                 current_output = &outputs.back();
461                         }
463                         if (!current_output->connector)
464                                 get_default_connector(card, *current_output);
466                         if (!current_output->crtc)
467                                 get_default_crtc(card, *current_output);
469                         int def_w, def_h;
471                         if (current_plane) {
472                                 def_w = current_plane->w;
473                                 def_h = current_plane->h;
474                         } else {
475                                 def_w = current_output->mode.hdisplay;
476                                 def_h = current_output->mode.vdisplay;
477                         }
479                         auto fbs = parse_fb(card, arg.arg, def_w, def_h);
481                         if (current_plane)
482                                 current_plane->fbs = fbs;
483                         else
484                                 current_output->fbs = fbs;
486                         break;
487                 }
488                 }
489         }
491         // create default framebuffers if needed
492         for (OutputInfo& o : outputs) {
493                 if (!o.crtc) {
494                         get_default_crtc(card, *current_output);
495                         o.user_set_crtc = true;
496                 }
498                 if (o.fbs.empty() && o.user_set_crtc)
499                         o.fbs = get_default_fb(card, o.mode.hdisplay, o.mode.vdisplay);
501                 for (PlaneInfo &p : o.planes) {
502                         if (p.fbs.empty())
503                                 p.fbs = get_default_fb(card, p.w, p.h);
504                 }
505         }
507         return outputs;
510 static std::string videomode_to_string(const Videomode& m)
512         string h = sformat("%u/%u/%u/%u", m.hdisplay, m.hfp(), m.hsw(), m.hbp());
513         string v = sformat("%u/%u/%u/%u", m.vdisplay, m.vfp(), m.vsw(), m.vbp());
515         return sformat("%s %.3f %s %s %u (%.2f) %#x %#x",
516                        m.name.c_str(),
517                        m.clock / 1000.0,
518                        h.c_str(), v.c_str(),
519                        m.vrefresh, m.calculated_vrefresh(),
520                        m.flags,
521                        m.type);
524 static void print_outputs(const vector<OutputInfo>& outputs)
526         for (unsigned i = 0; i < outputs.size(); ++i) {
527                 const OutputInfo& o = outputs[i];
529                 printf("Connector %u/@%u: %s\n", o.connector->idx(), o.connector->id(),
530                        o.connector->fullname().c_str());
531                 printf("  Crtc %u/@%u", o.crtc->idx(), o.crtc->id());
532                 if (o.primary_plane)
533                         printf(" (plane %u/@%u)", o.primary_plane->idx(), o.primary_plane->id());
534                 printf(": %s\n", videomode_to_string(o.mode).c_str());
535                 if (!o.fbs.empty()) {
536                         auto fb = o.fbs[0];
537                         printf("    Fb %u %ux%u-%s\n", fb->id(), fb->width(), fb->height(),
538                                PixelFormatToFourCC(fb->format()).c_str());
539                 }
541                 for (unsigned j = 0; j < o.planes.size(); ++j) {
542                         const PlaneInfo& p = o.planes[j];
543                         auto fb = p.fbs[0];
544                         printf("  Plane %u/@%u: %u,%u-%ux%u\n", p.plane->idx(), p.plane->id(),
545                                p.x, p.y, p.w, p.h);
546                         printf("    Fb %u %ux%u-%s\n", fb->id(), fb->width(), fb->height(),
547                                PixelFormatToFourCC(fb->format()).c_str());
548                 }
549         }
552 static void draw_test_patterns(const vector<OutputInfo>& outputs)
554         for (const OutputInfo& o : outputs) {
555                 for (auto fb : o.fbs)
556                         draw_test_pattern(*fb);
558                 for (const PlaneInfo& p : o.planes)
559                         for (auto fb : p.fbs)
560                                 draw_test_pattern(*fb);
561         }
564 static void set_crtcs_n_planes_legacy(Card& card, const vector<OutputInfo>& outputs)
566         for (const OutputInfo& o : outputs) {
567                 auto conn = o.connector;
568                 auto crtc = o.crtc;
570                 if (!o.fbs.empty()) {
571                         auto fb = o.fbs[0];
572                         int r = crtc->set_mode(conn, *fb, o.mode);
573                         if (r)
574                                 printf("crtc->set_mode() failed for crtc %u: %s\n",
575                                        crtc->id(), strerror(-r));
576                 }
578                 for (const PlaneInfo& p : o.planes) {
579                         auto fb = p.fbs[0];
580                         int r = crtc->set_plane(p.plane, *fb,
581                                                 p.x, p.y, p.w, p.h,
582                                                 0, 0, fb->width(), fb->height());
583                         if (r)
584                                 printf("crtc->set_plane() failed for plane %u: %s\n",
585                                        p.plane->id(), strerror(-r));
586                 }
587         }
590 static void set_crtcs_n_planes(Card& card, const vector<OutputInfo>& outputs)
592         // Keep blobs here so that we keep ref to them until we have committed the req
593         vector<unique_ptr<Blob>> blobs;
595         AtomicReq req(card);
597         for (const OutputInfo& o : outputs) {
598                 auto conn = o.connector;
599                 auto crtc = o.crtc;
601                 if (!o.fbs.empty()) {
602                         auto fb = o.fbs[0];
604                         blobs.emplace_back(o.mode.to_blob(card));
605                         Blob* mode_blob = blobs.back().get();
607                         req.add(conn, {
608                                         { "CRTC_ID", crtc->id() },
609                                 });
611                         req.add(crtc, {
612                                         { "ACTIVE", 1 },
613                                         { "MODE_ID", mode_blob->id() },
614                                 });
616                         req.add(o.primary_plane, {
617                                         { "FB_ID", fb->id() },
618                                         { "CRTC_ID", crtc->id() },
619                                         { "SRC_X", 0 << 16 },
620                                         { "SRC_Y", 0 << 16 },
621                                         { "SRC_W", fb->width() << 16 },
622                                         { "SRC_H", fb->height() << 16 },
623                                         { "CRTC_X", 0 },
624                                         { "CRTC_Y", 0 },
625                                         { "CRTC_W", fb->width() },
626                                         { "CRTC_H", fb->height() },
627                                 });
628                 }
630                 for (const PlaneInfo& p : o.planes) {
631                         auto fb = p.fbs[0];
633                         req.add(p.plane, {
634                                         { "FB_ID", fb->id() },
635                                         { "CRTC_ID", crtc->id() },
636                                         { "SRC_X", 0 << 16 },
637                                         { "SRC_Y", 0 << 16 },
638                                         { "SRC_W", fb->width() << 16 },
639                                         { "SRC_H", fb->height() << 16 },
640                                         { "CRTC_X", p.x },
641                                         { "CRTC_Y", p.y },
642                                         { "CRTC_W", p.w },
643                                         { "CRTC_H", p.h },
644                                 });
645                 }
646         }
648         int r;
650         r = req.test(true);
651         if (r)
652                 EXIT("Atomic test failed: %d\n", r);
654         r = req.commit_sync(true);
655         if (r)
656                 EXIT("Atomic commit failed: %d\n", r);
659 class FlipState : private PageFlipHandlerBase
661 public:
662         FlipState(Card& card, const string& name, vector<const OutputInfo*> outputs)
663                 : m_card(card), m_name(name), m_outputs(outputs)
664         {
665         }
667         void start_flipping()
668         {
669                 m_prev_frame = m_prev_print = std::chrono::steady_clock::now();
670                 m_slowest_frame = std::chrono::duration<float>::min();
671                 m_frame_num = 0;
672                 queue_next();
673         }
675 private:
676         void handle_page_flip(uint32_t frame, double time)
677         {
678                 m_frame_num++;
680                 auto now = std::chrono::steady_clock::now();
682                 std::chrono::duration<float> diff = now - m_prev_frame;
683                 if (diff > m_slowest_frame)
684                         m_slowest_frame = diff;
686                 if (m_frame_num  % 100 == 0) {
687                         std::chrono::duration<float> fsec = now - m_prev_print;
688                         printf("Connector %s: fps %f, slowest %.2f ms\n",
689                                m_name.c_str(),
690                                100.0 / fsec.count(),
691                                m_slowest_frame.count() * 1000);
692                         m_prev_print = now;
693                         m_slowest_frame = std::chrono::duration<float>::min();
694                 }
696                 m_prev_frame = now;
698                 queue_next();
699         }
701         static unsigned get_bar_pos(DumbFramebuffer* fb, unsigned frame_num)
702         {
703                 return (frame_num * bar_speed) % (fb->width() - bar_width + 1);
704         }
706         static void draw_bar(DumbFramebuffer* fb, unsigned frame_num)
707         {
708                 int old_xpos = frame_num < s_num_buffers ? -1 : get_bar_pos(fb, frame_num - s_num_buffers);
709                 int new_xpos = get_bar_pos(fb, frame_num);
711                 draw_color_bar(*fb, old_xpos, new_xpos, bar_width);
712                 draw_text(*fb, fb->width() / 2, 0, to_string(frame_num), RGB(255, 255, 255));
713         }
715         static void do_flip_output(AtomicReq& req, unsigned frame_num, const OutputInfo& o)
716         {
717                 unsigned cur = frame_num % s_num_buffers;
719                 if (!o.fbs.empty()) {
720                         auto fb = o.fbs[cur];
722                         draw_bar(fb, frame_num);
724                         req.add(o.primary_plane, {
725                                         { "FB_ID", fb->id() },
726                                 });
727                 }
729                 for (const PlaneInfo& p : o.planes) {
730                         auto fb = p.fbs[cur];
732                         draw_bar(fb, frame_num);
734                         req.add(p.plane, {
735                                         { "FB_ID", fb->id() },
736                                 });
737                 }
738         }
740         void do_flip_output_legacy(unsigned frame_num, const OutputInfo& o)
741         {
742                 unsigned cur = frame_num % s_num_buffers;
744                 if (!o.fbs.empty()) {
745                         auto fb = o.fbs[cur];
747                         draw_bar(fb, frame_num);
749                         int r = o.crtc->page_flip(*fb, this);
750                         ASSERT(r == 0);
751                 }
753                 for (const PlaneInfo& p : o.planes) {
754                         auto fb = p.fbs[cur];
756                         draw_bar(fb, frame_num);
758                         int r = o.crtc->set_plane(p.plane, *fb,
759                                                   p.x, p.y, p.w, p.h,
760                                                   0, 0, fb->width(), fb->height());
761                         ASSERT(r == 0);
762                 }
763         }
765         void queue_next()
766         {
767                 if (m_card.has_atomic()) {
768                         AtomicReq req(m_card);
770                         for (auto o : m_outputs)
771                                 do_flip_output(req, m_frame_num, *o);
773                         int r = req.commit(this);
774                         if (r)
775                                 EXIT("Flip commit failed: %d\n", r);
776                 } else {
777                         ASSERT(m_outputs.size() == 1);
778                         do_flip_output_legacy(m_frame_num, *m_outputs[0]);
779                 }
780         }
782         Card& m_card;
783         string m_name;
784         vector<const OutputInfo*> m_outputs;
785         unsigned m_frame_num;
787         chrono::steady_clock::time_point m_prev_print;
788         chrono::steady_clock::time_point m_prev_frame;
789         chrono::duration<float> m_slowest_frame;
791         static const unsigned bar_width = 20;
792         static const unsigned bar_speed = 8;
793 };
795 static void main_flip(Card& card, const vector<OutputInfo>& outputs)
797         fd_set fds;
799         FD_ZERO(&fds);
801         int fd = card.fd();
803         vector<unique_ptr<FlipState>> flipstates;
805         if (!s_flip_sync) {
806                 for (const OutputInfo& o : outputs) {
807                         auto fs = unique_ptr<FlipState>(new FlipState(card, to_string(o.connector->idx()), { &o }));
808                         flipstates.push_back(move(fs));
809                 }
810         } else {
811                 vector<const OutputInfo*> ois;
813                 string name;
814                 for (const OutputInfo& o : outputs) {
815                         name += to_string(o.connector->idx()) + ",";
816                         ois.push_back(&o);
817                 }
819                 auto fs = unique_ptr<FlipState>(new FlipState(card, name, ois));
820                 flipstates.push_back(move(fs));
821         }
823         for (unique_ptr<FlipState>& fs : flipstates)
824                 fs->start_flipping();
826         while (true) {
827                 int r;
829                 FD_SET(0, &fds);
830                 FD_SET(fd, &fds);
832                 r = select(fd + 1, &fds, NULL, NULL, NULL);
833                 if (r < 0) {
834                         fprintf(stderr, "select() failed with %d: %m\n", errno);
835                         break;
836                 } else if (FD_ISSET(0, &fds)) {
837                         fprintf(stderr, "Exit due to user-input\n");
838                         break;
839                 } else if (FD_ISSET(fd, &fds)) {
840                         card.call_page_flip_handlers();
841                 }
842         }
845 int main(int argc, char **argv)
847         vector<Arg> output_args = parse_cmdline(argc, argv);
849         Card card(s_device_path);
851         if (!card.has_atomic() && s_flip_sync)
852                 EXIT("Synchronized flipping requires atomic modesetting");
854         vector<OutputInfo> outputs = setups_to_outputs(card, output_args);
856         if (card.has_atomic()) {
857                 for (OutputInfo& o : outputs) {
858                         o.primary_plane = o.crtc->get_primary_plane();
860                         if (!o.fbs.empty() && !o.primary_plane)
861                                 EXIT("Could not get primary plane for crtc '%u'", o.crtc->id());
862                 }
863         }
865         if (!s_flip_mode)
866                 draw_test_patterns(outputs);
868         print_outputs(outputs);
870         if (card.has_atomic())
871                 set_crtcs_n_planes(card, outputs);
872         else
873                 set_crtcs_n_planes_legacy(card, outputs);
875         printf("press enter to exit\n");
877         if (s_flip_mode)
878                 main_flip(card, outputs);
879         else
880                 getchar();