#include #include #include "cube.h" #include "cube-egl.h" #include "cube-gles2.h" #include using namespace std; static void main_loop(Display* dpy, xcb_connection_t *c, xcb_window_t window, uint32_t width, uint32_t height) { EglState egl(dpy); EglSurface surface(egl, (void*)(uintptr_t)window); GlScene scene; scene.set_viewport(width, height); unsigned framenum = 0; surface.make_current(); surface.swap_buffers(); bool need_exit = false; xcb_generic_event_t *event; while (true) { while ((event = xcb_poll_for_event (c))) { bool handled = false; uint8_t response_type = event->response_type & ~0x80; switch (response_type) { case XCB_EXPOSE: { handled = true; break; } case XCB_KEY_PRESS: { handled = true; xcb_key_press_event_t *kp = (xcb_key_press_event_t *)event; if (kp->detail == 24 || kp->detail == 9) { printf("Exit due to keypress\n"); need_exit = true; } break; } } if (!handled) { // Check if a custom XEvent constructor was registered in xlib for this event type, and call it discarding the constructed XEvent if any. // XESetWireToEvent might be used by libraries to intercept messages from the X server e.g. the OpenGL lib waiting for DRI2 events. XLockDisplay(dpy); Bool (*proc)(Display*, XEvent*, xEvent*) = XESetWireToEvent(dpy, response_type, NULL); if (proc) { XESetWireToEvent(dpy, response_type, proc); XEvent dummy; event->sequence = LastKnownRequestProcessed(dpy); proc(dpy, &dummy, (xEvent*)event); } XUnlockDisplay(dpy); } free(event); } if (s_num_frames && framenum >= s_num_frames) need_exit = true; if (need_exit) break; // this should be in XCB_EXPOSE, but we don't get the event after swaps... scene.draw(framenum++); surface.swap_buffers(); } } void main_x11() { Display* dpy = XOpenDisplay(NULL); FAIL_IF(!dpy, "Failed to connect to the X server"); xcb_connection_t *c = XGetXCBConnection(dpy); /* Acquire event queue ownership */ XSetEventQueueOwner(dpy, XCBOwnsEventQueue); /* Get the first screen */ const xcb_setup_t *setup = xcb_get_setup (c); xcb_screen_t *screen = xcb_setup_roots_iterator (setup).data; /* Create the window */ uint32_t width; uint32_t height; if (s_fullscreen) { width = screen->width_in_pixels; height = screen->height_in_pixels; } else { width = 600; height = 600; } const uint32_t xcb_window_attrib_mask = XCB_CW_OVERRIDE_REDIRECT | XCB_CW_EVENT_MASK; const uint32_t xcb_window_attrib_list[] = { // OVERRIDE_REDIRECT 0, // EVENT_MASK XCB_EVENT_MASK_EXPOSURE | XCB_EVENT_MASK_KEY_PRESS, }; xcb_window_t window = xcb_generate_id (c); xcb_create_window (c, /* Connection */ XCB_COPY_FROM_PARENT, /* depth (same as root)*/ window, /* window Id */ screen->root, /* parent window */ 0, 0, /* x, y */ width, height, /* width, height */ 0, /* border_width */ XCB_WINDOW_CLASS_INPUT_OUTPUT, /* class */ screen->root_visual, /* visual */ xcb_window_attrib_mask, xcb_window_attrib_list); if (s_fullscreen) { const char *net_wm_state = "_NET_WM_STATE"; const char *net_wm_state_fullscreen = "_NET_WM_STATE_FULLSCREEN"; xcb_intern_atom_cookie_t cookie = xcb_intern_atom(c, 0, strlen(net_wm_state), net_wm_state); xcb_intern_atom_reply_t* reply = xcb_intern_atom_reply(c, cookie, 0); xcb_intern_atom_cookie_t cookie2 = xcb_intern_atom(c, 0, strlen(net_wm_state_fullscreen), net_wm_state_fullscreen); xcb_intern_atom_reply_t* reply2 = xcb_intern_atom_reply(c, cookie2, 0); xcb_change_property(c, XCB_PROP_MODE_REPLACE, window, reply->atom, XCB_ATOM_ATOM , 32, 1, (void*)&reply2->atom); } xcb_map_window (c, window); xcb_flush (c); main_loop(dpy, c, window, width, height); xcb_flush(c); xcb_unmap_window(c, window); xcb_destroy_window(c, window); XCloseDisplay(dpy); }