#pragma once #include #include #include #include "decls.h" #include "pipeline.h" namespace kms { class Card { friend class Framebuffer; public: Card(); Card(const std::string& device); ~Card(); Card(const Card& other) = delete; Card& operator=(const Card& other) = delete; int fd() const { return m_fd; } void drop_master(); Connector* get_first_connected_connector() const; DrmObject* get_object(uint32_t id) const; Connector* get_connector(uint32_t id) const; Crtc* get_crtc(uint32_t id) const; Encoder* get_encoder(uint32_t id) const; Plane* get_plane(uint32_t id) const; Property* get_prop(uint32_t id) const; Property* get_prop(const std::string& name) const; bool master() const { return m_master; } bool has_atomic() const { return m_has_atomic; } bool has_has_universal_planes() const { return m_has_universal_planes; } const std::vector get_connectors() const { return m_connectors; } const std::vector get_encoders() const { return m_encoders; } const std::vector get_crtcs() const { return m_crtcs; } const std::vector get_planes() const { return m_planes; } const std::vector get_properties() const { return m_properties; } const std::vector get_objects() const; std::vector get_connected_pipelines(); void call_page_flip_handlers(); private: void restore_modes(); std::map m_obmap; std::vector m_connectors; std::vector m_encoders; std::vector m_crtcs; std::vector m_planes; std::vector m_properties; std::vector m_framebuffers; int m_fd; bool m_master; bool m_has_atomic; bool m_has_universal_planes; }; }