#include #include #include #include #include #include "kms++.h" using namespace std; namespace kms { DrmObject::DrmObject(Card& card, uint32_t object_type) :m_card(card), m_id(-1), m_object_type(object_type) { } DrmObject::DrmObject(Card& card, uint32_t id, uint32_t object_type, uint32_t idx) :m_card(card), m_id(id), m_object_type(object_type), m_idx(idx) { refresh_props(); } DrmObject::~DrmObject() { } void DrmObject::refresh_props() { auto props = drmModeObjectGetProperties(card().fd(), this->id(), this->object_type()); if (props == nullptr) return; for (unsigned i = 0; i < props->count_props; ++i) { uint32_t prop_id = props->props[i]; uint64_t prop_value = props->prop_values[i]; m_prop_values[prop_id] = prop_value; } drmModeFreeObjectProperties(props); } uint64_t DrmObject::get_prop_value(uint32_t id) const { return m_prop_values.at(id); } uint64_t DrmObject::get_prop_value(const string& name) const { for (auto pair : m_prop_values) { auto prop = card().get_prop(pair.first); if (name == prop->name()) return m_prop_values.at(prop->id()); } throw invalid_argument(string(name) + ": property not found"); } void DrmObject::set_id(uint32_t id) { m_id = id; } }