#include #include #include #include #include #include #include #include using namespace std; using namespace kms; static void main_loop(Card& card); class Flipper { public: Flipper(Card& card, unsigned width, unsigned height) : m_current(0), m_bar_xpos(0) { auto format = PixelFormat::XRGB8888; m_fbs[0] = new DumbFramebuffer(card, width, height, format); m_fbs[1] = new DumbFramebuffer(card, width, height, format); } ~Flipper() { delete m_fbs[0]; delete m_fbs[1]; } Framebuffer* get_next() { m_current ^= 1; const int bar_width = 20; const int bar_speed = 8; auto fb = m_fbs[m_current]; int current_xpos = m_bar_xpos; int old_xpos = (current_xpos + (fb->width() - bar_width - bar_speed)) % (fb->width() - bar_width); int new_xpos = (current_xpos + bar_speed) % (fb->width() - bar_width); draw_color_bar(*fb, old_xpos, new_xpos, bar_width); m_bar_xpos = new_xpos; return fb; } private: DumbFramebuffer* m_fbs[2]; int m_current; int m_bar_xpos; }; class OutputFlipHandler : private PageFlipHandlerBase { public: OutputFlipHandler(Connector* conn, Crtc* crtc, const Videomode& mode) : m_connector(conn), m_crtc(crtc), m_mode(mode), m_flipper(conn->card(), mode.hdisplay, mode.vdisplay), m_plane(0), m_plane_flipper(0) { } OutputFlipHandler(Connector* conn, Crtc* crtc, const Videomode& mode, Plane* plane, unsigned pwidth, unsigned pheight) : m_connector(conn), m_crtc(crtc), m_mode(mode), m_flipper(conn->card(), mode.hdisplay, mode.vdisplay), m_plane(plane) { m_plane_flipper = new Flipper(conn->card(), pwidth, pheight); } ~OutputFlipHandler() { if (m_plane_flipper) delete m_plane_flipper; } OutputFlipHandler(const OutputFlipHandler& other) = delete; OutputFlipHandler& operator=(const OutputFlipHandler& other) = delete; void set_mode() { auto fb = m_flipper.get_next(); int r = m_crtc->set_mode(m_connector, *fb, m_mode); ASSERT(r == 0); if (m_crtc->card().has_atomic()) m_root_plane = m_crtc->get_primary_plane(); if (m_plane) { auto planefb = m_plane_flipper->get_next(); r = m_crtc->set_plane(m_plane, *planefb, 0, 0, planefb->width(), planefb->height(), 0, 0, planefb->width(), planefb->height()); ASSERT(r == 0); } } void start_flipping() { m_time_last = m_t1 = std::chrono::steady_clock::now(); m_slowest_frame = std::chrono::duration::min(); m_frame_num = 0; queue_next(); } private: void handle_page_flip(uint32_t frame, double time) { ++m_frame_num; auto now = std::chrono::steady_clock::now(); std::chrono::duration diff = now - m_time_last; if (diff > m_slowest_frame) m_slowest_frame = diff; if (m_frame_num % 100 == 0) { std::chrono::duration fsec = now - m_t1; printf("Output %d: fps %f, slowest %.2f ms\n", m_connector->idx(), 100.0 / fsec.count(), m_slowest_frame.count() * 1000); m_t1 = now; m_slowest_frame = std::chrono::duration::min(); } m_time_last = now; queue_next(); } void queue_next() { auto crtc = m_crtc; auto& card = crtc->card(); auto fb = m_flipper.get_next(); Framebuffer* planefb = m_plane ? m_plane_flipper->get_next() : 0; if (card.has_atomic()) { int r; AtomicReq req(card); req.add(m_root_plane, "FB_ID", fb->id()); if (m_plane) req.add(m_plane, "FB_ID", planefb->id()); r = req.test(); ASSERT(r == 0); r = req.commit(this); ASSERT(r == 0); } else { int r = crtc->page_flip(*fb, this); ASSERT(r == 0); if (m_plane) { r = m_crtc->set_plane(m_plane, *planefb, 0, 0, planefb->width(), planefb->height(), 0, 0, planefb->width(), planefb->height()); ASSERT(r == 0); } } } private: Connector* m_connector; Crtc* m_crtc; Videomode m_mode; Plane* m_root_plane; int m_frame_num; chrono::steady_clock::time_point m_t1; chrono::steady_clock::time_point m_time_last; chrono::duration m_slowest_frame; Flipper m_flipper; Plane* m_plane; Flipper* m_plane_flipper; }; int main() { Card card; if (card.master() == false) printf("Not DRM master, modeset may fail\n"); vector outputs; for (auto pipe : card.get_connected_pipelines()) { auto conn = pipe.connector; auto crtc = pipe.crtc; auto mode = conn->get_default_mode(); Plane* plane = 0; #if 0 // disable the plane for now for (Plane* p : crtc->get_possible_planes()) { if (p->plane_type() == PlaneType::Overlay) { plane = p; break; } } #endif OutputFlipHandler* output; if (plane) output = new OutputFlipHandler(conn, crtc, mode, plane, 500, 400); else output = new OutputFlipHandler(conn, crtc, mode); outputs.push_back(output); } for(auto out : outputs) out->set_mode(); for(auto out : outputs) out->start_flipping(); main_loop(card); for(auto out : outputs) delete out; } static void main_loop(Card& card) { fd_set fds; FD_ZERO(&fds); int fd = card.fd(); printf("press enter to exit\n"); while (true) { int r; FD_SET(0, &fds); FD_SET(fd, &fds); r = select(fd + 1, &fds, NULL, NULL, NULL); if (r < 0) { fprintf(stderr, "select() failed with %d: %m\n", errno); break; } else if (FD_ISSET(0, &fds)) { fprintf(stderr, "exit due to user-input\n"); break; } else if (FD_ISSET(fd, &fds)) { card.call_page_flip_handlers(); } } }