#include #include #include #include #include #include #include #include #include #include #include #include #include #define CAMERA_BUF_QUEUE_SIZE 3 #define MAX_CAMERA 9 using namespace std; using namespace kms; enum class BufferProvider { DRM, V4L2, }; class CameraPipeline { public: CameraPipeline(int cam_fd, Card& card, Crtc* crtc, Plane* plane, uint32_t x, uint32_t y, uint32_t iw, uint32_t ih, PixelFormat pixfmt, BufferProvider buffer_provider); ~CameraPipeline(); CameraPipeline(const CameraPipeline& other) = delete; CameraPipeline& operator=(const CameraPipeline& other) = delete; void show_next_frame(AtomicReq &req); int fd() const { return m_fd; } void start_streaming(); private: ExtFramebuffer* GetExtFrameBuffer(Card& card, uint32_t i, PixelFormat pixfmt); int m_fd; /* camera file descriptor */ Crtc* m_crtc; Plane* m_plane; BufferProvider m_buffer_provider; vector m_fb; /* framebuffers for DRM buffers */ vector m_extfb; /* framebuffers for V4L2 buffers */ int m_prev_fb_index; uint32_t m_in_width, m_in_height; /* camera capture resolution */ /* image properties for display */ uint32_t m_out_width, m_out_height; uint32_t m_out_x, m_out_y; }; static int buffer_export(int v4lfd, enum v4l2_buf_type bt, uint32_t index, int *dmafd) { struct v4l2_exportbuffer expbuf; memset(&expbuf, 0, sizeof(expbuf)); expbuf.type = bt; expbuf.index = index; if (ioctl(v4lfd, VIDIOC_EXPBUF, &expbuf) == -1) { perror("VIDIOC_EXPBUF"); return -1; } *dmafd = expbuf.fd; return 0; } ExtFramebuffer* CameraPipeline::GetExtFrameBuffer(Card& card, uint32_t i, PixelFormat pixfmt) { int r, dmafd; r = buffer_export(m_fd, V4L2_BUF_TYPE_VIDEO_CAPTURE, i, &dmafd); ASSERT(r == 0); uint32_t handle; r = drmPrimeFDToHandle(card.fd(), dmafd, &handle); ASSERT(r == 0); const PixelFormatInfo& format_info = get_pixel_format_info(pixfmt); ASSERT(format_info.num_planes == 1); uint32_t handles[4] { handle }; uint32_t pitches[4] { m_in_width * (format_info.planes[0].bitspp / 8) }; uint32_t offsets[4] { }; return new ExtFramebuffer(card, m_in_width, m_in_height, pixfmt, handles, pitches, offsets); } bool inline better_size(struct v4l2_frmsize_discrete* v4ldisc, uint32_t iw, uint32_t ih, uint32_t best_w, uint32_t best_h) { if (v4ldisc->width <= iw && v4ldisc->height <= ih && (v4ldisc->width >= best_w || v4ldisc->height >= best_h)) return true; return false; } CameraPipeline::CameraPipeline(int cam_fd, Card& card, Crtc *crtc, Plane* plane, uint32_t x, uint32_t y, uint32_t iw, uint32_t ih, PixelFormat pixfmt, BufferProvider buffer_provider) : m_fd(cam_fd), m_crtc(crtc), m_buffer_provider(buffer_provider), m_prev_fb_index(-1) { int r; uint32_t best_w = 320; uint32_t best_h = 240; struct v4l2_frmsizeenum v4lfrms = { }; v4lfrms.pixel_format = (uint32_t)pixfmt; while (ioctl(m_fd, VIDIOC_ENUM_FRAMESIZES, &v4lfrms) == 0) { if (v4lfrms.type == V4L2_FRMSIZE_TYPE_DISCRETE) { if (better_size(&v4lfrms.discrete, iw, ih, best_w, best_h)) { best_w = v4lfrms.discrete.width; best_h = v4lfrms.discrete.height; } } else { break; } v4lfrms.index++; }; m_out_width = m_in_width = best_w; m_out_height = m_in_height = best_h; /* Move it to the middle of the requested area */ m_out_x = x + iw / 2 - m_out_width / 2; m_out_y = y + ih / 2 - m_out_height / 2; struct v4l2_format v4lfmt = { }; v4lfmt.type = V4L2_BUF_TYPE_VIDEO_CAPTURE; r = ioctl(m_fd, VIDIOC_G_FMT, &v4lfmt); ASSERT(r == 0); v4lfmt.fmt.pix.pixelformat = (uint32_t)pixfmt; v4lfmt.fmt.pix.width = m_in_width; v4lfmt.fmt.pix.height = m_in_height; r = ioctl(m_fd, VIDIOC_S_FMT, &v4lfmt); ASSERT(r == 0); uint32_t v4l_mem; if (m_buffer_provider == BufferProvider::V4L2) v4l_mem = V4L2_MEMORY_MMAP; else v4l_mem = V4L2_MEMORY_DMABUF; struct v4l2_requestbuffers v4lreqbuf = { }; v4lreqbuf.type = V4L2_BUF_TYPE_VIDEO_CAPTURE; v4lreqbuf.memory = v4l_mem; v4lreqbuf.count = CAMERA_BUF_QUEUE_SIZE; r = ioctl(m_fd, VIDIOC_REQBUFS, &v4lreqbuf); ASSERT(r == 0); ASSERT(v4lreqbuf.count == CAMERA_BUF_QUEUE_SIZE); struct v4l2_buffer v4lbuf = { }; v4lbuf.type = V4L2_BUF_TYPE_VIDEO_CAPTURE; v4lbuf.memory = v4l_mem; for (unsigned i = 0; i < CAMERA_BUF_QUEUE_SIZE; i++) { DumbFramebuffer *fb = NULL; ExtFramebuffer *extfb = NULL; if (m_buffer_provider == BufferProvider::V4L2) extfb = GetExtFrameBuffer(card, i, pixfmt); else fb = new DumbFramebuffer(card, m_in_width, m_in_height, pixfmt); v4lbuf.index = i; if (m_buffer_provider == BufferProvider::DRM) v4lbuf.m.fd = fb->prime_fd(0); r = ioctl(m_fd, VIDIOC_QBUF, &v4lbuf); ASSERT(r == 0); if (m_buffer_provider == BufferProvider::V4L2) m_extfb.push_back(extfb); else m_fb.push_back(fb); } m_plane = plane; // Do initial plane setup with first fb, so that we only need to // set the FB when page flipping AtomicReq req(card); Framebuffer *fb; if (m_buffer_provider == BufferProvider::V4L2) fb = m_extfb[0]; else fb = m_fb[0]; req.add(m_plane, "CRTC_ID", m_crtc->id()); req.add(m_plane, "FB_ID", fb->id()); req.add(m_plane, "CRTC_X", m_out_x); req.add(m_plane, "CRTC_Y", m_out_y); req.add(m_plane, "CRTC_W", m_out_width); req.add(m_plane, "CRTC_H", m_out_height); req.add(m_plane, "SRC_X", 0); req.add(m_plane, "SRC_Y", 0); req.add(m_plane, "SRC_W", m_in_width << 16); req.add(m_plane, "SRC_H", m_in_height << 16); r = req.commit_sync(); FAIL_IF(r, "initial plane setup failed"); } CameraPipeline::~CameraPipeline() { for (unsigned i = 0; i < m_fb.size(); i++) delete m_fb[i]; for (unsigned i = 0; i < m_extfb.size(); i++) delete m_extfb[i]; ::close(m_fd); } void CameraPipeline::start_streaming() { enum v4l2_buf_type type = V4L2_BUF_TYPE_VIDEO_CAPTURE; int r = ioctl(m_fd, VIDIOC_STREAMON, &type); FAIL_IF(r, "Failed to enable camera stream: %d", r); } void CameraPipeline::show_next_frame(AtomicReq& req) { int r; uint32_t v4l_mem; if (m_buffer_provider == BufferProvider::V4L2) v4l_mem = V4L2_MEMORY_MMAP; else v4l_mem = V4L2_MEMORY_DMABUF; struct v4l2_buffer v4l2buf = { }; v4l2buf.type = V4L2_BUF_TYPE_VIDEO_CAPTURE; v4l2buf.memory = v4l_mem; r = ioctl(m_fd, VIDIOC_DQBUF, &v4l2buf); if (r != 0) { printf("VIDIOC_DQBUF ioctl failed with %d\n", errno); return; } unsigned fb_index = v4l2buf.index; Framebuffer *fb; if (m_buffer_provider == BufferProvider::V4L2) fb = m_extfb[fb_index]; else fb = m_fb[fb_index]; req.add(m_plane, "FB_ID", fb->id()); if (m_prev_fb_index >= 0) { memset(&v4l2buf, 0, sizeof(v4l2buf)); v4l2buf.type = V4L2_BUF_TYPE_VIDEO_CAPTURE; v4l2buf.memory = v4l_mem; v4l2buf.index = m_prev_fb_index; if (m_buffer_provider == BufferProvider::DRM) v4l2buf.m.fd = m_fb[m_prev_fb_index]->prime_fd(0); r = ioctl(m_fd, VIDIOC_QBUF, &v4l2buf); ASSERT(r == 0); } m_prev_fb_index = fb_index; } static bool is_capture_dev(int fd) { struct v4l2_capability cap = { }; int r = ioctl(fd, VIDIOC_QUERYCAP, &cap); ASSERT(r == 0); return cap.capabilities & V4L2_CAP_VIDEO_CAPTURE; } std::vector glob(const std::string& pat) { glob_t glob_result; glob(pat.c_str(), 0, NULL, &glob_result); vector ret; for(unsigned i = 0; i < glob_result.gl_pathc; ++i) ret.push_back(string(glob_result.gl_pathv[i])); globfree(&glob_result); return ret; } static const char* usage_str = "Usage: kmscapture [OPTIONS]\n\n" "Options:\n" " -s, --single Single camera mode. Open only /dev/video0\n" " --buffer-type= Use DRM or V4L provided buffers. Default: DRM\n" " -h, --help Print this help\n" ; int main(int argc, char** argv) { BufferProvider buffer_provider = BufferProvider::DRM; bool single_cam = false; OptionSet optionset = { Option("s|single", [&]() { single_cam = true; }), Option("|buffer-type=", [&](string s) { if (s == "v4l") buffer_provider = BufferProvider::V4L2; else if (s == "drm") buffer_provider = BufferProvider::DRM; else FAIL("Invalid buffer provider: %s", s.c_str()); }), Option("h|help", [&]() { puts(usage_str); exit(-1); }), }; optionset.parse(argc, argv); if (optionset.params().size() > 0) { puts(usage_str); exit(-1); } auto pixfmt = PixelFormat::YUYV; Card card; auto conn = card.get_first_connected_connector(); auto crtc = conn->get_current_crtc(); printf("Display: %dx%d\n", crtc->width(), crtc->height()); printf("Buffer provider: %s\n", buffer_provider == BufferProvider::V4L2? "V4L" : "DRM"); vector camera_fds; for (string vidpath : glob("/dev/video*")) { int fd = ::open(vidpath.c_str(), O_RDWR | O_NONBLOCK); if (fd < 0) continue; if (!is_capture_dev(fd)) { close(fd); continue; } camera_fds.push_back(fd); if (single_cam) break; } FAIL_IF(camera_fds.size() == 0, "No cameras found"); vector available_planes; for (Plane* p : crtc->get_possible_planes()) { if (p->plane_type() != PlaneType::Overlay) continue; if (!p->supports_format(pixfmt)) continue; available_planes.push_back(p); } FAIL_IF(available_planes.size() < camera_fds.size(), "Not enough video planes for cameras"); uint32_t plane_w = crtc->width() / camera_fds.size(); vector cameras; for (unsigned i = 0; i < camera_fds.size(); ++i) { int cam_fd = camera_fds[i]; Plane* plane = available_planes[i]; auto cam = new CameraPipeline(cam_fd, card, crtc, plane, i * plane_w, 0, plane_w, crtc->height(), pixfmt, buffer_provider); cameras.push_back(cam); } unsigned nr_cameras = cameras.size(); vector fds(nr_cameras + 1); for (unsigned i = 0; i < nr_cameras; i++) { fds[i].fd = cameras[i]->fd(); fds[i].events = POLLIN; } fds[nr_cameras].fd = 0; fds[nr_cameras].events = POLLIN; for (auto cam : cameras) cam->start_streaming(); while (true) { int r = poll(fds.data(), nr_cameras + 1, -1); ASSERT(r > 0); if (fds[nr_cameras].revents != 0) break; AtomicReq req(card); for (unsigned i = 0; i < nr_cameras; i++) { if (!fds[i].revents) continue; cameras[i]->show_next_frame(req); fds[i].revents = 0; } r = req.test(); FAIL_IF(r, "Atomic commit failed: %d", r); req.commit_sync(); } for (auto cam : cameras) delete cam; }