diff --git a/kmscube/cube-x11.cpp b/kmscube/cube-x11.cpp
index 82ef414b46f400a4f782fe7192c2d7ff97e0b6cb..dde4f61148214347522c0561fa2cc744fb2ad566 100644 (file)
--- a/kmscube/cube-x11.cpp
+++ b/kmscube/cube-x11.cpp
#include <X11/Xlib-xcb.h>
+#include <X11/Xlibint.h>
#include "cube.h"
#include "cube-egl.h"
#include "cube-gles2.h"
-#include "test.h"
+#include <kms++util.h>
using namespace std;
+static void main_loop(Display* dpy, xcb_connection_t *c, xcb_window_t window, uint32_t width, uint32_t height)
+{
+ EglState egl(dpy);
+ EglSurface surface(egl, (void*)(uintptr_t)window);
+ GlScene scene;
+
+ scene.set_viewport(width, height);
+
+ unsigned framenum = 0;
+
+ surface.make_current();
+ surface.swap_buffers();
+
+ bool need_exit = false;
+
+ xcb_generic_event_t *event;
+ while (true) {
+
+ while ((event = xcb_poll_for_event (c))) {
+ bool handled = false;
+ uint8_t response_type = event->response_type & ~0x80;
+
+ switch (response_type) {
+ case XCB_EXPOSE: {
+ handled = true;
+ break;
+ }
+ case XCB_KEY_PRESS: {
+ handled = true;
+
+ xcb_key_press_event_t *kp = (xcb_key_press_event_t *)event;
+ if (kp->detail == 24) {
+ printf("Exit due to keypress\n");
+ need_exit = true;
+ }
+
+ break;
+ }
+ }
+
+ if (!handled) {
+ // Check if a custom XEvent constructor was registered in xlib for this event type, and call it discarding the constructed XEvent if any.
+ // XESetWireToEvent might be used by libraries to intercept messages from the X server e.g. the OpenGL lib waiting for DRI2 events.
+
+ XLockDisplay(dpy);
+ Bool (*proc)(Display*, XEvent*, xEvent*) = XESetWireToEvent(dpy, response_type, NULL);
+ if (proc) {
+ XESetWireToEvent(dpy, response_type, proc);
+ XEvent dummy;
+ event->sequence = LastKnownRequestProcessed(dpy);
+ proc(dpy, &dummy, (xEvent*)event);
+ }
+ XUnlockDisplay(dpy);
+ }
+
+ free(event);
+ }
+
+ if (s_num_frames && framenum >= s_num_frames)
+ need_exit = true;
+
+ if (need_exit)
+ break;
+
+ // this should be in XCB_EXPOSE, but we don't get the event after swaps...
+ scene.draw(framenum++);
+ surface.swap_buffers();
+ }
+}
+
void main_x11()
{
Display* dpy = XOpenDisplay(NULL);
+ FAIL_IF(!dpy, "Failed to connect to the X server");
xcb_connection_t *c = XGetXCBConnection(dpy);
+ /* Acquire event queue ownership */
+ XSetEventQueueOwner(dpy, XCBOwnsEventQueue);
+
/* Get the first screen */
const xcb_setup_t *setup = xcb_get_setup (c);
xcb_screen_t *screen = xcb_setup_roots_iterator (setup).data;
height = 600;
}
- const uint32_t xcb_window_attrib_mask = XCB_CW_EVENT_MASK;
+ const uint32_t xcb_window_attrib_mask = XCB_CW_OVERRIDE_REDIRECT | XCB_CW_EVENT_MASK;
const uint32_t xcb_window_attrib_list[] = {
- XCB_EVENT_MASK_EXPOSURE,
+ // OVERRIDE_REDIRECT
+ 0,
+ // EVENT_MASK
+ XCB_EVENT_MASK_EXPOSURE | XCB_EVENT_MASK_KEY_PRESS,
};
xcb_window_t window = xcb_generate_id (c);
xcb_window_attrib_mask,
xcb_window_attrib_list);
-
#if 0 // Doesn't work
if (s_fullscreen) {
xcb_map_window (c, window);
xcb_flush (c);
- {
- EglState egl(dpy);
- EglSurface surface(egl, (void*)(uintptr_t)window);
- GlScene scene;
-
- scene.set_viewport(width, height);
-
- unsigned framenum = 0;
-
- surface.make_current();
- surface.swap_buffers();
-
- xcb_generic_event_t *event;
- while ( (event = xcb_poll_for_event (c)) ) {
-
- free(event);
-
- if (s_num_frames && framenum >= s_num_frames)
- break;
-
- surface.make_current();
- scene.draw(framenum++);
- surface.swap_buffers();
- }
- }
+ main_loop(dpy, c, window, width, height);
xcb_flush(c);
xcb_unmap_window(c, window);