Update README.md
[android/external-libkmsxx.git] / kmscube / cube-x11.cpp
index 82ef414b46f400a4f782fe7192c2d7ff97e0b6cb..dde4f61148214347522c0561fa2cc744fb2ad566 100644 (file)
@@ -1,20 +1,95 @@
 
 #include <X11/Xlib-xcb.h>
+#include <X11/Xlibint.h>
 
 #include "cube.h"
 #include "cube-egl.h"
 #include "cube-gles2.h"
 
-#include "test.h"
+#include <kms++util.h>
 
 using namespace std;
 
+static void main_loop(Display* dpy, xcb_connection_t *c, xcb_window_t window, uint32_t width, uint32_t height)
+{
+       EglState egl(dpy);
+       EglSurface surface(egl, (void*)(uintptr_t)window);
+       GlScene scene;
+
+       scene.set_viewport(width, height);
+
+       unsigned framenum = 0;
+
+       surface.make_current();
+       surface.swap_buffers();
+
+       bool need_exit = false;
+
+       xcb_generic_event_t *event;
+       while (true) {
+
+               while ((event = xcb_poll_for_event (c))) {
+                       bool handled = false;
+                       uint8_t response_type = event->response_type & ~0x80;
+
+                       switch (response_type) {
+                       case XCB_EXPOSE: {
+                               handled = true;
+                               break;
+                       }
+                       case XCB_KEY_PRESS: {
+                               handled = true;
+
+                               xcb_key_press_event_t *kp = (xcb_key_press_event_t *)event;
+                               if (kp->detail == 24) {
+                                       printf("Exit due to keypress\n");
+                                       need_exit = true;
+                               }
+
+                               break;
+                       }
+                       }
+
+                       if (!handled) {
+                               // Check if a custom XEvent constructor was registered in xlib for this event type, and call it discarding the constructed XEvent if any.
+                               // XESetWireToEvent might be used by libraries to intercept messages from the X server e.g. the OpenGL lib waiting for DRI2 events.
+
+                               XLockDisplay(dpy);
+                               Bool (*proc)(Display*, XEvent*, xEvent*) = XESetWireToEvent(dpy, response_type, NULL);
+                               if (proc) {
+                                       XESetWireToEvent(dpy, response_type, proc);
+                                       XEvent dummy;
+                                       event->sequence = LastKnownRequestProcessed(dpy);
+                                       proc(dpy, &dummy, (xEvent*)event);
+                               }
+                               XUnlockDisplay(dpy);
+                       }
+
+                       free(event);
+               }
+
+               if (s_num_frames && framenum >= s_num_frames)
+                       need_exit = true;
+
+               if (need_exit)
+                       break;
+
+               // this should be in XCB_EXPOSE, but we don't get the event after swaps...
+               scene.draw(framenum++);
+               surface.swap_buffers();
+       }
+}
+
 void main_x11()
 {
        Display* dpy = XOpenDisplay(NULL);
+       FAIL_IF(!dpy, "Failed to connect to the X server");
 
        xcb_connection_t *c = XGetXCBConnection(dpy);
 
+       /* Acquire event queue ownership */
+       XSetEventQueueOwner(dpy, XCBOwnsEventQueue);
+
        /* Get the first screen */
        const xcb_setup_t      *setup  = xcb_get_setup (c);
        xcb_screen_t           *screen = xcb_setup_roots_iterator (setup).data;
@@ -32,9 +107,12 @@ void main_x11()
                height = 600;
        }
 
-       const uint32_t xcb_window_attrib_mask = XCB_CW_EVENT_MASK;
+       const uint32_t xcb_window_attrib_mask = XCB_CW_OVERRIDE_REDIRECT | XCB_CW_EVENT_MASK;
        const uint32_t xcb_window_attrib_list[] = {
-               XCB_EVENT_MASK_EXPOSURE,
+               // OVERRIDE_REDIRECT
+               0,
+               // EVENT_MASK
+               XCB_EVENT_MASK_EXPOSURE | XCB_EVENT_MASK_KEY_PRESS,
        };
 
        xcb_window_t window = xcb_generate_id (c);
@@ -50,7 +128,6 @@ void main_x11()
                           xcb_window_attrib_mask,
                           xcb_window_attrib_list);
 
-
 #if 0 // Doesn't work
        if (s_fullscreen) {
 
@@ -67,31 +144,7 @@ void main_x11()
        xcb_map_window (c, window);
        xcb_flush (c);
 
-       {
-               EglState egl(dpy);
-               EglSurface surface(egl, (void*)(uintptr_t)window);
-               GlScene scene;
-
-               scene.set_viewport(width, height);
-
-               unsigned framenum = 0;
-
-               surface.make_current();
-               surface.swap_buffers();
-
-               xcb_generic_event_t *event;
-               while ( (event = xcb_poll_for_event (c)) ) {
-
-                       free(event);
-
-                       if (s_num_frames && framenum >= s_num_frames)
-                               break;
-
-                       surface.make_current();
-                       scene.draw(framenum++);
-                       surface.swap_buffers();
-               }
-       }
+       main_loop(dpy, c, window, width, height);
 
        xcb_flush(c);
        xcb_unmap_window(c, window);