diff --git a/libkms++/card.h b/libkms++/card.h
index fb45d04ca79a10b2b609d42fc47852c9832a3688..dc97703f2d5e18c2845adab9812b820f2ace6748 100644 (file)
--- a/libkms++/card.h
+++ b/libkms++/card.h
#include <map>
#include "decls.h"
+#include "pipeline.h"
namespace kms
{
-
class Card
{
public:
Connector* get_first_connected_connector() const;
DrmObject* get_object(uint32_t id) const;
+ Connector* get_connector(uint32_t id) const;
Crtc* get_crtc(uint32_t id) const;
Crtc* get_crtc_by_index(uint32_t idx) const;
Encoder* get_encoder(uint32_t id) const;
Property* get_prop(uint32_t id) const;
- Property* get_prop(const char *name) const;
+ Property* get_prop(const std::string& name) const;
bool master() const { return m_master; }
bool has_atomic() const { return m_has_atomic; }
+ bool has_has_universal_planes() const { return m_has_universal_planes; }
void print_short() const;
std::vector<Connector*> get_connectors() const;
+ std::vector<Crtc*> get_crtcs() const;
std::vector<DrmObject*> get_objects() const;
std::vector<Plane*> get_planes() const;
+ std::vector<Pipeline> get_connected_pipelines();
+
+ void call_page_flip_handlers();
+
private:
+ void restore_modes();
+
std::map<uint32_t, DrmObject*> m_obmap;
int m_fd;
bool m_master;
bool m_has_atomic;
+ bool m_has_universal_planes;
};
}