diff --git a/py/pykms/pykmsbase.cpp b/py/pykms/pykmsbase.cpp
index d626019b1d769f0baee6b2faf3b91f0611cf1c39..aae5ecec6ea32e31f5361ec6a52874064ab5c7ee 100644 (file)
--- a/py/pykms/pykmsbase.cpp
+++ b/py/pykms/pykmsbase.cpp
py::class_<Card>(m, "Card")
.def(py::init<>())
.def_property_readonly("fd", &Card::fd)
- .def("get_first_connected_connector", &Card::get_first_connected_connector)
- .def_property_readonly("connectors", &Card::get_connectors)
- .def_property_readonly("crtcs", &Card::get_crtcs)
- .def_property_readonly("encoders", &Card::get_encoders)
- .def_property_readonly("planes", &Card::get_planes)
+ .def_property_readonly("get_first_connected_connector", &Card::get_first_connected_connector)
+
+ // XXX pybind11 can't handle vector<T*> where T is non-copyable, and complains:
+ // RuntimeError: return_value_policy = move, but the object is neither movable nor copyable!
+ // So we do this manually.
+ .def_property_readonly("connectors", [](Card* self) {
+ vector<unique_ptr<Connector, py::nodelete>> v;
+ for (Connector* p : self->get_connectors())
+ v.push_back(unique_ptr<Connector, py::nodelete>(p));
+ return v;
+ })
+
+ .def_property_readonly("planes", [](Card* self) {
+ vector<unique_ptr<Plane, py::nodelete>> v;
+ for (Plane* p : self->get_planes())
+ v.push_back(unique_ptr<Plane, py::nodelete>(p));
+ return v;
+ })
+
.def_property_readonly("has_atomic", &Card::has_atomic)
.def("get_prop", (Property* (Card::*)(uint32_t) const)&Card::get_prop)
;
- py::class_<DrmObject, DrmObject*>(m, "DrmObject")
+ py::class_<DrmObject, unique_ptr<DrmObject, py::nodelete>>(m, "DrmObject")
.def_property_readonly("id", &DrmObject::id)
+ .def_property_readonly("idx", &DrmObject::idx)
.def_property_readonly("card", &DrmObject::card)
;
- py::class_<DrmPropObject, DrmPropObject*>(m, "DrmPropObject", py::base<DrmObject>())
+ py::class_<DrmPropObject, DrmObject, unique_ptr<DrmPropObject, py::nodelete>>(m, "DrmPropObject")
.def("refresh_props", &DrmPropObject::refresh_props)
.def_property_readonly("prop_map", &DrmPropObject::get_prop_map)
.def("get_prop_value", (uint64_t (DrmPropObject::*)(const string&) const)&DrmPropObject::get_prop_value)
.def("set_prop_value",(int (DrmPropObject::*)(const string&, uint64_t)) &DrmPropObject::set_prop_value)
.def("get_prop_value_as_blob", &DrmPropObject::get_prop_value_as_blob)
+ .def("get_prop", &DrmPropObject::get_prop)
;
- py::class_<Connector, Connector*>(m, "Connector", py::base<DrmPropObject>())
+ py::class_<Connector, DrmPropObject, unique_ptr<Connector, py::nodelete>>(m, "Connector")
.def_property_readonly("fullname", &Connector::fullname)
.def("get_default_mode", &Connector::get_default_mode)
.def("get_current_crtc", &Connector::get_current_crtc)
.def("get_modes", &Connector::get_modes)
.def("get_mode", (Videomode (Connector::*)(const string& mode) const)&Connector::get_mode)
.def("get_mode", (Videomode (Connector::*)(unsigned xres, unsigned yres, float refresh, bool ilace) const)&Connector::get_mode)
+ .def("connected", &Connector::connected)
.def("__repr__", [](const Connector& o) { return "<pykms.Connector " + to_string(o.id()) + ">"; })
.def("refresh", &Connector::refresh)
;
- py::class_<Crtc, Crtc*>(m, "Crtc", py::base<DrmPropObject>())
- .def("set_mode", &Crtc::set_mode)
+ py::class_<Crtc, DrmPropObject, unique_ptr<Crtc, py::nodelete>>(m, "Crtc")
+ .def("set_mode", (int (Crtc::*)(Connector*, const Videomode&))&Crtc::set_mode)
+ .def("set_mode", (int (Crtc::*)(Connector*, Framebuffer&, const Videomode&))&Crtc::set_mode)
+ .def("disable_mode", &Crtc::disable_mode)
.def("page_flip",
- [](Crtc* self, Framebuffer& fb, py::object ob)
+ [](Crtc* self, Framebuffer& fb, uint32_t data)
{
- // This adds a ref to the object, and must be unpacked with __ob_unpack_helper()
- PyObject* pob = ob.ptr();
- Py_XINCREF(pob);
- self->page_flip(fb, pob);
- })
+ self->page_flip(fb, (void*)(intptr_t)data);
+ }, py::arg("fb"), py::arg("data") = 0)
.def("set_plane", &Crtc::set_plane)
.def_property_readonly("possible_planes", &Crtc::get_possible_planes)
.def_property_readonly("primary_plane", &Crtc::get_primary_plane)
.def("refresh", &Crtc::refresh)
;
- py::class_<Encoder, Encoder*>(m, "Encoder", py::base<DrmPropObject>())
+ py::class_<Encoder, DrmPropObject, unique_ptr<Encoder, py::nodelete>>(m, "Encoder")
.def("refresh", &Encoder::refresh)
;
- py::class_<Plane, Plane*>(m, "Plane", py::base<DrmPropObject>())
+ py::class_<Plane, DrmPropObject, unique_ptr<Plane, py::nodelete>>(m, "Plane")
.def("supports_crtc", &Plane::supports_crtc)
+ .def_property_readonly("formats", &Plane::get_formats)
.def_property_readonly("plane_type", &Plane::plane_type)
.def("__repr__", [](const Plane& o) { return "<pykms.Plane " + to_string(o.id()) + ">"; })
;
.value("Cursor", PlaneType::Cursor)
;
- py::class_<Property, Property*>(m, "Property", py::base<DrmObject>())
+ py::class_<Property, DrmObject, unique_ptr<Property, py::nodelete>>(m, "Property")
.def_property_readonly("name", &Property::name)
+ .def_property_readonly("enums", &Property::get_enums)
;
- py::class_<Blob>(m, "Blob", py::base<DrmObject>())
+ py::class_<Blob>(m, "Blob")
.def("__init__", [](Blob& instance, Card& card, py::buffer buf) {
py::buffer_info info = buf.request();
if (info.ndim != 1)
new (&instance) Blob(card, info.ptr, info.size * info.itemsize);
})
.def_property_readonly("data", &Blob::data)
- ;
- py::class_<Framebuffer>(m, "Framebuffer", py::base<DrmObject>())
+ // XXX pybind11 doesn't support a base object (DrmObject) with custom holder-type,
+ // and a subclass with standard holder-type.
+ // So we just copy the DrmObject members here.
+ // Note that this means that python thinks we don't derive from DrmObject
+ .def_property_readonly("id", &DrmObject::id)
+ .def_property_readonly("idx", &DrmObject::idx)
+ .def_property_readonly("card", &DrmObject::card)
;
- py::class_<MappedFramebuffer>(m, "MappedFramebuffer", py::base<Framebuffer>())
- .def_property_readonly("width", &MappedFramebuffer::width)
- .def_property_readonly("height", &MappedFramebuffer::height)
+ py::class_<Framebuffer>(m, "Framebuffer")
+ .def_property_readonly("width", &Framebuffer::width)
+ .def_property_readonly("height", &Framebuffer::height)
+
+ // XXX pybind11 doesn't support a base object (DrmObject) with custom holder-type,
+ // and a subclass with standard holder-type.
+ // So we just copy the DrmObject members here.
+ // Note that this means that python thinks we don't derive from DrmObject
+ .def_property_readonly("id", &DrmObject::id)
+ .def_property_readonly("idx", &DrmObject::idx)
+ .def_property_readonly("card", &DrmObject::card)
;
- py::class_<DumbFramebuffer>(m, "DumbFramebuffer", py::base<MappedFramebuffer>())
+ py::class_<DumbFramebuffer, Framebuffer>(m, "DumbFramebuffer")
.def(py::init<Card&, uint32_t, uint32_t, const string&>(),
py::keep_alive<1, 2>()) // Keep Card alive until this is destructed
.def(py::init<Card&, uint32_t, uint32_t, PixelFormat>(),
.def("offset", &DumbFramebuffer::offset)
;
- py::class_<ExtFramebuffer>(m, "ExtFramebuffer", py::base<MappedFramebuffer>())
+ py::class_<ExtFramebuffer, Framebuffer>(m, "ExtFramebuffer")
.def(py::init<Card&, uint32_t, uint32_t, PixelFormat, vector<int>, vector<uint32_t>, vector<uint32_t>>(),
py::keep_alive<1, 2>()) // Keep Card alive until this is destructed
;
.value("ABGR8888", PixelFormat::ABGR8888)
.value("RGB888", PixelFormat::RGB888)
+ .value("BGR888", PixelFormat::BGR888)
.value("RGB565", PixelFormat::RGB565)
+ .value("BGR565", PixelFormat::BGR565)
+ ;
+
+ py::enum_<SyncPolarity>(m, "SyncPolarity")
+ .value("Undefined", SyncPolarity::Undefined)
+ .value("Positive", SyncPolarity::Positive)
+ .value("Negative", SyncPolarity::Negative)
;
py::class_<Videomode>(m, "Videomode")
.def_readwrite("type", &Videomode::type)
.def("__repr__", [](const Videomode& vm) { return "<pykms.Videomode " + to_string(vm.hdisplay) + "x" + to_string(vm.vdisplay) + ">"; })
+
+ .def("to_blob", &Videomode::to_blob)
+
+ .def_property("hsync", &Videomode::hsync, &Videomode::set_hsync)
+ .def_property("vsync", &Videomode::vsync, &Videomode::set_vsync)
;
+
+ m.def("videomode_from_timings", &videomode_from_timings);
+
py::class_<AtomicReq>(m, "AtomicReq")
.def(py::init<Card&>(),
py::keep_alive<1, 2>()) // Keep Card alive until this is destructed
.def("add", (void (AtomicReq::*)(DrmPropObject*, const map<string, uint64_t>&)) &AtomicReq::add)
.def("test", &AtomicReq::test, py::arg("allow_modeset") = false)
.def("commit",
- [](AtomicReq* self, py::object ob, bool allow)
+ [](AtomicReq* self, uint32_t data, bool allow)
{
- // This adds a ref to the object, and must be unpacked with __ob_unpack_helper()
- PyObject* pob = ob.ptr();
- Py_XINCREF(pob);
- return self->commit(pob, allow);
- }, py::arg("data"), py::arg("allow_modeset") = false)
+ return self->commit((void*)(intptr_t)data, allow);
+ }, py::arg("data") = 0, py::arg("allow_modeset") = false)
.def("commit_sync", &AtomicReq::commit_sync, py::arg("allow_modeset") = false)
;
}