diff --git a/utils/testpat.cpp b/utils/testpat.cpp
index ede176c69072d62edf5e52aa15ffca113c0c4c08..5f1095cb62cf7da2dccbcb284c35d599df2a5d89 100644 (file)
--- a/utils/testpat.cpp
+++ b/utils/testpat.cpp
#include <regex>
#include <set>
-#include "kms++.h"
-#include "modedb.h"
+#include <kms++.h>
+#include <modedb.h>
-#include "test.h"
-#include "opts.h"
+#include <kms++util.h>
+#include <opts.h>
using namespace std;
using namespace kms;
unsigned w;
unsigned h;
- DumbFramebuffer* fb;
+ vector<DumbFramebuffer*> fbs;
};
struct OutputInfo
Crtc* crtc;
Videomode mode;
bool user_set_crtc;
- DumbFramebuffer* fb;
+ vector<DumbFramebuffer*> fbs;
vector<PlaneInfo> planes;
};
static bool s_use_dmt;
static bool s_use_cea;
+static unsigned s_num_buffers = 1;
static set<Crtc*> s_used_crtcs;
static set<Plane*> s_used_planes;
@@ -243,14 +244,17 @@ static void parse_plane(Card& card, const string& plane_str, const OutputInfo& o
pinfo.y = output.mode.vdisplay / 2 - pinfo.h / 2;
}
-static DumbFramebuffer* get_default_fb(Card& card, unsigned width, unsigned height)
+static vector<DumbFramebuffer*> get_default_fb(Card& card, unsigned width, unsigned height)
{
- auto fb = new DumbFramebuffer(card, width, height, PixelFormat::XRGB8888);
- draw_test_pattern(*fb);
- return fb;
+ vector<DumbFramebuffer*> v;
+
+ for (unsigned i = 0; i < s_num_buffers; ++i)
+ v.push_back(new DumbFramebuffer(card, width, height, PixelFormat::XRGB8888));
+
+ return v;
}
-static DumbFramebuffer* parse_fb(Card& card, const string& fb_str, unsigned def_w, unsigned def_h)
+static vector<DumbFramebuffer*> parse_fb(Card& card, const string& fb_str, unsigned def_w, unsigned def_h)
{
unsigned w = def_w;
unsigned h = def_h;
@@ -273,9 +277,12 @@ static DumbFramebuffer* parse_fb(Card& card, const string& fb_str, unsigned def_
format = FourCCToPixelFormat(sm[3]);
}
- auto fb = new DumbFramebuffer(card, w, h, format);
- draw_test_pattern(*fb);
- return fb;
+ vector<DumbFramebuffer*> v;
+
+ for (unsigned i = 0; i < s_num_buffers; ++i)
+ v.push_back(new DumbFramebuffer(card, w, h, format));
+
+ return v;
}
static const char* usage_str =
@@ -395,7 +402,7 @@ static vector<OutputInfo> setups_to_outputs(Card& card, const vector<Arg>& outpu
output.crtc = pipe.crtc;
output.mode = output.connector->get_default_mode();
- output.fb = get_default_fb(card, output.mode.hdisplay, output.mode.vdisplay);
+ output.fbs = get_default_fb(card, output.mode.hdisplay, output.mode.vdisplay);
outputs.push_back(output);
}
@@ -482,12 +489,12 @@ static vector<OutputInfo> setups_to_outputs(Card& card, const vector<Arg>& outpu
def_h = current_output->mode.vdisplay;
}
- auto fb = parse_fb(card, arg.arg, def_w, def_h);
+ auto fbs = parse_fb(card, arg.arg, def_w, def_h);
if (current_plane)
- current_plane->fb = fb;
+ current_plane->fbs = fbs;
else
- current_output->fb = fb;
+ current_output->fbs = fbs;
break;
}
@@ -501,12 +508,12 @@ static vector<OutputInfo> setups_to_outputs(Card& card, const vector<Arg>& outpu
o.user_set_crtc = true;
}
- if (!o.fb && o.user_set_crtc)
- o.fb = get_default_fb(card, o.mode.hdisplay, o.mode.vdisplay);
+ if (o.fbs.empty() && o.user_set_crtc)
+ o.fbs = get_default_fb(card, o.mode.hdisplay, o.mode.vdisplay);
for (PlaneInfo &p : o.planes) {
- if (!p.fb)
- p.fb = get_default_fb(card, p.w, p.h);
+ if (p.fbs.empty())
+ p.fbs = get_default_fb(card, p.w, p.h);
}
}
printf(" Crtc %u/@%u: %ux%u-%u (%s)\n", o.crtc->id(), o.crtc->idx(),
o.mode.hdisplay, o.mode.vdisplay, o.mode.vrefresh,
videomode_to_string(o.mode).c_str());
- if (o.fb)
- printf(" Fb %ux%u-%s\n", o.fb->width(), o.fb->height(),
- PixelFormatToFourCC(o.fb->format()).c_str());
+ if (!o.fbs.empty()) {
+ auto fb = o.fbs[0];
+ printf(" Fb %ux%u-%s\n", fb->width(), fb->height(),
+ PixelFormatToFourCC(fb->format()).c_str());
+ }
for (unsigned j = 0; j < o.planes.size(); ++j) {
const PlaneInfo& p = o.planes[j];
+ auto fb = p.fbs[0];
printf(" Plane %u/@%u: %u,%u-%ux%u\n", p.plane->id(), p.plane->idx(),
p.x, p.y, p.w, p.h);
- printf(" Fb %ux%u-%s\n", p.fb->width(), p.fb->height(),
- PixelFormatToFourCC(p.fb->format()).c_str());
+ printf(" Fb %ux%u-%s\n", fb->width(), fb->height(),
+ PixelFormatToFourCC(fb->format()).c_str());
}
}
}
+static void draw_test_patterns(const vector<OutputInfo>& outputs)
+{
+ for (const OutputInfo& o : outputs) {
+ for (auto fb : o.fbs)
+ draw_test_pattern(*fb);
+
+ for (const PlaneInfo& p : o.planes)
+ for (auto fb : p.fbs)
+ draw_test_pattern(*fb);
+ }
+}
+
static void set_crtcs_n_planes(Card& card, const vector<OutputInfo>& outputs)
{
for (const OutputInfo& o : outputs) {
auto conn = o.connector;
auto crtc = o.crtc;
- if (o.fb) {
- int r = crtc->set_mode(conn, *o.fb, o.mode);
+ if (!o.fbs.empty()) {
+ auto fb = o.fbs[0];
+ int r = crtc->set_mode(conn, *fb, o.mode);
if (r)
printf("crtc->set_mode() failed for crtc %u: %s\n",
crtc->id(), strerror(-r));
}
for (const PlaneInfo& p : o.planes) {
- int r = crtc->set_plane(p.plane, *p.fb,
+ auto fb = p.fbs[0];
+ int r = crtc->set_plane(p.plane, *fb,
p.x, p.y, p.w, p.h,
- 0, 0, p.fb->width(), p.fb->height());
+ 0, 0, fb->width(), fb->height());
if (r)
printf("crtc->set_plane() failed for plane %u: %s\n",
p.plane->id(), strerror(-r));
vector<OutputInfo> outputs = setups_to_outputs(card, output_args);
+ draw_test_patterns(outputs);
+
print_outputs(outputs);
set_crtcs_n_planes(card, outputs);