summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: af3f989)
raw | patch | inline | side by side (parent: af3f989)
author | Tomi Valkeinen <tomi.valkeinen@ti.com> | |
Tue, 30 May 2017 10:56:28 +0000 (13:56 +0300) | ||
committer | Tomi Valkeinen <tomi.valkeinen@ti.com> | |
Tue, 30 May 2017 11:22:00 +0000 (14:22 +0300) |
index dcaaa4fd9a97039680cc42354607e0712ef74440..02ac79f3b3dce85ba06c595f8b2c9df0c4eceefb 100644 (file)
class OmapFramebuffer : public MappedFramebuffer
{
public:
- OmapFramebuffer(OmapCard& card, uint32_t width, uint32_t height, const std::string& fourcc, bool tiled = false);
- OmapFramebuffer(OmapCard& card, uint32_t width, uint32_t height, PixelFormat format, bool tiled = false);
+ enum Flags
+ {
+ None = 0,
+ Tiled = 1 << 0,
+ };
+
+ OmapFramebuffer(OmapCard& card, uint32_t width, uint32_t height, const std::string& fourcc, Flags flags = Flags::None);
+ OmapFramebuffer(OmapCard& card, uint32_t width, uint32_t height, PixelFormat format, Flags flags = Flags::None);
virtual ~OmapFramebuffer();
uint32_t width() const { return Framebuffer::width(); }
uint8_t* map;
};
- void Create(bool tiled);
+ void Create(Flags buffer_flags);
void Destroy();
unsigned m_num_planes;
index 9997933d85eff05aea5a78d7a1564e54d9adc4d0..4aa1cdb8703470bf03a875e8f08a8a0f272dab4d 100644 (file)
namespace kms
{
-OmapFramebuffer::OmapFramebuffer(OmapCard& card, uint32_t width, uint32_t height, const string& fourcc, bool tiled)
- : OmapFramebuffer(card, width, height, FourCCToPixelFormat(fourcc), tiled)
+OmapFramebuffer::OmapFramebuffer(OmapCard& card, uint32_t width, uint32_t height, const string& fourcc, Flags flags)
+ : OmapFramebuffer(card, width, height, FourCCToPixelFormat(fourcc), flags)
{
}
-OmapFramebuffer::OmapFramebuffer(OmapCard& card, uint32_t width, uint32_t height, PixelFormat format, bool tiled)
+OmapFramebuffer::OmapFramebuffer(OmapCard& card, uint32_t width, uint32_t height, PixelFormat format, Flags flags)
:MappedFramebuffer(card, width, height), m_omap_card(card), m_format(format)
{
- Create(tiled);
+ Create(flags);
}
OmapFramebuffer::~OmapFramebuffer()
Destroy();
}
-void OmapFramebuffer::Create(bool tiled)
+void OmapFramebuffer::Create(Flags buffer_flags)
{
const PixelFormatInfo& format_info = get_pixel_format_info(m_format);
uint32_t stride;
- if (!tiled) {
+ if (!(buffer_flags & Flags::Tiled)) {
stride = width() * pi.bitspp / 8;
uint32_t size = stride * height() / pi.ysub;
diff --git a/py/pykms/pykmsomap.cpp b/py/pykms/pykmsomap.cpp
index bad20fb0f3852c39ea25d3aeb7e82a7a70704fd3..20740929c48e1ddf7a1118ff034c7d23b7a339e4 100644 (file)
--- a/py/pykms/pykmsomap.cpp
+++ b/py/pykms/pykmsomap.cpp
.def(py::init<>())
;
- py::class_<OmapFramebuffer>(m, "OmapFramebuffer", py::base<MappedFramebuffer>())
- .def(py::init<OmapCard&, uint32_t, uint32_t, const string&, bool>(),
+ py::class_<OmapFramebuffer> omapfb(m, "OmapFramebuffer", py::base<MappedFramebuffer>());
+
+ // XXX we should use py::arithmetic() here to support or and and operators, but it's not supported in the pybind11 we use
+ py::enum_<OmapFramebuffer::Flags>(omapfb, "Flags")
+ .value("None", OmapFramebuffer::Flags::None)
+ .value("Tiled", OmapFramebuffer::Flags::Tiled)
+ .export_values()
+ ;
+
+ omapfb
+ .def(py::init<OmapCard&, uint32_t, uint32_t, const string&, OmapFramebuffer::Flags>(),
py::keep_alive<1, 2>(), // Keep Card alive until this is destructed
- py::arg("card"), py::arg("width"), py::arg("height"), py::arg("fourcc"), py::arg("tiled") = false)
- .def(py::init<OmapCard&, uint32_t, uint32_t, PixelFormat, bool>(),
+ py::arg("card"), py::arg("width"), py::arg("height"), py::arg("fourcc"), py::arg("flags") = OmapFramebuffer::None)
+ .def(py::init<OmapCard&, uint32_t, uint32_t, PixelFormat, OmapFramebuffer::Flags>(),
py::keep_alive<1, 2>(), // Keep OmapCard alive until this is destructed
- py::arg("card"), py::arg("width"), py::arg("height"), py::arg("pixfmt"), py::arg("tiled") = false)
+ py::arg("card"), py::arg("width"), py::arg("height"), py::arg("pixfmt"), py::arg("flags") = OmapFramebuffer::None)
.def_property_readonly("format", &OmapFramebuffer::format)
.def_property_readonly("num_planes", &OmapFramebuffer::num_planes)
.def("fd", &OmapFramebuffer::prime_fd)
diff --git a/py/tests/rottest.py b/py/tests/rottest.py
index d81a962a61ffb95028913ccaaad5e72f0bb003cc..8988134122e45569c4a73efedaa8ced73c44f2a3 100755 (executable)
--- a/py/tests/rottest.py
+++ b/py/tests/rottest.py
x_scale = 1
y_scale = 1
-fb = pykms.OmapFramebuffer(card, fb_w, fb_h, "NV12", tiled = True);
+fb = pykms.OmapFramebuffer(card, fb_w, fb_h, "NV12", flags = pykms.OmapFramebuffer.Tiled);
#fb = pykms.DumbFramebuffer(card, fb_w, fb_h, "NV12")
pykms.draw_test_pattern(fb);