remove the old cmdoptions.h
authorTomi Valkeinen <tomi.valkeinen@ti.com>
Thu, 26 Nov 2015 16:08:29 +0000 (18:08 +0200)
committerTomi Valkeinen <tomi.valkeinen@ti.com>
Thu, 26 Nov 2015 20:45:18 +0000 (22:45 +0200)
tests/CMakeLists.txt
tests/cmdoptions.h [deleted file]
tests/optiontester.cpp [deleted file]

index 092220f805e81bfd305b3a43157858ba601eb64e..e18081a4ce3f5a110743e5aecd6e5603aa681c0e 100644 (file)
@@ -12,5 +12,3 @@ target_link_libraries(kmsview kms++ kmstest ${LIBDRM_LIBRARIES})
 
 add_executable (kmsprint kmsprint.cpp)
 target_link_libraries(kmsprint kms++ kmstest ${LIBDRM_LIBRARIES})
 
 add_executable (kmsprint kmsprint.cpp)
 target_link_libraries(kmsprint kms++ kmstest ${LIBDRM_LIBRARIES})
-
-add_executable (optiontester optiontester.cpp)
diff --git a/tests/cmdoptions.h b/tests/cmdoptions.h
deleted file mode 100644 (file)
index 843e65a..0000000
+++ /dev/null
@@ -1,97 +0,0 @@
-#pragma once
-
-#include <cstdio>
-#include <string>
-#include <vector>
-#include <map>
-
-using namespace std;
-
-#define NO_PARAM(h) (CmdOption(false, h))
-#define HAS_PARAM(h) (CmdOption(true, h))
-
-class CmdOption
-{
-public:
-       CmdOption(bool has_param, string help) :
-               m_has_param(has_param), m_help(help), m_is_set(false) { }
-        bool has_param() const { return m_has_param; }
-       const string& help() const { return m_help; }
-
-       void oset() { m_is_set = true; }
-       void pset(const string& p) { m_param = p; oset(); }
-        bool is_set() const { return m_is_set; }
-        const string& param() const { return m_param; }
-private:
-       bool m_has_param;
-       string m_help;
-
-       bool m_is_set;
-       string m_param;
-};
-
-class CmdOptions
-{
-public:
-       CmdOptions(int argc, char **argv, map<string, CmdOption>& opts) :
-               m_opts(opts), m_cmd(argv[0]) {
-               for (int i = 1; i < argc; i++) {
-                       if (argv[i][0] == '-') {
-                               auto ii = m_opts.find(&argv[i][1]);
-                               if (ii == m_opts.end()) {
-                                       m_error += m_cmd + ": " +
-                                               string(argv[i]) +
-                                               ": unknown option\n";
-                                       continue;
-                               }
-                               if ((*ii).second.has_param()) {
-                                       if (++i == argc) {
-                                               m_error += m_cmd + ": -" +
-                                                       (*ii).first +
-                                                       ": parameter missing\n";
-                                               continue;
-                                       }
-                                       (*ii).second.pset(argv[i]);
-                               } else {
-                                       (*ii).second.oset();
-                               }
-                       } else {
-                               m_params.push_back(argv[i]);
-                       }
-               }
-       }
-       const string& error() const { return m_error; }
-       const string& cmd() const { return m_cmd; }
-
-       bool is_set(const string& name) const {
-               return m_opts.at(name).is_set();
-       }
-       const string& opt_param(const string& name) const {
-               return m_opts.at(name).param();
-       }
-       const vector<string>& params() const { return m_params; }
-       CmdOption& get_option(const string& name) { return m_opts.at(name); }
-
-       int num_options() const {
-               int ret(0);
-               for (const auto& p : m_opts)
-                       if (p.second.is_set())
-                               ret++;
-               return ret;
-       }
-
-       const string usage() const {
-               string ret("usage:\n");
-               for (const auto& p : m_opts)
-                       ret += "-" + p.first +
-                               (p.second.has_param() ? " <>: " : ": ") +
-                               p.second.help() + "\n";
-               return ret;
-       }
-
-private:
-       map<string, CmdOption>& m_opts;
-       string m_cmd;
-       vector<string> m_params;
-       string m_error;
-};
diff --git a/tests/optiontester.cpp b/tests/optiontester.cpp
deleted file mode 100644 (file)
index ccb9579..0000000
+++ /dev/null
@@ -1,29 +0,0 @@
-#include <cstdio>
-#include <algorithm>
-#include <iostream>
-
-#include "cmdoptions.h"
-
-using namespace std;
-
-static map<string, CmdOption> options = {
-       { "test", NO_PARAM("test") },
-       { "test2", HAS_PARAM("test2") },
-};
-
-int main(int argc, char **argv)
-{
-       CmdOptions opts(argc, argv, options);
-
-       if (opts.error().length()) {
-               cerr << opts.error() << opts.usage();
-               return -1;
-       }
-
-       for (auto p : options)
-               printf("Option %s set %d param %s\n", 
-                      p.first.c_str(), opts.is_set(p.first),
-                      opts.opt_param(p.first).c_str());;
-
-       return 0;
-}