testpat: add page flipping mode
authorTomi Valkeinen <tomi.valkeinen@ti.com>
Fri, 27 May 2016 20:06:29 +0000 (23:06 +0300)
committerTomi Valkeinen <tomi.valkeinen@ti.com>
Mon, 30 May 2016 10:52:51 +0000 (13:52 +0300)
utils/testpat.cpp

index 6aa658345e6cea14855350cf33fb20e2d870842f..d12e209cc0d395d74809c9f769ec43f54aeb8551 100644 (file)
@@ -3,6 +3,7 @@
 #include <algorithm>
 #include <regex>
 #include <set>
+#include <chrono>
 
 #include <kms++.h>
 #include <modedb.h>
@@ -41,6 +42,8 @@ struct OutputInfo
 static bool s_use_dmt;
 static bool s_use_cea;
 static unsigned s_num_buffers = 1;
+static bool s_flip_mode;
+static bool s_flip_sync;
 
 static set<Crtc*> s_used_crtcs;
 static set<Plane*> s_used_planes;
@@ -297,6 +300,8 @@ static const char* usage_str =
                "  -f, --fb=FB               FB is [<w>x<h>][-][<4cc>]\n"
                "      --dmt                 Search for the given mode from DMT tables\n"
                "      --cea                 Search for the given mode from CEA tables\n"
+               "      --flip                Do page flipping for each output\n"
+               "      --sync                Synchronize page flipping\n"
                "\n"
                "<connector>, <crtc> and <plane> can be given by id (<id>) or index (@<idx>).\n"
                "<connector> can also be given by name.\n"
@@ -374,6 +379,15 @@ static vector<Arg> parse_cmdline(int argc, char **argv)
                {
                        s_use_cea = true;
                }),
+               Option("|flip", []()
+               {
+                       s_flip_mode = true;
+                       s_num_buffers = 2;
+               }),
+               Option("|sync", []()
+               {
+                       s_flip_sync = true;
+               }),
                Option("h|help", [&]()
                {
                        usage();
@@ -683,12 +697,200 @@ static void set_crtcs_n_planes(Card& card, const vector<OutputInfo>& outputs)
                EXIT("Atomic commit failed: %d\n", r);
 }
 
+class FlipState : private PageFlipHandlerBase
+{
+public:
+       FlipState(Card& card, const string& name, vector<const OutputInfo*> outputs)
+               : m_card(card), m_name(name), m_outputs(outputs)
+       {
+       }
+
+       void start_flipping()
+       {
+               m_prev_frame = m_prev_print = std::chrono::steady_clock::now();
+               m_slowest_frame = std::chrono::duration<float>::min();
+               m_frame_num = 0;
+               queue_next();
+       }
+
+private:
+       void handle_page_flip(uint32_t frame, double time)
+       {
+               m_frame_num++;
+
+               auto now = std::chrono::steady_clock::now();
+
+               std::chrono::duration<float> diff = now - m_prev_frame;
+               if (diff > m_slowest_frame)
+                       m_slowest_frame = diff;
+
+               if (m_frame_num  % 100 == 0) {
+                       std::chrono::duration<float> fsec = now - m_prev_print;
+                       printf("Connector %s: fps %f, slowest %.2f ms\n",
+                              m_name.c_str(),
+                              100.0 / fsec.count(),
+                              m_slowest_frame.count() * 1000);
+                       m_prev_print = now;
+                       m_slowest_frame = std::chrono::duration<float>::min();
+               }
+
+               m_prev_frame = now;
+
+               queue_next();
+       }
+
+       static unsigned get_bar_pos(DumbFramebuffer* fb, unsigned frame_num)
+       {
+               return (frame_num * bar_speed) % (fb->width() - bar_width + 1);
+       }
+
+       static void draw_bar(DumbFramebuffer* fb, unsigned frame_num)
+       {
+               int old_xpos = frame_num < s_num_buffers ? -1 : get_bar_pos(fb, frame_num - s_num_buffers);
+               int new_xpos = get_bar_pos(fb, frame_num);
+
+               draw_color_bar(*fb, old_xpos, new_xpos, bar_width);
+       }
+
+       static void do_flip_output(AtomicReq& req, unsigned frame_num, const OutputInfo& o)
+       {
+               unsigned cur = frame_num % s_num_buffers;
+
+               if (!o.fbs.empty()) {
+                       auto fb = o.fbs[cur];
+
+                       draw_bar(fb, frame_num);
+
+                       req.add(o.primary_plane, {
+                                       { "FB_ID", fb->id() },
+                               });
+               }
+
+               for (const PlaneInfo& p : o.planes) {
+                       auto fb = p.fbs[cur];
+
+                       draw_bar(fb, frame_num);
+
+                       req.add(p.plane, {
+                                       { "FB_ID", fb->id() },
+                               });
+               }
+       }
+
+       void do_flip_output_legacy(unsigned frame_num, const OutputInfo& o)
+       {
+               unsigned cur = frame_num % s_num_buffers;
+
+               if (!o.fbs.empty()) {
+                       auto fb = o.fbs[cur];
+
+                       draw_bar(fb, frame_num);
+
+                       int r = o.crtc->page_flip(*fb, this);
+                       ASSERT(r == 0);
+               }
+
+               for (const PlaneInfo& p : o.planes) {
+                       auto fb = p.fbs[cur];
+
+                       draw_bar(fb, frame_num);
+
+                       int r = o.crtc->set_plane(p.plane, *fb,
+                                                 p.x, p.y, p.w, p.h,
+                                                 0, 0, fb->width(), fb->height());
+                       ASSERT(r == 0);
+               }
+       }
+
+       void queue_next()
+       {
+               if (m_card.has_atomic()) {
+                       AtomicReq req(m_card);
+
+                       for (auto o : m_outputs)
+                               do_flip_output(req, m_frame_num, *o);
+
+                       int r = req.commit(this);
+                       if (r)
+                               EXIT("Flip commit failed: %d\n", r);
+               } else {
+                       ASSERT(m_outputs.size() == 1);
+                       do_flip_output_legacy(m_frame_num, *m_outputs[0]);
+               }
+       }
+
+       Card& m_card;
+       string m_name;
+       vector<const OutputInfo*> m_outputs;
+       unsigned m_frame_num;
+
+       chrono::steady_clock::time_point m_prev_print;
+       chrono::steady_clock::time_point m_prev_frame;
+       chrono::duration<float> m_slowest_frame;
+
+       static const unsigned bar_width = 20;
+       static const unsigned bar_speed = 8;
+};
+
+static void main_flip(Card& card, const vector<OutputInfo>& outputs)
+{
+       fd_set fds;
+
+       FD_ZERO(&fds);
+
+       int fd = card.fd();
+
+       vector<unique_ptr<FlipState>> flipstates;
+
+       if (!s_flip_sync) {
+               for (const OutputInfo& o : outputs) {
+                       auto fs = unique_ptr<FlipState>(new FlipState(card, to_string(o.connector->idx()), { &o }));
+                       flipstates.push_back(move(fs));
+               }
+       } else {
+               vector<const OutputInfo*> ois;
+
+               string name;
+               for (const OutputInfo& o : outputs) {
+                       name += to_string(o.connector->idx()) + ",";
+                       ois.push_back(&o);
+               }
+
+               auto fs = unique_ptr<FlipState>(new FlipState(card, name, ois));
+               flipstates.push_back(move(fs));
+       }
+
+       for (unique_ptr<FlipState>& fs : flipstates)
+               fs->start_flipping();
+
+       while (true) {
+               int r;
+
+               FD_SET(0, &fds);
+               FD_SET(fd, &fds);
+
+               r = select(fd + 1, &fds, NULL, NULL, NULL);
+               if (r < 0) {
+                       fprintf(stderr, "select() failed with %d: %m\n", errno);
+                       break;
+               } else if (FD_ISSET(0, &fds)) {
+                       fprintf(stderr, "Exit due to user-input\n");
+                       break;
+               } else if (FD_ISSET(fd, &fds)) {
+                       card.call_page_flip_handlers();
+               }
+       }
+}
+
 int main(int argc, char **argv)
 {
        vector<Arg> output_args = parse_cmdline(argc, argv);
 
        Card card(s_device_path);
 
+       if (!card.has_atomic() && s_flip_sync)
+               EXIT("Synchronized flipping requires atomic modesetting");
+
        vector<OutputInfo> outputs = setups_to_outputs(card, output_args);
 
        if (card.has_atomic()) {
@@ -700,7 +902,8 @@ int main(int argc, char **argv)
                }
        }
 
-       draw_test_patterns(outputs);
+       if (!s_flip_mode)
+               draw_test_patterns(outputs);
 
        print_outputs(outputs);
 
@@ -711,5 +914,8 @@ int main(int argc, char **argv)
 
        printf("press enter to exit\n");
 
-       getchar();
+       if (s_flip_mode)
+               main_flip(card, outputs);
+       else
+               getchar();
 }