summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 653d738)
raw | patch | inline | side by side (parent: 653d738)
author | Tomi Valkeinen <tomi.valkeinen@ti.com> | |
Wed, 18 Nov 2015 20:15:43 +0000 (22:15 +0200) | ||
committer | Tomi Valkeinen <tomi.valkeinen@ti.com> | |
Thu, 26 Nov 2015 20:45:18 +0000 (22:45 +0200) |
tests/testpat.cpp | patch | blob | history |
diff --git a/tests/testpat.cpp b/tests/testpat.cpp
index 85c67a3938bc76e77036e75be2ae37630abd547a..c51d3ec4cc989ac373f610ff3b937e7c339da0b5 100644 (file)
--- a/tests/testpat.cpp
+++ b/tests/testpat.cpp
#include <cstdio>
#include <algorithm>
+#include <regex>
+#include <set>
#include "kms++.h"
#include "test.h"
-#include "cmdoptions.h"
+#include "opts.h"
using namespace std;
using namespace kms;
-static map<string, CmdOption> options = {
- { "m", HAS_PARAM("Set display mode, for example 1920x1080") },
+struct PlaneInfo
+{
+ Plane* plane;
+
+ unsigned x;
+ unsigned y;
+ unsigned w;
+ unsigned h;
+
+ DumbFramebuffer* fb;
};
-int main(int argc, char **argv)
+struct OutputInfo
{
- Card card;
- CmdOptions opts(argc, argv, options);
+ Connector* connector;
- if (card.master() == false)
- printf("Not DRM master, modeset may fail\n");
+ Crtc* crtc;
+ Videomode mode;
+ bool user_set_crtc;
+ DumbFramebuffer* fb;
- auto pipes = card.get_connected_pipelines();
+ vector<PlaneInfo> planes;
+};
- vector<Framebuffer*> fbs;
+static set<Crtc*> s_used_crtcs;
+static set<Plane*> s_used_planes;
- for (auto pipe : pipes)
- {
- auto conn = pipe.connector;
- auto crtc = pipe.crtc;
+__attribute__ ((unused))
+static void print_regex_match(smatch sm)
+{
+ for (unsigned i = 0; i < sm.size(); ++i) {
+ string str = sm[i].str();
+ printf("%u: %s\n", i, str.c_str());
+ }
+}
- // RG16 XR24 UYVY YUYV NV12
+static void get_default_connector(Card& card, OutputInfo& output)
+{
+ output.connector = card.get_first_connected_connector();
+ output.mode = output.connector->get_default_mode();
+}
- auto mode = conn->get_default_mode();
+static void parse_connector(Card& card, const string& str, OutputInfo& output)
+{
+ Connector* conn = nullptr;
- if (opts.is_set("m"))
- mode = conn->get_mode(opts.opt_param("m"));
+ auto connectors = card.get_connectors();
- auto fb = new DumbFramebuffer(card, mode.hdisplay, mode.vdisplay, PixelFormat::XRGB8888);
- draw_test_pattern(*fb);
- fbs.push_back(fb);
+ if (str[0] == '@') {
+ char* endptr;
+ unsigned idx = strtoul(str.c_str() + 1, &endptr, 10);
+ if (*endptr == 0) {
+ if (idx >= connectors.size())
+ EXIT("Bad connector number '%u'", idx);
- printf("conn %u, crtc %u, fb %u\n", conn->id(), crtc->id(), fb->id());
+ conn = connectors[idx];
+ }
+ } else {
+ char* endptr;
+ unsigned id = strtoul(str.c_str(), &endptr, 10);
+ if (*endptr == 0) {
+ Connector* c = card.get_connector(id);
+ if (!c)
+ EXIT("Bad connector id '%u'", id);
- int r = crtc->set_mode(conn, *fb, mode);
- ASSERT(r == 0);
+ conn = c;
+ }
}
- for (auto pipe: pipes)
- {
- auto crtc = pipe.crtc;
+ if (!conn) {
+ auto iter = find_if(connectors.begin(), connectors.end(), [&str](Connector *c) { return c->fullname() == str; });
+ if (iter != connectors.end())
+ conn = *iter;
+ }
+
+ if (!conn)
+ EXIT("No connector '%s'", str.c_str());
+
+ if (!conn->connected())
+ EXIT("Connector '%s' not connected", conn->fullname().c_str());
- Plane* plane = 0;
+ output.connector = conn;
+ output.mode = output.connector->get_default_mode();
+}
+
+static void get_default_crtc(Card& card, OutputInfo& output)
+{
+ Crtc* crtc = output.connector->get_current_crtc();
+
+ if (crtc && s_used_crtcs.find(crtc) == s_used_crtcs.end()) {
+ s_used_crtcs.insert(crtc);
+ output.crtc = crtc;
+ return;
+ }
+
+ for (const auto& possible : output.connector->get_possible_crtcs()) {
+ if (s_used_crtcs.find(possible) == s_used_crtcs.end()) {
+ s_used_crtcs.insert(possible);
+ output.crtc = possible;
+ return;
+ }
+ }
+
+ EXIT("Could not find available crtc");
+}
+
+static void parse_crtc(Card& card, const string& crtc_str, OutputInfo& output)
+{
+ // @12:1920x1200-60
+ const regex mode_re("(?:(@?)(\\d+):)?(?:(\\d+)x(\\d+))(?:-(\\d+))?");
+
+ smatch sm;
+ if (!regex_match(crtc_str, sm, mode_re))
+ EXIT("Failed to parse crtc option '%s'", crtc_str.c_str());
+
+ if (sm[2].matched) {
+ bool use_idx = sm[1].length() == 1;
+ unsigned num = stoul(sm[2].str());
+
+ if (use_idx) {
+ auto crtcs = card.get_crtcs();
+
+ if (num >= crtcs.size())
+ EXIT("Bad crtc number '%u'", num);
+
+ output.crtc = crtcs[num];
+ } else {
+ Crtc* c = card.get_crtc(num);
+ if (!c)
+ EXIT("Bad crtc id '%u'", num);
+
+ output.crtc = c;
+ }
+ } else {
+ output.crtc = output.connector->get_current_crtc();
+ }
+
+ unsigned w = stoul(sm[3]);
+ unsigned h = stoul(sm[4]);
+ unsigned refresh = 0;
+ if (sm[5].matched)
+ refresh = stoul(sm[5]);
+
+ output.mode = output.connector->get_mode(w, h, refresh);
+}
+
+static void parse_plane(Card& card, const string& plane_str, const OutputInfo& output, PlaneInfo& pinfo)
+{
+ // 3:400,400-400x400
+ const regex plane_re("(?:(@?)(\\d+):)?(?:(\\d+),(\\d+)-)?(\\d+)x(\\d+)");
- for (Plane* p : crtc->get_possible_planes()) {
- if (p->plane_type() == PlaneType::Overlay) {
- plane = p;
- break;
+ smatch sm;
+ if (!regex_match(plane_str, sm, plane_re))
+ EXIT("Failed to parse plane option '%s'", plane_str.c_str());
+
+ if (sm[2].matched) {
+ bool use_idx = sm[1].length() == 1;
+ unsigned num = stoul(sm[2].str());
+
+ if (use_idx) {
+ auto planes = card.get_planes();
+
+ if (num >= planes.size())
+ EXIT("Bad plane number '%u'", num);
+
+ pinfo.plane = planes[num];
+ } else {
+ Plane* p = card.get_plane(num);
+ if (!p)
+ EXIT("Bad plane id '%u'", num);
+
+ pinfo.plane = p;
+ }
+ } else {
+ for (Plane* p : output.crtc->get_possible_planes()) {
+ if (s_used_planes.find(p) != s_used_planes.end())
+ continue;
+
+ if (p->plane_type() != PlaneType::Overlay)
+ continue;
+
+ pinfo.plane = p;
+ }
+
+ if (!pinfo.plane)
+ EXIT("Failed to find available plane");
+ }
+
+ s_used_planes.insert(pinfo.plane);
+
+ pinfo.w = stoul(sm[5]);
+ pinfo.h = stoul(sm[6]);
+
+ if (sm[3].matched)
+ pinfo.x = stoul(sm[3]);
+ else
+ pinfo.x = output.mode.hdisplay / 2 - pinfo.w / 2;
+
+ if (sm[4].matched)
+ pinfo.y = stoul(sm[4]);
+ else
+ pinfo.y = output.mode.vdisplay / 2 - pinfo.h / 2;
+}
+
+static DumbFramebuffer* get_default_fb(Card& card, unsigned width, unsigned height)
+{
+ auto fb = new DumbFramebuffer(card, width, height, PixelFormat::XRGB8888);
+ draw_test_pattern(*fb);
+ return fb;
+}
+
+static DumbFramebuffer* parse_fb(Card& card, const string& fb_str, unsigned def_w, unsigned def_h)
+{
+ unsigned w = def_w;
+ unsigned h = def_h;
+ PixelFormat format = PixelFormat::XRGB8888;
+
+ if (!fb_str.empty()) {
+ // XXX the regexp is not quite correct
+ // 400x400-NV12
+ const regex fb_re("(?:(\\d+)x(\\d+))?(?:-)?(\\w\\w\\w\\w)?");
+
+ smatch sm;
+ if (!regex_match(fb_str, sm, fb_re))
+ EXIT("Failed to parse fb option '%s'", fb_str.c_str());
+
+ if (sm[1].matched)
+ w = stoul(sm[1]);
+ if (sm[2].matched)
+ h = stoul(sm[2]);
+ if (sm[3].matched)
+ format = FourCCToPixelFormat(sm[3]);
+ }
+
+ auto fb = new DumbFramebuffer(card, w, h, format);
+ draw_test_pattern(*fb);
+ return fb;
+}
+
+static const char* usage_str =
+ "Usage: testpat [OPTION]...\n\n"
+ "Show a test pattern on a display or plane\n\n"
+ "Options:\n"
+ " --device=DEVICE DEVICE is the path to DRM card to open\n"
+ " -c, --connector=CONN CONN is <connector>\n"
+ " -r, --crtc=CRTC CRTC is [<crtc>:]<w>x<h>[@<Hz>]\n"
+ " -p, --plane=PLANE PLANE is [<plane>:][<x>,<y>-]<w>x<h>\n"
+ " -f, --fb=FB FB is [<w>x<h>][-][<4cc>]\n"
+ "\n"
+ "<connector>, <crtc> and <plane> can be given by id (<id>) or index (@<idx>).\n"
+ "<connector> can also be given by name.\n"
+ "\n"
+ "Options can be given multiple times to set up multiple displays or planes.\n"
+ "Options may apply to previous options, e.g. a plane will be set on a crtc set in\n"
+ "an earlier option.\n"
+ "If you omit parameters, testpat tries to guess what you mean\n"
+ "\n"
+ "Examples:\n"
+ "\n"
+ "Set eDP-1 mode to 1920x1080@60, show XR24 framebuffer on the crtc, and a 400x400 XB24 plane:\n"
+ " testpat -c eDP-1 -r 1920x1080@60 -f XR24 -p 400x400 -f XB24\n\n"
+ "XR24 framebuffer on first connected connector in the default mode:\n"
+ " testpat -f XR24\n\n"
+ "XR24 framebuffer on a 400x400 plane on the first connected connector in the default mode:\n"
+ " testpat -p 400x400 -f XR24\n\n"
+ "Test pattern on the second connector with default mode:\n"
+ " testpat -c @1\n"
+ ;
+
+static void usage()
+{
+ puts(usage_str);
+}
+
+enum class ObjectType
+{
+ Connector,
+ Crtc,
+ Plane,
+ Framebuffer,
+};
+
+struct Arg
+{
+ ObjectType type;
+ string arg;
+};
+
+static string s_device_path = "/dev/dri/card0";
+
+static vector<Arg> parse_cmdline(int argc, char **argv)
+{
+ vector<Arg> args;
+
+ OptionSet optionset = {
+ Option("|device=",
+ [&](string s)
+ {
+ s_device_path = s;
+ }),
+ Option("c|connector=",
+ [&](string s)
+ {
+ args.push_back(Arg { ObjectType::Connector, s });
+ }),
+ Option("r|crtc=", [&](string s)
+ {
+ args.push_back(Arg { ObjectType::Crtc, s });
+ }),
+ Option("p|plane=", [&](string s)
+ {
+ args.push_back(Arg { ObjectType::Plane, s });
+ }),
+ Option("f|fb=", [&](string s)
+ {
+ args.push_back(Arg { ObjectType::Framebuffer, s });
+ }),
+ Option("h|help", [&]()
+ {
+ usage();
+ exit(-1);
+ }),
+ };
+
+ optionset.parse(argc, argv);
+
+ if (optionset.params().size() > 0) {
+ usage();
+ exit(-1);
+ }
+
+ return args;
+}
+
+static vector<OutputInfo> setups_to_outputs(Card& card, const vector<Arg>& output_args)
+{
+ vector<OutputInfo> outputs;
+
+ if (output_args.size() == 0) {
+ // no output args, show a pattern on all screens
+ for (auto& pipe : card.get_connected_pipelines()) {
+ OutputInfo output = { };
+ output.connector = pipe.connector;
+ output.crtc = pipe.crtc;
+ output.mode = output.connector->get_default_mode();
+
+ output.fb = get_default_fb(card, output.mode.hdisplay, output.mode.vdisplay);
+
+ outputs.push_back(output);
+ }
+
+ return outputs;
+ }
+
+ OutputInfo* current_output = 0;
+ PlaneInfo* current_plane = 0;
+
+ for (auto& arg : output_args) {
+ switch (arg.type) {
+ case ObjectType::Connector:
+ {
+ outputs.push_back(OutputInfo { });
+ current_output = &outputs.back();
+
+ parse_connector(card, arg.arg, *current_output);
+ current_plane = 0;
+
+ break;
+ }
+
+ case ObjectType::Crtc:
+ {
+ if (!current_output) {
+ outputs.push_back(OutputInfo { });
+ current_output = &outputs.back();
+ }
+
+ if (!current_output->connector)
+ get_default_connector(card, *current_output);
+
+ parse_crtc(card, arg.arg, *current_output);
+
+ current_output->user_set_crtc = true;
+
+ current_plane = 0;
+
+ break;
+ }
+
+ case ObjectType::Plane:
+ {
+ if (!current_output) {
+ outputs.push_back(OutputInfo { });
+ current_output = &outputs.back();
+ }
+
+ if (!current_output->connector)
+ get_default_connector(card, *current_output);
+
+ if (!current_output->crtc)
+ get_default_crtc(card, *current_output);
+
+ current_output->planes.push_back(PlaneInfo { });
+ current_plane = ¤t_output->planes.back();
+
+ parse_plane(card, arg.arg, *current_output, *current_plane);
+
+ break;
+ }
+
+ case ObjectType::Framebuffer:
+ {
+ if (!current_output) {
+ outputs.push_back(OutputInfo { });
+ current_output = &outputs.back();
+ }
+
+ if (!current_output->connector)
+ get_default_connector(card, *current_output);
+
+ if (!current_output->crtc)
+ get_default_crtc(card, *current_output);
+
+ int def_w, def_h;
+
+ if (current_plane) {
+ def_w = current_plane->w;
+ def_h = current_plane->h;
+ } else {
+ def_w = current_output->mode.hdisplay;
+ def_h = current_output->mode.vdisplay;
}
+
+ auto fb = parse_fb(card, arg.arg, def_w, def_h);
+
+ if (current_plane)
+ current_plane->fb = fb;
+ else
+ current_output->fb = fb;
+
+ break;
+ }
+ }
+ }
+
+ // create default framebuffers if needed
+ for (OutputInfo& o : outputs) {
+ if (!o.crtc) {
+ get_default_crtc(card, *current_output);
+ o.user_set_crtc = true;
+ }
+
+ if (!o.fb && o.user_set_crtc)
+ o.fb = get_default_fb(card, o.mode.hdisplay, o.mode.vdisplay);
+
+ for (PlaneInfo &p : o.planes) {
+ if (!p.fb)
+ p.fb = get_default_fb(card, p.w, p.h);
+ }
+ }
+
+ return outputs;
+}
+
+static std::string videomode_to_string(const Videomode& mode)
+{
+ unsigned hfp, hsw, hbp;
+ unsigned vfp, vsw, vbp;
+
+ hfp = mode.hsync_start - mode.hdisplay;
+ hsw = mode.hsync_end - mode.hsync_start;
+ hbp = mode.htotal - mode.hsync_end;
+
+ vfp = mode.vsync_start - mode.vdisplay;
+ vsw = mode.vsync_end - mode.vsync_start;
+ vbp = mode.vtotal - mode.vsync_end;
+
+ char buf[256];
+
+ sprintf(buf, "%.2f MHz %u/%u/%u/%u %u/%u/%u/%u %uHz",
+ mode.clock / 1000.0,
+ mode.hdisplay, hfp, hsw, hbp,
+ mode.vdisplay, vfp, vsw, vbp,
+ mode.vrefresh);
+
+ return std::string(buf);
+}
+
+static void print_outputs(const vector<OutputInfo>& outputs)
+{
+ for (unsigned i = 0; i < outputs.size(); ++i) {
+ const OutputInfo& o = outputs[i];
+
+ printf("Connector %u/@%u: %s\n", o.connector->id(), o.connector->idx(),
+ o.connector->fullname().c_str());
+ printf(" Crtc %u/@%u: %ux%u-%u (%s)\n", o.crtc->id(), o.crtc->idx(),
+ o.mode.hdisplay, o.mode.vdisplay, o.mode.vrefresh,
+ videomode_to_string(o.mode).c_str());
+ if (o.fb)
+ printf(" Fb %ux%u-%s\n", o.fb->width(), o.fb->height(),
+ PixelFormatToFourCC(o.fb->format()).c_str());
+
+ for (unsigned j = 0; j < o.planes.size(); ++j) {
+ const PlaneInfo& p = o.planes[j];
+ printf(" Plane %u/@%u: %u,%u-%ux%u\n", p.plane->id(), p.plane->idx(),
+ p.x, p.y, p.w, p.h);
+ printf(" Fb %ux%u-%s\n", p.fb->width(), p.fb->height(),
+ PixelFormatToFourCC(p.fb->format()).c_str());
}
+ }
+}
- if (plane) {
- auto planefb = new DumbFramebuffer(card, 400, 400, PixelFormat::YUYV);
- draw_test_pattern(*planefb);
- fbs.push_back(planefb);
+static void set_crtcs_n_planes(Card& card, const vector<OutputInfo>& outputs)
+{
+ for (const OutputInfo& o : outputs) {
+ auto conn = o.connector;
+ auto crtc = o.crtc;
- int r = crtc->set_plane(plane, *planefb,
- 0, 0, planefb->width(), planefb->height(),
- 0, 0, planefb->width(), planefb->height());
+ if (o.fb) {
+ int r = crtc->set_mode(conn, *o.fb, o.mode);
+ if (r)
+ printf("crtc->set_mode() failed for crtc %u: %s\n",
+ crtc->id(), strerror(-r));
+ }
- ASSERT(r == 0);
+ for (const PlaneInfo& p : o.planes) {
+ int r = crtc->set_plane(p.plane, *p.fb,
+ p.x, p.y, p.w, p.h,
+ 0, 0, p.fb->width(), p.fb->height());
+ if (r)
+ printf("crtc->set_plane() failed for plane %u: %s\n",
+ p.plane->id(), strerror(-r));
}
}
+}
+
+int main(int argc, char **argv)
+{
+ vector<Arg> output_args = parse_cmdline(argc, argv);
+
+ Card card(s_device_path);
+
+ vector<OutputInfo> outputs = setups_to_outputs(card, output_args);
+
+ print_outputs(outputs);
+
+ set_crtcs_n_planes(card, outputs);
printf("press enter to exit\n");
getchar();
-
- for(auto fb : fbs)
- delete fb;
}