Audio: setParam improve status_t to Result consistency
The rest of the API (*::analyseStatus) returns NOT_SUPPORTED
when the legacy API returns -ENOSYS.
setParameter legacy -> treble shim did not follow this
conversion due to the legacy API stating that for get_paramers,
-ENOSYS should be returned if
"the implementation does not accept a parameter change while the
output is active but the parameter is acceptable otherwise",
aka INVALID_STATE.
Thus setParameter shim used to return
- OK for OK
- INVALID_STATE for -ENOSYS
- INVALID_ARGUMENTS for everything else
This leads to several problems:
- an implementation of the legacy API can not report NOT_SUPPORTED
- is inconsistent with the rest of the status_t conversion methods
- shim methods implemented over getParameter can not distinguish
failures error required by the .hal documentation
Most importantly, on the system side, the Result is transformed to a
status_t again but without any special logic for methods wrapping
getParameter in the shim.
This can not be changed as the system can not know which methods
are implemented with a legacy wrapper under the Treble API boundary.
Thus setParam now converts status_t to Result in the same way
as all the other shim methods.
Bug: 72873273
Bug: 69811500
Bug: 69010523
Test: playback and record for media and voice call
Change-Id: I41204c0807d2bd4675e941771cbc9a43d7d14855
Merged-In: I41204c0807d2bd4675e941771cbc9a43d7d14855
Signed-off-by: Kevin Rocard <krocard@google.com>
- [DH] audio/core/4.0/default/Device.cpp
- [DH] audio/core/4.0/default/ParametersUtil.cpp
- [DH] audio/core/4.0/default/PrimaryDevice.cpp
- [DH] audio/core/4.0/default/Stream.cpp
- [DH] audio/core/4.0/default/StreamIn.cpp
- [DH] audio/core/4.0/default/StreamOut.cpp
- [DH] audio/core/4.0/default/include/core/4.0/default/Util.h