Merge "DRM 1.1: Add VINTF doc"
[android/platform-hardware-interfaces.git] / audio / README
1 Directory structure of the audio HIDL related code.
3 audio
4 |-- 2.0              <== HIDL (.hal) can not be moved to fit the directory structure
5 |                        because that would create a separate HAL
6 |-- 4.0              <== Version 4.0 of the core API
7 |
8 |-- common           <== code common to audio core and effect API
9 |   |-- 2.0
10 |   |   |-- default  <== code that wraps the legacy API
11 |   |   `-- vts      <== vts of 2.0 core and effect API common code
12 |   |-- 4.0
13 |   |   |-- default
14 |   |   `-- vts
15 |   |-- ...          <== The future versions should continue this structure
16 |   |   |-- default
17 |   |   `-- vts
18 |   `-- all_versions <== code common to all version of both core and effect API
19 |       |-- default
20 |       `-- vts      <== vts of core and effect API common version independent code
21 |
22 |-- core           <== code relative to the core API
23 |   |-- 2.0          <== 2.0 core API code (except .hal, see audio/2.0)
24 |   |   |-- default
25 |   |   `-- vts
26 |   |-- 4.0
27 |   |   |-- default  <== default implementation of the core 4.0 api
28 |   |   `-- vts      <== vts code of the 4.0 API
29 |   |-- ...
30 |   |   |-- default
31 |   |   `-- vts
32 |   `-- all_versions
33 |       |-- default
34 |       `-- vts      <== vts of core API common version independent code
35 |
36 `-- effect           <== idem for the effect API
37     |-- 2.0
38     |   |-- default
39     |   `-- vts
40     |-- 4.0
41     |   |-- default
42     |   `-- vts
43     |-- ...
44     |   |-- default
45     |   `-- vts
46     `-- all_versions
47         |-- default
48         `-- vts