]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android/platform-hardware-interfaces.git/blob - audio/common/2.0/types.hal
Merge "Remove redundant dependencies" am: 62769b7196 am: 170e2e85a2
[android/platform-hardware-interfaces.git] / audio / common / 2.0 / types.hal
1 /*
2  * Copyright (C) 2016 The Android Open Source Project
3  *
4  * Licensed under the Apache License, Version 2.0 (the "License");
5  * you may not use this file except in compliance with the License.
6  * You may obtain a copy of the License at
7  *
8  *      http://www.apache.org/licenses/LICENSE-2.0
9  *
10  * Unless required by applicable law or agreed to in writing, software
11  * distributed under the License is distributed on an "AS IS" BASIS,
12  * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
13  * See the License for the specific language governing permissions and
14  * limitations under the License.
15  */
17 package android.hardware.audio.common@2.0;
19 /**
20  *
21  *  IDs and Handles
22  *
23  */
25 /**
26  * Handle type for identifying audio sources and sinks.
27  */
28 typedef int32_t AudioIoHandle;
30 /**
31  * Audio hw module handle functions or structures referencing a module.
32  */
33 typedef int32_t AudioModuleHandle;
35 /**
36  * Each port has a unique ID or handle allocated by policy manager.
37  */
38 typedef int32_t AudioPortHandle;
40 /**
41  * Each patch is identified by a handle at the interface used to create that
42  * patch. For instance, when a patch is created by the audio HAL, the HAL
43  * allocates and returns a handle.  This handle is unique to a given audio HAL
44  * hardware module.  But the same patch receives another system wide unique
45  * handle allocated by the framework.  This unique handle is used for all
46  * transactions inside the framework.
47  */
48 typedef int32_t AudioPatchHandle;
50 /**
51  * A HW synchronization source returned by the audio HAL.
52  */
53 typedef uint32_t AudioHwSync;
55 /**
56  * Each port has a unique ID or handle allocated by policy manager.
57  */
58 @export(name="")
59 enum AudioHandleConsts : int32_t {
60     AUDIO_IO_HANDLE_NONE = 0,
61     AUDIO_MODULE_HANDLE_NONE = 0,
62     AUDIO_PORT_HANDLE_NONE = 0,
63     AUDIO_PATCH_HANDLE_NONE = 0,
64 };
66 /**
67  * Commonly used structure for passing unique identifieds (UUID).
68  * For the definition of UUID, refer to ITU-T X.667 spec.
69  */
70 struct Uuid {
71     uint32_t timeLow;
72     uint16_t timeMid;
73     uint16_t versionAndTimeHigh;
74     uint16_t variantAndClockSeqHigh;
75     uint8_t[6] node;
76 };
79 /**
80  *
81  *  Audio streams
82  *
83  */
85 /**
86  * Audio stream type describing the intented use case of a stream.
87  */
88 @export(name="audio_stream_type_t", value_prefix="AUDIO_STREAM_")
89 enum AudioStreamType : int32_t {
90     // These values must kept in sync with
91     //  frameworks/base/media/java/android/media/AudioSystem.java
92     DEFAULT          = -1,
93     MIN              = 0,
94     VOICE_CALL       = 0,
95     SYSTEM           = 1,
96     RING             = 2,
97     MUSIC            = 3,
98     ALARM            = 4,
99     NOTIFICATION     = 5,
100     BLUETOOTH_SCO    = 6,
101     ENFORCED_AUDIBLE = 7,  // Sounds that cannot be muted by user and must be
102                            // routed to speaker
103     DTMF             = 8,
104     TTS              = 9,  // Transmitted Through Speaker.  Plays over speaker
105                            // only, silent on other devices
106     ACCESSIBILITY    = 10, // For accessibility talk back prompts
107     REROUTING        = 11, // For dynamic policy output mixes
108     PATCH            = 12, // For internal audio flinger tracks.  Fixed volume
109     PUBLIC_CNT       = ACCESSIBILITY + 1,
110     // Number of streams considered by audio policy for volume and routing
111     FOR_POLICY_CNT   = PATCH,
112     CNT              = PATCH + 1
113 };
115 @export(name="audio_source_t", value_prefix="AUDIO_SOURCE_")
116 enum AudioSource : int32_t {
117     // These values must kept in sync with
118     //  frameworks/base/media/java/android/media/MediaRecorder.java,
119     //  frameworks/av/services/audiopolicy/AudioPolicyService.cpp,
120     //  system/media/audio_effects/include/audio_effects/audio_effects_conf.h
121     DEFAULT             = 0,
122     MIC                 = 1,
123     VOICE_UPLINK        = 2,
124     VOICE_DOWNLINK      = 3,
125     VOICE_CALL          = 4,
126     CAMCORDER           = 5,
127     VOICE_RECOGNITION   = 6,
128     VOICE_COMMUNICATION = 7,
129     /**
130      * Source for the mix to be presented remotely. An example of remote
131      * presentation is Wifi Display where a dongle attached to a TV can be used
132      * to play the mix captured by this audio source.
133      */
134     REMOTE_SUBMIX       = 8,
135     /**
136      * Source for unprocessed sound. Usage examples include level measurement
137      * and raw signal analysis.
138      */
139     UNPROCESSED         = 9,
141     CNT,
142     MAX                 = CNT - 1,
143     FM_TUNER            = 1998,
144     /**
145      * A low-priority, preemptible audio source for for background software
146      * hotword detection. Same tuning as VOICE_RECOGNITION.  Used only
147      * internally by the framework.
148      */
149     HOTWORD             = 1999
150 };
152 typedef int32_t AudioSession;
153 /**
154  * Special audio session values.
155  */
156 @export(name="audio_session_t", value_prefix="AUDIO_SESSION_")
157 enum AudioSessionConsts : int32_t {
158     /**
159      * Session for effects attached to a particular output stream
160      * (value must be less than 0)
161      */
162     OUTPUT_STAGE = -1,
163     /**
164      * Session for effects applied to output mix. These effects can
165      * be moved by audio policy manager to another output stream
166      * (value must be 0)
167      */
168     OUTPUT_MIX = 0,
169     /**
170      * Application does not specify an explicit session ID to be used, and
171      * requests a new session ID to be allocated. Corresponds to
172      * AudioManager.AUDIO_SESSION_ID_GENERATE and
173      * AudioSystem.AUDIO_SESSION_ALLOCATE.
174      */
175     ALLOCATE = 0,
176     /**
177      * For use with AudioRecord::start(), this indicates no trigger session.
178      * It is also used with output tracks and patch tracks, which never have a
179      * session.
180      */
181     NONE = 0
182 };
184 /**
185  * Audio format  is a 32-bit word that consists of:
186  *   main format field (upper 8 bits)
187  *   sub format field (lower 24 bits).
188  *
189  * The main format indicates the main codec type. The sub format field indicates
190  * options and parameters for each format. The sub format is mainly used for
191  * record to indicate for instance the requested bitrate or profile.  It can
192  * also be used for certain formats to give informations not present in the
193  * encoded audio stream (e.g. octet alignement for AMR).
194  */
195 @export(name="audio_format_t", value_prefix="AUDIO_FORMAT_")
196 enum AudioFormat : uint32_t {
197     INVALID             = 0xFFFFFFFFUL,
198     DEFAULT             = 0,
199     PCM                 = 0x00000000UL, /** DO NOT CHANGE */
200     MP3                 = 0x01000000UL,
201     AMR_NB              = 0x02000000UL,
202     AMR_WB              = 0x03000000UL,
203     AAC                 = 0x04000000UL,
204     HE_AAC_V1           = 0x05000000UL, /** Deprecated, Use AAC_HE_V1 */
205     HE_AAC_V2           = 0x06000000UL, /** Deprecated, Use AAC_HE_V2 */
206     VORBIS              = 0x07000000UL,
207     OPUS                = 0x08000000UL,
208     AC3                 = 0x09000000UL,
209     E_AC3               = 0x0A000000UL,
210     DTS                 = 0x0B000000UL,
211     DTS_HD              = 0x0C000000UL,
212     // IEC61937 is encoded audio wrapped in 16-bit PCM.
213     IEC61937            = 0x0D000000UL,
214     DOLBY_TRUEHD        = 0x0E000000UL,
215     EVRC                = 0x10000000UL,
216     EVRCB               = 0x11000000UL,
217     EVRCWB              = 0x12000000UL,
218     EVRCNW              = 0x13000000UL,
219     AAC_ADIF            = 0x14000000UL,
220     WMA                 = 0x15000000UL,
221     WMA_PRO             = 0x16000000UL,
222     AMR_WB_PLUS         = 0x17000000UL,
223     MP2                 = 0x18000000UL,
224     QCELP               = 0x19000000UL,
225     DSD                 = 0x1A000000UL,
226     FLAC                = 0x1B000000UL,
227     ALAC                = 0x1C000000UL,
228     APE                 = 0x1D000000UL,
229     AAC_ADTS            = 0x1E000000UL,
230     SBC                 = 0x1F000000UL,
231     APTX                = 0x20000000UL,
232     APTX_HD             = 0x21000000UL,
233     AC4                 = 0x22000000UL,
234     LDAC                = 0x23000000UL,
235     MAIN_MASK           = 0xFF000000UL, /** Deprecated */
236     SUB_MASK            = 0x00FFFFFFUL,
238     /** Subformats */
239     PCM_SUB_16_BIT        = 0x1, // PCM signed 16 bits
240     PCM_SUB_8_BIT         = 0x2, // PCM unsigned 8 bits
241     PCM_SUB_32_BIT        = 0x3, // PCM signed .31 fixed point
242     PCM_SUB_8_24_BIT      = 0x4, // PCM signed 8.23 fixed point
243     PCM_SUB_FLOAT         = 0x5, // PCM single-precision float pt
244     PCM_SUB_24_BIT_PACKED = 0x6, // PCM signed .23 fix pt (3 bytes)
246     MP3_SUB_NONE          = 0x0,
248     AMR_SUB_NONE          = 0x0,
250     AAC_SUB_MAIN          = 0x1,
251     AAC_SUB_LC            = 0x2,
252     AAC_SUB_SSR           = 0x4,
253     AAC_SUB_LTP           = 0x8,
254     AAC_SUB_HE_V1         = 0x10,
255     AAC_SUB_SCALABLE      = 0x20,
256     AAC_SUB_ERLC          = 0x40,
257     AAC_SUB_LD            = 0x80,
258     AAC_SUB_HE_V2         = 0x100,
259     AAC_SUB_ELD           = 0x200,
261     VORBIS_SUB_NONE       = 0x0,
263     /** Aliases */
264     /** note != AudioFormat.ENCODING_PCM_16BIT */
265     PCM_16_BIT          = (PCM | PCM_SUB_16_BIT),
266     /** note != AudioFormat.ENCODING_PCM_8BIT */
267     PCM_8_BIT           = (PCM | PCM_SUB_8_BIT),
268     PCM_32_BIT          = (PCM | PCM_SUB_32_BIT),
269     PCM_8_24_BIT        = (PCM | PCM_SUB_8_24_BIT),
270     PCM_FLOAT           = (PCM | PCM_SUB_FLOAT),
271     PCM_24_BIT_PACKED   = (PCM | PCM_SUB_24_BIT_PACKED),
272     AAC_MAIN            = (AAC | AAC_SUB_MAIN),
273     AAC_LC              = (AAC | AAC_SUB_LC),
274     AAC_SSR             = (AAC | AAC_SUB_SSR),
275     AAC_LTP             = (AAC | AAC_SUB_LTP),
276     AAC_HE_V1           = (AAC | AAC_SUB_HE_V1),
277     AAC_SCALABLE        = (AAC | AAC_SUB_SCALABLE),
278     AAC_ERLC            = (AAC | AAC_SUB_ERLC),
279     AAC_LD              = (AAC | AAC_SUB_LD),
280     AAC_HE_V2           = (AAC | AAC_SUB_HE_V2),
281     AAC_ELD             = (AAC | AAC_SUB_ELD),
282     AAC_ADTS_MAIN       = (AAC_ADTS | AAC_SUB_MAIN),
283     AAC_ADTS_LC         = (AAC_ADTS | AAC_SUB_LC),
284     AAC_ADTS_SSR        = (AAC_ADTS | AAC_SUB_SSR),
285     AAC_ADTS_LTP        = (AAC_ADTS | AAC_SUB_LTP),
286     AAC_ADTS_HE_V1      = (AAC_ADTS | AAC_SUB_HE_V1),
287     AAC_ADTS_SCALABLE   = (AAC_ADTS | AAC_SUB_SCALABLE),
288     AAC_ADTS_ERLC       = (AAC_ADTS | AAC_SUB_ERLC),
289     AAC_ADTS_LD         = (AAC_ADTS | AAC_SUB_LD),
290     AAC_ADTS_HE_V2      = (AAC_ADTS | AAC_SUB_HE_V2),
291     AAC_ADTS_ELD        = (AAC_ADTS | AAC_SUB_ELD)
292 };
294 /**
295  * Usage of these values highlights places in the code that use 2- or 8- channel
296  * assumptions.
297  */
298 @export(name="")
299 enum FixedChannelCount : int32_t {
300     FCC_2 = 2, // This is typically due to legacy implementation of stereo I/O
301     FCC_8 = 8  // This is typically due to audio mixer and resampler limitations
302 };
304 /**
305  * A channel mask per se only defines the presence or absence of a channel, not
306  * the order.  See AUDIO_INTERLEAVE_* for the platform convention of order.
307  *
308  * AudioChannelMask is an opaque type and its internal layout should not be
309  * assumed as it may change in the future.  Instead, always use functions
310  * to examine it.
311  *
312  * These are the current representations:
313  *
314  *   REPRESENTATION_POSITION
315  *     is a channel mask representation for position assignment.  Each low-order
316  *     bit corresponds to the spatial position of a transducer (output), or
317  *     interpretation of channel (input).  The user of a channel mask needs to
318  *     know the context of whether it is for output or input.  The constants
319  *     OUT_* or IN_* apply to the bits portion.  It is not permitted for no bits
320  *     to be set.
321  *
322  *   REPRESENTATION_INDEX
323  *     is a channel mask representation for index assignment.  Each low-order
324  *     bit corresponds to a selected channel.  There is no platform
325  *     interpretation of the various bits.  There is no concept of output or
326  *     input.  It is not permitted for no bits to be set.
327  *
328  * All other representations are reserved for future use.
329  *
330  * Warning: current representation distinguishes between input and output, but
331  * this will not the be case in future revisions of the platform. Wherever there
332  * is an ambiguity between input and output that is currently resolved by
333  * checking the channel mask, the implementer should look for ways to fix it
334  * with additional information outside of the mask.
335  */
336 @export(name="", value_prefix="AUDIO_CHANNEL_")
337 enum AudioChannelMask : uint32_t {
338     REPRESENTATION_POSITION = 0, /** must be 0 for compatibility */
339     /** 1 is reserved for future use */
340     REPRESENTATION_INDEX    = 2,
341     /** 3 is reserved for future use */
343     /** These can be a complete value of AudioChannelMask */
344     NONE                      = 0x0,
345     INVALID                   = 0xC0000000,
347    /**
348     * These can be the bits portion of an AudioChannelMask
349     * with representation REPRESENTATION_POSITION.
350     */
352     /** output channels */
353     OUT_FRONT_LEFT            = 0x1,
354     OUT_FRONT_RIGHT           = 0x2,
355     OUT_FRONT_CENTER          = 0x4,
356     OUT_LOW_FREQUENCY         = 0x8,
357     OUT_BACK_LEFT             = 0x10,
358     OUT_BACK_RIGHT            = 0x20,
359     OUT_FRONT_LEFT_OF_CENTER  = 0x40,
360     OUT_FRONT_RIGHT_OF_CENTER = 0x80,
361     OUT_BACK_CENTER           = 0x100,
362     OUT_SIDE_LEFT             = 0x200,
363     OUT_SIDE_RIGHT            = 0x400,
364     OUT_TOP_CENTER            = 0x800,
365     OUT_TOP_FRONT_LEFT        = 0x1000,
366     OUT_TOP_FRONT_CENTER      = 0x2000,
367     OUT_TOP_FRONT_RIGHT       = 0x4000,
368     OUT_TOP_BACK_LEFT         = 0x8000,
369     OUT_TOP_BACK_CENTER       = 0x10000,
370     OUT_TOP_BACK_RIGHT        = 0x20000,
372     OUT_MONO     = OUT_FRONT_LEFT,
373     OUT_STEREO   = (OUT_FRONT_LEFT | OUT_FRONT_RIGHT),
374     OUT_2POINT1  = (OUT_FRONT_LEFT | OUT_FRONT_RIGHT | OUT_LOW_FREQUENCY),
375     OUT_QUAD     = (OUT_FRONT_LEFT | OUT_FRONT_RIGHT |
376             OUT_BACK_LEFT | OUT_BACK_RIGHT),
377     OUT_QUAD_BACK = OUT_QUAD,
378     /** like OUT_QUAD_BACK with *_SIDE_* instead of *_BACK_* */
379     OUT_QUAD_SIDE = (OUT_FRONT_LEFT | OUT_FRONT_RIGHT |
380             OUT_SIDE_LEFT | OUT_SIDE_RIGHT),
381     OUT_SURROUND = (OUT_FRONT_LEFT | OUT_FRONT_RIGHT |
382             OUT_FRONT_CENTER | OUT_BACK_CENTER),
383     OUT_PENTA = (OUT_QUAD | OUT_FRONT_CENTER),
384     OUT_5POINT1   = (OUT_FRONT_LEFT | OUT_FRONT_RIGHT |
385             OUT_FRONT_CENTER | OUT_LOW_FREQUENCY |
386             OUT_BACK_LEFT | OUT_BACK_RIGHT),
387     OUT_5POINT1_BACK = OUT_5POINT1,
388     /** like OUT_5POINT1_BACK with *_SIDE_* instead of *_BACK_* */
389     OUT_5POINT1_SIDE = (OUT_FRONT_LEFT | OUT_FRONT_RIGHT |
390             OUT_FRONT_CENTER | OUT_LOW_FREQUENCY |
391             OUT_SIDE_LEFT | OUT_SIDE_RIGHT),
392     OUT_6POINT1 = (OUT_FRONT_LEFT | OUT_FRONT_RIGHT |
393             OUT_FRONT_CENTER | OUT_LOW_FREQUENCY |
394             OUT_BACK_LEFT | OUT_BACK_RIGHT |
395             OUT_BACK_CENTER),
396     /** matches the correct AudioFormat.CHANNEL_OUT_7POINT1_SURROUND */
397     OUT_7POINT1  = (OUT_FRONT_LEFT | OUT_FRONT_RIGHT |
398             OUT_FRONT_CENTER | OUT_LOW_FREQUENCY |
399             OUT_BACK_LEFT | OUT_BACK_RIGHT |
400             OUT_SIDE_LEFT | OUT_SIDE_RIGHT),
401     OUT_ALL      = (OUT_FRONT_LEFT | OUT_FRONT_RIGHT |
402             OUT_FRONT_CENTER | OUT_LOW_FREQUENCY |
403             OUT_BACK_LEFT | OUT_BACK_RIGHT |
404             OUT_FRONT_LEFT_OF_CENTER | OUT_FRONT_RIGHT_OF_CENTER |
405             OUT_BACK_CENTER |
406             OUT_SIDE_LEFT | OUT_SIDE_RIGHT |
407             OUT_TOP_CENTER |
408             OUT_TOP_FRONT_LEFT | OUT_TOP_FRONT_CENTER | OUT_TOP_FRONT_RIGHT |
409             OUT_TOP_BACK_LEFT | OUT_TOP_BACK_CENTER | OUT_TOP_BACK_RIGHT),
411     /** These are bits only, not complete values */
413     /** input channels */
414     IN_LEFT            = 0x4,
415     IN_RIGHT           = 0x8,
416     IN_FRONT           = 0x10,
417     IN_BACK            = 0x20,
418     IN_LEFT_PROCESSED  = 0x40,
419     IN_RIGHT_PROCESSED = 0x80,
420     IN_FRONT_PROCESSED = 0x100,
421     IN_BACK_PROCESSED  = 0x200,
422     IN_PRESSURE        = 0x400,
423     IN_X_AXIS          = 0x800,
424     IN_Y_AXIS          = 0x1000,
425     IN_Z_AXIS          = 0x2000,
426     IN_VOICE_UPLINK    = 0x4000,
427     IN_VOICE_DNLINK    = 0x8000,
429     IN_MONO   = IN_FRONT,
430     IN_STEREO = (IN_LEFT | IN_RIGHT),
431     IN_FRONT_BACK = (IN_FRONT | IN_BACK),
432     IN_6 = (IN_LEFT | IN_RIGHT |
433             IN_FRONT | IN_BACK |
434             IN_LEFT_PROCESSED | IN_RIGHT_PROCESSED),
435     IN_VOICE_UPLINK_MONO = (IN_VOICE_UPLINK | IN_MONO),
436     IN_VOICE_DNLINK_MONO = (IN_VOICE_DNLINK | IN_MONO),
437     IN_VOICE_CALL_MONO   = (IN_VOICE_UPLINK_MONO |
438             IN_VOICE_DNLINK_MONO),
439     IN_ALL    = (IN_LEFT | IN_RIGHT | IN_FRONT | IN_BACK|
440             IN_LEFT_PROCESSED | IN_RIGHT_PROCESSED |
441             IN_FRONT_PROCESSED | IN_BACK_PROCESSED|
442             IN_PRESSURE |
443             IN_X_AXIS | IN_Y_AXIS | IN_Z_AXIS |
444             IN_VOICE_UPLINK | IN_VOICE_DNLINK),
446     COUNT_MAX    = 30,
447     INDEX_HDR    = REPRESENTATION_INDEX << COUNT_MAX,
448     INDEX_MASK_1 = INDEX_HDR | ((1 << 1) - 1),
449     INDEX_MASK_2 = INDEX_HDR | ((1 << 2) - 1),
450     INDEX_MASK_3 = INDEX_HDR | ((1 << 3) - 1),
451     INDEX_MASK_4 = INDEX_HDR | ((1 << 4) - 1),
452     INDEX_MASK_5 = INDEX_HDR | ((1 << 5) - 1),
453     INDEX_MASK_6 = INDEX_HDR | ((1 << 6) - 1),
454     INDEX_MASK_7 = INDEX_HDR | ((1 << 7) - 1),
455     INDEX_MASK_8 = INDEX_HDR | ((1 << 8) - 1)
456 };
459 /**
460  * Expresses the convention when stereo audio samples are stored interleaved
461  * in an array.  This should improve readability by allowing code to use
462  * symbolic indices instead of hard-coded [0] and [1].
463  *
464  * For multi-channel beyond stereo, the platform convention is that channels
465  * are interleaved in order from least significant channel mask bit to most
466  * significant channel mask bit, with unused bits skipped.  Any exceptions
467  * to this convention will be noted at the appropriate API.
468  */
469 @export(name="", value_prefix="AUDIO_INTERLEAVE_")
470 enum AudioInterleave : int32_t {
471     LEFT   = 0,
472     RIGHT  = 1,
473 };
475 /**
476  * Major modes for a mobile device. The current mode setting affects audio
477  * routing.
478  */
479 @export(name="audio_mode_t", value_prefix="AUDIO_MODE_")
480 enum AudioMode : int32_t {
481     INVALID          = -2,
482     CURRENT          = -1,
483     NORMAL           = 0,
484     RINGTONE         = 1,
485     IN_CALL          = 2,
486     IN_COMMUNICATION = 3,
488     CNT,
489     MAX              = CNT - 1,
490 };
492 @export(name="", value_prefix="AUDIO_DEVICE_")
493 enum AudioDevice : uint32_t {
494     NONE                          = 0x0,
495     /** reserved bits */
496     BIT_IN                        = 0x80000000,
497     BIT_DEFAULT                   = 0x40000000,
498     /** output devices */
499     OUT_EARPIECE                  = 0x1,
500     OUT_SPEAKER                   = 0x2,
501     OUT_WIRED_HEADSET             = 0x4,
502     OUT_WIRED_HEADPHONE           = 0x8,
503     OUT_BLUETOOTH_SCO             = 0x10,
504     OUT_BLUETOOTH_SCO_HEADSET     = 0x20,
505     OUT_BLUETOOTH_SCO_CARKIT      = 0x40,
506     OUT_BLUETOOTH_A2DP            = 0x80,
507     OUT_BLUETOOTH_A2DP_HEADPHONES = 0x100,
508     OUT_BLUETOOTH_A2DP_SPEAKER    = 0x200,
509     OUT_AUX_DIGITAL               = 0x400,
510     OUT_HDMI                      = OUT_AUX_DIGITAL,
511     /** uses an analog connection (multiplexed over the USB pins for instance) */
512     OUT_ANLG_DOCK_HEADSET         = 0x800,
513     OUT_DGTL_DOCK_HEADSET         = 0x1000,
514     /** USB accessory mode: Android device is USB device and dock is USB host */
515     OUT_USB_ACCESSORY             = 0x2000,
516     /** USB host mode: Android device is USB host and dock is USB device */
517     OUT_USB_DEVICE                = 0x4000,
518     OUT_REMOTE_SUBMIX             = 0x8000,
519     /** Telephony voice TX path */
520     OUT_TELEPHONY_TX              = 0x10000,
521     /** Analog jack with line impedance detected */
522     OUT_LINE                      = 0x20000,
523     /** HDMI Audio Return Channel */
524     OUT_HDMI_ARC                  = 0x40000,
525     /** S/PDIF out */
526     OUT_SPDIF                     = 0x80000,
527     /** FM transmitter out */
528     OUT_FM                        = 0x100000,
529     /** Line out for av devices */
530     OUT_AUX_LINE                  = 0x200000,
531     /** limited-output speaker device for acoustic safety */
532     OUT_SPEAKER_SAFE              = 0x400000,
533     OUT_IP                        = 0x800000,
534     /** audio bus implemented by the audio system (e.g an MOST stereo channel) */
535     OUT_BUS                       = 0x1000000,
536     OUT_PROXY                     = 0x2000000,
537     OUT_USB_HEADSET               = 0x4000000,
538     OUT_DEFAULT                   = BIT_DEFAULT,
539     OUT_ALL      = (OUT_EARPIECE |
540             OUT_SPEAKER |
541             OUT_WIRED_HEADSET |
542             OUT_WIRED_HEADPHONE |
543             OUT_BLUETOOTH_SCO |
544             OUT_BLUETOOTH_SCO_HEADSET |
545             OUT_BLUETOOTH_SCO_CARKIT |
546             OUT_BLUETOOTH_A2DP |
547             OUT_BLUETOOTH_A2DP_HEADPHONES |
548             OUT_BLUETOOTH_A2DP_SPEAKER |
549             OUT_HDMI |
550             OUT_ANLG_DOCK_HEADSET |
551             OUT_DGTL_DOCK_HEADSET |
552             OUT_USB_ACCESSORY |
553             OUT_USB_DEVICE |
554             OUT_REMOTE_SUBMIX |
555             OUT_TELEPHONY_TX |
556             OUT_LINE |
557             OUT_HDMI_ARC |
558             OUT_SPDIF |
559             OUT_FM |
560             OUT_AUX_LINE |
561             OUT_SPEAKER_SAFE |
562             OUT_IP |
563             OUT_BUS |
564             OUT_PROXY |
565             OUT_USB_HEADSET |
566             OUT_DEFAULT),
567     OUT_ALL_A2DP = (OUT_BLUETOOTH_A2DP |
568             OUT_BLUETOOTH_A2DP_HEADPHONES |
569             OUT_BLUETOOTH_A2DP_SPEAKER),
570     OUT_ALL_SCO  = (OUT_BLUETOOTH_SCO |
571             OUT_BLUETOOTH_SCO_HEADSET |
572             OUT_BLUETOOTH_SCO_CARKIT),
573     OUT_ALL_USB  = (OUT_USB_ACCESSORY | OUT_USB_DEVICE | OUT_USB_HEADSET),
574     /** input devices */
575     IN_COMMUNICATION         = BIT_IN | 0x1,
576     IN_AMBIENT               = BIT_IN | 0x2,
577     IN_BUILTIN_MIC           = BIT_IN | 0x4,
578     IN_BLUETOOTH_SCO_HEADSET = BIT_IN | 0x8,
579     IN_WIRED_HEADSET         = BIT_IN | 0x10,
580     IN_AUX_DIGITAL           = BIT_IN | 0x20,
581     IN_HDMI                  = IN_AUX_DIGITAL,
582     /** Telephony voice RX path */
583     IN_VOICE_CALL            = BIT_IN | 0x40,
584     IN_TELEPHONY_RX          = IN_VOICE_CALL,
585     IN_BACK_MIC              = BIT_IN | 0x80,
586     IN_REMOTE_SUBMIX         = BIT_IN | 0x100,
587     IN_ANLG_DOCK_HEADSET     = BIT_IN | 0x200,
588     IN_DGTL_DOCK_HEADSET     = BIT_IN | 0x400,
589     IN_USB_ACCESSORY         = BIT_IN | 0x800,
590     IN_USB_DEVICE            = BIT_IN | 0x1000,
591     /** FM tuner input */
592     IN_FM_TUNER              = BIT_IN | 0x2000,
593     /** TV tuner input */
594     IN_TV_TUNER              = BIT_IN | 0x4000,
595     /** Analog jack with line impedance detected */
596     IN_LINE                  = BIT_IN | 0x8000,
597     /** S/PDIF in */
598     IN_SPDIF                 = BIT_IN | 0x10000,
599     IN_BLUETOOTH_A2DP        = BIT_IN | 0x20000,
600     IN_LOOPBACK              = BIT_IN | 0x40000,
601     IN_IP                    = BIT_IN | 0x80000,
602     /** audio bus implemented by the audio system (e.g an MOST stereo channel) */
603     IN_BUS                   = BIT_IN | 0x100000,
604     IN_PROXY                 = BIT_IN | 0x1000000,
605     IN_USB_HEADSET           = BIT_IN | 0x2000000,
606     IN_DEFAULT               = BIT_IN | BIT_DEFAULT,
608     IN_ALL     = (IN_COMMUNICATION |
609             IN_AMBIENT |
610             IN_BUILTIN_MIC |
611             IN_BLUETOOTH_SCO_HEADSET |
612             IN_WIRED_HEADSET |
613             IN_HDMI |
614             IN_TELEPHONY_RX |
615             IN_BACK_MIC |
616             IN_REMOTE_SUBMIX |
617             IN_ANLG_DOCK_HEADSET |
618             IN_DGTL_DOCK_HEADSET |
619             IN_USB_ACCESSORY |
620             IN_USB_DEVICE |
621             IN_FM_TUNER |
622             IN_TV_TUNER |
623             IN_LINE |
624             IN_SPDIF |
625             IN_BLUETOOTH_A2DP |
626             IN_LOOPBACK |
627             IN_IP |
628             IN_BUS |
629             IN_PROXY |
630             IN_USB_HEADSET |
631             IN_DEFAULT),
632     IN_ALL_SCO = IN_BLUETOOTH_SCO_HEADSET,
633     IN_ALL_USB  = (IN_USB_ACCESSORY | IN_USB_DEVICE | IN_USB_HEADSET),
634 };
636 /**
637  * The audio output flags serve two purposes:
638  *
639  *  - when an AudioTrack is created they indicate a "wish" to be connected to an
640  *    output stream with attributes corresponding to the specified flags;
641  *
642  *  - when present in an output profile descriptor listed for a particular audio
643  *    hardware module, they indicate that an output stream can be opened that
644  *    supports the attributes indicated by the flags.
645  *
646  * The audio policy manager will try to match the flags in the request
647  * (when getOuput() is called) to an available output stream.
648  */
649 @export(name="audio_output_flags_t", value_prefix="AUDIO_OUTPUT_FLAG_")
650 enum AudioOutputFlag : int32_t {
651     NONE    = 0x0, // no attributes
652     DIRECT  = 0x1, // this output directly connects a track
653                    // to one output stream: no software mixer
654     PRIMARY = 0x2, // this output is the primary output of the device. It is
655                    // unique and must be present. It is opened by default and
656                    // receives routing, audio mode and volume controls related
657                    // to voice calls.
658     FAST    = 0x4,    // output supports "fast tracks", defined elsewhere
659     DEEP_BUFFER      = 0x8,   // use deep audio buffers
660     COMPRESS_OFFLOAD = 0x10,  // offload playback of compressed streams to
661                               // hardware codec
662     NON_BLOCKING     = 0x20,  // use non-blocking write
663     HW_AV_SYNC = 0x40,   // output uses a hardware A/V sync
664     TTS        = 0x80,   // output for streams transmitted through speaker at a
665                          // sample rate high enough to accommodate lower-range
666                          // ultrasonic p/b
667     RAW        = 0x100,  // minimize signal processing
668     SYNC       = 0x200,  // synchronize I/O streams
669     IEC958_NONAUDIO = 0x400, // Audio stream contains compressed audio in SPDIF
670                              // data bursts, not PCM.
671     DIRECT_PCM = 0x2000,     // Audio stream containing PCM data that needs
672                              // to pass through compress path for DSP post proc.
673     MMAP_NOIRQ = 0x4000, // output operates in MMAP no IRQ mode.
674     VOIP_RX = 0x8000,    // preferred output for VoIP calls.
675 };
677 /**
678  * The audio input flags are analogous to audio output flags.
679  * Currently they are used only when an AudioRecord is created,
680  * to indicate a preference to be connected to an input stream with
681  * attributes corresponding to the specified flags.
682  */
683 @export(name="audio_input_flags_t", value_prefix="AUDIO_INPUT_FLAG_")
684 enum AudioInputFlag : int32_t {
685     NONE         = 0x0,  // no attributes
686     FAST         = 0x1,  // prefer an input that supports "fast tracks"
687     HW_HOTWORD   = 0x2,  // prefer an input that captures from hw hotword source
688     RAW          = 0x4,  // minimize signal processing
689     SYNC         = 0x8,  // synchronize I/O streams
690     MMAP_NOIRQ   = 0x10, // input operates in MMAP no IRQ mode.
691     VOIP_TX      = 0x20, // preferred input for VoIP calls.
692 };
694 @export(name="audio_usage_t", value_prefix="AUDIO_USAGE_")
695 enum AudioUsage : int32_t {
696     // These values must kept in sync with
697     //  frameworks/base/media/java/android/media/AudioAttributes.java
698     UNKNOWN                            = 0,
699     MEDIA                              = 1,
700     VOICE_COMMUNICATION                = 2,
701     VOICE_COMMUNICATION_SIGNALLING     = 3,
702     ALARM                              = 4,
703     NOTIFICATION                       = 5,
704     NOTIFICATION_TELEPHONY_RINGTONE    = 6,
705     NOTIFICATION_COMMUNICATION_REQUEST = 7,
706     NOTIFICATION_COMMUNICATION_INSTANT = 8,
707     NOTIFICATION_COMMUNICATION_DELAYED = 9,
708     NOTIFICATION_EVENT                 = 10,
709     ASSISTANCE_ACCESSIBILITY           = 11,
710     ASSISTANCE_NAVIGATION_GUIDANCE     = 12,
711     ASSISTANCE_SONIFICATION            = 13,
712     GAME                               = 14,
713     VIRTUAL_SOURCE                     = 15,
714     ASSISTANT                          = 16,
716     CNT,
717     MAX                                = CNT - 1,
718 };
720 /**
721  * Additional information about the stream passed to hardware decoders.
722  */
723 struct AudioOffloadInfo {
724     uint32_t sampleRateHz;
725     AudioChannelMask channelMask;
726     AudioFormat format;
727     AudioStreamType streamType;
728     uint32_t bitRatePerSecond;
729     int64_t durationMicroseconds;  // -1 if unknown
730     bool hasVideo;
731     bool isStreaming;
732     uint32_t bitWidth;
733     uint32_t bufferSize;
734     AudioUsage usage;
735 };
737 /**
738  * Commonly used audio stream configuration parameters.
739  */
740 struct AudioConfig {
741     uint32_t sampleRateHz;
742     AudioChannelMask channelMask;
743     AudioFormat format;
744     AudioOffloadInfo offloadInfo;
745     uint64_t frameCount;
746 };
749 /**
750  *
751  *  Volume control
752  *
753  */
755 /**
756  * Type of gain control exposed by an audio port.
757  */
758 @export(name="", value_prefix="AUDIO_GAIN_MODE_")
759 enum AudioGainMode : uint32_t {
760     JOINT = 0x1,    // supports joint channel gain control
761     CHANNELS = 0x2, // supports separate channel gain control
762     RAMP = 0x4      // supports gain ramps
763 };
765 /**
766  * An audio_gain struct is a representation of a gain stage.
767  * A gain stage is always attached to an audio port.
768  */
769 struct AudioGain {
770     AudioGainMode mode;
771     AudioChannelMask channelMask; // channels which gain an be controlled
772     int32_t minValue;     // minimum gain value in millibels
773     int32_t maxValue;     // maximum gain value in millibels
774     int32_t defaultValue; // default gain value in millibels
775     uint32_t stepValue;   // gain step in millibels
776     uint32_t minRampMs;   // minimum ramp duration in ms
777     uint32_t maxRampMs;   // maximum ramp duration in ms
778 };
780 /**
781  * The gain configuration structure is used to get or set the gain values of a
782  * given port.
783  */
784 struct AudioGainConfig {
785     int32_t index;  // index of the corresponding AudioGain in AudioPort.gains
786     AudioGainMode mode;
787     AudioChannelMask channelMask;  // channels which gain value follows
788     /**
789      * 4 = sizeof(AudioChannelMask),
790      * 8 is not "FCC_8", so it won't need to be changed for > 8 channels.
791      * Gain values in millibels for each channel ordered from LSb to MSb in
792      * channel mask. The number of values is 1 in joint mode or
793      * popcount(channel_mask).
794      */
795     int32_t[4 * 8] values;
796     uint32_t rampDurationMs;  // ramp duration in ms
797 };
800 /**
801  *
802  *  Routing control
803  *
804  */
806 /**
807  * Types defined here are used to describe an audio source or sink at internal
808  * framework interfaces (audio policy, patch panel) or at the audio HAL.
809  * Sink and sources are grouped in a concept of “audio port” representing an
810  * audio end point at the edge of the system managed by the module exposing
811  * the interface.
812  */
814 /** Audio port role: either source or sink */
815 @export(name="audio_port_role_t", value_prefix="AUDIO_PORT_ROLE_")
816 enum AudioPortRole : int32_t {
817     NONE,
818     SOURCE,
819     SINK,
820 };
822 /**
823  * Audio port type indicates if it is a session (e.g AudioTrack), a mix (e.g
824  * PlaybackThread output) or a physical device (e.g OUT_SPEAKER)
825  */
826 @export(name="audio_port_type_t", value_prefix="AUDIO_PORT_TYPE_")
827 enum AudioPortType : int32_t {
828     NONE,
829     DEVICE,
830     MIX,
831     SESSION,
832 };
834 /**
835  * Extension for audio port configuration structure when the audio port is a
836  * hardware device.
837  */
838 struct AudioPortConfigDeviceExt {
839     AudioModuleHandle hwModule;  // module the device is attached to
840     AudioDevice type;            // device type (e.g OUT_SPEAKER)
841     uint8_t[32] address;         // device address. "" if N/A
842 };
844 /**
845  * Extension for audio port configuration structure when the audio port is an
846  * audio session.
847  */
848 struct AudioPortConfigSessionExt {
849     AudioSession session;
850 };
852 /**
853  * Flags indicating which fields are to be considered in AudioPortConfig.
854  */
855 @export(name="", value_prefix="AUDIO_PORT_CONFIG_")
856 enum AudioPortConfigMask : uint32_t {
857     SAMPLE_RATE = 0x1,
858     CHANNEL_MASK =  0x2,
859     FORMAT = 0x4,
860     GAIN = 0x8,
861     ALL = SAMPLE_RATE | CHANNEL_MASK | FORMAT | GAIN
862 };
864 /**
865  * Audio port configuration structure used to specify a particular configuration
866  * of an audio port.
867  */
868 struct AudioPortConfig {
869     AudioPortHandle id;
870     AudioPortConfigMask configMask;
871     uint32_t sampleRateHz;
872     AudioChannelMask channelMask;
873     AudioFormat format;
874     AudioGainConfig gain;
875     AudioPortType type;  // type is used as a discriminator for Ext union
876     AudioPortRole role;  // role is used as a discriminator for UseCase union
877     union Ext {
878         AudioPortConfigDeviceExt device;
879         struct AudioPortConfigMixExt {
880             AudioModuleHandle hwModule; // module the stream is attached to
881             AudioIoHandle ioHandle;     // I/O handle of the input/output stream
882             union UseCase {
883                 AudioStreamType stream;
884                 AudioSource source;
885             } useCase;
886         } mix;
887         AudioPortConfigSessionExt session;
888     } ext;
889 };
891 /**
892  * Extension for audio port structure when the audio port is a hardware device.
893  */
894 struct AudioPortDeviceExt {
895     AudioModuleHandle hwModule;    // module the device is attached to
896     AudioDevice type;
897     uint8_t[32] address;
898 };
900 /**
901  * Latency class of the audio mix.
902  */
903 @export(name="audio_mix_latency_class_t", value_prefix="AUDIO_LATENCY_")
904 enum AudioMixLatencyClass : int32_t {
905     LOW,
906     NORMAL
907 } ;
909 struct AudioPortMixExt {
910     AudioModuleHandle hwModule;     // module the stream is attached to
911     AudioIoHandle ioHandle;         // I/O handle of the stream
912     AudioMixLatencyClass latencyClass;
913 };
915 /**
916  * Extension for audio port structure when the audio port is an audio session.
917  */
918 struct AudioPortSessionExt {
919     AudioSession session;
920 };
922 struct AudioPort {
923     AudioPortHandle id;
924     AudioPortRole role;
925     string name;
926     vec<uint32_t> sampleRates;
927     vec<AudioChannelMask> channelMasks;
928     vec<AudioFormat> formats;
929     vec<AudioGain> gains;
930     AudioPortConfig activeConfig; // current audio port configuration
931     AudioPortType type;  // type is used as a discriminator
932     union Ext {
933         AudioPortDeviceExt device;
934         AudioPortMixExt mix;
935         AudioPortSessionExt session;
936     } ext;
937 };
939 struct ThreadInfo {
940     int64_t pid;
941     int64_t tid;
942 };