]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android/platform-hardware-interfaces.git/blob - bluetooth/a2dp/1.0/vts/functional/VtsHalBluetoothA2dpV1_0TargetTest.cpp
Merge "DRM 1.1: Add VINTF doc"
[android/platform-hardware-interfaces.git] / bluetooth / a2dp / 1.0 / vts / functional / VtsHalBluetoothA2dpV1_0TargetTest.cpp
1 /*
2  * Copyright (C) 2018 The Android Open Source Project
3  *
4  * Licensed under the Apache License, Version 2.0 (the "License");
5  * you may not use this file except in compliance with the License.
6  * You may obtain a copy of the License at
7  *
8  *      http://www.apache.org/licenses/LICENSE-2.0
9  *
10  * Unless required by applicable law or agreed to in writing, software
11  * distributed under the License is distributed on an "AS IS" BASIS,
12  * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
13  * See the License for the specific language governing permissions and
14  * limitations under the License.
15  */
17 #define LOG_TAG "bluetooth_a2dp_hidl_hal_test"
19 #include <android-base/logging.h>
20 #include <android/hardware/bluetooth/a2dp/1.0/IBluetoothAudioHost.h>
21 #include <android/hardware/bluetooth/a2dp/1.0/IBluetoothAudioOffload.h>
22 #include <hardware/bluetooth.h>
23 #include <utils/Log.h>
25 #include <VtsHalHidlTargetCallbackBase.h>
26 #include <VtsHalHidlTargetTestBase.h>
27 #include <VtsHalHidlTargetTestEnvBase.h>
29 using ::android::sp;
30 using ::android::hardware::Return;
31 using ::android::hardware::Void;
32 using ::android::hardware::bluetooth::a2dp::V1_0::BitsPerSample;
33 using ::android::hardware::bluetooth::a2dp::V1_0::ChannelMode;
34 using ::android::hardware::bluetooth::a2dp::V1_0::CodecConfiguration;
35 using ::android::hardware::bluetooth::a2dp::V1_0::CodecType;
36 using ::android::hardware::bluetooth::a2dp::V1_0::IBluetoothAudioHost;
37 using ::android::hardware::bluetooth::a2dp::V1_0::IBluetoothAudioOffload;
38 using ::android::hardware::bluetooth::a2dp::V1_0::SampleRate;
39 using ::android::hardware::bluetooth::a2dp::V1_0::Status;
41 // Test environment for Bluetooth HIDL A2DP HAL.
42 class BluetoothA2dpHidlEnvironment
43     : public ::testing::VtsHalHidlTargetTestEnvBase {
44  public:
45   // get the test environment singleton
46   static BluetoothA2dpHidlEnvironment* Instance() {
47     static BluetoothA2dpHidlEnvironment* instance =
48         new BluetoothA2dpHidlEnvironment;
49     return instance;
50   }
52   virtual void registerTestServices() override {
53     registerTestService<IBluetoothAudioOffload>();
54   }
56  private:
57   BluetoothA2dpHidlEnvironment() {}
58 };
60 // The main test class for Bluetooth A2DP HIDL HAL.
61 class BluetoothA2dpHidlTest : public ::testing::VtsHalHidlTargetTestBase {
62  public:
63   virtual void SetUp() override {
64     // currently test passthrough mode only
65     audio_offload =
66         ::testing::VtsHalHidlTargetTestBase::getService<IBluetoothAudioOffload>(
67             BluetoothA2dpHidlEnvironment::Instance()
68                 ->getServiceName<IBluetoothAudioOffload>());
69     ASSERT_NE(audio_offload, nullptr);
71     audio_host = new BluetoothAudioHost(*this);
72     ASSERT_NE(audio_host, nullptr);
74     codec.codecType = CodecType::AAC;
75     codec.sampleRate = SampleRate::RATE_44100;
76     codec.bitsPerSample = BitsPerSample::BITS_16;
77     codec.channelMode = ChannelMode::STEREO;
78     codec.encodedAudioBitrate = 320000;
79     codec.peerMtu = 1000;
80   }
82   virtual void TearDown() override {}
84   // A simple test implementation of IBluetoothAudioHost.
85   class BluetoothAudioHost
86       : public ::testing::VtsHalHidlTargetCallbackBase<BluetoothA2dpHidlTest>,
87         public IBluetoothAudioHost {
88     BluetoothA2dpHidlTest& parent_;
90    public:
91     BluetoothAudioHost(BluetoothA2dpHidlTest& parent) : parent_(parent){};
92     virtual ~BluetoothAudioHost() = default;
94     Return<void> startStream() override {
95       parent_.audio_offload->streamStarted(Status::SUCCESS);
96       return Void();
97     };
99     Return<void> suspendStream() override {
100       parent_.audio_offload->streamSuspended(Status::SUCCESS);
101       return Void();
102     };
104     Return<void> stopStream() override { return Void(); };
105   };
107   // audio_host is for the Audio HAL to send stream start/suspend/stop commands
108   // to Bluetooth
109   sp<IBluetoothAudioHost> audio_host;
110   // audio_offload is for the Bluetooth HAL to report session started/ended and
111   // handled audio stream started/suspended
112   sp<IBluetoothAudioOffload> audio_offload;
113   // codec is the currently used codec
114   CodecConfiguration codec;
115 };
117 // Empty test: Initialize()/Close() are called in SetUp()/TearDown().
118 TEST_F(BluetoothA2dpHidlTest, InitializeAndClose) {}
120 // Test start and end session
121 TEST_F(BluetoothA2dpHidlTest, StartAndEndSession) {
122   EXPECT_EQ(Status::SUCCESS, audio_offload->startSession(audio_host, codec));
123   audio_offload->endSession();
126 int main(int argc, char** argv) {
127   ::testing::AddGlobalTestEnvironment(BluetoothA2dpHidlEnvironment::Instance());
128   ::testing::InitGoogleTest(&argc, argv);
129   BluetoothA2dpHidlEnvironment::Instance()->init(&argc, argv);
130   int status = RUN_ALL_TESTS();
131   LOG(INFO) << "Test result = " << status;
132   return status;