1 /*
2 * Copyright (C) 2018 The Android Open Source Project
3 *
4 * Licensed under the Apache License, Version 2.0 (the "License");
5 * you may not use this file except in compliance with the License.
6 * You may obtain a copy of the License at
7 *
8 * http://www.apache.org/licenses/LICENSE-2.0
9 *
10 * Unless required by applicable law or agreed to in writing, software
11 * distributed under the License is distributed on an "AS IS" BASIS,
12 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
13 * See the License for the specific language governing permissions and
14 * limitations under the License.
15 */
16 package android.hardware.fastboot@1.0;
18 /**
19 * IFastboot interface implements vendor specific fastboot commands.
20 */
21 interface IFastboot {
22 /**
23 * Returns the file system type of the partition. This is only required for
24 * physical partitions that need to be wiped and reformatted.
25 *
26 * @return type Can be ext4, f2fs or raw.
27 * @return result SUCCESS if the operation is successful,
28 * FAILURE_UNKNOWN if the partition is invalid or does not require
29 * reformatting.
30 */
31 getPartitionType(string partitionName) generates (FileSystemType type, Result result);
32 };