1 /*
2 * Copyright 2016 The Android Open Source Project
3 *
4 * Licensed under the Apache License, Version 2.0 (the "License");
5 * you may not use this file except in compliance with the License.
6 * You may obtain a copy of the License at
7 *
8 * http://www.apache.org/licenses/LICENSE-2.0
9 *
10 * Unless required by applicable law or agreed to in writing, software
11 * distributed under the License is distributed on an "AS IS" BASIS,
12 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
13 * See the License for the specific language governing permissions and
14 * limitations under the License.
15 */
17 #ifndef ANDROID_HARDWARE_GRAPHICS_COMPOSER_V2_1_HWC_H
18 #define ANDROID_HARDWARE_GRAPHICS_COMPOSER_V2_1_HWC_H
20 #include <atomic>
21 #include <condition_variable>
22 #include <memory>
23 #include <mutex>
24 #include <unordered_set>
25 #include <vector>
27 #include <android/hardware/graphics/composer/2.1/IComposer.h>
28 #define HWC2_INCLUDE_STRINGIFICATION
29 #define HWC2_USE_CPP11
30 #include <hardware/hwcomposer2.h>
31 #undef HWC2_INCLUDE_STRINGIFICATION
32 #undef HWC2_USE_CPP11
33 #include "ComposerBase.h"
35 namespace android {
36 class HWC2On1Adapter;
37 class HWC2OnFbAdapter;
38 }
40 namespace android {
41 namespace hardware {
42 namespace graphics {
43 namespace composer {
44 namespace V2_1 {
45 namespace implementation {
47 using android::hardware::graphics::common::V1_0::PixelFormat;
48 using android::hardware::graphics::common::V1_0::Transform;
49 using android::hardware::graphics::common::V1_0::Dataspace;
50 using android::hardware::graphics::common::V1_0::ColorMode;
51 using android::hardware::graphics::common::V1_0::ColorTransform;
52 using android::hardware::graphics::common::V1_0::Hdr;
54 class ComposerClient;
56 class HwcHal : public IComposer, public ComposerBase {
57 public:
58 HwcHal(const hw_module_t* module);
59 virtual ~HwcHal();
61 bool hasCapability(Capability capability) const;
63 // IComposer interface
64 Return<void> getCapabilities(getCapabilities_cb hidl_cb) override;
65 Return<void> dumpDebugInfo(dumpDebugInfo_cb hidl_cb) override;
66 Return<void> createClient(createClient_cb hidl_cb) override;
68 // ComposerBase interface
69 void removeClient() override;
70 void enableCallback(bool enable) override;
71 uint32_t getMaxVirtualDisplayCount() override;
72 Error createVirtualDisplay(uint32_t width, uint32_t height,
73 PixelFormat* format, Display* outDisplay) override;
74 Error destroyVirtualDisplay(Display display) override;
76 Error createLayer(Display display, Layer* outLayer) override;
77 Error destroyLayer(Display display, Layer layer) override;
79 Error getActiveConfig(Display display, Config* outConfig) override;
80 Error getClientTargetSupport(Display display,
81 uint32_t width, uint32_t height,
82 PixelFormat format, Dataspace dataspace) override;
83 Error getColorModes(Display display,
84 hidl_vec<ColorMode>* outModes) override;
85 Error getDisplayAttribute(Display display, Config config,
86 IComposerClient::Attribute attribute, int32_t* outValue) override;
87 Error getDisplayConfigs(Display display,
88 hidl_vec<Config>* outConfigs) override;
89 Error getDisplayName(Display display, hidl_string* outName) override;
90 Error getDisplayType(Display display,
91 IComposerClient::DisplayType* outType) override;
92 Error getDozeSupport(Display display, bool* outSupport) override;
93 Error getHdrCapabilities(Display display, hidl_vec<Hdr>* outTypes,
94 float* outMaxLuminance, float* outMaxAverageLuminance,
95 float* outMinLuminance) override;
97 Error setActiveConfig(Display display, Config config) override;
98 Error setColorMode(Display display, ColorMode mode) override;
99 Error setPowerMode(Display display,
100 IComposerClient::PowerMode mode) override;
101 Error setVsyncEnabled(Display display,
102 IComposerClient::Vsync enabled) override;
104 Error setColorTransform(Display display, const float* matrix,
105 int32_t hint) override;
106 Error setClientTarget(Display display, buffer_handle_t target,
107 int32_t acquireFence, int32_t dataspace,
108 const std::vector<hwc_rect_t>& damage) override;
109 Error setOutputBuffer(Display display, buffer_handle_t buffer,
110 int32_t releaseFence) override;
111 Error validateDisplay(Display display,
112 std::vector<Layer>* outChangedLayers,
113 std::vector<IComposerClient::Composition>* outCompositionTypes,
114 uint32_t* outDisplayRequestMask,
115 std::vector<Layer>* outRequestedLayers,
116 std::vector<uint32_t>* outRequestMasks) override;
117 Error acceptDisplayChanges(Display display) override;
118 Error presentDisplay(Display display, int32_t* outPresentFence,
119 std::vector<Layer>* outLayers,
120 std::vector<int32_t>* outReleaseFences) override;
122 Error setLayerCursorPosition(Display display, Layer layer,
123 int32_t x, int32_t y) override;
124 Error setLayerBuffer(Display display, Layer layer,
125 buffer_handle_t buffer, int32_t acquireFence) override;
126 Error setLayerSurfaceDamage(Display display, Layer layer,
127 const std::vector<hwc_rect_t>& damage) override;
128 Error setLayerBlendMode(Display display, Layer layer,
129 int32_t mode) override;
130 Error setLayerColor(Display display, Layer layer,
131 IComposerClient::Color color) override;
132 Error setLayerCompositionType(Display display, Layer layer,
133 int32_t type) override;
134 Error setLayerDataspace(Display display, Layer layer,
135 int32_t dataspace) override;
136 Error setLayerDisplayFrame(Display display, Layer layer,
137 const hwc_rect_t& frame) override;
138 Error setLayerPlaneAlpha(Display display, Layer layer,
139 float alpha) override;
140 Error setLayerSidebandStream(Display display, Layer layer,
141 buffer_handle_t stream) override;
142 Error setLayerSourceCrop(Display display, Layer layer,
143 const hwc_frect_t& crop) override;
144 Error setLayerTransform(Display display, Layer layer,
145 int32_t transform) override;
146 Error setLayerVisibleRegion(Display display, Layer layer,
147 const std::vector<hwc_rect_t>& visible) override;
148 Error setLayerZOrder(Display display, Layer layer, uint32_t z) override;
150 private:
151 uint32_t initWithHwc(const hw_module_t* module);
152 uint32_t initWithFb(const hw_module_t* module);
154 void initCapabilities();
156 template<typename T>
157 void initDispatch(hwc2_function_descriptor_t desc, T* outPfn);
158 void initDispatch();
160 sp<ComposerClient> getClient();
162 static void hotplugHook(hwc2_callback_data_t callbackData,
163 hwc2_display_t display, int32_t connected);
164 static void refreshHook(hwc2_callback_data_t callbackData,
165 hwc2_display_t display);
166 static void vsyncHook(hwc2_callback_data_t callbackData,
167 hwc2_display_t display, int64_t timestamp);
169 hwc2_device_t* mDevice;
171 std::unordered_set<Capability> mCapabilities;
173 struct {
174 HWC2_PFN_ACCEPT_DISPLAY_CHANGES acceptDisplayChanges;
175 HWC2_PFN_CREATE_LAYER createLayer;
176 HWC2_PFN_CREATE_VIRTUAL_DISPLAY createVirtualDisplay;
177 HWC2_PFN_DESTROY_LAYER destroyLayer;
178 HWC2_PFN_DESTROY_VIRTUAL_DISPLAY destroyVirtualDisplay;
179 HWC2_PFN_DUMP dump;
180 HWC2_PFN_GET_ACTIVE_CONFIG getActiveConfig;
181 HWC2_PFN_GET_CHANGED_COMPOSITION_TYPES getChangedCompositionTypes;
182 HWC2_PFN_GET_CLIENT_TARGET_SUPPORT getClientTargetSupport;
183 HWC2_PFN_GET_COLOR_MODES getColorModes;
184 HWC2_PFN_GET_DISPLAY_ATTRIBUTE getDisplayAttribute;
185 HWC2_PFN_GET_DISPLAY_CONFIGS getDisplayConfigs;
186 HWC2_PFN_GET_DISPLAY_NAME getDisplayName;
187 HWC2_PFN_GET_DISPLAY_REQUESTS getDisplayRequests;
188 HWC2_PFN_GET_DISPLAY_TYPE getDisplayType;
189 HWC2_PFN_GET_DOZE_SUPPORT getDozeSupport;
190 HWC2_PFN_GET_HDR_CAPABILITIES getHdrCapabilities;
191 HWC2_PFN_GET_MAX_VIRTUAL_DISPLAY_COUNT getMaxVirtualDisplayCount;
192 HWC2_PFN_GET_RELEASE_FENCES getReleaseFences;
193 HWC2_PFN_PRESENT_DISPLAY presentDisplay;
194 HWC2_PFN_REGISTER_CALLBACK registerCallback;
195 HWC2_PFN_SET_ACTIVE_CONFIG setActiveConfig;
196 HWC2_PFN_SET_CLIENT_TARGET setClientTarget;
197 HWC2_PFN_SET_COLOR_MODE setColorMode;
198 HWC2_PFN_SET_COLOR_TRANSFORM setColorTransform;
199 HWC2_PFN_SET_CURSOR_POSITION setCursorPosition;
200 HWC2_PFN_SET_LAYER_BLEND_MODE setLayerBlendMode;
201 HWC2_PFN_SET_LAYER_BUFFER setLayerBuffer;
202 HWC2_PFN_SET_LAYER_COLOR setLayerColor;
203 HWC2_PFN_SET_LAYER_COMPOSITION_TYPE setLayerCompositionType;
204 HWC2_PFN_SET_LAYER_DATASPACE setLayerDataspace;
205 HWC2_PFN_SET_LAYER_DISPLAY_FRAME setLayerDisplayFrame;
206 HWC2_PFN_SET_LAYER_PLANE_ALPHA setLayerPlaneAlpha;
207 HWC2_PFN_SET_LAYER_SIDEBAND_STREAM setLayerSidebandStream;
208 HWC2_PFN_SET_LAYER_SOURCE_CROP setLayerSourceCrop;
209 HWC2_PFN_SET_LAYER_SURFACE_DAMAGE setLayerSurfaceDamage;
210 HWC2_PFN_SET_LAYER_TRANSFORM setLayerTransform;
211 HWC2_PFN_SET_LAYER_VISIBLE_REGION setLayerVisibleRegion;
212 HWC2_PFN_SET_LAYER_Z_ORDER setLayerZOrder;
213 HWC2_PFN_SET_OUTPUT_BUFFER setOutputBuffer;
214 HWC2_PFN_SET_POWER_MODE setPowerMode;
215 HWC2_PFN_SET_VSYNC_ENABLED setVsyncEnabled;
216 HWC2_PFN_VALIDATE_DISPLAY validateDisplay;
217 } mDispatch;
219 std::mutex mClientMutex;
220 std::condition_variable mClientDestroyedWait;
221 wp<ComposerClient> mClient;
223 std::atomic<bool> mMustValidateDisplay;
225 // If the HWC implementation version is < 2.0, use an adapter to interface
226 // between HWC 2.0 <-> HWC 1.X.
227 std::unique_ptr<HWC2On1Adapter> mAdapter;
229 // If there is no HWC implementation, use an adapter to interface between
230 // HWC 2.0 <-> FB HAL.
231 std::unique_ptr<HWC2OnFbAdapter> mFbAdapter;
232 };
234 extern "C" IComposer* HIDL_FETCH_IComposer(const char* name);
236 } // namespace implementation
237 } // namespace V2_1
238 } // namespace composer
239 } // namespace graphics
240 } // namespace hardware
241 } // namespace android
243 #endif // ANDROID_HARDWARE_GRAPHICS_COMPOSER_V2_1_HWC_H