1 /*
2 * Copyright 2016 The Android Open Source Project
3 *
4 * Licensed under the Apache License, Version 2.0 (the "License");
5 * you may not use this file except in compliance with the License.
6 * You may obtain a copy of the License at
7 *
8 * http://www.apache.org/licenses/LICENSE-2.0
9 *
10 * Unless required by applicable law or agreed to in writing, software
11 * distributed under the License is distributed on an "AS IS" BASIS,
12 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
13 * See the License for the specific language governing permissions and
14 * limitations under the License.
15 */
17 #ifndef ANDROID_HARDWARE_GRAPHICS_COMPOSER_V2_1_HWC_H
18 #define ANDROID_HARDWARE_GRAPHICS_COMPOSER_V2_1_HWC_H
20 #include <mutex>
21 #include <memory>
22 #include <unordered_set>
23 #include <vector>
25 #include <android/hardware/graphics/composer/2.1/IComposer.h>
26 #define HWC2_INCLUDE_STRINGIFICATION
27 #define HWC2_USE_CPP11
28 #include <hardware/hwcomposer2.h>
29 #undef HWC2_INCLUDE_STRINGIFICATION
30 #undef HWC2_USE_CPP11
31 #include "ComposerBase.h"
33 namespace android {
34 class HWC2On1Adapter;
35 }
37 namespace android {
38 namespace hardware {
39 namespace graphics {
40 namespace composer {
41 namespace V2_1 {
42 namespace implementation {
44 using android::hardware::graphics::common::V1_0::PixelFormat;
45 using android::hardware::graphics::common::V1_0::Transform;
46 using android::hardware::graphics::common::V1_0::Dataspace;
47 using android::hardware::graphics::common::V1_0::ColorMode;
48 using android::hardware::graphics::common::V1_0::ColorTransform;
49 using android::hardware::graphics::common::V1_0::Hdr;
51 class ComposerClient;
53 class HwcHal : public IComposer, public ComposerBase {
54 public:
55 HwcHal(const hw_module_t* module);
56 virtual ~HwcHal();
58 bool hasCapability(Capability capability) const;
60 // IComposer interface
61 Return<void> getCapabilities(getCapabilities_cb hidl_cb) override;
62 Return<void> dumpDebugInfo(dumpDebugInfo_cb hidl_cb) override;
63 Return<void> createClient(createClient_cb hidl_cb) override;
65 // ComposerBase interface
66 void removeClient() override;
67 void enableCallback(bool enable) override;
68 uint32_t getMaxVirtualDisplayCount() override;
69 Error createVirtualDisplay(uint32_t width, uint32_t height,
70 PixelFormat* format, Display* outDisplay) override;
71 Error destroyVirtualDisplay(Display display) override;
73 Error createLayer(Display display, Layer* outLayer) override;
74 Error destroyLayer(Display display, Layer layer) override;
76 Error getActiveConfig(Display display, Config* outConfig) override;
77 Error getClientTargetSupport(Display display,
78 uint32_t width, uint32_t height,
79 PixelFormat format, Dataspace dataspace) override;
80 Error getColorModes(Display display,
81 hidl_vec<ColorMode>* outModes) override;
82 Error getDisplayAttribute(Display display, Config config,
83 IComposerClient::Attribute attribute, int32_t* outValue) override;
84 Error getDisplayConfigs(Display display,
85 hidl_vec<Config>* outConfigs) override;
86 Error getDisplayName(Display display, hidl_string* outName) override;
87 Error getDisplayType(Display display,
88 IComposerClient::DisplayType* outType) override;
89 Error getDozeSupport(Display display, bool* outSupport) override;
90 Error getHdrCapabilities(Display display, hidl_vec<Hdr>* outTypes,
91 float* outMaxLuminance, float* outMaxAverageLuminance,
92 float* outMinLuminance) override;
94 Error setActiveConfig(Display display, Config config) override;
95 Error setColorMode(Display display, ColorMode mode) override;
96 Error setPowerMode(Display display,
97 IComposerClient::PowerMode mode) override;
98 Error setVsyncEnabled(Display display,
99 IComposerClient::Vsync enabled) override;
101 Error setColorTransform(Display display, const float* matrix,
102 int32_t hint) override;
103 Error setClientTarget(Display display, buffer_handle_t target,
104 int32_t acquireFence, int32_t dataspace,
105 const std::vector<hwc_rect_t>& damage) override;
106 Error setOutputBuffer(Display display, buffer_handle_t buffer,
107 int32_t releaseFence) override;
108 Error validateDisplay(Display display,
109 std::vector<Layer>* outChangedLayers,
110 std::vector<IComposerClient::Composition>* outCompositionTypes,
111 uint32_t* outDisplayRequestMask,
112 std::vector<Layer>* outRequestedLayers,
113 std::vector<uint32_t>* outRequestMasks) override;
114 Error acceptDisplayChanges(Display display) override;
115 Error presentDisplay(Display display, int32_t* outPresentFence,
116 std::vector<Layer>* outLayers,
117 std::vector<int32_t>* outReleaseFences) override;
119 Error setLayerCursorPosition(Display display, Layer layer,
120 int32_t x, int32_t y) override;
121 Error setLayerBuffer(Display display, Layer layer,
122 buffer_handle_t buffer, int32_t acquireFence) override;
123 Error setLayerSurfaceDamage(Display display, Layer layer,
124 const std::vector<hwc_rect_t>& damage) override;
125 Error setLayerBlendMode(Display display, Layer layer,
126 int32_t mode) override;
127 Error setLayerColor(Display display, Layer layer,
128 IComposerClient::Color color) override;
129 Error setLayerCompositionType(Display display, Layer layer,
130 int32_t type) override;
131 Error setLayerDataspace(Display display, Layer layer,
132 int32_t dataspace) override;
133 Error setLayerDisplayFrame(Display display, Layer layer,
134 const hwc_rect_t& frame) override;
135 Error setLayerPlaneAlpha(Display display, Layer layer,
136 float alpha) override;
137 Error setLayerSidebandStream(Display display, Layer layer,
138 buffer_handle_t stream) override;
139 Error setLayerSourceCrop(Display display, Layer layer,
140 const hwc_frect_t& crop) override;
141 Error setLayerTransform(Display display, Layer layer,
142 int32_t transform) override;
143 Error setLayerVisibleRegion(Display display, Layer layer,
144 const std::vector<hwc_rect_t>& visible) override;
145 Error setLayerZOrder(Display display, Layer layer, uint32_t z) override;
147 private:
148 void initCapabilities();
150 template<typename T>
151 void initDispatch(hwc2_function_descriptor_t desc, T* outPfn);
152 void initDispatch();
154 sp<ComposerClient> getClient();
156 static void hotplugHook(hwc2_callback_data_t callbackData,
157 hwc2_display_t display, int32_t connected);
158 static void refreshHook(hwc2_callback_data_t callbackData,
159 hwc2_display_t display);
160 static void vsyncHook(hwc2_callback_data_t callbackData,
161 hwc2_display_t display, int64_t timestamp);
163 hwc2_device_t* mDevice;
165 std::unordered_set<Capability> mCapabilities;
167 struct {
168 HWC2_PFN_ACCEPT_DISPLAY_CHANGES acceptDisplayChanges;
169 HWC2_PFN_CREATE_LAYER createLayer;
170 HWC2_PFN_CREATE_VIRTUAL_DISPLAY createVirtualDisplay;
171 HWC2_PFN_DESTROY_LAYER destroyLayer;
172 HWC2_PFN_DESTROY_VIRTUAL_DISPLAY destroyVirtualDisplay;
173 HWC2_PFN_DUMP dump;
174 HWC2_PFN_GET_ACTIVE_CONFIG getActiveConfig;
175 HWC2_PFN_GET_CHANGED_COMPOSITION_TYPES getChangedCompositionTypes;
176 HWC2_PFN_GET_CLIENT_TARGET_SUPPORT getClientTargetSupport;
177 HWC2_PFN_GET_COLOR_MODES getColorModes;
178 HWC2_PFN_GET_DISPLAY_ATTRIBUTE getDisplayAttribute;
179 HWC2_PFN_GET_DISPLAY_CONFIGS getDisplayConfigs;
180 HWC2_PFN_GET_DISPLAY_NAME getDisplayName;
181 HWC2_PFN_GET_DISPLAY_REQUESTS getDisplayRequests;
182 HWC2_PFN_GET_DISPLAY_TYPE getDisplayType;
183 HWC2_PFN_GET_DOZE_SUPPORT getDozeSupport;
184 HWC2_PFN_GET_HDR_CAPABILITIES getHdrCapabilities;
185 HWC2_PFN_GET_MAX_VIRTUAL_DISPLAY_COUNT getMaxVirtualDisplayCount;
186 HWC2_PFN_GET_RELEASE_FENCES getReleaseFences;
187 HWC2_PFN_PRESENT_DISPLAY presentDisplay;
188 HWC2_PFN_REGISTER_CALLBACK registerCallback;
189 HWC2_PFN_SET_ACTIVE_CONFIG setActiveConfig;
190 HWC2_PFN_SET_CLIENT_TARGET setClientTarget;
191 HWC2_PFN_SET_COLOR_MODE setColorMode;
192 HWC2_PFN_SET_COLOR_TRANSFORM setColorTransform;
193 HWC2_PFN_SET_CURSOR_POSITION setCursorPosition;
194 HWC2_PFN_SET_LAYER_BLEND_MODE setLayerBlendMode;
195 HWC2_PFN_SET_LAYER_BUFFER setLayerBuffer;
196 HWC2_PFN_SET_LAYER_COLOR setLayerColor;
197 HWC2_PFN_SET_LAYER_COMPOSITION_TYPE setLayerCompositionType;
198 HWC2_PFN_SET_LAYER_DATASPACE setLayerDataspace;
199 HWC2_PFN_SET_LAYER_DISPLAY_FRAME setLayerDisplayFrame;
200 HWC2_PFN_SET_LAYER_PLANE_ALPHA setLayerPlaneAlpha;
201 HWC2_PFN_SET_LAYER_SIDEBAND_STREAM setLayerSidebandStream;
202 HWC2_PFN_SET_LAYER_SOURCE_CROP setLayerSourceCrop;
203 HWC2_PFN_SET_LAYER_SURFACE_DAMAGE setLayerSurfaceDamage;
204 HWC2_PFN_SET_LAYER_TRANSFORM setLayerTransform;
205 HWC2_PFN_SET_LAYER_VISIBLE_REGION setLayerVisibleRegion;
206 HWC2_PFN_SET_LAYER_Z_ORDER setLayerZOrder;
207 HWC2_PFN_SET_OUTPUT_BUFFER setOutputBuffer;
208 HWC2_PFN_SET_POWER_MODE setPowerMode;
209 HWC2_PFN_SET_VSYNC_ENABLED setVsyncEnabled;
210 HWC2_PFN_VALIDATE_DISPLAY validateDisplay;
211 } mDispatch;
213 std::mutex mClientMutex;
214 wp<ComposerClient> mClient;
216 // If the HWC implementation version is < 2.0, use an adapter to interface
217 // between HWC 2.0 <-> HWC 1.X.
218 std::unique_ptr<HWC2On1Adapter> mAdapter;
219 };
221 extern "C" IComposer* HIDL_FETCH_IComposer(const char* name);
223 } // namespace implementation
224 } // namespace V2_1
225 } // namespace composer
226 } // namespace graphics
227 } // namespace hardware
228 } // namespace android
230 #endif // ANDROID_HARDWARE_GRAPHICS_COMPOSER_V2_1_HWC_H