run vts build rule updater when hal make files are updated
[android/platform-hardware-interfaces.git] / keymaster / 4.0 / support / Keymaster.cpp
1 /*
2  ** Copyright 2018, The Android Open Source Project
3  **
4  ** Licensed under the Apache License, Version 2.0 (the "License");
5  ** you may not use this file except in compliance with the License.
6  ** You may obtain a copy of the License at
7  **
8  **     http://www.apache.org/licenses/LICENSE-2.0
9  **
10  ** Unless required by applicable law or agreed to in writing, software
11  ** distributed under the License is distributed on an "AS IS" BASIS,
12  ** WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
13  ** See the License for the specific language governing permissions and
14  ** limitations under the License.
15  */
17 #include <keymasterV4_0/Keymaster.h>
19 #include <iomanip>
21 #include <android-base/logging.h>
22 #include <android/hidl/manager/1.0/IServiceManager.h>
23 #include <keymasterV4_0/Keymaster3.h>
24 #include <keymasterV4_0/Keymaster4.h>
25 #include <keymasterV4_0/key_param_output.h>
26 #include <keymasterV4_0/keymaster_utils.h>
28 namespace android {
29 namespace hardware {
31 template <class T>
32 std::ostream& operator<<(std::ostream& os, const hidl_vec<T>& vec) {
33     os << "{ ";
34     if (vec.size()) {
35         for (size_t i = 0; i < vec.size() - 1; ++i) os << vec[i] << ", ";
36         os << vec[vec.size() - 1];
37     }
38     os << " }";
39     return os;
40 }
42 std::ostream& operator<<(std::ostream& os, const hidl_vec<uint8_t>& vec) {
43     std::ios_base::fmtflags flags(os.flags());
44     os << std::setw(2) << std::setfill('0') << std::hex;
45     for (uint8_t c : vec) os << static_cast<int>(c);
46     os.flags(flags);
47     return os;
48 }
50 template <size_t N>
51 std::ostream& operator<<(std::ostream& os, const hidl_array<uint8_t, N>& vec) {
52     std::ios_base::fmtflags flags(os.flags());
53     os << std::setw(2) << std::setfill('0') << std::hex;
54     for (size_t i = 0; i < N; ++i) os << static_cast<int>(vec[i]);
55     os.flags(flags);
56     return os;
57 }
59 namespace keymaster {
60 namespace V4_0 {
62 std::ostream& operator<<(std::ostream& os, const HmacSharingParameters& params) {
63     // Note that by design, although seed and nonce are used to compute a secret, they are
64     // not secrets and it's just fine to log them.
65     os << "(seed: " << params.seed << ", nonce: " << params.nonce << ')';
66     return os;
67 }
69 namespace support {
71 using ::android::sp;
72 using ::android::hidl::manager::V1_0::IServiceManager;
74 std::ostream& operator<<(std::ostream& os, const Keymaster& keymaster) {
75     auto& version = keymaster.halVersion();
76     os << version.keymasterName << " from " << version.authorName
77        << " SecurityLevel: " << toString(version.securityLevel)
78        << " HAL: " << keymaster.descriptor() << "/" << keymaster.instanceName();
79     return os;
80 }
82 template <typename Wrapper>
83 std::vector<std::unique_ptr<Keymaster>> enumerateDevices(
84     const sp<IServiceManager>& serviceManager) {
85     Keymaster::KeymasterSet result;
87     bool foundDefault = false;
88     auto& descriptor = Wrapper::WrappedIKeymasterDevice::descriptor;
89     serviceManager->listByInterface(descriptor, [&](const hidl_vec<hidl_string>& names) {
90         for (auto& name : names) {
91             if (name == "default") foundDefault = true;
92             auto device = Wrapper::WrappedIKeymasterDevice::getService(name);
93             CHECK(device) << "Failed to get service for " << descriptor << " with interface name "
94                           << name;
95             result.push_back(std::unique_ptr<Keymaster>(new Wrapper(device, name)));
96         }
97     });
99     if (!foundDefault) {
100         // "default" wasn't provided by listByInterface.  Maybe there's a passthrough
101         // implementation.
102         auto device = Wrapper::WrappedIKeymasterDevice::getService("default");
103         if (device) result.push_back(std::unique_ptr<Keymaster>(new Wrapper(device, "default")));
104     }
106     return result;
109 Keymaster::KeymasterSet Keymaster::enumerateAvailableDevices() {
110     auto serviceManager = IServiceManager::getService();
111     CHECK(serviceManager) << "Could not retrieve ServiceManager";
113     auto km4s = enumerateDevices<Keymaster4>(serviceManager);
114     auto km3s = enumerateDevices<Keymaster3>(serviceManager);
116     auto result = std::move(km4s);
117     result.insert(result.end(), std::make_move_iterator(km3s.begin()),
118                   std::make_move_iterator(km3s.end()));
120     std::sort(result.begin(), result.end(),
121               [](auto& a, auto& b) { return a->halVersion() > b->halVersion(); });
123     size_t i = 1;
124     LOG(INFO) << "List of Keymaster HALs found:";
125     for (auto& hal : result) LOG(INFO) << "Keymaster HAL #" << i++ << ": " << *hal;
127     return result;
130 static hidl_vec<HmacSharingParameters> getHmacParameters(
131     const Keymaster::KeymasterSet& keymasters) {
132     std::vector<HmacSharingParameters> params_vec;
133     params_vec.reserve(keymasters.size());
134     for (auto& keymaster : keymasters) {
135         if (keymaster->halVersion().majorVersion < 4) continue;
136         auto rc = keymaster->getHmacSharingParameters([&](auto error, auto& params) {
137             CHECK(error == ErrorCode::OK)
138                 << "Failed to get HMAC parameters from " << *keymaster << " error " << error;
139             params_vec.push_back(params);
140         });
141         CHECK(rc.isOk()) << "Failed to communicate with " << *keymaster
142                          << " error: " << rc.description();
143     }
144     std::sort(params_vec.begin(), params_vec.end());
146     return params_vec;
149 static void computeHmac(const Keymaster::KeymasterSet& keymasters,
150                         const hidl_vec<HmacSharingParameters>& params) {
151     if (!params.size()) return;
153     hidl_vec<uint8_t> sharingCheck;
154     bool firstKeymaster = true;
155     LOG(DEBUG) << "Computing HMAC with params " << params;
156     for (auto& keymaster : keymasters) {
157         if (keymaster->halVersion().majorVersion < 4) continue;
158         LOG(DEBUG) << "Computing HMAC for " << *keymaster;
159         auto rc = keymaster->computeSharedHmac(
160             params, [&](ErrorCode error, const hidl_vec<uint8_t>& curSharingCheck) {
161                 CHECK(error == ErrorCode::OK)
162                     << "Failed to get HMAC parameters from " << *keymaster << " error " << error;
163                 if (firstKeymaster) {
164                     sharingCheck = curSharingCheck;
165                     firstKeymaster = false;
166                 }
167                 CHECK(curSharingCheck == sharingCheck)
168                     << "HMAC computation failed for " << *keymaster  //
169                     << " Expected: " << sharingCheck                 //
170                     << " got: " << curSharingCheck;
171             });
172         CHECK(rc.isOk()) << "Failed to communicate with " << *keymaster
173                          << " error: " << rc.description();
174     }
177 void Keymaster::performHmacKeyAgreement(const KeymasterSet& keymasters) {
178     computeHmac(keymasters, getHmacParameters(keymasters));
181 }  // namespace support
182 }  // namespace V4_0
183 }  // namespace keymaster
184 }  // namespace hardware
185 }  // namespace android