run vts build rule updater when hal make files are updated
[android/platform-hardware-interfaces.git] / neuralnetworks / 1.2 / vts / functional / ValidateModel.cpp
1 /*
2  * Copyright (C) 2018 The Android Open Source Project
3  *
4  * Licensed under the Apache License, Version 2.0 (the "License");
5  * you may not use this file except in compliance with the License.
6  * You may obtain a copy of the License at
7  *
8  *      http://www.apache.org/licenses/LICENSE-2.0
9  *
10  * Unless required by applicable law or agreed to in writing, software
11  * distributed under the License is distributed on an "AS IS" BASIS,
12  * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
13  * See the License for the specific language governing permissions and
14  * limitations under the License.
15  */
17 #define LOG_TAG "neuralnetworks_hidl_hal_test"
19 #include "VtsHalNeuralnetworks.h"
21 #include "Callbacks.h"
23 namespace android {
24 namespace hardware {
25 namespace neuralnetworks {
26 namespace V1_2 {
28 using V1_0::IPreparedModel;
29 using V1_0::Operand;
30 using V1_0::OperandLifeTime;
31 using V1_0::OperandType;
32 using V1_1::ExecutionPreference;
34 namespace vts {
35 namespace functional {
37 using ::android::hardware::neuralnetworks::V1_0::implementation::ExecutionCallback;
38 using ::android::hardware::neuralnetworks::V1_0::implementation::PreparedModelCallback;
40 ///////////////////////// UTILITY FUNCTIONS /////////////////////////
42 static void validateGetSupportedOperations(const sp<IDevice>& device, const std::string& message,
43                                            const Model& model) {
44     SCOPED_TRACE(message + " [getSupportedOperations_1_2]");
46     Return<void> ret =
47         device->getSupportedOperations_1_2(model, [&](ErrorStatus status, const hidl_vec<bool>&) {
48             EXPECT_EQ(ErrorStatus::INVALID_ARGUMENT, status);
49         });
50     EXPECT_TRUE(ret.isOk());
51 }
53 static void validatePrepareModel(const sp<IDevice>& device, const std::string& message,
54                                  const Model& model, ExecutionPreference preference) {
55     SCOPED_TRACE(message + " [prepareModel_1_2]");
57     sp<PreparedModelCallback> preparedModelCallback = new PreparedModelCallback();
58     ASSERT_NE(nullptr, preparedModelCallback.get());
59     Return<ErrorStatus> prepareLaunchStatus =
60         device->prepareModel_1_2(model, preference, preparedModelCallback);
61     ASSERT_TRUE(prepareLaunchStatus.isOk());
62     ASSERT_EQ(ErrorStatus::INVALID_ARGUMENT, static_cast<ErrorStatus>(prepareLaunchStatus));
64     preparedModelCallback->wait();
65     ErrorStatus prepareReturnStatus = preparedModelCallback->getStatus();
66     ASSERT_EQ(ErrorStatus::INVALID_ARGUMENT, prepareReturnStatus);
67     sp<IPreparedModel> preparedModel = preparedModelCallback->getPreparedModel();
68     ASSERT_EQ(nullptr, preparedModel.get());
69 }
71 static bool validExecutionPreference(ExecutionPreference preference) {
72     return preference == ExecutionPreference::LOW_POWER ||
73            preference == ExecutionPreference::FAST_SINGLE_ANSWER ||
74            preference == ExecutionPreference::SUSTAINED_SPEED;
75 }
77 // Primary validation function. This function will take a valid model, apply a
78 // mutation to it to invalidate the model, then pass it to interface calls that
79 // use the model. Note that the model here is passed by value, and any mutation
80 // to the model does not leave this function.
81 static void validate(const sp<IDevice>& device, const std::string& message, Model model,
82                      const std::function<void(Model*)>& mutation,
83                      ExecutionPreference preference = ExecutionPreference::FAST_SINGLE_ANSWER) {
84     mutation(&model);
85     if (validExecutionPreference(preference)) {
86         validateGetSupportedOperations(device, message, model);
87     }
88     validatePrepareModel(device, message, model, preference);
89 }
91 // Delete element from hidl_vec. hidl_vec doesn't support a "remove" operation,
92 // so this is efficiently accomplished by moving the element to the end and
93 // resizing the hidl_vec to one less.
94 template <typename Type>
95 static void hidl_vec_removeAt(hidl_vec<Type>* vec, uint32_t index) {
96     if (vec) {
97         std::rotate(vec->begin() + index, vec->begin() + index + 1, vec->end());
98         vec->resize(vec->size() - 1);
99     }
102 template <typename Type>
103 static uint32_t hidl_vec_push_back(hidl_vec<Type>* vec, const Type& value) {
104     // assume vec is valid
105     const uint32_t index = vec->size();
106     vec->resize(index + 1);
107     (*vec)[index] = value;
108     return index;
111 static uint32_t addOperand(Model* model) {
112     return hidl_vec_push_back(&model->operands,
113                               {
114                                   .type = OperandType::INT32,
115                                   .dimensions = {},
116                                   .numberOfConsumers = 0,
117                                   .scale = 0.0f,
118                                   .zeroPoint = 0,
119                                   .lifetime = OperandLifeTime::MODEL_INPUT,
120                                   .location = {.poolIndex = 0, .offset = 0, .length = 0},
121                               });
124 static uint32_t addOperand(Model* model, OperandLifeTime lifetime) {
125     uint32_t index = addOperand(model);
126     model->operands[index].numberOfConsumers = 1;
127     model->operands[index].lifetime = lifetime;
128     return index;
131 ///////////////////////// VALIDATE MODEL OPERAND TYPE /////////////////////////
133 static const int32_t invalidOperandTypes[] = {
134     static_cast<int32_t>(OperandType::FLOAT32) - 1,              // lower bound fundamental
135     static_cast<int32_t>(OperandType::TENSOR_QUANT8_ASYMM) + 1,  // upper bound fundamental
136     static_cast<int32_t>(OperandType::OEM) - 1,                  // lower bound OEM
137     static_cast<int32_t>(OperandType::TENSOR_OEM_BYTE) + 1,      // upper bound OEM
138 };
140 static void mutateOperandTypeTest(const sp<IDevice>& device, const Model& model) {
141     for (size_t operand = 0; operand < model.operands.size(); ++operand) {
142         for (int32_t invalidOperandType : invalidOperandTypes) {
143             const std::string message = "mutateOperandTypeTest: operand " +
144                                         std::to_string(operand) + " set to value " +
145                                         std::to_string(invalidOperandType);
146             validate(device, message, model, [operand, invalidOperandType](Model* model) {
147                 model->operands[operand].type = static_cast<OperandType>(invalidOperandType);
148             });
149         }
150     }
153 ///////////////////////// VALIDATE OPERAND RANK /////////////////////////
155 static uint32_t getInvalidRank(OperandType type) {
156     switch (type) {
157         case OperandType::FLOAT32:
158         case OperandType::INT32:
159         case OperandType::UINT32:
160             return 1;
161         case OperandType::TENSOR_FLOAT32:
162         case OperandType::TENSOR_INT32:
163         case OperandType::TENSOR_QUANT8_ASYMM:
164             return 0;
165         default:
166             return 0;
167     }
170 static void mutateOperandRankTest(const sp<IDevice>& device, const Model& model) {
171     for (size_t operand = 0; operand < model.operands.size(); ++operand) {
172         const uint32_t invalidRank = getInvalidRank(model.operands[operand].type);
173         const std::string message = "mutateOperandRankTest: operand " + std::to_string(operand) +
174                                     " has rank of " + std::to_string(invalidRank);
175         validate(device, message, model, [operand, invalidRank](Model* model) {
176             model->operands[operand].dimensions = std::vector<uint32_t>(invalidRank, 0);
177         });
178     }
181 ///////////////////////// VALIDATE OPERAND SCALE /////////////////////////
183 static float getInvalidScale(OperandType type) {
184     switch (type) {
185         case OperandType::FLOAT32:
186         case OperandType::INT32:
187         case OperandType::UINT32:
188         case OperandType::TENSOR_FLOAT32:
189             return 1.0f;
190         case OperandType::TENSOR_INT32:
191             return -1.0f;
192         case OperandType::TENSOR_QUANT8_ASYMM:
193             return 0.0f;
194         default:
195             return 0.0f;
196     }
199 static void mutateOperandScaleTest(const sp<IDevice>& device, const Model& model) {
200     for (size_t operand = 0; operand < model.operands.size(); ++operand) {
201         const float invalidScale = getInvalidScale(model.operands[operand].type);
202         const std::string message = "mutateOperandScaleTest: operand " + std::to_string(operand) +
203                                     " has scale of " + std::to_string(invalidScale);
204         validate(device, message, model, [operand, invalidScale](Model* model) {
205             model->operands[operand].scale = invalidScale;
206         });
207     }
210 ///////////////////////// VALIDATE OPERAND ZERO POINT /////////////////////////
212 static std::vector<int32_t> getInvalidZeroPoints(OperandType type) {
213     switch (type) {
214         case OperandType::FLOAT32:
215         case OperandType::INT32:
216         case OperandType::UINT32:
217         case OperandType::TENSOR_FLOAT32:
218         case OperandType::TENSOR_INT32:
219             return {1};
220         case OperandType::TENSOR_QUANT8_ASYMM:
221             return {-1, 256};
222         default:
223             return {};
224     }
227 static void mutateOperandZeroPointTest(const sp<IDevice>& device, const Model& model) {
228     for (size_t operand = 0; operand < model.operands.size(); ++operand) {
229         const std::vector<int32_t> invalidZeroPoints =
230             getInvalidZeroPoints(model.operands[operand].type);
231         for (int32_t invalidZeroPoint : invalidZeroPoints) {
232             const std::string message = "mutateOperandZeroPointTest: operand " +
233                                         std::to_string(operand) + " has zero point of " +
234                                         std::to_string(invalidZeroPoint);
235             validate(device, message, model, [operand, invalidZeroPoint](Model* model) {
236                 model->operands[operand].zeroPoint = invalidZeroPoint;
237             });
238         }
239     }
242 ///////////////////////// VALIDATE EXTRA ??? /////////////////////////
244 // TODO: Operand::lifetime
245 // TODO: Operand::location
247 ///////////////////////// VALIDATE OPERATION OPERAND TYPE /////////////////////////
249 static void mutateOperand(Operand* operand, OperandType type) {
250     Operand newOperand = *operand;
251     newOperand.type = type;
252     switch (type) {
253         case OperandType::FLOAT32:
254         case OperandType::INT32:
255         case OperandType::UINT32:
256             newOperand.dimensions = hidl_vec<uint32_t>();
257             newOperand.scale = 0.0f;
258             newOperand.zeroPoint = 0;
259             break;
260         case OperandType::TENSOR_FLOAT32:
261             newOperand.dimensions =
262                 operand->dimensions.size() > 0 ? operand->dimensions : hidl_vec<uint32_t>({1});
263             newOperand.scale = 0.0f;
264             newOperand.zeroPoint = 0;
265             break;
266         case OperandType::TENSOR_INT32:
267             newOperand.dimensions =
268                 operand->dimensions.size() > 0 ? operand->dimensions : hidl_vec<uint32_t>({1});
269             newOperand.zeroPoint = 0;
270             break;
271         case OperandType::TENSOR_QUANT8_ASYMM:
272             newOperand.dimensions =
273                 operand->dimensions.size() > 0 ? operand->dimensions : hidl_vec<uint32_t>({1});
274             newOperand.scale = operand->scale != 0.0f ? operand->scale : 1.0f;
275             break;
276         case OperandType::OEM:
277         case OperandType::TENSOR_OEM_BYTE:
278         default:
279             break;
280     }
281     *operand = newOperand;
284 static bool mutateOperationOperandTypeSkip(size_t operand, const Model& model) {
285     // LSH_PROJECTION's second argument is allowed to have any type. This is the
286     // only operation that currently has a type that can be anything independent
287     // from any other type. Changing the operand type to any other type will
288     // result in a valid model for LSH_PROJECTION. If this is the case, skip the
289     // test.
290     for (const Operation& operation : model.operations) {
291         if (operation.type == OperationType::LSH_PROJECTION && operand == operation.inputs[1]) {
292             return true;
293         }
294     }
295     return false;
298 static void mutateOperationOperandTypeTest(const sp<IDevice>& device, const Model& model) {
299     for (size_t operand = 0; operand < model.operands.size(); ++operand) {
300         if (mutateOperationOperandTypeSkip(operand, model)) {
301             continue;
302         }
303         for (OperandType invalidOperandType : hidl_enum_range<OperandType>{}) {
304             // Do not test OEM types
305             if (invalidOperandType == model.operands[operand].type ||
306                 invalidOperandType == OperandType::OEM ||
307                 invalidOperandType == OperandType::TENSOR_OEM_BYTE) {
308                 continue;
309             }
310             const std::string message = "mutateOperationOperandTypeTest: operand " +
311                                         std::to_string(operand) + " set to type " +
312                                         toString(invalidOperandType);
313             validate(device, message, model, [operand, invalidOperandType](Model* model) {
314                 mutateOperand(&model->operands[operand], invalidOperandType);
315             });
316         }
317     }
320 ///////////////////////// VALIDATE MODEL OPERATION TYPE /////////////////////////
322 static const int32_t invalidOperationTypes[] = {
323     static_cast<int32_t>(OperationType::ADD) - 1,            // lower bound fundamental
324     static_cast<int32_t>(OperationType::TRANSPOSE) + 1,      // upper bound fundamental
325     static_cast<int32_t>(OperationType::OEM_OPERATION) - 1,  // lower bound OEM
326     static_cast<int32_t>(OperationType::OEM_OPERATION) + 1,  // upper bound OEM
327 };
329 static void mutateOperationTypeTest(const sp<IDevice>& device, const Model& model) {
330     for (size_t operation = 0; operation < model.operations.size(); ++operation) {
331         for (int32_t invalidOperationType : invalidOperationTypes) {
332             const std::string message = "mutateOperationTypeTest: operation " +
333                                         std::to_string(operation) + " set to value " +
334                                         std::to_string(invalidOperationType);
335             validate(device, message, model, [operation, invalidOperationType](Model* model) {
336                 model->operations[operation].type =
337                     static_cast<OperationType>(invalidOperationType);
338             });
339         }
340     }
343 ///////////////////////// VALIDATE MODEL OPERATION INPUT OPERAND INDEX /////////////////////////
345 static void mutateOperationInputOperandIndexTest(const sp<IDevice>& device, const Model& model) {
346     for (size_t operation = 0; operation < model.operations.size(); ++operation) {
347         const uint32_t invalidOperand = model.operands.size();
348         for (size_t input = 0; input < model.operations[operation].inputs.size(); ++input) {
349             const std::string message = "mutateOperationInputOperandIndexTest: operation " +
350                                         std::to_string(operation) + " input " +
351                                         std::to_string(input);
352             validate(device, message, model, [operation, input, invalidOperand](Model* model) {
353                 model->operations[operation].inputs[input] = invalidOperand;
354             });
355         }
356     }
359 ///////////////////////// VALIDATE MODEL OPERATION OUTPUT OPERAND INDEX /////////////////////////
361 static void mutateOperationOutputOperandIndexTest(const sp<IDevice>& device, const Model& model) {
362     for (size_t operation = 0; operation < model.operations.size(); ++operation) {
363         const uint32_t invalidOperand = model.operands.size();
364         for (size_t output = 0; output < model.operations[operation].outputs.size(); ++output) {
365             const std::string message = "mutateOperationOutputOperandIndexTest: operation " +
366                                         std::to_string(operation) + " output " +
367                                         std::to_string(output);
368             validate(device, message, model, [operation, output, invalidOperand](Model* model) {
369                 model->operations[operation].outputs[output] = invalidOperand;
370             });
371         }
372     }
375 ///////////////////////// REMOVE OPERAND FROM EVERYTHING /////////////////////////
377 static void removeValueAndDecrementGreaterValues(hidl_vec<uint32_t>* vec, uint32_t value) {
378     if (vec) {
379         // remove elements matching "value"
380         auto last = std::remove(vec->begin(), vec->end(), value);
381         vec->resize(std::distance(vec->begin(), last));
383         // decrement elements exceeding "value"
384         std::transform(vec->begin(), vec->end(), vec->begin(),
385                        [value](uint32_t v) { return v > value ? v-- : v; });
386     }
389 static void removeOperand(Model* model, uint32_t index) {
390     hidl_vec_removeAt(&model->operands, index);
391     for (Operation& operation : model->operations) {
392         removeValueAndDecrementGreaterValues(&operation.inputs, index);
393         removeValueAndDecrementGreaterValues(&operation.outputs, index);
394     }
395     removeValueAndDecrementGreaterValues(&model->inputIndexes, index);
396     removeValueAndDecrementGreaterValues(&model->outputIndexes, index);
399 static void removeOperandTest(const sp<IDevice>& device, const Model& model) {
400     for (size_t operand = 0; operand < model.operands.size(); ++operand) {
401         const std::string message = "removeOperandTest: operand " + std::to_string(operand);
402         validate(device, message, model,
403                  [operand](Model* model) { removeOperand(model, operand); });
404     }
407 ///////////////////////// REMOVE OPERATION /////////////////////////
409 static void removeOperation(Model* model, uint32_t index) {
410     for (uint32_t operand : model->operations[index].inputs) {
411         model->operands[operand].numberOfConsumers--;
412     }
413     hidl_vec_removeAt(&model->operations, index);
416 static void removeOperationTest(const sp<IDevice>& device, const Model& model) {
417     for (size_t operation = 0; operation < model.operations.size(); ++operation) {
418         const std::string message = "removeOperationTest: operation " + std::to_string(operation);
419         validate(device, message, model,
420                  [operation](Model* model) { removeOperation(model, operation); });
421     }
424 ///////////////////////// REMOVE OPERATION INPUT /////////////////////////
426 static void removeOperationInputTest(const sp<IDevice>& device, const Model& model) {
427     for (size_t operation = 0; operation < model.operations.size(); ++operation) {
428         for (size_t input = 0; input < model.operations[operation].inputs.size(); ++input) {
429             const Operation& op = model.operations[operation];
430             // CONCATENATION has at least 2 inputs, with the last element being
431             // INT32. Skip this test if removing one of CONCATENATION's
432             // inputs still produces a valid model.
433             if (op.type == OperationType::CONCATENATION && op.inputs.size() > 2 &&
434                 input != op.inputs.size() - 1) {
435                 continue;
436             }
437             const std::string message = "removeOperationInputTest: operation " +
438                                         std::to_string(operation) + ", input " +
439                                         std::to_string(input);
440             validate(device, message, model, [operation, input](Model* model) {
441                 uint32_t operand = model->operations[operation].inputs[input];
442                 model->operands[operand].numberOfConsumers--;
443                 hidl_vec_removeAt(&model->operations[operation].inputs, input);
444             });
445         }
446     }
449 ///////////////////////// REMOVE OPERATION OUTPUT /////////////////////////
451 static void removeOperationOutputTest(const sp<IDevice>& device, const Model& model) {
452     for (size_t operation = 0; operation < model.operations.size(); ++operation) {
453         for (size_t output = 0; output < model.operations[operation].outputs.size(); ++output) {
454             const std::string message = "removeOperationOutputTest: operation " +
455                                         std::to_string(operation) + ", output " +
456                                         std::to_string(output);
457             validate(device, message, model, [operation, output](Model* model) {
458                 hidl_vec_removeAt(&model->operations[operation].outputs, output);
459             });
460         }
461     }
464 ///////////////////////// MODEL VALIDATION /////////////////////////
466 // TODO: remove model input
467 // TODO: remove model output
468 // TODO: add unused operation
470 ///////////////////////// ADD OPERATION INPUT /////////////////////////
472 static void addOperationInputTest(const sp<IDevice>& device, const Model& model) {
473     for (size_t operation = 0; operation < model.operations.size(); ++operation) {
474         const std::string message = "addOperationInputTest: operation " + std::to_string(operation);
475         validate(device, message, model, [operation](Model* model) {
476             uint32_t index = addOperand(model, OperandLifeTime::MODEL_INPUT);
477             hidl_vec_push_back(&model->operations[operation].inputs, index);
478             hidl_vec_push_back(&model->inputIndexes, index);
479         });
480     }
483 ///////////////////////// ADD OPERATION OUTPUT /////////////////////////
485 static void addOperationOutputTest(const sp<IDevice>& device, const Model& model) {
486     for (size_t operation = 0; operation < model.operations.size(); ++operation) {
487         const std::string message =
488             "addOperationOutputTest: operation " + std::to_string(operation);
489         validate(device, message, model, [operation](Model* model) {
490             uint32_t index = addOperand(model, OperandLifeTime::MODEL_OUTPUT);
491             hidl_vec_push_back(&model->operations[operation].outputs, index);
492             hidl_vec_push_back(&model->outputIndexes, index);
493         });
494     }
497 ///////////////////////// VALIDATE EXECUTION PREFERENCE /////////////////////////
499 static const int32_t invalidExecutionPreferences[] = {
500     static_cast<int32_t>(ExecutionPreference::LOW_POWER) - 1,        // lower bound
501     static_cast<int32_t>(ExecutionPreference::SUSTAINED_SPEED) + 1,  // upper bound
502 };
504 static void mutateExecutionPreferenceTest(const sp<IDevice>& device, const Model& model) {
505     for (int32_t preference : invalidExecutionPreferences) {
506         const std::string message =
507             "mutateExecutionPreferenceTest: preference " + std::to_string(preference);
508         validate(device, message, model, [](Model*) {},
509                  static_cast<ExecutionPreference>(preference));
510     }
513 ////////////////////////// ENTRY POINT //////////////////////////////
515 void ValidationTest::validateModel(const Model& model) {
516     mutateOperandTypeTest(device, model);
517     mutateOperandRankTest(device, model);
518     mutateOperandScaleTest(device, model);
519     mutateOperandZeroPointTest(device, model);
520     mutateOperationOperandTypeTest(device, model);
521     mutateOperationTypeTest(device, model);
522     mutateOperationInputOperandIndexTest(device, model);
523     mutateOperationOutputOperandIndexTest(device, model);
524     removeOperandTest(device, model);
525     removeOperationTest(device, model);
526     removeOperationInputTest(device, model);
527     removeOperationOutputTest(device, model);
528     addOperationInputTest(device, model);
529     addOperationOutputTest(device, model);
530     mutateExecutionPreferenceTest(device, model);
533 }  // namespace functional
534 }  // namespace vts
535 }  // namespace V1_2
536 }  // namespace neuralnetworks
537 }  // namespace hardware
538 }  // namespace android