Merge "Fix implicit-fallthrough warnings."
[android/platform-hardware-interfaces.git] / neuralnetworks / 1.2 / vts / functional / ValidateModel.cpp
1 /*
2  * Copyright (C) 2018 The Android Open Source Project
3  *
4  * Licensed under the Apache License, Version 2.0 (the "License");
5  * you may not use this file except in compliance with the License.
6  * You may obtain a copy of the License at
7  *
8  *      http://www.apache.org/licenses/LICENSE-2.0
9  *
10  * Unless required by applicable law or agreed to in writing, software
11  * distributed under the License is distributed on an "AS IS" BASIS,
12  * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
13  * See the License for the specific language governing permissions and
14  * limitations under the License.
15  */
17 #define LOG_TAG "neuralnetworks_hidl_hal_test"
19 #include "VtsHalNeuralnetworks.h"
21 #include "Callbacks.h"
23 namespace android {
24 namespace hardware {
25 namespace neuralnetworks {
26 namespace V1_2 {
28 using V1_0::IPreparedModel;
29 using V1_0::OperandLifeTime;
30 using V1_1::ExecutionPreference;
32 namespace vts {
33 namespace functional {
35 using ::android::hardware::neuralnetworks::V1_0::implementation::ExecutionCallback;
36 using ::android::hardware::neuralnetworks::V1_0::implementation::PreparedModelCallback;
38 ///////////////////////// UTILITY FUNCTIONS /////////////////////////
40 static void validateGetSupportedOperations(const sp<IDevice>& device, const std::string& message,
41                                            const Model& model) {
42     SCOPED_TRACE(message + " [getSupportedOperations_1_2]");
44     Return<void> ret =
45         device->getSupportedOperations_1_2(model, [&](ErrorStatus status, const hidl_vec<bool>&) {
46             EXPECT_EQ(ErrorStatus::INVALID_ARGUMENT, status);
47         });
48     EXPECT_TRUE(ret.isOk());
49 }
51 static void validatePrepareModel(const sp<IDevice>& device, const std::string& message,
52                                  const Model& model, ExecutionPreference preference) {
53     SCOPED_TRACE(message + " [prepareModel_1_2]");
55     sp<PreparedModelCallback> preparedModelCallback = new PreparedModelCallback();
56     ASSERT_NE(nullptr, preparedModelCallback.get());
57     Return<ErrorStatus> prepareLaunchStatus =
58         device->prepareModel_1_2(model, preference, preparedModelCallback);
59     ASSERT_TRUE(prepareLaunchStatus.isOk());
60     ASSERT_EQ(ErrorStatus::INVALID_ARGUMENT, static_cast<ErrorStatus>(prepareLaunchStatus));
62     preparedModelCallback->wait();
63     ErrorStatus prepareReturnStatus = preparedModelCallback->getStatus();
64     ASSERT_EQ(ErrorStatus::INVALID_ARGUMENT, prepareReturnStatus);
65     sp<IPreparedModel> preparedModel = preparedModelCallback->getPreparedModel();
66     ASSERT_EQ(nullptr, preparedModel.get());
67 }
69 static bool validExecutionPreference(ExecutionPreference preference) {
70     return preference == ExecutionPreference::LOW_POWER ||
71            preference == ExecutionPreference::FAST_SINGLE_ANSWER ||
72            preference == ExecutionPreference::SUSTAINED_SPEED;
73 }
75 // Primary validation function. This function will take a valid model, apply a
76 // mutation to it to invalidate the model, then pass it to interface calls that
77 // use the model. Note that the model here is passed by value, and any mutation
78 // to the model does not leave this function.
79 static void validate(const sp<IDevice>& device, const std::string& message, Model model,
80                      const std::function<void(Model*)>& mutation,
81                      ExecutionPreference preference = ExecutionPreference::FAST_SINGLE_ANSWER) {
82     mutation(&model);
83     if (validExecutionPreference(preference)) {
84         validateGetSupportedOperations(device, message, model);
85     }
86     validatePrepareModel(device, message, model, preference);
87 }
89 // Delete element from hidl_vec. hidl_vec doesn't support a "remove" operation,
90 // so this is efficiently accomplished by moving the element to the end and
91 // resizing the hidl_vec to one less.
92 template <typename Type>
93 static void hidl_vec_removeAt(hidl_vec<Type>* vec, uint32_t index) {
94     if (vec) {
95         std::rotate(vec->begin() + index, vec->begin() + index + 1, vec->end());
96         vec->resize(vec->size() - 1);
97     }
98 }
100 template <typename Type>
101 static uint32_t hidl_vec_push_back(hidl_vec<Type>* vec, const Type& value) {
102     // assume vec is valid
103     const uint32_t index = vec->size();
104     vec->resize(index + 1);
105     (*vec)[index] = value;
106     return index;
109 static uint32_t addOperand(Model* model) {
110     return hidl_vec_push_back(&model->operands,
111                               {
112                                   .type = OperandType::INT32,
113                                   .dimensions = {},
114                                   .numberOfConsumers = 0,
115                                   .scale = 0.0f,
116                                   .zeroPoint = 0,
117                                   .lifetime = OperandLifeTime::MODEL_INPUT,
118                                   .location = {.poolIndex = 0, .offset = 0, .length = 0},
119                               });
122 static uint32_t addOperand(Model* model, OperandLifeTime lifetime) {
123     uint32_t index = addOperand(model);
124     model->operands[index].numberOfConsumers = 1;
125     model->operands[index].lifetime = lifetime;
126     return index;
129 ///////////////////////// VALIDATE MODEL OPERAND TYPE /////////////////////////
131 static const int32_t invalidOperandTypes[] = {
132     static_cast<int32_t>(OperandType::FLOAT32) - 1,               // lower bound fundamental
133     static_cast<int32_t>(OperandType::TENSOR_QUANT16_ASYMM) + 1,  // upper bound fundamental
134     static_cast<int32_t>(OperandType::OEM) - 1,                   // lower bound OEM
135     static_cast<int32_t>(OperandType::TENSOR_OEM_BYTE) + 1,       // upper bound OEM
136 };
138 static void mutateOperandTypeTest(const sp<IDevice>& device, const Model& model) {
139     for (size_t operand = 0; operand < model.operands.size(); ++operand) {
140         for (int32_t invalidOperandType : invalidOperandTypes) {
141             const std::string message = "mutateOperandTypeTest: operand " +
142                                         std::to_string(operand) + " set to value " +
143                                         std::to_string(invalidOperandType);
144             validate(device, message, model, [operand, invalidOperandType](Model* model) {
145                 model->operands[operand].type = static_cast<OperandType>(invalidOperandType);
146             });
147         }
148     }
151 ///////////////////////// VALIDATE OPERAND RANK /////////////////////////
153 static uint32_t getInvalidRank(OperandType type) {
154     switch (type) {
155         case OperandType::FLOAT32:
156         case OperandType::INT32:
157         case OperandType::UINT32:
158         case OperandType::BOOL:
159             return 1;
160         case OperandType::TENSOR_FLOAT16:
161         case OperandType::TENSOR_FLOAT32:
162         case OperandType::TENSOR_INT32:
163         case OperandType::TENSOR_QUANT8_ASYMM:
164         case OperandType::TENSOR_QUANT16_ASYMM:
165             return 0;
166         default:
167             return 0;
168     }
171 static void mutateOperandRankTest(const sp<IDevice>& device, const Model& model) {
172     for (size_t operand = 0; operand < model.operands.size(); ++operand) {
173         const uint32_t invalidRank = getInvalidRank(model.operands[operand].type);
174         const std::string message = "mutateOperandRankTest: operand " + std::to_string(operand) +
175                                     " has rank of " + std::to_string(invalidRank);
176         validate(device, message, model, [operand, invalidRank](Model* model) {
177             model->operands[operand].dimensions = std::vector<uint32_t>(invalidRank, 0);
178         });
179     }
182 ///////////////////////// VALIDATE OPERAND SCALE /////////////////////////
184 static float getInvalidScale(OperandType type) {
185     switch (type) {
186         case OperandType::FLOAT32:
187         case OperandType::INT32:
188         case OperandType::UINT32:
189         case OperandType::BOOL:
190         case OperandType::TENSOR_FLOAT16:
191         case OperandType::TENSOR_FLOAT32:
192             return 1.0f;
193         case OperandType::TENSOR_INT32:
194             return -1.0f;
195         case OperandType::TENSOR_QUANT8_ASYMM:
196         case OperandType::TENSOR_QUANT16_ASYMM:
197             return 0.0f;
198         default:
199             return 0.0f;
200     }
203 static void mutateOperandScaleTest(const sp<IDevice>& device, const Model& model) {
204     for (size_t operand = 0; operand < model.operands.size(); ++operand) {
205         const float invalidScale = getInvalidScale(model.operands[operand].type);
206         const std::string message = "mutateOperandScaleTest: operand " + std::to_string(operand) +
207                                     " has scale of " + std::to_string(invalidScale);
208         validate(device, message, model, [operand, invalidScale](Model* model) {
209             model->operands[operand].scale = invalidScale;
210         });
211     }
214 ///////////////////////// VALIDATE OPERAND ZERO POINT /////////////////////////
216 static std::vector<int32_t> getInvalidZeroPoints(OperandType type) {
217     switch (type) {
218         case OperandType::FLOAT32:
219         case OperandType::INT32:
220         case OperandType::UINT32:
221         case OperandType::BOOL:
222         case OperandType::TENSOR_FLOAT16:
223         case OperandType::TENSOR_FLOAT32:
224         case OperandType::TENSOR_INT32:
225             return {1};
226         case OperandType::TENSOR_QUANT8_ASYMM:
227         case OperandType::TENSOR_QUANT16_ASYMM:
228             return {-1, 256};
229         default:
230             return {};
231     }
234 static void mutateOperandZeroPointTest(const sp<IDevice>& device, const Model& model) {
235     for (size_t operand = 0; operand < model.operands.size(); ++operand) {
236         const std::vector<int32_t> invalidZeroPoints =
237             getInvalidZeroPoints(model.operands[operand].type);
238         for (int32_t invalidZeroPoint : invalidZeroPoints) {
239             const std::string message = "mutateOperandZeroPointTest: operand " +
240                                         std::to_string(operand) + " has zero point of " +
241                                         std::to_string(invalidZeroPoint);
242             validate(device, message, model, [operand, invalidZeroPoint](Model* model) {
243                 model->operands[operand].zeroPoint = invalidZeroPoint;
244             });
245         }
246     }
249 ///////////////////////// VALIDATE EXTRA ??? /////////////////////////
251 // TODO: Operand::lifetime
252 // TODO: Operand::location
254 ///////////////////////// VALIDATE OPERATION OPERAND TYPE /////////////////////////
256 static void mutateOperand(Operand* operand, OperandType type) {
257     Operand newOperand = *operand;
258     newOperand.type = type;
259     switch (type) {
260         case OperandType::FLOAT32:
261         case OperandType::INT32:
262         case OperandType::UINT32:
263         case OperandType::BOOL:
264             newOperand.dimensions = hidl_vec<uint32_t>();
265             newOperand.scale = 0.0f;
266             newOperand.zeroPoint = 0;
267             break;
268         case OperandType::TENSOR_FLOAT16:
269         case OperandType::TENSOR_FLOAT32:
270             newOperand.dimensions =
271                 operand->dimensions.size() > 0 ? operand->dimensions : hidl_vec<uint32_t>({1});
272             newOperand.scale = 0.0f;
273             newOperand.zeroPoint = 0;
274             break;
275         case OperandType::TENSOR_INT32:
276             newOperand.dimensions =
277                 operand->dimensions.size() > 0 ? operand->dimensions : hidl_vec<uint32_t>({1});
278             newOperand.zeroPoint = 0;
279             break;
280         case OperandType::TENSOR_QUANT8_ASYMM:
281         case OperandType::TENSOR_QUANT16_ASYMM:
282             newOperand.dimensions =
283                 operand->dimensions.size() > 0 ? operand->dimensions : hidl_vec<uint32_t>({1});
284             newOperand.scale = operand->scale != 0.0f ? operand->scale : 1.0f;
285             break;
286         case OperandType::OEM:
287         case OperandType::TENSOR_OEM_BYTE:
288         default:
289             break;
290     }
291     *operand = newOperand;
294 static bool mutateOperationOperandTypeSkip(size_t operand, const Model& model) {
295     // LSH_PROJECTION's second argument is allowed to have any type. This is the
296     // only operation that currently has a type that can be anything independent
297     // from any other type. Changing the operand type to any other type will
298     // result in a valid model for LSH_PROJECTION. If this is the case, skip the
299     // test.
300     for (const Operation& operation : model.operations) {
301         if (operation.type == OperationType::LSH_PROJECTION && operand == operation.inputs[1]) {
302             return true;
303         }
304     }
305     return false;
308 static void mutateOperationOperandTypeTest(const sp<IDevice>& device, const Model& model) {
309     for (size_t operand = 0; operand < model.operands.size(); ++operand) {
310         if (mutateOperationOperandTypeSkip(operand, model)) {
311             continue;
312         }
313         for (OperandType invalidOperandType : hidl_enum_range<OperandType>{}) {
314             // Do not test OEM types
315             if (invalidOperandType == model.operands[operand].type ||
316                 invalidOperandType == OperandType::OEM ||
317                 invalidOperandType == OperandType::TENSOR_OEM_BYTE) {
318                 continue;
319             }
320             const std::string message = "mutateOperationOperandTypeTest: operand " +
321                                         std::to_string(operand) + " set to type " +
322                                         toString(invalidOperandType);
323             validate(device, message, model, [operand, invalidOperandType](Model* model) {
324                 mutateOperand(&model->operands[operand], invalidOperandType);
325             });
326         }
327     }
330 ///////////////////////// VALIDATE MODEL OPERATION TYPE /////////////////////////
332 static const int32_t invalidOperationTypes[] = {
333     static_cast<int32_t>(OperationType::ADD) - 1,            // lower bound fundamental
334     static_cast<int32_t>(OperationType::TRANSPOSE) + 1,      // upper bound fundamental
335     static_cast<int32_t>(OperationType::OEM_OPERATION) - 1,  // lower bound OEM
336     static_cast<int32_t>(OperationType::OEM_OPERATION) + 1,  // upper bound OEM
337 };
339 static void mutateOperationTypeTest(const sp<IDevice>& device, const Model& model) {
340     for (size_t operation = 0; operation < model.operations.size(); ++operation) {
341         for (int32_t invalidOperationType : invalidOperationTypes) {
342             const std::string message = "mutateOperationTypeTest: operation " +
343                                         std::to_string(operation) + " set to value " +
344                                         std::to_string(invalidOperationType);
345             validate(device, message, model, [operation, invalidOperationType](Model* model) {
346                 model->operations[operation].type =
347                     static_cast<OperationType>(invalidOperationType);
348             });
349         }
350     }
353 ///////////////////////// VALIDATE MODEL OPERATION INPUT OPERAND INDEX /////////////////////////
355 static void mutateOperationInputOperandIndexTest(const sp<IDevice>& device, const Model& model) {
356     for (size_t operation = 0; operation < model.operations.size(); ++operation) {
357         const uint32_t invalidOperand = model.operands.size();
358         for (size_t input = 0; input < model.operations[operation].inputs.size(); ++input) {
359             const std::string message = "mutateOperationInputOperandIndexTest: operation " +
360                                         std::to_string(operation) + " input " +
361                                         std::to_string(input);
362             validate(device, message, model, [operation, input, invalidOperand](Model* model) {
363                 model->operations[operation].inputs[input] = invalidOperand;
364             });
365         }
366     }
369 ///////////////////////// VALIDATE MODEL OPERATION OUTPUT OPERAND INDEX /////////////////////////
371 static void mutateOperationOutputOperandIndexTest(const sp<IDevice>& device, const Model& model) {
372     for (size_t operation = 0; operation < model.operations.size(); ++operation) {
373         const uint32_t invalidOperand = model.operands.size();
374         for (size_t output = 0; output < model.operations[operation].outputs.size(); ++output) {
375             const std::string message = "mutateOperationOutputOperandIndexTest: operation " +
376                                         std::to_string(operation) + " output " +
377                                         std::to_string(output);
378             validate(device, message, model, [operation, output, invalidOperand](Model* model) {
379                 model->operations[operation].outputs[output] = invalidOperand;
380             });
381         }
382     }
385 ///////////////////////// REMOVE OPERAND FROM EVERYTHING /////////////////////////
387 static void removeValueAndDecrementGreaterValues(hidl_vec<uint32_t>* vec, uint32_t value) {
388     if (vec) {
389         // remove elements matching "value"
390         auto last = std::remove(vec->begin(), vec->end(), value);
391         vec->resize(std::distance(vec->begin(), last));
393         // decrement elements exceeding "value"
394         std::transform(vec->begin(), vec->end(), vec->begin(),
395                        [value](uint32_t v) { return v > value ? v-- : v; });
396     }
399 static void removeOperand(Model* model, uint32_t index) {
400     hidl_vec_removeAt(&model->operands, index);
401     for (Operation& operation : model->operations) {
402         removeValueAndDecrementGreaterValues(&operation.inputs, index);
403         removeValueAndDecrementGreaterValues(&operation.outputs, index);
404     }
405     removeValueAndDecrementGreaterValues(&model->inputIndexes, index);
406     removeValueAndDecrementGreaterValues(&model->outputIndexes, index);
409 static void removeOperandTest(const sp<IDevice>& device, const Model& model) {
410     for (size_t operand = 0; operand < model.operands.size(); ++operand) {
411         const std::string message = "removeOperandTest: operand " + std::to_string(operand);
412         validate(device, message, model,
413                  [operand](Model* model) { removeOperand(model, operand); });
414     }
417 ///////////////////////// REMOVE OPERATION /////////////////////////
419 static void removeOperation(Model* model, uint32_t index) {
420     for (uint32_t operand : model->operations[index].inputs) {
421         model->operands[operand].numberOfConsumers--;
422     }
423     hidl_vec_removeAt(&model->operations, index);
426 static void removeOperationTest(const sp<IDevice>& device, const Model& model) {
427     for (size_t operation = 0; operation < model.operations.size(); ++operation) {
428         const std::string message = "removeOperationTest: operation " + std::to_string(operation);
429         validate(device, message, model,
430                  [operation](Model* model) { removeOperation(model, operation); });
431     }
434 ///////////////////////// REMOVE OPERATION INPUT /////////////////////////
436 static void removeOperationInputTest(const sp<IDevice>& device, const Model& model) {
437     for (size_t operation = 0; operation < model.operations.size(); ++operation) {
438         for (size_t input = 0; input < model.operations[operation].inputs.size(); ++input) {
439             const Operation& op = model.operations[operation];
440             // CONCATENATION has at least 2 inputs, with the last element being
441             // INT32. Skip this test if removing one of CONCATENATION's
442             // inputs still produces a valid model.
443             if (op.type == OperationType::CONCATENATION && op.inputs.size() > 2 &&
444                 input != op.inputs.size() - 1) {
445                 continue;
446             }
447             const std::string message = "removeOperationInputTest: operation " +
448                                         std::to_string(operation) + ", input " +
449                                         std::to_string(input);
450             validate(device, message, model, [operation, input](Model* model) {
451                 uint32_t operand = model->operations[operation].inputs[input];
452                 model->operands[operand].numberOfConsumers--;
453                 hidl_vec_removeAt(&model->operations[operation].inputs, input);
454             });
455         }
456     }
459 ///////////////////////// REMOVE OPERATION OUTPUT /////////////////////////
461 static void removeOperationOutputTest(const sp<IDevice>& device, const Model& model) {
462     for (size_t operation = 0; operation < model.operations.size(); ++operation) {
463         for (size_t output = 0; output < model.operations[operation].outputs.size(); ++output) {
464             const std::string message = "removeOperationOutputTest: operation " +
465                                         std::to_string(operation) + ", output " +
466                                         std::to_string(output);
467             validate(device, message, model, [operation, output](Model* model) {
468                 hidl_vec_removeAt(&model->operations[operation].outputs, output);
469             });
470         }
471     }
474 ///////////////////////// MODEL VALIDATION /////////////////////////
476 // TODO: remove model input
477 // TODO: remove model output
478 // TODO: add unused operation
480 ///////////////////////// ADD OPERATION INPUT /////////////////////////
482 static void addOperationInputTest(const sp<IDevice>& device, const Model& model) {
483     for (size_t operation = 0; operation < model.operations.size(); ++operation) {
484         const std::string message = "addOperationInputTest: operation " + std::to_string(operation);
485         validate(device, message, model, [operation](Model* model) {
486             uint32_t index = addOperand(model, OperandLifeTime::MODEL_INPUT);
487             hidl_vec_push_back(&model->operations[operation].inputs, index);
488             hidl_vec_push_back(&model->inputIndexes, index);
489         });
490     }
493 ///////////////////////// ADD OPERATION OUTPUT /////////////////////////
495 static void addOperationOutputTest(const sp<IDevice>& device, const Model& model) {
496     for (size_t operation = 0; operation < model.operations.size(); ++operation) {
497         const std::string message =
498             "addOperationOutputTest: operation " + std::to_string(operation);
499         validate(device, message, model, [operation](Model* model) {
500             uint32_t index = addOperand(model, OperandLifeTime::MODEL_OUTPUT);
501             hidl_vec_push_back(&model->operations[operation].outputs, index);
502             hidl_vec_push_back(&model->outputIndexes, index);
503         });
504     }
507 ///////////////////////// VALIDATE EXECUTION PREFERENCE /////////////////////////
509 static const int32_t invalidExecutionPreferences[] = {
510     static_cast<int32_t>(ExecutionPreference::LOW_POWER) - 1,        // lower bound
511     static_cast<int32_t>(ExecutionPreference::SUSTAINED_SPEED) + 1,  // upper bound
512 };
514 static void mutateExecutionPreferenceTest(const sp<IDevice>& device, const Model& model) {
515     for (int32_t preference : invalidExecutionPreferences) {
516         const std::string message =
517             "mutateExecutionPreferenceTest: preference " + std::to_string(preference);
518         validate(device, message, model, [](Model*) {},
519                  static_cast<ExecutionPreference>(preference));
520     }
523 ////////////////////////// ENTRY POINT //////////////////////////////
525 void ValidationTest::validateModel(const Model& model) {
526     mutateOperandTypeTest(device, model);
527     mutateOperandRankTest(device, model);
528     mutateOperandScaleTest(device, model);
529     mutateOperandZeroPointTest(device, model);
530     mutateOperationOperandTypeTest(device, model);
531     mutateOperationTypeTest(device, model);
532     mutateOperationInputOperandIndexTest(device, model);
533     mutateOperationOutputOperandIndexTest(device, model);
534     removeOperandTest(device, model);
535     removeOperationTest(device, model);
536     removeOperationInputTest(device, model);
537     removeOperationOutputTest(device, model);
538     addOperationInputTest(device, model);
539     addOperationOutputTest(device, model);
540     mutateExecutionPreferenceTest(device, model);
543 }  // namespace functional
544 }  // namespace vts
545 }  // namespace V1_2
546 }  // namespace neuralnetworks
547 }  // namespace hardware
548 }  // namespace android