Radio Interface changes to allow the modem to query the framework
[android/platform-hardware-interfaces.git] / radio / 1.1 / types.hal
1 /*
2  * Copyright (C) 2016 The Android Open Source Project
3  *
4  * Licensed under the Apache License, Version 2.0 (the "License");
5  * you may not use this file except in compliance with the License.
6  * You may obtain a copy of the License at
7  *
8  *      http://www.apache.org/licenses/LICENSE-2.0
9  *
10  * Unless required by applicable law or agreed to in writing, software
11  * distributed under the License is distributed on an "AS IS" BASIS,
12  * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
13  * See the License for the specific language governing permissions and
14  * limitations under the License.
15  */
17 package android.hardware.radio@1.1;
19 import @1.0::CellInfo;
20 import @1.0::RadioError;
22 enum CardPowerState : int32_t {
23     POWER_DOWN,
24     POWER_UP,
25     POWER_UP_PASS_THROUGH,
26 };
28 enum RadioAccessNetworks : int32_t {
29     GERAN = 1,                              // GSM EDGE Radio Access Network
30     UTRAN = 2,                              // Universal Terrestrial Radio Access Network
31     EUTRAN = 3,                             // Evolved Universal Terrestrial Radio Access Network
32 };
34 enum GeranBands : int32_t {
35     BAND_T380 = 1,
36     BAND_T410 = 2,
37     BAND_450 = 3,
38     BAND_480 = 4,
39     BAND_710 = 5,
40     BAND_750 = 6,
41     BAND_T810 = 7,
42     BAND_850 = 8,
43     BAND_P900 = 9,
44     BAND_E900 = 10,
45     BAND_R900 = 11,
46     BAND_DCS1800 = 12,
47     BAND_PCS1900 = 13,
48     BAND_ER900 = 14,
49 };
51 enum UtranBands : int32_t {
52     BAND_1 = 1,
53     BAND_2 = 2,
54     BAND_3 = 3,
55     BAND_4 = 4,
56     BAND_5 = 5,
57     BAND_6 = 6,
58     BAND_7 = 7,
59     BAND_8 = 8,
60     BAND_9 = 9,
61     BAND_10 = 10,
62     BAND_11 = 11,
63     BAND_12 = 12,
64     BAND_13 = 13,
65     BAND_14 = 14,
66     BAND_19 = 19,
67     BAND_20 = 20,
68     BAND_21 = 21,
69     BAND_22 = 22,
70     BAND_25 = 25,
71     BAND_26 = 26,
72 };
74 enum EutranBands : int32_t {
75     BAND_1 = 1,
76     BAND_2 = 2,
77     BAND_3 = 3,
78     BAND_4 = 4,
79     BAND_5 = 5,
80     BAND_6 = 6,
81     BAND_7 = 7,
82     BAND_8 = 8,
83     BAND_9 = 9,
84     BAND_10 = 10,
85     BAND_11 = 11,
86     BAND_12 = 12,
87     BAND_13 = 13,
88     BAND_14 = 14,
89     BAND_17 = 17,
90     BAND_18 = 18,
91     BAND_19 = 19,
92     BAND_20 = 20,
93     BAND_21 = 21,
94     BAND_22 = 22,
95     BAND_23 = 23,
96     BAND_24 = 24,
97     BAND_25 = 25,
98     BAND_26 = 26,
99     BAND_27 = 27,
100     BAND_28 = 28,
101     BAND_30 = 30,
102     BAND_31 = 31,
103     BAND_33 = 33,
104     BAND_34 = 34,
105     BAND_35 = 35,
106     BAND_36 = 36,
107     BAND_37 = 37,
108     BAND_38 = 38,
109     BAND_39 = 39,
110     BAND_40 = 40,
111     BAND_41 = 41,
112     BAND_42 = 42,
113     BAND_43 = 43,
114     BAND_44 = 44,
115     BAND_45 = 45,
116     BAND_46 = 46,
117     BAND_47 = 47,
118     BAND_48 = 48,
119     BAND_65 = 65,
120     BAND_66 = 66,
121     BAND_68 = 68,
122     BAND_70 = 70,
123 };
125 enum ScanType : int32_t {
126     ONE_SHOT = 0,                           // Performs the scan only once
127     PERIODIC = 1,                           // Performs the scan periodically until cancelled
128 };
130 enum ScanStatus : int32_t {
131     PARTIAL = 1,                            // The result contains a part of the scan results
132     COMPLETE = 2,                           // The result contains the last part of the scan results
133 };
135 struct RadioAccessSpecifier {
136     RadioAccessNetworks radioAccessNetwork; // The type of network to scan
137     vec<GeranBands> geranBands;             // Valid only if radioAccessNetwork = GERAN
138                                             // otherwise must be empty
139                                             // Maximum length of the vector is 8
140     vec<UtranBands> utranBands;             // Valid only if radioAccessNetwork = UTRAN
141                                             // otherwise must be empty
142                                             // Maximum length of the vector is 8
143     vec<EutranBands> eutranBands;           // Valid only if radioAccessNetwork = EUTRAN
144                                             // otherwise must be empty
145                                             // Maximum length of the vector is 8
146     vec<int32_t> channels;                  // The radio channels to scan as defined in
147                                             // 3GPP TS 25.101 and 36.101
148                                             // Maximum length of the vector is 32
149 };
151 struct NetworkScanRequest {
152     ScanType type;                          // One shot scan or periodic
153     int32_t interval;                       // Time interval in seconds between periodic scans, only
154                                             // valid when type = PERIODIC
155                                             // Range: 5 to 600
156     vec<RadioAccessSpecifier> specifiers;   // networks with bands/channels to scan
157                                             // Maximum length of the vector is 8
158 };
160 struct NetworkScanResult {
161     ScanStatus status;                      // The status of the scan
162     RadioError error;                       // The error code of the incremental result
163     vec<CellInfo> networkInfos;             // List of network information as CellInfo
164 };
166 struct ImsiEncryptionInfo {
167     string mcc;                   // MCC of the Carrier.
168     string mnc;                   // MNC of the Carrier.
169     vec<uint8_t> carrierKey;      // Carrier specific key to be used for encryption. It must
170                                   // be opaque to the framework. This is the byte-stream
171                                   // representation of the key. This is an external encoded
172                                   // form for the key used when a standard representation of
173                                   // the key is needed outside the Java Virtual Machine, as
174                                   // when transmitting the key to some other party.
175                                   // The key is encoded according to a standard format
176                                   // (such as X.509 SubjectPublicKeyInfo or PKCS#8), and is
177                                   // returned using the getEncoded method as defined on the
178                                   // java.security.Key interface.
179     string keyIdentifier;         // This is an opaque value we're given by the carrier
180                                   // and is returned to the carrier. This is used by the server to
181                                   // help it locate the private key to decrypt the permanent
182                                   // identity.
183     int64_t expirationTime;       // date-time in UTC when the key will expire.
184 };