/* ** ** Copyright 2017, The Android Open Source Project ** ** Licensed under the Apache License, Version 2.0 (the "License"); ** you may not use this file except in compliance with the License. ** You may obtain a copy of the License at ** ** http://www.apache.org/licenses/LICENSE-2.0 ** ** Unless required by applicable law or agreed to in writing, software ** distributed under the License is distributed on an "AS IS" BASIS, ** WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied. ** See the License for the specific language governing permissions and ** limitations under the License. */ #include namespace android { namespace hardware { namespace confirmationui { namespace support { namespace { inline uint8_t getByte(const uint64_t& v, const uint8_t index) { return v >> (index * 8); } WriteState writeBytes(WriteState state, uint64_t value, uint8_t size) { auto pos = state.data_; if (!(state += size)) return state; switch (size) { case 8: *pos++ = getByte(value, 7); *pos++ = getByte(value, 6); *pos++ = getByte(value, 5); *pos++ = getByte(value, 4); case 4: *pos++ = getByte(value, 3); *pos++ = getByte(value, 2); case 2: *pos++ = getByte(value, 1); case 1: *pos++ = value; break; default: state.error_ = Error::MALFORMED; } return state; } } // anonymous namespace WriteState writeHeader(WriteState wState, Type type, const uint64_t value) { if (!wState) return wState; uint8_t& header = *wState.data_; if (!++wState) return wState; header = static_cast(type) << 5; if (value < 24) { header |= static_cast(value); } else if (value < 0x100) { header |= 24; wState = writeBytes(wState, value, 1); } else if (value < 0x10000) { header |= 25; wState = writeBytes(wState, value, 2); } else if (value < 0x100000000) { header |= 26; wState = writeBytes(wState, value, 4); } else { header |= 27; wState = writeBytes(wState, value, 8); } return wState; } bool checkUTF8Copy(const char* begin, const char* const end, uint8_t* out) { uint32_t multi_byte_length = 0; while (begin != end) { if (multi_byte_length) { // parsing multi byte character - must start with 10xxxxxx --multi_byte_length; if ((*begin & 0xc0) != 0x80) return false; } else if (!((*begin) & 0x80)) { // 7bit character -> nothing to be done } else { // msb is set and we were not parsing a multi byte character // so this must be a header byte char c = *begin << 1; while (c & 0x80) { ++multi_byte_length; c <<= 1; } // headers of the form 10xxxxxx are not allowed if (multi_byte_length < 1) return false; // chars longer than 4 bytes are not allowed (multi_byte_length does not count the // header thus > 3 if (multi_byte_length > 3) return false; } if (out) *out++ = *reinterpret_cast(begin++); } // if the string ends in the middle of a multi byte char it is invalid if (multi_byte_length) return false; return true; } } // namespace support } // namespace confirmationui } // namespace hardware } // namespace android