/* * Copyright (C) 2018 The Android Open Source Project * * Licensed under the Apache License, Version 2.0 (the "License"); * you may not use this file except in compliance with the License. * You may obtain a copy of the License at * * http://www.apache.org/licenses/LICENSE-2.0 * * Unless required by applicable law or agreed to in writing, software * distributed under the License is distributed on an "AS IS" BASIS, * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied. * See the License for the specific language governing permissions and * limitations under the License. */ #define LOG_TAG "graphics_composer_hidl_hal_test@2.2" #include #include #include #include #include #include #include namespace android { namespace hardware { namespace graphics { namespace composer { namespace V2_2 { namespace vts { namespace { using android::hardware::graphics::common::V1_0::BufferUsage; using android::hardware::graphics::common::V1_0::ColorTransform; using android::hardware::graphics::common::V1_0::Transform; using android::hardware::graphics::common::V1_1::ColorMode; using android::hardware::graphics::common::V1_1::Dataspace; using android::hardware::graphics::common::V1_1::PixelFormat; using android::hardware::graphics::common::V1_1::RenderIntent; using android::hardware::graphics::composer::V2_2::IComposerClient; using android::hardware::graphics::mapper::V2_1::IMapper; using android::hardware::graphics::mapper::V2_1::vts::Gralloc; using GrallocError = android::hardware::graphics::mapper::V2_0::Error; // Test environment for graphics.composer class GraphicsComposerHidlEnvironment : public ::testing::VtsHalHidlTargetTestEnvBase { public: // get the test environment singleton static GraphicsComposerHidlEnvironment* Instance() { static GraphicsComposerHidlEnvironment* instance = new GraphicsComposerHidlEnvironment; return instance; } virtual void registerTestServices() override { registerTestService(); } private: GraphicsComposerHidlEnvironment() {} GTEST_DISALLOW_COPY_AND_ASSIGN_(GraphicsComposerHidlEnvironment); }; class GraphicsComposerHidlTest : public ::testing::VtsHalHidlTargetTestBase { protected: void SetUp() override { ASSERT_NO_FATAL_FAILURE( mComposer = std::make_unique( GraphicsComposerHidlEnvironment::Instance()->getServiceName())); ASSERT_NO_FATAL_FAILURE(mComposerClient = mComposer->createClient_v2_2()); mComposerCallback = new V2_1::vts::GraphicsComposerCallback; mComposerClient->registerCallback(mComposerCallback); // assume the first display is primary and is never removed mPrimaryDisplay = waitForFirstDisplay(); // explicitly disable vsync mComposerClient->setVsyncEnabled(mPrimaryDisplay, false); mComposerCallback->setVsyncAllowed(false); mComposerClient->getRaw()->getReadbackBufferAttributes( mPrimaryDisplay, [&](const auto& tmpError, const auto&, const auto&) { mHasReadbackBuffer = tmpError == Error::NONE; }); } void TearDown() override { if (mComposerCallback != nullptr) { EXPECT_EQ(0, mComposerCallback->getInvalidHotplugCount()); EXPECT_EQ(0, mComposerCallback->getInvalidRefreshCount()); EXPECT_EQ(0, mComposerCallback->getInvalidVsyncCount()); } } // use the slot count usually set by SF static constexpr uint32_t kBufferSlotCount = 64; std::unique_ptr mComposer; std::unique_ptr mComposerClient; sp mComposerCallback; // the first display and is assumed never to be removed Display mPrimaryDisplay; bool mHasReadbackBuffer; private: Display waitForFirstDisplay() { while (true) { std::vector displays = mComposerCallback->getDisplays(); if (displays.empty()) { usleep(5 * 1000); continue; } return displays[0]; } } }; // Tests for IComposerClient::Command. class GraphicsComposerHidlCommandTest : public GraphicsComposerHidlTest { protected: void SetUp() override { ASSERT_NO_FATAL_FAILURE(GraphicsComposerHidlTest::SetUp()); ASSERT_NO_FATAL_FAILURE(mGralloc = std::make_unique()); mWriter = std::make_unique(1024); mReader = std::make_unique(); } void TearDown() override { ASSERT_NO_FATAL_FAILURE(GraphicsComposerHidlTest::TearDown()); } const native_handle_t* allocate() { IMapper::BufferDescriptorInfo info{}; info.width = 64; info.height = 64; info.layerCount = 1; info.format = PixelFormat::RGBA_8888; info.usage = static_cast(BufferUsage::CPU_WRITE_OFTEN | BufferUsage::CPU_READ_OFTEN); return mGralloc->allocate(info); } void execute() { mComposerClient->execute_v2_2(mReader.get(), mWriter.get()); } std::unique_ptr mWriter; std::unique_ptr mReader; private: std::unique_ptr mGralloc; }; /** * Test IComposerClient::Command::SET_LAYER_PER_FRAME_METADATA. */ TEST_F(GraphicsComposerHidlCommandTest, SET_LAYER_PER_FRAME_METADATA) { Layer layer; ASSERT_NO_FATAL_FAILURE(layer = mComposerClient->createLayer(mPrimaryDisplay, kBufferSlotCount)); mWriter->selectDisplay(mPrimaryDisplay); mWriter->selectLayer(layer); /** * DISPLAY_P3 is a color space that uses the DCI_P3 primaries, * the D65 white point and the SRGB transfer functions. * Rendering Intent: Colorimetric * Primaries: * x y * green 0.265 0.690 * blue 0.150 0.060 * red 0.680 0.320 * white (D65) 0.3127 0.3290 */ std::vector hidlMetadata; hidlMetadata.push_back({IComposerClient::PerFrameMetadataKey::DISPLAY_RED_PRIMARY_X, 0.680}); hidlMetadata.push_back({IComposerClient::PerFrameMetadataKey::DISPLAY_RED_PRIMARY_Y, 0.320}); hidlMetadata.push_back({IComposerClient::PerFrameMetadataKey::DISPLAY_GREEN_PRIMARY_X, 0.265}); hidlMetadata.push_back({IComposerClient::PerFrameMetadataKey::DISPLAY_GREEN_PRIMARY_Y, 0.690}); hidlMetadata.push_back({IComposerClient::PerFrameMetadataKey::DISPLAY_BLUE_PRIMARY_X, 0.150}); hidlMetadata.push_back({IComposerClient::PerFrameMetadataKey::DISPLAY_BLUE_PRIMARY_Y, 0.060}); hidlMetadata.push_back({IComposerClient::PerFrameMetadataKey::WHITE_POINT_X, 0.3127}); hidlMetadata.push_back({IComposerClient::PerFrameMetadataKey::WHITE_POINT_Y, 0.3290}); hidlMetadata.push_back({IComposerClient::PerFrameMetadataKey::MAX_LUMINANCE, 100.0}); hidlMetadata.push_back({IComposerClient::PerFrameMetadataKey::MIN_LUMINANCE, 0.1}); hidlMetadata.push_back({IComposerClient::PerFrameMetadataKey::MAX_CONTENT_LIGHT_LEVEL, 78.0}); hidlMetadata.push_back( {IComposerClient::PerFrameMetadataKey::MAX_FRAME_AVERAGE_LIGHT_LEVEL, 62.0}); mWriter->setLayerPerFrameMetadata(hidlMetadata); execute(); } /** * Test IComposerClient::getPerFrameMetadataKeys. */ TEST_F(GraphicsComposerHidlTest, GetPerFrameMetadataKeys) { mComposerClient->getPerFrameMetadataKeys(mPrimaryDisplay); } /** * Test IComposerClient::createVirtualDisplay_2_2 and * IComposerClient::destroyVirtualDisplay. * * Test that virtual displays can be created and has the correct display type. */ TEST_F(GraphicsComposerHidlTest, CreateVirtualDisplay_2_2) { if (mComposerClient->getMaxVirtualDisplayCount() == 0) { GTEST_SUCCEED() << "no virtual display support"; return; } Display display; PixelFormat format; ASSERT_NO_FATAL_FAILURE( display = mComposerClient->createVirtualDisplay_2_2( 64, 64, PixelFormat::IMPLEMENTATION_DEFINED, kBufferSlotCount, &format)); // test display type IComposerClient::DisplayType type = mComposerClient->getDisplayType(display); EXPECT_EQ(IComposerClient::DisplayType::VIRTUAL, type); mComposerClient->destroyVirtualDisplay(display); } /** * Test IComposerClient::getClientTargetSupport_2_2. * * Test that IComposerClient::getClientTargetSupport returns true for the * required client targets. */ TEST_F(GraphicsComposerHidlTest, GetClientTargetSupport_2_2) { std::vector configs = mComposerClient->getDisplayConfigs(mPrimaryDisplay); for (auto config : configs) { int32_t width = mComposerClient->getDisplayAttribute(mPrimaryDisplay, config, IComposerClient::Attribute::WIDTH); int32_t height = mComposerClient->getDisplayAttribute(mPrimaryDisplay, config, IComposerClient::Attribute::HEIGHT); ASSERT_LT(0, width); ASSERT_LT(0, height); mComposerClient->setActiveConfig(mPrimaryDisplay, config); ASSERT_TRUE(mComposerClient->getClientTargetSupport_2_2( mPrimaryDisplay, width, height, PixelFormat::RGBA_8888, Dataspace::UNKNOWN)); } } /** * Test IComposerClient::setPowerMode_2_2. */ TEST_F(GraphicsComposerHidlTest, setPowerMode_2_2) { std::vector modes; modes.push_back(IComposerClient::PowerMode::OFF); modes.push_back(IComposerClient::PowerMode::ON_SUSPEND); modes.push_back(IComposerClient::PowerMode::ON); for (auto mode : modes) { mComposerClient->setPowerMode_2_2(mPrimaryDisplay, mode); } } TEST_F(GraphicsComposerHidlTest, setReadbackBuffer) { if (!mHasReadbackBuffer) { return; } PixelFormat pixelFormat; Dataspace dataspace; mComposerClient->getReadbackBufferAttributes(mPrimaryDisplay, &pixelFormat, &dataspace); ASSERT_LT(static_cast(0), pixelFormat); ASSERT_NE(Dataspace::UNKNOWN, dataspace); IMapper::BufferDescriptorInfo info{}; Config config = mComposerClient->getActiveConfig(mPrimaryDisplay); info.width = mComposerClient->getDisplayAttribute(mPrimaryDisplay, config, IComposerClient::Attribute::WIDTH); info.height = mComposerClient->getDisplayAttribute(mPrimaryDisplay, config, IComposerClient::Attribute::HEIGHT); info.layerCount = 1; info.format = pixelFormat; // BufferUsage::COMPOSER_OUTPUT is missing info.usage = static_cast(BufferUsage::COMPOSER_OVERLAY | BufferUsage::CPU_READ_OFTEN); std::unique_ptr gralloc; const native_handle_t* buffer; ASSERT_NO_FATAL_FAILURE(gralloc = std::make_unique()); ASSERT_NO_FATAL_FAILURE(buffer = gralloc->allocate(info)); mComposerClient->setReadbackBuffer(mPrimaryDisplay, buffer, -1); } TEST_F(GraphicsComposerHidlTest, getReadbackBufferFenceInactive) { if (!mHasReadbackBuffer) { return; } mComposerClient->getRaw()->getReadbackBufferFence( mPrimaryDisplay, [&](const auto& tmpError, const auto&) { ASSERT_EQ(Error::UNSUPPORTED, tmpError) << "readback buffer is active"; }); } /** * Test IComposerClient::Command::SET_LAYER_FLOAT_COLOR. */ TEST_F(GraphicsComposerHidlCommandTest, SET_LAYER_FLOAT_COLOR) { V2_1::Layer layer; ASSERT_NO_FATAL_FAILURE(layer = mComposerClient->createLayer(mPrimaryDisplay, kBufferSlotCount)); mWriter->selectDisplay(mPrimaryDisplay); mWriter->selectLayer(layer); mWriter->setLayerFloatColor(IComposerClient::FloatColor{1.0, 1.0, 1.0, 1.0}); mWriter->setLayerFloatColor(IComposerClient::FloatColor{0.0, 0.0, 0.0, 0.0}); } /** * Test IComposerClient::getDataspaceSaturationMatrix. */ TEST_F(GraphicsComposerHidlTest, getDataspaceSaturationMatrix) { auto matrix = mComposerClient->getDataspaceSaturationMatrix(Dataspace::SRGB_LINEAR); // the last row is known ASSERT_EQ(0.0f, matrix[12]); ASSERT_EQ(0.0f, matrix[13]); ASSERT_EQ(0.0f, matrix[14]); ASSERT_EQ(1.0f, matrix[15]); } /** * Test IComposerClient::getColorMode_2_2. */ TEST_F(GraphicsComposerHidlTest, GetColorMode_2_2) { std::vector modes = mComposerClient->getColorModes(mPrimaryDisplay); auto nativeMode = std::find(modes.cbegin(), modes.cend(), ColorMode::NATIVE); EXPECT_NE(modes.cend(), nativeMode); } /** * Test IComposerClient::getRenderIntent. */ TEST_F(GraphicsComposerHidlTest, GetRenderIntent) { std::vector modes = mComposerClient->getColorModes(mPrimaryDisplay); for (auto mode : modes) { std::vector intents = mComposerClient->getRenderIntents(mPrimaryDisplay, mode); auto colorimetricIntent = std::find(intents.cbegin(), intents.cend(), RenderIntent::COLORIMETRIC); EXPECT_NE(intents.cend(), colorimetricIntent); } } /** * Test IComposerClient::setColorMode_2_2. */ TEST_F(GraphicsComposerHidlTest, SetColorMode_2_2) { std::vector modes = mComposerClient->getColorModes(mPrimaryDisplay); for (auto mode : modes) { std::vector intents = mComposerClient->getRenderIntents(mPrimaryDisplay, mode); for (auto intent : intents) { mComposerClient->setColorMode(mPrimaryDisplay, mode, intent); } } } } // namespace } // namespace vts } // namespace V2_2 } // namespace composer } // namespace graphics } // namespace hardware } // namespace android int main(int argc, char** argv) { using android::hardware::graphics::composer::V2_2::vts::GraphicsComposerHidlEnvironment; ::testing::AddGlobalTestEnvironment(GraphicsComposerHidlEnvironment::Instance()); ::testing::InitGoogleTest(&argc, argv); GraphicsComposerHidlEnvironment::Instance()->init(&argc, argv); int status = RUN_ALL_TESTS(); return status; }