/* * Copyright (C) 2017 The Android Open Source Project * * Licensed under the Apache License, Version 2.0 (the "License"); * you may not use this file except in compliance with the License. * You may obtain a copy of the License at * * http://www.apache.org/licenses/LICENSE-2.0 * * Unless required by applicable law or agreed to in writing, software * distributed under the License is distributed on an "AS IS" BASIS, * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied. * See the License for the specific language governing permissions and * limitations under the License. */ #define LOG_TAG "media_omx_hidl_audio_dec_test" #ifdef __LP64__ #define OMX_ANDROID_COMPILE_AS_32BIT_ON_64BIT_PLATFORMS #endif #include #include #include #include #include #include #include #include using ::android::hardware::media::omx::V1_0::IOmx; using ::android::hardware::media::omx::V1_0::IOmxObserver; using ::android::hardware::media::omx::V1_0::IOmxNode; using ::android::hardware::media::omx::V1_0::Message; using ::android::hardware::media::omx::V1_0::CodecBuffer; using ::android::hardware::media::omx::V1_0::PortMode; using ::android::hidl::allocator::V1_0::IAllocator; using ::android::hidl::memory::V1_0::IMemory; using ::android::hidl::memory::V1_0::IMapper; using ::android::hardware::Return; using ::android::hardware::Void; using ::android::hardware::hidl_vec; using ::android::hardware::hidl_string; using ::android::sp; #include #include #include #include #include // A class for test environment setup class ComponentTestEnvironment : public ::testing::Environment { public: virtual void SetUp() {} virtual void TearDown() {} ComponentTestEnvironment() : instance("default"), res("/sdcard/media/") {} void setInstance(const char* _instance) { instance = _instance; } void setComponent(const char* _component) { component = _component; } void setRole(const char* _role) { role = _role; } void setRes(const char* _res) { res = _res; } const hidl_string getInstance() const { return instance; } const hidl_string getComponent() const { return component; } const hidl_string getRole() const { return role; } const hidl_string getRes() const { return res; } int initFromOptions(int argc, char** argv) { static struct option options[] = { {"instance", required_argument, 0, 'I'}, {"component", required_argument, 0, 'C'}, {"role", required_argument, 0, 'R'}, {"res", required_argument, 0, 'P'}, {0, 0, 0, 0}}; while (true) { int index = 0; int c = getopt_long(argc, argv, "I:C:R:P:", options, &index); if (c == -1) { break; } switch (c) { case 'I': setInstance(optarg); break; case 'C': setComponent(optarg); break; case 'R': setRole(optarg); break; case 'P': setRes(optarg); break; case '?': break; } } if (optind < argc) { fprintf(stderr, "unrecognized option: %s\n\n" "usage: %s \n\n" "test options are:\n\n" "-I, --instance: HAL instance to test\n" "-C, --component: OMX component to test\n" "-R, --role: OMX component Role\n" "-P, --res: Resource files directory location\n", argv[optind ?: 1], argv[0]); return 2; } return 0; } private: hidl_string instance; hidl_string component; hidl_string role; hidl_string res; }; static ComponentTestEnvironment* gEnv = nullptr; // audio decoder test fixture class class AudioDecHidlTest : public ::testing::VtsHalHidlTargetTestBase { private: typedef ::testing::VtsHalHidlTargetTestBase Super; public: ::std::string getTestCaseInfo() const override { return ::std::string() + "Component: " + gEnv->getComponent().c_str() + " | " + "Role: " + gEnv->getRole().c_str() + " | " + "Instance: " + gEnv->getInstance().c_str() + " | " + "Res: " + gEnv->getRes().c_str(); } virtual void SetUp() override { Super::SetUp(); disableTest = false; android::hardware::media::omx::V1_0::Status status; omx = Super::getService(gEnv->getInstance()); ASSERT_NE(omx, nullptr); observer = new CodecObserver([this](Message msg, const BufferInfo* buffer) { handleMessage(msg, buffer); }); ASSERT_NE(observer, nullptr); if (strncmp(gEnv->getComponent().c_str(), "OMX.", 4) != 0) disableTest = true; EXPECT_TRUE(omx->allocateNode( gEnv->getComponent(), observer, [&](android::hardware::media::omx::V1_0::Status _s, sp const& _nl) { status = _s; this->omxNode = _nl; }) .isOk()); ASSERT_EQ(status, ::android::hardware::media::omx::V1_0::Status::OK); ASSERT_NE(omxNode, nullptr); ASSERT_NE(gEnv->getRole().empty(), true) << "Invalid Component Role"; struct StringToName { const char* Name; standardComp CompName; }; const StringToName kStringToName[] = { {"mp3", mp3}, {"amrnb", amrnb}, {"amrwb", amrwb}, {"aac", aac}, {"vorbis", vorbis}, {"opus", opus}, {"pcm", pcm}, {"g711alaw", g711alaw}, {"g711mlaw", g711mlaw}, {"gsm", gsm}, {"raw", raw}, {"flac", flac}, }; const size_t kNumStringToName = sizeof(kStringToName) / sizeof(kStringToName[0]); const char* pch; char substring[OMX_MAX_STRINGNAME_SIZE]; strcpy(substring, gEnv->getRole().c_str()); pch = strchr(substring, '.'); ASSERT_NE(pch, nullptr); compName = unknown_comp; for (size_t i = 0; i < kNumStringToName; ++i) { if (!strcasecmp(pch + 1, kStringToName[i].Name)) { compName = kStringToName[i].CompName; break; } } if (compName == unknown_comp) disableTest = true; struct CompToCoding { standardComp CompName; OMX_AUDIO_CODINGTYPE eEncoding; }; static const CompToCoding kCompToCoding[] = { {mp3, OMX_AUDIO_CodingMP3}, {amrnb, OMX_AUDIO_CodingAMR}, {amrwb, OMX_AUDIO_CodingAMR}, {aac, OMX_AUDIO_CodingAAC}, {vorbis, OMX_AUDIO_CodingVORBIS}, {pcm, OMX_AUDIO_CodingPCM}, {opus, (OMX_AUDIO_CODINGTYPE)OMX_AUDIO_CodingAndroidOPUS}, {g711alaw, OMX_AUDIO_CodingG711}, {g711mlaw, OMX_AUDIO_CodingG711}, {gsm, OMX_AUDIO_CodingGSMFR}, {raw, OMX_AUDIO_CodingPCM}, {flac, OMX_AUDIO_CodingFLAC}, }; static const size_t kNumCompToCoding = sizeof(kCompToCoding) / sizeof(kCompToCoding[0]); size_t i; for (i = 0; i < kNumCompToCoding; ++i) { if (kCompToCoding[i].CompName == compName) { eEncoding = kCompToCoding[i].eEncoding; break; } } if (i == kNumCompToCoding) disableTest = true; eosFlag = false; framesReceived = 0; timestampUs = 0; timestampDevTest = false; if (disableTest) std::cout << "[ WARN ] Test Disabled \n"; } virtual void TearDown() override { if (omxNode != nullptr) { // If you have encountered a fatal failure, it is possible that // freeNode() will not go through. Instead of hanging the app. // let it pass through and report errors if (::testing::Test::HasFatalFailure()) return; EXPECT_TRUE((omxNode->freeNode()).isOk()); omxNode = nullptr; } Super::TearDown(); } // callback function to process messages received by onMessages() from IL // client. void handleMessage(Message msg, const BufferInfo* buffer) { (void)buffer; if (msg.type == Message::Type::FILL_BUFFER_DONE) { if (msg.data.extendedBufferData.flags & OMX_BUFFERFLAG_EOS) { eosFlag = true; } if (msg.data.extendedBufferData.rangeLength != 0) { framesReceived += 1; // For decoder components current timestamp always exceeds // previous timestamp EXPECT_GE(msg.data.extendedBufferData.timestampUs, timestampUs); timestampUs = msg.data.extendedBufferData.timestampUs; // Test if current timestamp is among the list of queued // timestamps if (timestampDevTest) { bool tsHit = false; android::List::iterator it = timestampUslist.begin(); while (it != timestampUslist.end()) { if (*it == timestampUs) { timestampUslist.erase(it); tsHit = true; break; } it++; } if (tsHit == false) { if (timestampUslist.empty() == false) { EXPECT_EQ(tsHit, true) << "TimeStamp not recognized"; } else { std::cout << "[ INFO ] Received non-zero " "output / TimeStamp not recognized \n"; } } } #define WRITE_OUTPUT 0 #if WRITE_OUTPUT static int count = 0; FILE* ofp = nullptr; if (count) ofp = fopen("out.bin", "ab"); else ofp = fopen("out.bin", "wb"); if (ofp != nullptr) { fwrite(static_cast(buffer->mMemory->getPointer()), sizeof(char), msg.data.extendedBufferData.rangeLength, ofp); fclose(ofp); count++; } #endif } } } enum standardComp { mp3, amrnb, amrwb, aac, vorbis, opus, pcm, g711alaw, g711mlaw, gsm, raw, flac, unknown_comp, }; sp omx; sp observer; sp omxNode; standardComp compName; OMX_AUDIO_CODINGTYPE eEncoding; bool disableTest; bool eosFlag; uint32_t framesReceived; uint64_t timestampUs; ::android::List timestampUslist; bool timestampDevTest; protected: static void description(const std::string& description) { RecordProperty("description", description); } }; // Set Default port param. void setDefaultPortParam( sp omxNode, OMX_U32 portIndex, OMX_AUDIO_CODINGTYPE eEncoding, int32_t nChannels = 2, int32_t nSampleRate = 44100, OMX_AUDIO_PCMMODETYPE ePCMMode = OMX_AUDIO_PCMModeLinear, OMX_NUMERICALDATATYPE eNumData = OMX_NumericalDataSigned, int32_t nBitPerSample = 16) { android::hardware::media::omx::V1_0::Status status; OMX_PARAM_PORTDEFINITIONTYPE portDef; status = getPortParam(omxNode, OMX_IndexParamPortDefinition, portIndex, &portDef); EXPECT_EQ(status, ::android::hardware::media::omx::V1_0::Status::OK); portDef.format.audio.bFlagErrorConcealment = OMX_TRUE; portDef.format.audio.eEncoding = eEncoding; status = setPortParam(omxNode, OMX_IndexParamPortDefinition, portIndex, &portDef); EXPECT_EQ(status, ::android::hardware::media::omx::V1_0::Status::OK); switch ((int)eEncoding) { case OMX_AUDIO_CodingPCM: setupPCMPort(omxNode, portIndex, nChannels, eNumData, nBitPerSample, nSampleRate, ePCMMode); break; case OMX_AUDIO_CodingAAC: setupAACPort(omxNode, portIndex, OMX_AUDIO_AACObjectNull, OMX_AUDIO_AACStreamFormatMP4FF, nChannels, 0, nSampleRate); default: break; } } // In decoder components, often the input port parameters get updated upon // parsing the header of elementary stream. Client needs to collect this // information to reconfigure other ports that share data with this input // port. void getInputChannelInfo(sp omxNode, OMX_U32 kPortIndexInput, OMX_AUDIO_CODINGTYPE eEncoding, int32_t* nChannels, int32_t* nSampleRate) { android::hardware::media::omx::V1_0::Status status; *nChannels = 0; *nSampleRate = 0; switch ((int)eEncoding) { case OMX_AUDIO_CodingGSMFR: case OMX_AUDIO_CodingG711: case OMX_AUDIO_CodingPCM: { OMX_AUDIO_PARAM_PCMMODETYPE param; status = getPortParam(omxNode, OMX_IndexParamAudioPcm, kPortIndexInput, ¶m); ASSERT_EQ(status, ::android::hardware::media::omx::V1_0::Status::OK); *nChannels = param.nChannels; *nSampleRate = param.nSamplingRate; break; } case OMX_AUDIO_CodingMP3: { OMX_AUDIO_PARAM_MP3TYPE param; status = getPortParam(omxNode, OMX_IndexParamAudioMp3, kPortIndexInput, ¶m); ASSERT_EQ(status, ::android::hardware::media::omx::V1_0::Status::OK); *nChannels = param.nChannels; *nSampleRate = param.nSampleRate; break; } case OMX_AUDIO_CodingAndroidOPUS: { OMX_AUDIO_PARAM_ANDROID_OPUSTYPE param; status = getPortParam(omxNode, (OMX_INDEXTYPE)OMX_IndexParamAudioAndroidOpus, kPortIndexInput, ¶m); ASSERT_EQ(status, ::android::hardware::media::omx::V1_0::Status::OK); *nChannels = param.nChannels; *nSampleRate = param.nSampleRate; break; } case OMX_AUDIO_CodingVORBIS: { OMX_AUDIO_PARAM_VORBISTYPE param; status = getPortParam(omxNode, OMX_IndexParamAudioVorbis, kPortIndexInput, ¶m); ASSERT_EQ(status, ::android::hardware::media::omx::V1_0::Status::OK); *nChannels = param.nChannels; *nSampleRate = param.nSampleRate; break; } case OMX_AUDIO_CodingAMR: { OMX_AUDIO_PARAM_AMRTYPE param; status = getPortParam(omxNode, OMX_IndexParamAudioAmr, kPortIndexInput, ¶m); ASSERT_EQ(status, ::android::hardware::media::omx::V1_0::Status::OK); *nChannels = param.nChannels; // NOTE: For amrnb sample rate is 8k and amrwb sample rate is 16k. // There is no nSampleRate field in OMX_AUDIO_PARAM_AMRTYPE. Just // return 8k to avoid returning uninit variable. *nSampleRate = 8000; break; } case OMX_AUDIO_CodingAAC: { OMX_AUDIO_PARAM_AACPROFILETYPE param; status = getPortParam(omxNode, OMX_IndexParamAudioAac, kPortIndexInput, ¶m); ASSERT_EQ(status, ::android::hardware::media::omx::V1_0::Status::OK); *nChannels = param.nChannels; *nSampleRate = param.nSampleRate; break; } case OMX_AUDIO_CodingFLAC: { OMX_AUDIO_PARAM_FLACTYPE param; status = getPortParam(omxNode, OMX_IndexParamAudioFlac, kPortIndexInput, ¶m); ASSERT_EQ(status, ::android::hardware::media::omx::V1_0::Status::OK); *nChannels = param.nChannels; *nSampleRate = param.nSampleRate; break; } default: ASSERT_TRUE(false); break; } } // LookUpTable of clips and metadata for component testing void GetURLForComponent(AudioDecHidlTest::standardComp comp, char* mURL, char* info) { struct CompToURL { AudioDecHidlTest::standardComp comp; const char* mURL; const char* info; }; static const CompToURL kCompToURL[] = { {AudioDecHidlTest::standardComp::mp3, "bbb_mp3_stereo_192kbps_48000hz.mp3", "bbb_mp3_stereo_192kbps_48000hz.info"}, {AudioDecHidlTest::standardComp::aac, "bbb_aac_stereo_128kbps_48000hz.aac", "bbb_aac_stereo_128kbps_48000hz.info"}, {AudioDecHidlTest::standardComp::amrnb, "sine_amrnb_1ch_12kbps_8000hz.amrnb", "sine_amrnb_1ch_12kbps_8000hz.info"}, {AudioDecHidlTest::standardComp::amrwb, "bbb_amrwb_1ch_14kbps_16000hz.amrwb", "bbb_amrwb_1ch_14kbps_16000hz.info"}, {AudioDecHidlTest::standardComp::vorbis, "bbb_vorbis_stereo_128kbps_48000hz.vorbis", "bbb_vorbis_stereo_128kbps_48000hz.info"}, {AudioDecHidlTest::standardComp::opus, "bbb_opus_stereo_128kbps_48000hz.opus", "bbb_opus_stereo_128kbps_48000hz.info"}, {AudioDecHidlTest::standardComp::g711alaw, "bbb_g711alaw_1ch_8khz.raw", "bbb_g711alaw_1ch_8khz.info"}, {AudioDecHidlTest::standardComp::g711mlaw, "bbb_g711mulaw_1ch_8khz.raw", "bbb_g711mulaw_1ch_8khz.info"}, {AudioDecHidlTest::standardComp::gsm, "bbb_gsm_1ch_8khz_13kbps.raw", "bbb_gsm_1ch_8khz_13kbps.info"}, {AudioDecHidlTest::standardComp::raw, "bbb_raw_1ch_8khz_s32le.raw", "bbb_raw_1ch_8khz_s32le.info"}, {AudioDecHidlTest::standardComp::flac, "bbb_flac_stereo_680kbps_48000hz.flac", "bbb_flac_stereo_680kbps_48000hz.info"}, }; for (size_t i = 0; i < sizeof(kCompToURL) / sizeof(kCompToURL[0]); ++i) { if (kCompToURL[i].comp == comp) { strcat(mURL, kCompToURL[i].mURL); strcat(info, kCompToURL[i].info); return; } } } // port settings reconfiguration during runtime. reconfigures sample rate and // number typedef struct { OMX_AUDIO_CODINGTYPE eEncoding; AudioDecHidlTest::standardComp comp; } packedArgs; void portReconfiguration(sp omxNode, sp observer, android::Vector* iBuffer, android::Vector* oBuffer, OMX_U32 kPortIndexInput, OMX_U32 kPortIndexOutput, Message msg, PortMode oPortMode, void* args) { android::hardware::media::omx::V1_0::Status status; packedArgs* audioArgs = static_cast(args); OMX_AUDIO_CODINGTYPE eEncoding = audioArgs->eEncoding; AudioDecHidlTest::standardComp comp = audioArgs->comp; (void)oPortMode; if (msg.data.eventData.event == OMX_EventPortSettingsChanged) { ASSERT_EQ(msg.data.eventData.data1, kPortIndexOutput); status = omxNode->sendCommand(toRawCommandType(OMX_CommandPortDisable), kPortIndexOutput); ASSERT_EQ(status, android::hardware::media::omx::V1_0::Status::OK); status = observer->dequeueMessage(&msg, DEFAULT_TIMEOUT, iBuffer, oBuffer); if (status == android::hardware::media::omx::V1_0::Status::TIMED_OUT) { for (size_t i = 0; i < oBuffer->size(); ++i) { // test if client got all its buffers back EXPECT_EQ((*oBuffer)[i].owner, client); // free the buffers status = omxNode->freeBuffer(kPortIndexOutput, (*oBuffer)[i].id); ASSERT_EQ(status, android::hardware::media::omx::V1_0::Status::OK); } status = observer->dequeueMessage(&msg, DEFAULT_TIMEOUT, iBuffer, oBuffer); ASSERT_EQ(status, android::hardware::media::omx::V1_0::Status::OK); ASSERT_EQ(msg.type, Message::Type::EVENT); ASSERT_EQ(msg.data.eventData.event, OMX_EventCmdComplete); ASSERT_EQ(msg.data.eventData.data1, OMX_CommandPortDisable); ASSERT_EQ(msg.data.eventData.data2, kPortIndexOutput); // set Port Params int32_t nChannels; int32_t nSampleRate; ASSERT_NO_FATAL_FAILURE(getInputChannelInfo( omxNode, kPortIndexInput, eEncoding, &nChannels, &nSampleRate)); // Configure output port // SPECIAL CASE: Soft Vorbis, Opus and Raw Decoders do not offer way // to configure output PCM port. The port undergoes auto // configuration internally basing on parsed elementary stream // information. if (comp != AudioDecHidlTest::standardComp::vorbis && comp != AudioDecHidlTest::standardComp::opus && comp != AudioDecHidlTest::standardComp::raw) { setDefaultPortParam(omxNode, kPortIndexOutput, OMX_AUDIO_CodingPCM, nChannels, nSampleRate); } // If you can disable a port, then you should be able to enable it // as well status = omxNode->sendCommand( toRawCommandType(OMX_CommandPortEnable), kPortIndexOutput); ASSERT_EQ(status, android::hardware::media::omx::V1_0::Status::OK); // do not enable the port until all the buffers are supplied status = observer->dequeueMessage(&msg, DEFAULT_TIMEOUT, iBuffer, oBuffer); ASSERT_EQ(status, android::hardware::media::omx::V1_0::Status::TIMED_OUT); ASSERT_NO_FATAL_FAILURE( allocatePortBuffers(omxNode, oBuffer, kPortIndexOutput)); status = observer->dequeueMessage(&msg, DEFAULT_TIMEOUT, iBuffer, oBuffer); ASSERT_EQ(status, android::hardware::media::omx::V1_0::Status::OK); ASSERT_EQ(msg.type, Message::Type::EVENT); ASSERT_EQ(msg.data.eventData.data1, OMX_CommandPortEnable); ASSERT_EQ(msg.data.eventData.data2, kPortIndexOutput); // dispatch output buffers for (size_t i = 0; i < oBuffer->size(); i++) { ASSERT_NO_FATAL_FAILURE( dispatchOutputBuffer(omxNode, oBuffer, i)); } } else { ASSERT_TRUE(false); } } else { ASSERT_TRUE(false); } } // blocking call to ensures application to Wait till all the inputs are consumed void waitOnInputConsumption(sp omxNode, sp observer, android::Vector* iBuffer, android::Vector* oBuffer, OMX_AUDIO_CODINGTYPE eEncoding, OMX_U32 kPortIndexInput, OMX_U32 kPortIndexOutput, AudioDecHidlTest::standardComp comp) { android::hardware::media::omx::V1_0::Status status; Message msg; int timeOut = TIMEOUT_COUNTER_Q; while (timeOut--) { size_t i = 0; status = observer->dequeueMessage(&msg, DEFAULT_TIMEOUT_Q, iBuffer, oBuffer); if (status == android::hardware::media::omx::V1_0::Status::OK) { ASSERT_EQ(msg.type, Message::Type::EVENT); packedArgs audioArgs = {eEncoding, comp}; ASSERT_NO_FATAL_FAILURE( portReconfiguration(omxNode, observer, iBuffer, oBuffer, kPortIndexInput, kPortIndexOutput, msg, PortMode::PRESET_BYTE_BUFFER, &audioArgs)); } // status == TIMED_OUT, it could be due to process time being large // than DEFAULT_TIMEOUT or component needs output buffers to start // processing. for (; i < iBuffer->size(); i++) { if ((*iBuffer)[i].owner != client) break; } if (i == iBuffer->size()) break; // Dispatch an output buffer assuming outQueue.empty() is true size_t index; if ((index = getEmptyBufferID(oBuffer)) < oBuffer->size()) { ASSERT_NO_FATAL_FAILURE( dispatchOutputBuffer(omxNode, oBuffer, index)); timeOut = TIMEOUT_COUNTER_Q; } } } // Decode N Frames void decodeNFrames(sp omxNode, sp observer, android::Vector* iBuffer, android::Vector* oBuffer, OMX_AUDIO_CODINGTYPE eEncoding, OMX_U32 kPortIndexInput, OMX_U32 kPortIndexOutput, std::ifstream& eleStream, android::Vector* Info, int offset, int range, AudioDecHidlTest::standardComp comp, bool signalEOS = true) { android::hardware::media::omx::V1_0::Status status; Message msg; size_t index; uint32_t flags = 0; int frameID = offset; int timeOut = TIMEOUT_COUNTER_Q; bool iQueued, oQueued; while (1) { iQueued = oQueued = false; status = observer->dequeueMessage(&msg, DEFAULT_TIMEOUT_Q, iBuffer, oBuffer); // Port Reconfiguration if (status == android::hardware::media::omx::V1_0::Status::OK && msg.type == Message::Type::EVENT) { packedArgs audioArgs = {eEncoding, comp}; ASSERT_NO_FATAL_FAILURE( portReconfiguration(omxNode, observer, iBuffer, oBuffer, kPortIndexInput, kPortIndexOutput, msg, PortMode::PRESET_BYTE_BUFFER, &audioArgs)); } if (frameID == (int)Info->size() || frameID == (offset + range)) break; // Dispatch input buffer if ((index = getEmptyBufferID(iBuffer)) < iBuffer->size()) { char* ipBuffer = static_cast( static_cast((*iBuffer)[index].mMemory->getPointer())); ASSERT_LE((*Info)[frameID].bytesCount, static_cast((*iBuffer)[index].mMemory->getSize())); eleStream.read(ipBuffer, (*Info)[frameID].bytesCount); ASSERT_EQ(eleStream.gcount(), (*Info)[frameID].bytesCount); flags = (*Info)[frameID].flags; // Indicate to omx core that the buffer contains a full frame worth // of data flags |= OMX_BUFFERFLAG_ENDOFFRAME; // Indicate the omx core that this is the last buffer it needs to // process if (signalEOS && ((frameID == (int)Info->size() - 1) || (frameID == (offset + range - 1)))) flags |= OMX_BUFFERFLAG_EOS; ASSERT_NO_FATAL_FAILURE(dispatchInputBuffer( omxNode, iBuffer, index, (*Info)[frameID].bytesCount, flags, (*Info)[frameID].timestamp)); frameID++; iQueued = true; } // Dispatch output buffer if ((index = getEmptyBufferID(oBuffer)) < oBuffer->size()) { ASSERT_NO_FATAL_FAILURE( dispatchOutputBuffer(omxNode, oBuffer, index)); oQueued = true; } // Reset Counters when either input or output buffer is dispatched if (iQueued || oQueued) timeOut = TIMEOUT_COUNTER_Q; else timeOut--; if (timeOut == 0) { ASSERT_TRUE(false) << "Wait on Input/Output is found indefinite"; } } } // set component role TEST_F(AudioDecHidlTest, SetRole) { description("Test Set Component Role"); if (disableTest) return; android::hardware::media::omx::V1_0::Status status; status = setRole(omxNode, gEnv->getRole().c_str()); ASSERT_EQ(status, ::android::hardware::media::omx::V1_0::Status::OK); } // port format enumeration TEST_F(AudioDecHidlTest, EnumeratePortFormat) { description("Test Component on Mandatory Port Parameters (Port Format)"); if (disableTest) return; android::hardware::media::omx::V1_0::Status status; uint32_t kPortIndexInput = 0, kPortIndexOutput = 1; status = setRole(omxNode, gEnv->getRole().c_str()); ASSERT_EQ(status, ::android::hardware::media::omx::V1_0::Status::OK); OMX_PORT_PARAM_TYPE params; status = getParam(omxNode, OMX_IndexParamAudioInit, ¶ms); if (status == ::android::hardware::media::omx::V1_0::Status::OK) { ASSERT_EQ(params.nPorts, 2U); kPortIndexInput = params.nStartPortNumber; kPortIndexOutput = kPortIndexInput + 1; } status = setAudioPortFormat(omxNode, kPortIndexInput, eEncoding); EXPECT_EQ(status, ::android::hardware::media::omx::V1_0::Status::OK); status = setAudioPortFormat(omxNode, kPortIndexOutput, OMX_AUDIO_CodingPCM); EXPECT_EQ(status, ::android::hardware::media::omx::V1_0::Status::OK); } // test port settings reconfiguration, elementary stream decode and timestamp // deviation TEST_F(AudioDecHidlTest, DecodeTest) { description("Tests Port Reconfiguration, Decode and timestamp deviation"); if (disableTest) return; android::hardware::media::omx::V1_0::Status status; uint32_t kPortIndexInput = 0, kPortIndexOutput = 1; status = setRole(omxNode, gEnv->getRole().c_str()); ASSERT_EQ(status, ::android::hardware::media::omx::V1_0::Status::OK); OMX_PORT_PARAM_TYPE params; status = getParam(omxNode, OMX_IndexParamAudioInit, ¶ms); if (status == ::android::hardware::media::omx::V1_0::Status::OK) { ASSERT_EQ(params.nPorts, 2U); kPortIndexInput = params.nStartPortNumber; kPortIndexOutput = kPortIndexInput + 1; } char mURL[512], info[512]; strcpy(mURL, gEnv->getRes().c_str()); strcpy(info, gEnv->getRes().c_str()); GetURLForComponent(compName, mURL, info); std::ifstream eleStream, eleInfo; eleInfo.open(info); ASSERT_EQ(eleInfo.is_open(), true); android::Vector Info; int bytesCount = 0; uint32_t flags = 0; uint32_t timestamp = 0; timestampDevTest = false; while (1) { if (!(eleInfo >> bytesCount)) break; eleInfo >> flags; eleInfo >> timestamp; Info.push_back({bytesCount, flags, timestamp}); if (timestampDevTest && (flags != OMX_BUFFERFLAG_CODECCONFIG)) timestampUslist.push_back(timestamp); } eleInfo.close(); int32_t nChannels, nSampleRate; // Configure input port setDefaultPortParam(omxNode, kPortIndexInput, eEncoding); if (compName == raw) setDefaultPortParam(omxNode, kPortIndexInput, eEncoding, 1, 8000, OMX_AUDIO_PCMModeLinear, OMX_NumericalDataSigned, 32); ASSERT_NO_FATAL_FAILURE(getInputChannelInfo( omxNode, kPortIndexInput, eEncoding, &nChannels, &nSampleRate)); // Configure output port // SPECIAL CASE: Soft Vorbis, Opus and Raw Decoders do not offer way to // configure output PCM port. The port undergoes auto configuration // internally basing on parsed elementary stream information. if (compName != vorbis && compName != opus && compName != raw) { setDefaultPortParam(omxNode, kPortIndexOutput, OMX_AUDIO_CodingPCM, nChannels, nSampleRate); } android::Vector iBuffer, oBuffer; // set state to idle ASSERT_NO_FATAL_FAILURE(changeStateLoadedtoIdle(omxNode, observer, &iBuffer, &oBuffer, kPortIndexInput, kPortIndexOutput)); // set state to executing ASSERT_NO_FATAL_FAILURE(changeStateIdletoExecute(omxNode, observer)); // Port Reconfiguration eleStream.open(mURL, std::ifstream::binary); ASSERT_EQ(eleStream.is_open(), true); ASSERT_NO_FATAL_FAILURE(decodeNFrames( omxNode, observer, &iBuffer, &oBuffer, eEncoding, kPortIndexInput, kPortIndexOutput, eleStream, &Info, 0, (int)Info.size(), compName)); eleStream.close(); ASSERT_NO_FATAL_FAILURE( waitOnInputConsumption(omxNode, observer, &iBuffer, &oBuffer, eEncoding, kPortIndexInput, kPortIndexOutput, compName)); packedArgs audioArgs = {eEncoding, compName}; ASSERT_NO_FATAL_FAILURE(testEOS( omxNode, observer, &iBuffer, &oBuffer, false, eosFlag, nullptr, portReconfiguration, kPortIndexInput, kPortIndexOutput, &audioArgs)); if (timestampDevTest) EXPECT_EQ(timestampUslist.empty(), true); // set state to idle ASSERT_NO_FATAL_FAILURE( changeStateExecutetoIdle(omxNode, observer, &iBuffer, &oBuffer)); // set state to executing ASSERT_NO_FATAL_FAILURE(changeStateIdletoLoaded(omxNode, observer, &iBuffer, &oBuffer, kPortIndexInput, kPortIndexOutput)); } // end of sequence test TEST_F(AudioDecHidlTest, EOSTest_M) { description("Test end of stream monkeying"); if (disableTest) return; android::hardware::media::omx::V1_0::Status status; uint32_t kPortIndexInput = 0, kPortIndexOutput = 1; status = setRole(omxNode, gEnv->getRole().c_str()); ASSERT_EQ(status, ::android::hardware::media::omx::V1_0::Status::OK); OMX_PORT_PARAM_TYPE params; status = getParam(omxNode, OMX_IndexParamAudioInit, ¶ms); if (status == ::android::hardware::media::omx::V1_0::Status::OK) { ASSERT_EQ(params.nPorts, 2U); kPortIndexInput = params.nStartPortNumber; kPortIndexOutput = kPortIndexInput + 1; } int32_t nChannels, nSampleRate; // Configure input port setDefaultPortParam(omxNode, kPortIndexInput, eEncoding); if (compName == raw) setDefaultPortParam(omxNode, kPortIndexInput, eEncoding, 1, 8000, OMX_AUDIO_PCMModeLinear, OMX_NumericalDataSigned, 32); ASSERT_NO_FATAL_FAILURE(getInputChannelInfo( omxNode, kPortIndexInput, eEncoding, &nChannels, &nSampleRate)); // Configure output port // SPECIAL CASE: Soft Vorbis, Opus and Raw Decoders do not offer way to // configure output PCM port. The port undergoes auto configuration // internally basing on parsed elementary stream information. if (compName != vorbis && compName != opus && compName != raw) { setDefaultPortParam(omxNode, kPortIndexOutput, OMX_AUDIO_CodingPCM, nChannels, nSampleRate); } android::Vector iBuffer, oBuffer; // set state to idle ASSERT_NO_FATAL_FAILURE(changeStateLoadedtoIdle(omxNode, observer, &iBuffer, &oBuffer, kPortIndexInput, kPortIndexOutput)); // set state to executing ASSERT_NO_FATAL_FAILURE(changeStateIdletoExecute(omxNode, observer)); // request EOS at the start packedArgs audioArgs = {eEncoding, compName}; ASSERT_NO_FATAL_FAILURE(testEOS( omxNode, observer, &iBuffer, &oBuffer, true, eosFlag, nullptr, portReconfiguration, kPortIndexInput, kPortIndexOutput, &audioArgs)); ASSERT_NO_FATAL_FAILURE(flushPorts(omxNode, observer, &iBuffer, &oBuffer, kPortIndexInput, kPortIndexOutput)); EXPECT_GE(framesReceived, 0U); framesReceived = 0; timestampUs = 0; // set state to idle ASSERT_NO_FATAL_FAILURE( changeStateExecutetoIdle(omxNode, observer, &iBuffer, &oBuffer)); // set state to executing ASSERT_NO_FATAL_FAILURE(changeStateIdletoLoaded(omxNode, observer, &iBuffer, &oBuffer, kPortIndexInput, kPortIndexOutput)); } // end of sequence test TEST_F(AudioDecHidlTest, ThumbnailTest) { description("Test Request for thumbnail"); if (disableTest) return; android::hardware::media::omx::V1_0::Status status; uint32_t kPortIndexInput = 0, kPortIndexOutput = 1; status = setRole(omxNode, gEnv->getRole().c_str()); ASSERT_EQ(status, ::android::hardware::media::omx::V1_0::Status::OK); OMX_PORT_PARAM_TYPE params; status = getParam(omxNode, OMX_IndexParamAudioInit, ¶ms); if (status == ::android::hardware::media::omx::V1_0::Status::OK) { ASSERT_EQ(params.nPorts, 2U); kPortIndexInput = params.nStartPortNumber; kPortIndexOutput = kPortIndexInput + 1; } char mURL[512], info[512]; strcpy(mURL, gEnv->getRes().c_str()); strcpy(info, gEnv->getRes().c_str()); GetURLForComponent(compName, mURL, info); std::ifstream eleStream, eleInfo; eleInfo.open(info); ASSERT_EQ(eleInfo.is_open(), true); android::Vector Info; int bytesCount = 0; uint32_t flags = 0; uint32_t timestamp = 0; while (1) { if (!(eleInfo >> bytesCount)) break; eleInfo >> flags; eleInfo >> timestamp; Info.push_back({bytesCount, flags, timestamp}); } eleInfo.close(); int32_t nChannels, nSampleRate; // Configure input port setDefaultPortParam(omxNode, kPortIndexInput, eEncoding); if (compName == raw) setDefaultPortParam(omxNode, kPortIndexInput, eEncoding, 1, 8000, OMX_AUDIO_PCMModeLinear, OMX_NumericalDataSigned, 32); ASSERT_NO_FATAL_FAILURE(getInputChannelInfo( omxNode, kPortIndexInput, eEncoding, &nChannels, &nSampleRate)); // Configure output port // SPECIAL CASE: Soft Vorbis, Opus and Raw Decoders do not offer way to // configure output PCM port. The port undergoes auto configuration // internally basing on parsed elementary stream information. if (compName != vorbis && compName != opus && compName != raw) { setDefaultPortParam(omxNode, kPortIndexOutput, OMX_AUDIO_CodingPCM, nChannels, nSampleRate); } android::Vector iBuffer, oBuffer; // set state to idle ASSERT_NO_FATAL_FAILURE(changeStateLoadedtoIdle(omxNode, observer, &iBuffer, &oBuffer, kPortIndexInput, kPortIndexOutput)); // set state to executing ASSERT_NO_FATAL_FAILURE(changeStateIdletoExecute(omxNode, observer)); // request EOS for thumbnail // signal EOS flag with last frame size_t i = 0; while (!(Info[i].flags & OMX_BUFFERFLAG_SYNCFRAME)) i++; eleStream.open(mURL, std::ifstream::binary); ASSERT_EQ(eleStream.is_open(), true); ASSERT_NO_FATAL_FAILURE(decodeNFrames( omxNode, observer, &iBuffer, &oBuffer, eEncoding, kPortIndexInput, kPortIndexOutput, eleStream, &Info, 0, i + 1, compName)); eleStream.close(); ASSERT_NO_FATAL_FAILURE( waitOnInputConsumption(omxNode, observer, &iBuffer, &oBuffer, eEncoding, kPortIndexInput, kPortIndexOutput, compName)); packedArgs audioArgs = {eEncoding, compName}; ASSERT_NO_FATAL_FAILURE(testEOS( omxNode, observer, &iBuffer, &oBuffer, false, eosFlag, nullptr, portReconfiguration, kPortIndexInput, kPortIndexOutput, &audioArgs)); ASSERT_NO_FATAL_FAILURE(flushPorts(omxNode, observer, &iBuffer, &oBuffer, kPortIndexInput, kPortIndexOutput)); EXPECT_GE(framesReceived, 1U); framesReceived = 0; timestampUs = 0; // signal EOS flag after last frame eleStream.open(mURL, std::ifstream::binary); ASSERT_EQ(eleStream.is_open(), true); ASSERT_NO_FATAL_FAILURE(decodeNFrames( omxNode, observer, &iBuffer, &oBuffer, eEncoding, kPortIndexInput, kPortIndexOutput, eleStream, &Info, 0, i + 1, compName, false)); eleStream.close(); ASSERT_NO_FATAL_FAILURE( waitOnInputConsumption(omxNode, observer, &iBuffer, &oBuffer, eEncoding, kPortIndexInput, kPortIndexOutput, compName)); ASSERT_NO_FATAL_FAILURE(testEOS( omxNode, observer, &iBuffer, &oBuffer, true, eosFlag, nullptr, portReconfiguration, kPortIndexInput, kPortIndexOutput, &audioArgs)); ASSERT_NO_FATAL_FAILURE(flushPorts(omxNode, observer, &iBuffer, &oBuffer, kPortIndexInput, kPortIndexOutput)); EXPECT_GE(framesReceived, 1U); framesReceived = 0; timestampUs = 0; // set state to idle ASSERT_NO_FATAL_FAILURE( changeStateExecutetoIdle(omxNode, observer, &iBuffer, &oBuffer)); // set state to executing ASSERT_NO_FATAL_FAILURE(changeStateIdletoLoaded(omxNode, observer, &iBuffer, &oBuffer, kPortIndexInput, kPortIndexOutput)); } // end of sequence test TEST_F(AudioDecHidlTest, SimpleEOSTest) { description("Test end of stream"); if (disableTest) return; android::hardware::media::omx::V1_0::Status status; uint32_t kPortIndexInput = 0, kPortIndexOutput = 1; status = setRole(omxNode, gEnv->getRole().c_str()); ASSERT_EQ(status, ::android::hardware::media::omx::V1_0::Status::OK); OMX_PORT_PARAM_TYPE params; status = getParam(omxNode, OMX_IndexParamAudioInit, ¶ms); if (status == ::android::hardware::media::omx::V1_0::Status::OK) { ASSERT_EQ(params.nPorts, 2U); kPortIndexInput = params.nStartPortNumber; kPortIndexOutput = kPortIndexInput + 1; } char mURL[512], info[512]; strcpy(mURL, gEnv->getRes().c_str()); strcpy(info, gEnv->getRes().c_str()); GetURLForComponent(compName, mURL, info); std::ifstream eleStream, eleInfo; eleInfo.open(info); ASSERT_EQ(eleInfo.is_open(), true); android::Vector Info; int bytesCount = 0; uint32_t flags = 0; uint32_t timestamp = 0; while (1) { if (!(eleInfo >> bytesCount)) break; eleInfo >> flags; eleInfo >> timestamp; Info.push_back({bytesCount, flags, timestamp}); } eleInfo.close(); int32_t nChannels, nSampleRate; // Configure input port setDefaultPortParam(omxNode, kPortIndexInput, eEncoding); if (compName == raw) setDefaultPortParam(omxNode, kPortIndexInput, eEncoding, 1, 8000, OMX_AUDIO_PCMModeLinear, OMX_NumericalDataSigned, 32); ASSERT_NO_FATAL_FAILURE(getInputChannelInfo( omxNode, kPortIndexInput, eEncoding, &nChannels, &nSampleRate)); // Configure output port // SPECIAL CASE: Soft Vorbis, Opus and Raw Decoders do not offer way to // configure output PCM port. The port undergoes auto configuration // internally basing on parsed elementary stream information. if (compName != vorbis && compName != opus && compName != raw) { setDefaultPortParam(omxNode, kPortIndexOutput, OMX_AUDIO_CodingPCM, nChannels, nSampleRate); } android::Vector iBuffer, oBuffer; // set state to idle ASSERT_NO_FATAL_FAILURE(changeStateLoadedtoIdle(omxNode, observer, &iBuffer, &oBuffer, kPortIndexInput, kPortIndexOutput)); // set state to executing ASSERT_NO_FATAL_FAILURE(changeStateIdletoExecute(omxNode, observer)); // request EOS at the end eleStream.open(mURL, std::ifstream::binary); ASSERT_EQ(eleStream.is_open(), true); ASSERT_NO_FATAL_FAILURE(decodeNFrames(omxNode, observer, &iBuffer, &oBuffer, eEncoding, kPortIndexInput, kPortIndexOutput, eleStream, &Info, 0, (int)Info.size(), compName, false)); eleStream.close(); ASSERT_NO_FATAL_FAILURE( waitOnInputConsumption(omxNode, observer, &iBuffer, &oBuffer, eEncoding, kPortIndexInput, kPortIndexOutput, compName)); packedArgs audioArgs = {eEncoding, compName}; ASSERT_NO_FATAL_FAILURE(testEOS( omxNode, observer, &iBuffer, &oBuffer, true, eosFlag, nullptr, portReconfiguration, kPortIndexInput, kPortIndexOutput, &audioArgs)); ASSERT_NO_FATAL_FAILURE(flushPorts(omxNode, observer, &iBuffer, &oBuffer, kPortIndexInput, kPortIndexOutput)); framesReceived = 0; timestampUs = 0; // set state to idle ASSERT_NO_FATAL_FAILURE( changeStateExecutetoIdle(omxNode, observer, &iBuffer, &oBuffer)); // set state to executing ASSERT_NO_FATAL_FAILURE(changeStateIdletoLoaded(omxNode, observer, &iBuffer, &oBuffer, kPortIndexInput, kPortIndexOutput)); } // test input/output port flush TEST_F(AudioDecHidlTest, FlushTest) { description("Test Flush"); if (disableTest) return; android::hardware::media::omx::V1_0::Status status; uint32_t kPortIndexInput = 0, kPortIndexOutput = 1; status = setRole(omxNode, gEnv->getRole().c_str()); ASSERT_EQ(status, ::android::hardware::media::omx::V1_0::Status::OK); OMX_PORT_PARAM_TYPE params; status = getParam(omxNode, OMX_IndexParamAudioInit, ¶ms); if (status == ::android::hardware::media::omx::V1_0::Status::OK) { ASSERT_EQ(params.nPorts, 2U); kPortIndexInput = params.nStartPortNumber; kPortIndexOutput = kPortIndexInput + 1; } char mURL[512], info[512]; strcpy(mURL, gEnv->getRes().c_str()); strcpy(info, gEnv->getRes().c_str()); GetURLForComponent(compName, mURL, info); std::ifstream eleStream, eleInfo; eleInfo.open(info); ASSERT_EQ(eleInfo.is_open(), true); android::Vector Info; int bytesCount = 0; uint32_t flags = 0; uint32_t timestamp = 0; while (1) { if (!(eleInfo >> bytesCount)) break; eleInfo >> flags; eleInfo >> timestamp; Info.push_back({bytesCount, flags, timestamp}); } eleInfo.close(); int32_t nChannels, nSampleRate; // Configure input port setDefaultPortParam(omxNode, kPortIndexInput, eEncoding); if (compName == raw) setDefaultPortParam(omxNode, kPortIndexInput, eEncoding, 1, 8000, OMX_AUDIO_PCMModeLinear, OMX_NumericalDataSigned, 32); ASSERT_NO_FATAL_FAILURE(getInputChannelInfo( omxNode, kPortIndexInput, eEncoding, &nChannels, &nSampleRate)); // Configure output port // SPECIAL CASE: Soft Vorbis, Opus and Raw Decoders do not offer way to // configure output PCM port. The port undergoes auto configuration // internally basing on parsed elementary stream information. if (compName != vorbis && compName != opus && compName != raw) { setDefaultPortParam(omxNode, kPortIndexOutput, OMX_AUDIO_CodingPCM, nChannels, nSampleRate); } android::Vector iBuffer, oBuffer; // set state to idle ASSERT_NO_FATAL_FAILURE(changeStateLoadedtoIdle(omxNode, observer, &iBuffer, &oBuffer, kPortIndexInput, kPortIndexOutput)); // set state to executing ASSERT_NO_FATAL_FAILURE(changeStateIdletoExecute(omxNode, observer)); // Decode 128 frames and flush. here 128 is chosen to ensure there is a key // frame after this so that the below section can be convered for all // components int nFrames = 128; eleStream.open(mURL, std::ifstream::binary); ASSERT_EQ(eleStream.is_open(), true); ASSERT_NO_FATAL_FAILURE(decodeNFrames( omxNode, observer, &iBuffer, &oBuffer, eEncoding, kPortIndexInput, kPortIndexOutput, eleStream, &Info, 0, nFrames, compName, false)); ASSERT_NO_FATAL_FAILURE(flushPorts(omxNode, observer, &iBuffer, &oBuffer, kPortIndexInput, kPortIndexOutput)); framesReceived = 0; // Seek to next key frame and start decoding till the end int index = nFrames; bool keyFrame = false; while (index < (int)Info.size()) { if ((Info[index].flags & OMX_BUFFERFLAG_SYNCFRAME) == OMX_BUFFERFLAG_SYNCFRAME) { timestampUs = Info[index - 1].timestamp; keyFrame = true; break; } eleStream.ignore(Info[index].bytesCount); index++; } if (keyFrame) { ASSERT_NO_FATAL_FAILURE( decodeNFrames(omxNode, observer, &iBuffer, &oBuffer, eEncoding, kPortIndexInput, kPortIndexOutput, eleStream, &Info, index, Info.size() - index, compName, false)); } ASSERT_NO_FATAL_FAILURE(flushPorts(omxNode, observer, &iBuffer, &oBuffer, kPortIndexInput, kPortIndexOutput)); framesReceived = 0; // set state to idle ASSERT_NO_FATAL_FAILURE( changeStateExecutetoIdle(omxNode, observer, &iBuffer, &oBuffer)); // set state to executing ASSERT_NO_FATAL_FAILURE(changeStateIdletoLoaded(omxNode, observer, &iBuffer, &oBuffer, kPortIndexInput, kPortIndexOutput)); } int main(int argc, char** argv) { gEnv = new ComponentTestEnvironment(); ::testing::AddGlobalTestEnvironment(gEnv); ::testing::InitGoogleTest(&argc, argv); int status = gEnv->initFromOptions(argc, argv); if (status == 0) { status = RUN_ALL_TESTS(); ALOGI("Test result = %d", status); } return status; }